Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Product List
ROHM’s SMLVN6RGB and MSL0402RGB LED includes a reflector to concentrate the light forward, resulting in increased luminosity and color mixing area. Shown here on the left is a graphic of a standard RGB LED. The light radiates in all directions and the color mixing area, shown in white, is small. On the right is ROHM’s SMLVN6 and MSL0402RGB packaged LEDs with the reflector. As seen in the diagram, the light is reflected forward, increasing the luminosity and the color mixing area as seen by the larger white area.
PTM Published on: 2011-10-17
PTM Updated on: 2018-08-20