Maker.io main logo

Simple Volume Indicator - GC9A01 Display Using Visuino

27

2026-04-08 | By Ron Cutts

License: GNU Lesser General Public License Displays SPI Arduino ESP32

In this tutorial, we will make a simple volume indicator using a GC9A01 SPI display, a rotary encoder, an Arduino, and the Visuino program.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

  1. Arduino UNO (or any other Arduino or ESP)

  2. GC9A01 SPI Display

  3. Rotary encoder module

  4. Jumper wires

  5. Breadboard

  6. Visuino program: Download Visuino

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

The Circuit

  1. Connect GC9A01 Display pin [VCC] to Arduino pin [3.3V]

  2. Connect GC9A01 Display pin [GND] to Arduino pin [GND]

  3. Connect GC9A01 Display pin [SCL] to Arduino pin [13]

  4. Connect GC9A01 Display pin [SDA] to Arduino pin [11]

  5. Connect GC9A01 Display pin [DC] to Arduino pin [9]

  6. Connect GC9A01 Display pin [CS] to Arduino pin [10]

  7. Connect GC9A01 Display pin [RST ] to Arduino pin [8]

  8. Connect the Encoder module pin [CLK] to the Arduino digital pin [2]

  9. Connect the Encoder module pin [DT] to Arduino digital pin [3]

  10. Connect the encoder module pin [+] to Arduino pin [5v]

  11. Connect the encoder module pin [-] to Arduino pin [GND]

The Circuit

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  1. Add "GC9A01" component

  2. Add "Rotary Encoder Sensor" component

  3. Add "Integer Multi Source" component

  4. Add "Integer To Text" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Set Components

  1. Select "RotaryEncoderSensor1" and in the properties window, set "Max" > "Roll Over" to False and "Max" > "Value" to 360

  2. Select "RotaryEncoderSensor1" and in the properties window, set "Min" > "Roll Over" to False and "Min" > "Value" to 0

  3. Select "MultiSource1" and in the properties window set "Output pins" to 7

  1. Double-click on "Display1" and in the "Elements" window, drag "Draw Angled Line" to the left side, and in the properties window, set "Color" to aclWhite, "X" to 120, "Y" to 120, "Begin" to 51, "End" to 100. Select "Angle" and click on the pin icon, and select "Float SinkPin"

  2. Drag another "Draw Angled Line" to the left side and in the properties window set "Color" to aclBlack, "X" to 120, "Y" to 120, "Begin" to 51, "End" to 100; select "Angle" and click on the pin icon and select "Float SinkPin"

  3. Drag "Draw Ellipse" to the left side and in the properties window set "Height" to 100, "Width" to 100, "Fill Color" to aclBlue, "Color" to aclBlack, "X" to 70, "Y" to 70

  4. Drag "Text Field" to the left side and in the properties window set "Size" to 2, "Fill Color" to aclBlue, "Color" to aclWhite, "X" to 100, "Y" to 90

  5. For Text Field elements in the properties, select "Elements", click on the 3-dot button, and in the "Elements" window, drag "Font" to the left side, and in the properties window, set "Font" to Adafruit\FreeSansBold18pt7b or any other font

  6. Close all the windows

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Set Components photo 5

In Visuino Set Components photo 6

In Visuino Set Components photo 7

In Visuino Set Components photo 8

In Visuino Set Components photo 9

In Visuino Connect Components

  1. Connect Arduino digital pin [3] to "RotaryEncoderSensor1" pin [Direction]

  2. Connect Arduino digital pin [2] to "RotaryEncoderSensor1" pin [Clock]

  3. Connect "RotaryEncoderSensor1" pin [Out] to "MultiSource1" pin [In]

  4. Connect "MultiSource1" pin [0] to "Display1" > "Draw Ellipse1" pin [Clock]

  5. Connect "MultiSource1" pin [1] to "Display1" > "Draw Angled Line2" pin [Clock]

  6. Connect "MultiSource1" pin [2] to "Display1" > "Draw Angled Line1" pin [Angle]

  7. Connect "MultiSource1" pin [3] to "Display1" > "Draw Angled Line2" pin [Angle]

  8. Connect "MultiSource1" pin [4] to "Display1" > "Draw Angled Line1" pin [Clock]

  9. Connect "MultiSource1" pin [5] to "IntegerToText1" pin [In]

  10. Connect "IntegerToText1" pin [Out] to "Display1" > "TextField1" pin [In]

  11. Connect "MultiSource1" pin [6] to "Display1" > "TextField1" pin [Clock]

  1. Connect "Display1" pin [Chip Select] to Arduino digital pin [10]

  2. Connect "Display1" pin [Data Command] to Arduino digital pin [9]

  3. Connect "Display1" pin [Reset] to Arduino digital pin [8]

  4. Connect "Display1" Control pin [SPI] to Arduino SPI pin [In]

In Visuino Connect Components

In Visuino Connect Components photo 2

In Visuino Connect Components photo 3

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this tutorial; you can download it and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.