Maker.io main logo

Sign Language Glove

24

2016-07-18 | By Monica Lin

License: None

Sign language has helped the hearing-impaired communicate for many centuries before it was formalized and officially recognized, but this long-standing language of gestures has now been given a 21st-century technological upgrade. Introducing a revolution in sign language technology, the Sign Language Glove. This glove is a device that helps people with hearing impairments communicate by identifying and translating the user's signs into spoken English.

Sign Language Glove

Sign Language Glove

The device uses five Spectra Symbol Flex-Sensors which are used to quantify how much each finger is bent, and the  MPU-6050 (a three-axis accelerometer and gyroscope) is used to detect the orientation and rotational movement of the hand. A computer program then translates the motion coming from the glove into words displayed on a screen. Additionally, it incorporates a text-to-speech feature but is limited to that feature due to given time constraints. The project uses a machine learning algorithm that can train over any input selected by the user, and can then be generalized to gesture recognition, rather than just sign language translation.

It is always a great pride to “design for a cause,” and to produce products that will help a broader community. The goal of this project is to create a way for the hearing and speech-impaired to be able to communicate with the general public more easily. In the process of facilitating communication between people, it breaks down language barriers in the process.

Project Source

 

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.