Maker.io main logo

Minimalist Arduino-Based IoT RGB Mood Light

76

2022-04-28 | By Maker.io Staff

License: See Original Project

Colorful LED lights can easily brighten up a room and change its entire atmosphere. Dim, red ‎light is perfect for relaxing, and blue-ish lights often help us focus on mentally demanding tasks, ‎such as studying or working. This article discusses an IoT mood light, a simple, beginner-friendly ‎Arduino-based IoT project that lets users change the atmosphere in just about any room. In ‎addition, you can give others access to the online dashboard so that they can change the color to ‎remind you of appointments or to let you know they are thinking about you.‎

finish_1 

This image shows the finished device.‎

Building the Hardware‎

This project is very beginner-friendly: it requires only a handful of components and is incredibly ‎easy to assemble. An Arduino Nano 33 IoT development board forms the base of this project. It ‎establishes a connection to the Arduino IoT cloud and synchronizes its local variables with the ‎online service. This service also enables users to change the mood light’s color and toggle an ‎automatic color-fading mode. The Arduino then communicates with a WS2812-based LED strip ‎to display the color chosen by the user. Luckily, communicating with the LEDs requires only ‎three wires:‎

 

This image shows the schematic diagram of this project. This build only contains two ‎components, and the device's firmware does most of the heavy lifting.

Two of the three wires supply the LEDs with power, and the Arduino uses the third connection to ‎send the color and brightness data to the individual LEDs on the strip.‎

Lastly, the project also contains a minimalistic, modern 3D-printed enclosure that neatly houses ‎all the electronic components. I used two colors to print the case, and I printed the top part of the ‎enclosure using semi-translucent white PLA. This semi-transparent material acts as a diffuser ‎that evenly distributes the light emitted by the LEDs. In summary, the build contains the following ‎parts:‎

build_2

The build consists of four 3D-printed parts, two short LED strip pieces, and an Arduino Nano 33 ‎IoT development board.‎

To follow along with what I did step by step, you’ll need access to a 3D printer. However, you ‎can always employ a professional-grade 3D-printing service such as the one offered by Digi-Key. ‎You can download the 3D files at the end of this article.‎

Assembling the Device‎

The 3D-printed enclosure consists of four parts. The base part houses the Arduino board, and it ‎exposes the USB port of the Arduino so that you can plug in the device to power it. Make sure ‎you close the small solder jumper on the bottom side of the Arduino before you start assembling ‎the case:‎

board_3

Bridge the two PCB jumper pads using a small blob of solder, as shown in this image.‎

Closing this jumper will provide the +5V GPIO pin of the Arduino with power from the USB port. ‎If you don’t close this jumper, the LED strip won’t get any power, and the build won’t function as ‎intended.‎

Next, remove the adhesive backing from the LED strip parts and attach the two small pieces to ‎the center part of the plastic case. Then, add some wires to the flexible PCBs. Make sure to pay ‎close attention to the arrows on the LED strip pieces before you attach them to the case part. ‎The arrows indicate the direction of the data flow coming from the Arduino:‎

connect_4 

Connect the LED strips as shown in this image.‎

Attach the wires that will go to the Arduino to the side of the LED strip that contains a DI pad. ‎Then, connect the first LED strip's DO pin to the second row's DI pin. The figure above shows ‎that the arrows point from left to right on the top LED strip and in the opposite direction on the ‎second strip. Once you’re done, connect the three remaining wires to the Arduino board, as ‎shown in the schematic diagram above. Then, place the Arduino in the bottom half of the case ‎before adding the piece that contains the LED strips:‎

case_5

Place the Arduino in the bottom half of the case. Then, gently but firmly press the second plastic ‎piece in place. It should be a tight fit, but it shouldn’t be too difficult to insert the part that the LED ‎strips are attached to.‎

You can attach a USB cable to the Arduino to keep the board in place while pushing the second ‎plastic piece in place. All the parts in the case snap together and hold each other in place. Next, ‎you can add the second thin plastic piece to keep the LED strips in place if they don’t have an ‎adhesive backing. However, I omitted that piece in my build, as my strips came with a sticky ‎back layer. Lastly, push on the semi-translucent top part. Make sure that the four pegs align with ‎the four holes in the bottom half of the enclosure. You should feel some resistance when you ‎snap together the parts. However, if the resistance is too strong, check whether any cables are ‎in the way or whether you need to drill out the holes due to material shrinking.‎

The Firmware‎

Similar to the hardware, the software component of this project is straightforward and suitable for ‎beginners, as the Arduino IoT Cloud service does most of the heavy lifting. You can read more ‎about getting started with the Arduino IoT Cloud here if you need a refresher. Start by creating a ‎new thing in the IoT cloud. Then, add five variables, as shown in the following screenshot:‎

screen_5

Create a new thing and add five variables, as shown in this image.‎

As you can see, the IoT sketch contains five synchronized variables: one integer for each color ‎value, another one for the brightness, and a boolean value that toggles the color fading animation. ‎Next, build a dashboard so that users can set the mood light's color, change the brightness, and ‎toggle the animation:‎

dashboard_6 

This image shows an example of how the project’s dashboard may look. However, you can ‎arrange the dashboard as you like.‎

Then, edit the thing’s sketch so that it contains the following code:‎

Copy Code
#include "thingProperties.h"
#include <Adafruit_NeoPixel.h>

#define LED_DATA_PIN 3
#define NUM_LEDS 4
#define ANIMATION_DELAY 50

unsigned long lastAnimationStep = 0UL;
unsigned animationMode = 0;

Adafruit_NeoPixel leds(NUM_LEDS, LED_DATA_PIN, NEO_GRB + NEO_KHZ800);

void setup()
{
Serial.begin(9600);

// Defined in thingProperties.h
initProperties();

// Connect to Arduino IoT Cloud
ArduinoCloud.begin(ArduinoIoTPreferredConnection);

leds.begin();
updateBrightness();
updateColor();
}

void updateColor(void)
{
leds.clear();

for(int i = 0; i < NUM_LEDS; i++)
leds.setPixelColor(i, leds.Color(r, g, b));

leds.show();
}

void updateBrightness(void)
{
leds.setBrightness(brightness);
leds.show();
}

void loop()
{
ArduinoCloud.update();

if(animate)
{
unsigned long currentMillis = millis();

if(currentMillis - lastAnimationStep > ANIMATION_DELAY)
{
animateValues();
updateColor();
lastAnimationStep = currentMillis;
}
}
}

void animateValues(void)
{
switch(animationMode)
{
case 0:
g++;
r--;
if(r < 0 || g > 255)
switchAnimationMode();
break;

case 1:
b++;
g--;
if(g < 0 || b > 255)
switchAnimationMode();
break;

case 2:
r++;
b--;
if(b < 0 || r > 255)
switchAnimationMode();
break;
break;
}
}

void switchAnimationMode(void)
{
if(animationMode == 0)
{
r = 0;
g = 255;
b = 0;
animationMode = 1;
}
else if(animationMode == 1)
{
r = 0;
g = 0;
b = 255;
animationMode = 2;
}
else
{
r = 255;
g = 0;
b = 0;
animationMode = 0;
}
}

void onRChange()
{
updateColor();
}

void onGChange()
{
updateColor();
}

void onBChange()
{
updateColor();
}

void onAnimateChange()
{ }

void onBrightnessChange()
{
updateBrightness();
}

Let’s break down what this code is doing. First, I import the libraries for communicating with the ‎IoT cloud service and the LED strip. The setup function then initializes the connection with the ‎Arduino IoT cloud before setting the initial color and brightness of the LEDs using two helper ‎functions. The updateColor helper method iterates over all the LEDs on the strip (four in this case) ‎and assigns them with the color value stored in the r, g, and b variables. Similarly, the ‎updateBrightness helper function calls the LED library’s setBrightness function using the value of ‎the synchronized brightness function.‎

Whenever the user changes one of the synchronized variables using the IoT cloud dashboard, ‎the IoT cloud library on the Arduino calls the appropriate onChange() function towards the end of ‎the script. For example, all the color value update callback functions call the updateColor helper. ‎Similarly, the onBrightnessChange function calls the updateBrightness helper.‎

The product would function in this state. However, the loop method implements a simple color ‎fading animation. First, the loop method checks whether the animate variable is true. If it is, it ‎checks whether enough time has elapsed since it last updated the animation. If that’s the case, ‎the loop method calls the animateValues helper and the updateColor function to display the ‎changed color. Depending on the current animation mode, the animateValues helper function ‎increments one of the color channels while simultaneously decrementing a second channel. If ‎either of the updated colors reaches one of the extreme values, the helper function switches to ‎the next mode. During a mode switch, the firmware resets the values so that one color channel ‎is at full brightness while all others are completely off. Then, the cycle repeats for two other ‎channels.‎

Download the Case Design Files‎

You can download the case design files here.‎

Summary‎

finish_7

This IoT mood light project might be simple to assemble and understand, but it still yields an ‎impressive-looking decoration item that lets you change the atmosphere in an entire room. The ‎build consists of only a handful of readily available low-cost components. An Arduino Nano 33 ‎IoT does most of the heavy lifting. It establishes a connection to the Arduino IoT cloud service, ‎listens for changes in the synchronized variables, and updates the LED values accordingly. A ‎custom 3D-printed enclosure houses all the electronic components.‎

The software part of this project mainly deals with synchronizing the variables with the IoT cloud ‎and reacting to changes made by a user. Whenever somebody changes one of the ‎synchronized color variables, the Arduino detects this change and propagates it to the LED strip. ‎Additionally, the firmware also implements a simple color-fade animation. The program ‎decreases one color channel’s value while simultaneously increasing another channel, ‎depending on its internal state.

制造商零件编号 ABX00027
ARDUINO NANO 33 IOT
Arduino
制造商零件编号 104990000
ADDRESS LED STRIP SERIAL RGB 1M
Seeed Technology Co., Ltd
制造商零件编号 KT-PR0047NA
LULZBOT MINI 2 NORTH AMERICA
LulzBot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.