Maker.io main logo

Make Custom Chassis Designs for the Kitronik Drag Racer Module

36

2026-04-23 | By Kitronik Maker

License: See Original Project DC Motor Drivers / Controllers Robot Kits Servo Wheels / Casters

Courtesy of Kitronik Maker

Guide by Kitronik Maker

Building a project from the ground up can be intimidating, especially when designing around an existing electronics kit. That is why we are giving you the design files for three different Timed Drag Racer Module chassis! These are a basic design, a Formula 1 style car, and a traditional elongated drag racer!

Whether you just build the chassis as it is or use it as a base to build the body of the car, this is a great project for hobbyists and students alike!

The Timed Drag Racer Module

module_1

Set classroom design challenges & test outcomes with fun timed racing activities with the Kitronik Timed Drag Racer Module! Assemble the Kits, create a chassis, & race!

Get the kit!

Get The Design Files

Each of the three chassis design downloads contains two files, a DXF and a PDF instruction document.

original_2

Original Chassis!

f1_3

F1 Chassis!

drag_4

Drag Racer!

Sometimes discrepancies in scaling can occur when downloading a dxf file. This is down to the specific software that you use. We have included a scaling document for your reference when downloading our templates.

scaling_5

Building Tips:

The assembly of the chassis is detailed on pages 17 to 21 of the teaching resources and can be applied to the other two chassis designs also. It should be noted however, that while the original chassis is front wheel drive, the drag racer and F1 car are both back wheel drive. As such, your rubber band should be attached to one of the back wheels instead of the front.

View Teaching Notes!

Suggested Materials:

The below items have also been used in the creation of these chassis! Please note that should you choose to use a different laserable material, it should be 3mm thick. The designs are made for this thickness.

acrylic_6

Value Acrylic!

mdf_7

MDF!

birch_8

Birch Faced Ply!

Other Components:

wheels_9

Wheels!

m3_10

M3 Screws!

spacers_11

Spacers!

dowel_12

Dowel Rods!

clips_13

Motor Clips!

misc_14

Misc Parts!

制造商零件编号 25120
KITRONIK TIMED DRAG RACER MODULE
Kitronik Ltd.
制造商零件编号 5683
:MOVE MOTOR FOR THE BBC MICRO:BI
Kitronik Ltd.
制造商零件编号 56112
KITRONIK SIMPLE SERVOS STARTER P
Kitronik Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.