Maker.io main logo

Assembling Wireless Plasma Kit

26

2023-01-19 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

Wireless Plasma Kit will let you build an internet connected mood-light-in-a-‎bottle that's easy to program using MicroPython or CircuitPython.‎

In this beginner friendly tutorial, we'll show you:‎

  • how to put the bits in the kit together
  • how to program it using MicroPython and Thonny
  • a few tricks for hooking up other hardware and sensors

What You'll Need

  • A Wireless Plasma Kit (we'll be showing you our Skully Edition kit)
  • A computer to program from (Windows, Mac, or Linux/Raspberry Pi)
  • Small flathead screwdriver for wrangling the screw terminals
  • Pair of scissors for separating the wire ends

Kit Contents

contents_1

You should have the following items in your kit. If you're missing ‎something drop a message to support and they'll get it sorted.‎

  • Plasma Stick 2040 W (with Pico W Aboard)
  • A bottle (with a cork)‎
  • ‎5m of WS2812/Neopixel-compatible addressable LED wire (50 LEDs)‎
  • USB A to micro-B cable
  • Velcro dots for attaching the board

If you have the BYOB Edition kit, it won't include the Velcro dots or bottle.‎

About Plasma Stick

stick_2

This board is your LED controller. We've added a set of screw terminals to ‎make it easy to connect the LED wire and boost circuitry so that the LEDs ‎get a nice clean 5V on the power and data lines (some LED strips don't work ‎very well with 3.3V on their data lines). We've also added a reset ‎button (because unplugging your USB cable all the time is tedious) and ‎a Qw/ST (Qwiic/STEMMA QT) connector so you can connect it to other ‎components, without soldering.‎

We've designed this board with doing cool LED things with wireless in mind, ‎so it doesn't have current sensing or some of the other mod cons that you ‎can find on Plasma 2040. You can also only use it with 5V ‎WS2812/Neopixel/SK6812 LED strip (that's the kind that has three wires).‎

Assembling the Kit

PLUGGING IN THE LEDS

Unfurl the LEDs and locate the end that has bare wires poking out. This is the ‎end that needs connecting to the screw connectors.‎

These LEDs are WS2812 LEDs, so they have three wires - 5V ( ), data ‎‎(PIXELS) and ground (-). With more traditional LED strips you can tell which ‎wire is which from the markings on the strip, but with this LED wire the 5v ( ) ‎wire is the one that's marked with dots. The data (PIXELS) line is the one in ‎the middle, and the ground (-) line is the one that's leftover.‎

To make it easier to plug in the wires we'd suggest separating them a bit at ‎the end - snip the insulation between the wires with scissors, taking care not ‎to nick the wires.‎

wires_3

Loosen the screws on the connector on Plasma Stick with a flathead ‎screwdriver, poke the wire ends into the connector, and tighten the screws ‎back up. You'll probably find it easier to do one wire at a time. Give the wires ‎a little tug when you're done to make sure they're anchored solidly in the ‎connector. Be sure that the terminal is gripping the metal wire, and not the ‎plastic sleeve (you can strip off a little bit of the plastic sleeve to expose ‎more of the wire if that helps).‎

connect_4

Once the wires are securely fastened in place that's the fiddly bit done - you ‎can start feeding the other end of your LED wire into the bottle. We used a ‎pencil to help poke the LEDs into the bottle and make sure they were nicely ‎distributed.‎

secure_5

If you have a Star bottle kit, you might find that getting the LEDs evenly ‎distributed is a bit trickier. We ended up making a curved tool out of thick ‎wire to help poke the LEDs into the points.‎

STICKING PLASMA STICK TO THE BOTTLE

We've included some Velcro dots for sticking the controller board to the bottle ‎so it's out of the way - we mounted ours on the flat surface on the rear of the ‎skull. We found it helpful to stick both sides of the dots to the bottle first to ‎get the placement right, and then add the Plasma Stick.‎

velcro_6

Once you're happy with the placement, make sure they're securely pressed ‎down to both surfaces - the adhesive will take 10 minutes to achieve full ‎stickiness.‎

place_7

Feed any excess wire into the bottle and plug in the cork to keep it in place ‎‎(and to stop the LED magic from escaping).‎

PLUGGING IN THE USB CABLE

Plug the little end of your USB cable into the micro-B connector on Plasma ‎Stick, and the big end into your computer (or some other source of USB ‎power). We've preloaded Plasma Stick with software, so hopefully now some ‎stuff should happen!‎

Help! No Stuff is Happening!‎

If nothing lights up, then double check you plugged the correct wires into the ‎correct screw terminals, and they're anchored securely in the connector.‎

Running the Examples

The demo script that we've loaded on Plasma Stick looks for a Wi-Fi ‎connection, and if it can't connect to one it generates some spooky rainbows ‎instead. Once you've finished enjoying those, you'll probably want to start ‎modifying the code, or give your board the capabilities to connect to your Wi-‎Fi so it can do some other stuff!‎

TALKING TO PLASMA STICK WITH THONNY

When it's running MicroPython, Plasma Stick won't show up as a drive on ‎your computer. To edit files on it or run code on it, you'll need to talk to it ‎through an interpreter - we're using Thonny, which is available for Windows, ‎Mac or Linux.‎

  • Install Thonny
  • Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)'
  • Plug Plasma Stick into your computer if it's not plugged in ‎already. Because main.py will already be running, you'll need to stop it ‎with the stop button in Thonny before sending it any instructions
  • After you press stop, you should get a MicroPython prompt that looks ‎something like this. The flashing cursor next to the >>> in the 'Shell' box ‎tells you that Plasma Stick is talking to your computer and is ready to ‎accept instructions

thonny_8

If you're having trouble using Thonny to communicate with your board, ‎there's some troubleshooting suggestions at the link below:‎

EDITING FILES

Using Thonny, you can open up the .py example files on the device and edit ‎them. To see the files on your board, you will need to have the Files window ‎visible - if you can't see it, you can make it show up with View > Files.

files_9

The top box can be used to browse the local files in on your computer, and ‎the bottom box shows the files on your board. If you want to transfer files to ‎‎(or from) your board, right click on the file you want to copy and select ‎‎'upload to /' or 'download to /'.‎

MAKING THE RAINBOWS LESS SPOOKY

‎"But it is no longer Halloween", I hear you cry. "Please, I need a more ‎appropriately coloured LED effect to display to my fancy festive guests, ‎otherwise they will point and laugh at me!"‎

Open up main.py in Thonny by double clicking on it in the Files window and look ‎for the function that starts def spooky_rainbows(): This section of code generates a ‎triangle wave that moves up and down the LEDs, with colours picked from a ‎specific segment of the Hue Saturation Value (HSV) colour wheel (if you ‎scroll down to the bottom of that page, there's a useful graphic that shows ‎you where different colours are located on the wheel). You can change the ‎colours by changing the numbers next to HUE_START and HUE_END - ‎try 180 to 240 degrees for an icy blue effect.‎

code_10

Press the green run button to save your changes and run your code.‎

We can make things icier still by turning down the Saturation a bit - find this ‎line of code in the same function. This is the line that actually sets the colour ‎of the LEDs.‎

Copy Code
led_strip.set_hsv(i, hue / 360, 1.0, 0.8)

Change the Saturation value to 0.75 (that's 75% colour saturation), like this:‎

Copy Code
led_strip.set_hsv(i, hue / 360, 0.75, 0.8)

‎Any effect which involves cycling rainbows or shifting colours gradually will ‎probably involve adjusting the Hue, so HSV is a very handy thing to learn ‎about!‎

You can also find a few more seasonal examples on Github.‎

ADDING YOUR WIRELESS CREDENTIALS

For the examples that use wireless to work, your Pico W will need to know ‎your wireless network details. Double click on the copy of WIFI_CONFIG.py that's ‎on your Pico W to open it up. Add your network's SSID, password and country ‎code (if you're in the UK like us then your country code should be "GB" - if not ‎check this list). Note that SSID and password are case sensitive!‎

creds_11

Once you've finished editing, click save, and then hit the RESET button to ‎reboot the board. When it tries to connect this time (and if you got your ‎credentials correct), you should get...‎

‎#FEARLIGHTS‎

Instead of spooky (or icy) rainbows once the board has finishing connecting ‎the LEDs will now show the most recent Cheerlights colour.‎

Cheerlights is a simple API that controls the colour of LED ‎skulls, dinosaurs and other fun illuminated things all over the world. Tweet a ‎colour @cheerlights (or with the #cheerlights hashtag) to change the colour ‎of everybody's lights. This example polls the API every 2 minutes, so it might ‎take a little while for your light to change.‎

Find out more here:‎

Other examples

There's a bunch of other preloaded examples too. weather.py connects to a ‎weather API and fills your bottle with appropriate LED effects. moon.py makes ‎your bottle glow brighter as it gets closer to midnight. And there's a couple of ‎simple LED effects to get you started customising/coding up your own decor.‎

Double click on an example to open it up and press the green run button to ‎start it running. If you want to make your code run every time the Pico is ‎powered up (useful if you want to untether your bottle from your computer), ‎replace the contents of main.py with some different code.‎

If you accidentally overwrite/lose something, don't worry - you can find all the ‎preloaded examples on GitHub at the link below, plus a few extras - just copy ‎and paste the code you want to run/save into a new tab in Thonny (clicking ‎the 'raw' button first will make it easier to copy).‎

Adding Moar Hardware

PIR SENSOR

For Halloween, we wanted to rig up something spooky to surprise ‎unfortunate Pirate HQ guests. We connected a PIR infrared motion sensor up ‎to the Qw/ST connector using a Qw/ST to DuPont socket cable. We used one ‎of these simple micro PIR sensors a) because they work nicely with 3.3V and ‎b) they happen to anchor neatly into a glass eye socket with a blob of blu-tak, ‎making your skull into a cool cyborg.‎

The pin labelled V on the sensor is power - so connect it to the red wire from ‎the Qw/ST cable. G is ground, which goes to the black wire. Either the blue or ‎the yellow wires can be used for data (S on the sensor), our example uses ‎the yellow wire (GP5). You don't need to connect the other wire, so tuck it ‎away safely.‎

You can find the code for the PIR example here:‎

Once it's running on your Plasma Stick, the sensor will toggle its data pin high ‎when it detects movement. When the Pico W receives this signal, it will ‎randomly trigger a different LED effect.‎

led_12

TEMPERATURE AND CO2 SENSING

What scares us? Getting too hot and having to spend time in places with poor ‎ventilation, of course. Our bottle makes a really neat eye-catching sensor ‎display - we've made examples that change colour based on readings from ‎our BME280 Temperature, Humidity and Pressure Sensor and SCD41 CO2 ‎Sensor breakout, but it would be easy to adapt this code to work with other ‎sensors if you wanted.‎

We've had a Plasma 2040 powered carbon dioxide sensing skull living at ‎Pirate HQ for a while (it was our inspiration for making this kit, in fact) and he ‎does a great job of reminding us when it's time to open a window.‎

Both these breakouts have Qw/ST connectors, so you can plug them straight ‎in to Plasma Stick with a Qw/ST cable.‎

ADJUSTING THE COLOURS WITH AN ENCODER

Plasma Stick has no user buttons, so how can we change the colour of our ‎lights if we don't have a computer handy to program it with? This example ‎uses an RGB Encoder breakout to adjust the hue. Because the encoder ‎breakout has its own RGB lighting, we can even set it to match!‎

This breakout doesn't have a Qw/ST connector, so we needed to use ‎a Qw/ST cable coupled with a Qw/ST to Breakout Garden adapter to plug it ‎in.‎

KEEPING TIME WITH AN RTC

If you've tried out the moon.py example untethered from a computer, you might ‎have noticed that it can't tell the correct time when it doesn't have access to ‎Thonny. If you're making something clock related (or something that adjusts ‎the lights depending on the time of day, perhaps?) you might want to ‎consider adding a Real Time Clock breakout, which has its own tiny battery ‎to keep track of the correct time, even when your Pico W is unpowered.‎

If you're using a brand new RTC breakout, you'll need to do some setup and ‎set the correct time before running the code above - you can do that by ‎running this code in Thonny:‎

This breakout doesn't have a Qw/ST connector, so we needed to use ‎a Qw/ST cable coupled with a Qw/ST to Breakout Garden adapter to plug it ‎in.‎

Next Steps

Ready to start making your own examples and effects? Check out ‎our Plasma 2040 tutorial for an introduction to the basic functions in the ‎Plasma library, such as controlling the colour of individual and multiple LEDs. ‎You might also find the Plasma function reference handy. As always, we'd ‎love to see what you come up with - do consider sharing your projects with ‎us on Twitter or our forums!‎

That's all folks!‎

制造商零件编号 PIM582
PLASMA 2040
Pimoroni Ltd
制造商零件编号 PIM472
BME280 BREAKOUT - TEMPERATURE, P
Pimoroni Ltd
制造商零件编号 PIM522
RGB ENCODER BREAKOUT
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.