Maker.io main logo

Arduino Display Date & Time on MAX7219 8-digit Digital LED Display Using

30

2026-04-30 | By Ron Cutts

License: GNU Lesser General Public License Displays Microcontrollers Wifi Arduino ESP32

In this tutorial, we will learn how to display date and time using the RTC DS1307 module, the MAX7219 8-digit digital LED display, and Visuino.

Watch the video.

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

The Circuit

  • Connect RTC DS1307 module pin[VCC] to Arduino pin[5V]

  • Connect RTC DS1307 module pin[GND] to Arduino pin[GND]

  • Connect the RTC DS1307 module pin[SDA] to the Arduino pin [SDA].

  • Connect RTC DS1307 module pin[SCL] to Arduino pin[SCL]

  • Connect LED module pin[VCC] to Arduino pin[5V]

  • Connect LED module pin[GND] to Arduino pin[GND]

  • Connect LED module pin[DIN] to Arduino digital pin[11]

  • Connect LED module pin[CS] to Arduino digital pin[10]

  • Connect LED module pin[CLK] to Arduino digital pin[13]

The Circuit

Start Visuino, and Select the Arduino UNO Board Type

The Visuino: https://www.visuino.eu also needs to be installed. Download the free version or register for a free trial.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino Add Components

  • Add "Clock Generator" component

  • Add "Date/Time Value" component

  • Add ""Real Time Clock(RTC) DS1307" component

  • Add "Decode(Split) Date/Time" component

  • Add 2X "Split Integer Digits" component

  • Add "Maxim LED Display Controller SPI MAX7219/MAX7221" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Add Components photo 5

In Visuino Add Components photo 6

In Visuino Set Components

  • Select "DateTimeValue1" and in the properties window set Value to your current Date and Time

  • Select "SplitIntegerDigits1" and in the properties window, set Output Pins to 2

  • Select "SplitIntegerDigits2" and in the properties window, set Output Pins to 2

Double click on the "LedController1" and in the "PixelGroups" window, drag:

  • "Integer Display 7 Segments" to the left side, and in the properties window, set "Count Digits" to 2 and "Leading Zeroes" to True

  • "Value Section 7 Segments" to the left side, and in the properties window, set "Initial Decmal Point Value" to True

  • "Value Section 7 Segments" to the left side

  • "Integer Display 7 Segments" to the left side, and in the properties window, set "Count Digits" to 2 and "Leading Zeroes" to True

  • "Value Section 7 Segments" to the left side, and in the properties window, set "Initial Decmal Point Value" to True

  • "Value Section 7 Segments" to the left side

Close the "PixelGroups" window

In Visuino Set  Components

In Visuino Set  Components photo 2

In Visuino Set  Components photo 3

In Visuino Set  Components photo 4

In Visuino Set  Components photo 5

In Visuino Set  Components photo 6

In Visuino Set  Components photo 7

In Visuino Connect Components

  • Connect "ClockGenerator1" pin Out to "RealTimeClock1" pin Clock

  • Connect "DateTimeValue1" pin Out to "RealTimeClock1" pin Set

  • Connect "RealTimeClock1" pin Out to "DecodeDateTime1" pin In

  • Connect "RealTimeClock1" pin Control I2C to "Arduino" pin I2C In

  • Connect "DecodeDateTime1" pin Month to LedController1 > Integer Display 7 Segments1 pin In

  • Connect "DecodeDateTime1" pin Day to "SplitIntegerDigits1" pin In

  • Connect "DecodeDateTime1" pin Hour to "SplitIntegerDigits2" pin In

  • Connect "SplitIntegerDigits1" pin 0 to LedController1 > Value Section 7 Segments1 pin In

  • Connect "SplitIntegerDigits1" pin 1 to LedController1 > Value Section 7 Segments2 pin In

  • Connect "SplitIntegerDigits2" pin 0 to LedController1 > Value Section 7 Segments3 pin In
    Connect "SplitIntegerDigits2" pin 1 to LedController1 > Value Section 7 Segments4 pin In

  • Connect "DecodeDateTime1" pin Minute to LedController1 > Integer Display 7 Segments2 pin In

  • Connect "LedController1" pin Out SPI to Arduino Pin SPI In

  • Connect "LedController1" pin Chip Select to Arduino Digital Pin [10]

In Visuino Connect Components

In Visuino Connect Components photo 2

In Visuino Connect Components photo 3

In Visuino Connect Components photo 4

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino module, the LED display will start to display a date and time.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.