Maker.io main logo

Meet the New Raspberry Pi 3 Model B+

498

2018-03-14 | By Maker.io Staff

Raspberry Pi SBC

On this glorious Pi Day, the Raspberry Pi Foundation announced their latest computer, the Raspberry Pi 3 Model B+!

A New Pi Joins the Family

As the latest Pi to be released, the Raspberry Pi 3 Model B+ contains a wide range of improvements and features that will benefit the designers, developers, and even engineers who are looking to integrate Pi systems into their products. Here are some of the new Pi’s specs:

  • Quad core 64-bit processor clocked at 1.4GHz
  • 1GB LPDDR2 SRAM
  • Dual-band 2.4GHz and 5GHz wireless LAN
  • Bluetooth 4.2 / BLE
  • Higher speed ethernet up to 300Mbps
  • Power-over-Ethernet capability (via a separate PoE HAT)

The table below shows the specs of the Raspberry Pi 3 B and the Raspberry Pi 3 B+ side by side.

Spec Raspberry Pi 3 B Raspberry Pi 3 B+
CPU type/speed ARM Cortex-A53 1.2GHz ARM Cortex-A53 1.4GHz
RAM size 1GB SRAM 1GB SRAM
Integrated Wi-Fi 2.4GHz 2.4GHz and 5GHz
Ethernet speed 10/100 Mbps 300Mbps
PoE No Yes
Bluetooth 4.1 4.2

Boosts All Around

Thanks to the ever-increasing technological capabilities of electronics, this Raspberry Pi does not fall behind in any category, at least compared to other Pi computers. It either matches the old model’s speed or significantly improves upon it. For example, the CPU has been clocked at 1.4GHz, which is 200MHz faster than the Pi 3 B, and the ethernet speed has been boosted from 100Mbps to 300Mbps.

The heart of the Raspberry Pi 3 Model B+

The heart of the Raspberry Pi 3 Model B+

EMC Compliance

One feature included with the Raspberry Pi 3 Model B+ is a wireless dual-band LAN that comes with modular compliance certification. For those who are unaware, electronic products cannot be constructed and then released to the market without having some tests done to them (see CE and FCC), and many of these tests look for interference. Testing for interference (also known as EMC) can be incredibly costly and difficult to isolate, but, thanks to the WLAN’s modular compliance certification, you can expect significantly lower EMC issues when integrating the Pi into a product.

The Wi-Fi module in its metal housing

The Wi-Fi module in its metal housing

Physical Features

While the mechanical layout of the Pi has not changed (GPIO location, drill holes, etc.), the PCB itself has clearly undergone some physical changes. The main processor is no longer housed in a plastic package. Instead, it has a metal package, which may be beneficial for those who want to keep the temperature of the Pi as low as possible (with the aid of a heat sink). The top side also shows fewer components, and a four-pin header (used for PoE) has been included in the top right of the PCB.

Comparison of the Raspberry 3 and 3 B+

Comparison of the Raspberry 3 and 3 B+

制造商零件编号 SC0073
SBC 1.4GHZ 4 CORE 1GB RAM
Raspberry Pi
制造商零件编号 SC0022
SBC 1.2GHZ 4 CORE 1GB RAM
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.