• Preferred Supplier

Allegro MicroSystems

Image of Allegro Replace the Shunt

更换分流器

探索 Allegro 的集成无分流传感器解决方案,无需外部分流电阻器,即可为您的所有电子系统提供更高的效率和隔离度、更小的尺寸和整体提升的性能。现可从 DigiKey 订购!

Image of Allegro XtremeSense TMR Technology

XtremeSense™ TMR 技术

与霍尔、AMR 和 GMR 相比,采用 XtremeSense TMR 技术的 Allegro 传感器具有最高的磁灵敏度、最低的功耗和最小的尺寸。

Image of Allegro APS12753/APS11753 Sensors

APS12753/APS11753 微功率磁传感器

Allegro MicroSystems APS12753 和 APS11753 微功率磁性霍尔效应传感器旨在改变电池供电和节能型应用。

Image of Allegro New Era of Robotics

机器人新时代。更智能的感知。更流畅的动作

Allegro 提供动态的传感器和电机驱动器产品组合,能够让工程师快速轻松地开发高性能机器人系统,同时保持稳健性和可靠性。

Image of Allegro 48V Solutions

48V 系统解决方案

探索 Allegro 的各种 48V 系统;为汽车、工业、清洁能源和数据中心应用提供传感器和电源 IC、栅极驱动器、评估板以及各种解决方案。

工具和支持

精选视频

Allegro MicroSystems Micropower Switch and Latch Sensors
Allegro MicroSystems Micropower Switch and Latch Sensors
AGV and AMR Application Video
AGV and AMR Application Video
ACS37041 - Integrated Hall Effect Current Sensor
ACS37041 - Integrated Hall Effect Current Sensor
How magnetic current sensors outperform shunt-based solutions
How magnetic current sensors outperform shunt-based solutions
查看全部

近期 PTM

Image of Allegro Microsystems APM80950 and APM80951 LED Driver Modules
10 minutes
APM80950 and APM80951 LED Driver Modules
This presentation will introduce the APM80950 and APM80951 LED driver modules from Allegro MicroSystems.
Allegro's A17700 Pressure Sensor Interface IC
5 minutes
A17700 Pressure Sensor Interface IC
This presentation will discuss the features, specifications, and applications for the A17700 pressure sensor IC.
Image of Allegro MicroSystems' ATS19580LSNxxx-xxxxxx-x Back-Biased GMR Speed and Direction Sensor
5 minutes
ATS19580LSNx Back-Biased GMR Speed and Direction Sensor
Allegro MicroSystems' back-biased GMR speed and direction sensor is ideal for gear tooth sensing in applications such as automotive transmission.
Allegro's Alternatives to Shunts for Current Sensing
5 minutes
Alternatives to Shunts for Current Sensing
Comparison between shunt current measurement and magnetic current measurement. What are the advantages and disadvantages of both technologies and where to use which technique.
Image of Allegro Microsystems Magnetic High-Current Sensors - Magnetic High-Current Sensors
10 minutes
Magnetic High-Current Sensors
This presentation will provide an introduction to the different Hall-based high-current sensor IC solutions from Allegro Microsystems.
Image of Allegro's AC/DC Highly Isolated Power Monitoring Sensor
5 minutes
AC/DC Highly Isolated Power Monitoring Sensor
This presentation will provide an introduction of the Power Monitoring challenges, applications and solutions that Allegro Microsystems can provide to customers searching for better energy efficiencies in their system, or just giving an indication of the power consumption in real time to the user.
查看全部

关于 Allegro MicroSystems

Allegro MicroSystems 正在重新定义电源和传感技术的未来。从绿色能源到先进的移动性和运动控制系统,他们的团队热衷于开发智能解决方案,以推动世界前进,并为我们的客户带来竞争优势。凭借全球设计、制造和支持能力,Allegro 成为全球大型企业和区域市场领导者信赖的合作伙伴。