Maker.io main logo

Arduino Proximity Sensor -Activated OLED Display for Smart & Industrial

34

2026-04-13 | By Ron Cutts

License: GNU Lesser General Public License Bluetooth / BLE Displays Wifi Arduino ESP32

Project Description:

A compact and efficient smart display system that uses an IR obstacle sensor to detect motion or presence. When a hand or object is extended towards the sensor, an OLED display automatically turns on, showing useful information such as status updates, sensor readings, or notifications. After 3 seconds of inactivity, the display turns off to conserve power.

Potential Applications:

Smart Home Automation – Display room temperature, security alerts, or appliance statuses only when someone is nearby.

Industrial Use – Hands-free status monitoring in factories, reducing distractions and energy consumption.

Smart Gadgets – Interactive control panels for IoT devices that activate only when needed.

Energy-Saving Display Systems – Reduce power consumption in battery-operated or low-power devices.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

  1. Arduino UNO (Or any other Arduino)

  2. Breadboard

  3. OLED Display I2C

  4. Obstacle avoidance sensor

  5. Jumper wires

  6. Visuino program: Download Visuino

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

The Circuit

  1. Connect Obstacle avoidance sensor pin[VCC] to Arduino pin[5V]

  2. Connect Obstacle avoidance sensor pin[GND] to Arduino pin[GND]

  3. Connect Obstacle avoidance sensor pin[D0] to Arduino digital pin[2]

  4. Connect OLED Display pin [SCL] to Arduino pin [SCL]

  5. Connect OLED Display pin [SDA] to Arduino pin [SDA]

  6. Connect OLED Display pin [VCC] to Arduino pin [5v]

  7. Connect OLED Display pin [GND] to Arduino pin [GND]

The Circuit

Start Visuino, and Select the Arduino Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino Board Type

Start Visuino, and Select the Arduino Board Type photo 2

In Visuino Add & Set Components

  1. Add "Debounce Button" component

  2. Add "Digital Multi Source" component

  3. Add "Delay" component

  4. Add "Toggle(T) Flip-Flop" component

  5. Add "OLED I2C" component

  1. Select "Button1" and in the properties window set "Debounce Interval (mS)" to 10

  2. Select "Delay1" and in the properties window set "Interval" to 3000000. You can adjust this by setting any other value

  3. Select "DisplayOLED1" and in the properties window, select "Power On." Click on the pin icon and select "Boolean SinkPin"

  4. Double-click on "DisplayOLED1" and in the Elements window, drag "Draw Text" to the left side, and in the properties window, set "Size" to 3 and "Text" to ARDUINO or any other text

In Visuino Add & Set Components

In Visuino Add & Set Components photo 2

In Visuino Add & Set Components photo 3

In Visuino Add & Set Components photo 4

In Visuino Add & Set Components photo 5

In Visuino Add & Set Components photo 6

In Visuino Add & Set Components photo 7

In Visuino Add & Set Components photo 8

In Visuino Add & Set Components photo 9

In Visuino Add & Set Components photo 10

In Visuino Connect Components

  1. Connect Arduino digital pin[2] to "Button1" pin [In]

  2. Connect "Button1" pin [Out] to "MultiSource1" pin [In]

  3. Connect "MultiSource1" pin [0] to "TFlipFlop1" pin [Set]

  4. Connect "MultiSource1" pin [1] to "Delay1" pin [Start]

  5. Connect "Delay1" pin [Out] to "TFlipFlop1" pin [Reset]

  6. Connect "TFlipFlop1" pin [Out] to "DisplayOLED1" pin [Power On]

  7. Connect "DisplayOLED1" pin [I2C] to Arduino pin [I2C]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this tutorial; you can download it and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.