Maker.io main logo

8-bit Space Shooter on ESP8266 & LED Matrix - DIY Arduino Gaming

126

2025-06-10 | By Mirko Pavleski

License: General Public License LED Matrix WS2812/SK6812 (NeoPixel) Arduino ESP8266

Arcade games are fast-paced, simple-to-play video games, and the Goal is usually to get the highest score, not complete a story. In this type of game, you’re always doing something (shooting, jumping, etc.), often using just a joystick with 1–3 buttons.

bvn

From one of my projects, I have an 8x32 LED matrix with WS2812B LEDs, so I decided to make a simple horizontal shooting game on it, somewhat in the style of the popular Space Invaders. On one side, spaceships constantly appear randomly and move towards us, and the goal is to destroy as many enemy ships as possible before they destroy us.

Detailed video description at: https://youtu.be/e2iRH_F6sv4

The game is extremely simple to make and consists of only a few components:

- ESP8266 microcontroller board

- 8x32 Led Matrix with WS2812B leds

- 3 Buttons

- and Buzzer

I simplified the device's construction as much as possible. The matrix was first glued to the substrate, and then I placed frosted glass in front of it for a better visual effect with some light diffusion. Then I made a simple two-dimensional joystick that contains three colorful buttons with built-in LEDs, but standard buttons can also be used.

This project is sponsored by PCBWay. They have all the services you need to create your project, whether it's a school project or a complex professional project.

First, let me explain how the game works. When you turn on the display, a scrolling text appears with the content "Press Fire to Start".

cxgx

Now, if we press the FIRE button, the game starts by generating characteristic sounds.

Our weapon is located on the left side of the display and is green. With each press of the up or down buttons, the weapon moves one space. On the other side, on the far right, enemy ships marked in red appear randomly, with a magenta missile on their tip. If we destroy the enemy, the missile remains until the end, and we must avoid it so that it does not destroy us.

vgbjgv

At the bottom right of the display, as many green dots appear as we have destroyed enemy ships. If an enemy ship hits our weapon, the game ends, and the Game Over message appears on the display with appropriate sounds.

cfhcf

If we press the Fire button, a score appears where, for each destroyed enemy ship, we get 10 points. By pressing the Fire button again, we return to the beginning, and pressing the Fire button again starts a new game.

hjbk

The destruction of an enemy object is accompanied by a simple animation, and otherwise, the entire game is accompanied by appropriate sounds. Honestly, I spent more time introducing these simple sounds than I did for the entire development before, because the sound generation caused more problems than the graphic part of the game. Even at the expense of the sound, some glitches remained in the game.

As for the code, it should be noted that it is not as simple as I initially imagined, but it is highly customizable, and at the beginning of the code, we can change many parameters, of which the most important for the gameplay are: PLAYER_SPEED, MISSILE_SPEED, ENEMY_SPEED, and ENEMY_FIRE_RATE. Regarding the installation of the code, I used Arduino IDE v 1.8.16, and ESP8266 Core v 3.1.2.

bvhjk

And finally, a short conclusion. This is a retro-style space shooting game built using an ESP8266 microcontroller and a 32x8 WS2812B LED matrix display, controlled by three push buttons for up/down movement and firing, with a buzzer for sound effects, and programmed using the Arduino IDE with the FastLED library.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.