Single Pair Ethernet

Single Pair Ethernet (SPE) has created a whole new world of possibilities in IIoT and Industry 4.0. By transmitting data as well as PoDL using a single pair of copper wires, manufacturers can utilize gigabit Ethernet over distances of up to 40 meters for machine to machine communication. SPE is ideal for applications such as Industrial Robotics, Railway, Smart Cars, Building Automation through its increased flexibility, size and weight reduction.

SPE Industrial Partner Network

SPE Industrial Partner Network

The SPE Industrial Partner Network is an equal association of companies that promote Single Pair Ethernet technology as the basis for rapid and successful growth of the IIoT (Industrial Ethernet of Things).

For future users it is the first point of contact for all questions concerning the construction of SPE networks and devices. It provides clear recommendations for the development of future IIoT applications and is the central information and exchange platform.

Related Resources

Harting Single Pair Ethernet
Single Pair Ethernet
Harting Drives Standardization of Single Pair Ethernet
Single Pair Ethernet - Harting
Single Pair Ethernet - Würth Elektronik
Ethernet reinvented - Phoenix Contact
SPE in Industrial Applications - Phoenix Contact
How a 10BASE-T1L MAC-PHY Simplifies Low Power Processor Ethernet Connectivity - Analog Devices
Single Pair Ethernet: High Quality Asset Health Insights and Power on Two Wires for Condition Monitoring Applications - Analog Devices
Single Pair Ethernet: 10BASE-T1L Market and Technology Insights - Analog Devices
Enabling Ethernet to the Field with 10BASE-T1L Connectivity - Analog Devices
ADIN1100: A Robust, Industrial, Low Power 10Base-T1L Ethernet PHY - Analog Devices
New Data, New Insights - Analog Devices