Maker.io main logo

Value Acrylic Custom Phone Holder

12

2026-02-19 | By Kitronik Maker

License: See Original Project Laser Cutters

Courtesy of Kitronik Maker

Guide by Kitronik Maker

This is a nice easy project for a class just learning how to laser cut and heat bend acrylic. The stand features space for a charging cable - considering this sort of feature can elevate a project and lead to a more considered and usable final product.

This blog was was written by Emma and is one of the 6 included projects in the Book of Projects Volume 5. Background Image by Joe Woods on Unsplash.

This make covers:

covers_1

What did we use?

Note:

  • Price per student calculated based on the exVAT price for one sheet of 3mm thick 600mm x 400mm Blue Value Acrylic, with each sheet fitting 9 Phone Stands.

  • The price may fluctuate slightly over time but was correct at the time of printing.

phone-stand_2

Step 1 - Check out the design files.

This DXF contains the design for this project. The diagram below shows you how to work with the file.

design_3

This design can be tiled nine to a sheet of 600 x 400mm material. The black lines should be kiss-cut (a cut that doesn’t go all the way through the material), and then after that the green lines should be cut through all the way.

Step 2 - Laser cut the phone stand.

As specified above, cut out the phone stand. You could also use a fine-tooth saw if you do not have a laser cutter available.

step2_4

Step 3 - Heat and bend the phone stand.

Bend the acrylic along the kiss-cut lines, forming the stand. Remember to heat gradually to avoid warping and bubbling and take care not to burn yourself!

step3_5

Step 4 - Let it cool, and you’re done!

Your phone can sit on the stand as pictured below, and your charging cable can thread through the holes too!

step4_6

©Kitronik Ltd – You may print this page & link to it, but must not copy the page or part thereof without Kitronik's prior written consent.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.