Maker.io main logo

Using Adafruit's Sound FX Board with Red Pitaya!

16

2022-04-28 | By Will Siffer

License: Attribution Sound

The Big Picture

This project is a part of a much larger project I am working on, a 3 foot scale model of the Purdue Mascot, The Boilermaker Special. Since the real full-sized version makes sound and plays music, I wanted to make sure that my model could play the same sounds of the train horns and play some of the songs that the train plays. This left me to looking for a device that could handle clean audio output, and I found the Adafruit Audio FX Sound Board.

Specs:

The board I chose to go with for this project was the Adafruit Audio FX Sound Board with 16 MB flash memory and an integrated 2x2 W amplifier. This allowed me to put higher quality and longer audio onto the board. I also thought the integrated amplifier was especially important so I could make sure to eliminate sources of noise in my circuit that could lead to unpleasent audio coming out of the speakers. 

Along with the sound board, I am using a pair of 3 W speakers to deliver the sound signal. I chose these speakers since they are rated beyond what the amplifier can supply and are unlikely to blow out when I am using them. 

A little bit about the Red Pitaya IZD0021 Home Lab

I have used 3 different products designed to be a home lab device during my time studying Electrical Engineering. But the thing that makes the Red Pitaya platform so intruiging is the fact that the tool itself can run fully "headless" from your computer, allowing you to use a tablet, phone, laptop, or any device that can connect to the internet with a screen to become a control surface for your measurements. 

Not only does this allow for simplicity, but it allows measurements to be made in a completely different way. With the Red Pitaya board I have been able to treat my oscilloscope like it was my handheld multimeter! I can plug it in to an external phone charger and use a tablet to display the measurements so I don't have to worry about finding an outlet to plug in to. While this use case may be not very often, having the option to be mobile during a measurement makes taking on challenging projects just a little more realistic.

I look forward to continuing to use this home lab through the remainder of this project and learn more about how it works so I can be more successful in my designs. But until then, I hope you get an oppertunity to try out this device because it changed how I prototype my electrical designs.

制造商零件编号 IZD0021
SDRLAB 122-16 STANDARD KIT
Red Pitaya d.d.
制造商零件编号 ASE06008MR-LW150-R
SPEAKER 8OHM 3W TOP PORT 83DB
PUI Audio, Inc.
BRUSH SNGL HEAD 1 PC
制造商零件编号 1209
BRUSH SNGL HEAD 1 PC
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.