Maker.io main logo

Setting Up Picade Max

105

2025-03-13 | By Pimoroni

License: See Original Project Memory Card Single Board Computers Raspberry Pi SBC

Courtesy of Pimoroni

Guide by Pimoroni

Congratulations on buying the best arcade machine available! This guide will walk you ‎through installing two of the popular retrogaming platforms onto the SD card or solid-state ‎drive of your Raspberry Pi.‎

We'll be discussing two different software options in this guide:‎

Recalbox is a user-friendly platform that lets you play games from more than 100 different ‎gaming systems, including consoles, arcade machines, computers, and handheld ‎devices. It uses a system called RetroArch to work.‎

RetroPie is a long-time favourite of many people and is installed on top of Raspberry Pi OS. ‎This means you will have all the familiar functionality of the Raspberry Pi OS with the ‎addition of a retrogaming platform.‎

In this guide we'll be showing you how to:‎

  • install Recalbox or RetroPie to your SD card

  • setup the power button to turn off your Picade safely

  • transfer files to your Picade Max

  • change the button settings to make your controller feel like the one you like best

  • make sure the sound and volume control is working correctly

Recalbox and RetroPie come with some free emulators and games already installed, but ‎you can also add your own. We'd encourage you to obtain game ROMs and BIOS files by ‎legitimate means - it's important to support the creators for their hard work, no matter how ‎long ago they made them.‎

What you'll need

  • An assembled Picade Max kit with a Raspberry Pi 5 installed in it*. If you've not yet ‎assembled your Picade Max our online assembly guide can be found here.‎

  • A microSD card

‎*If you want to use an older Pi with this kit that's also possible (as long as it's one of the ‎ones with a 40 pin header). These instructions should still work as long as you flash the ‎correct OS for your version of Pi.‎

Prerequisites

Download and install Raspberry Pi Imager on your computer (it's available for Windows, ‎Mac and Linux). We'll be using this to load the platform of choice onto your SD card.‎

Whilst an 8GB card microSD card would work, we recommend that you use one that's at ‎least 16 GB to allow you to install all the platforms and games; the larger the card, the more ‎you can install on it.‎

Recalbox

Right now, Recalbox is the simplest retrogaming platform to set up thanks to it being an ‎option within Raspberry Pi Imager. It also comes with a bunch of free games built in, so it's ‎a great choice if you're a beginner.‎

Installing Recalbox

Start Raspberry Pi Imager on your computer.

install_1

Click on Choose Device and then pick Raspberry Pi 5.

device_2

Next, click on Choose OS and then scroll down to find Emulation and Game OS.

choose_3

Here, you’ll find the options for the emulator. Right now, the only one available for the ‎Raspberry Pi 5 is Recalbox.‎

options_4

Choosing Recalbox will bring you back to the main Imager screen.‎

main_5

Insert an SD card into your card reader, then click on Choose Storage. You will see a list of ‎storage devices. Select your SD card.‎

insert_6

By clicking Next, you’ll be notified that all data on your SD card will be deleted. Click Yes to ‎confirm that you want to install Recalbox on the SD card.‎

confirm_7

Wait for the card to finish writing. Once it's done, take the card out of your card reader and ‎put it into the Raspberry Pi 5 inside the Picade Max.‎

writing_8

Press the button on the left side of the Picade Max to turn it on, and then wait for Recalbox ‎to load up.‎

Recalbox will start with a few basic emulators and games, but you can easily add more ‎whenever you like. You'll only notice the emulators that have games added.‎

Controlling Recalbox

When you turn Recalbox on for the first time, the buttons and joystick controls should be ‎pre-configured to be as shown in the images below (depending on if you have built the ‎Picade Max for two or one player, and assuming you've connected up the buttons to the ‎correct terminals on the USB Controller board!). The in-game controls are shown on the ‎buttons here, with the Recalbox menu controls shown within [brackets] under the buttons.‎

For the two-controller setup, this is:‎

two_9

For the single controller setup, this is:‎

single_10

There is another button on the right-hand side of the Picade Max, known as the ‘Hotkey’. ‎More about that later!‎

Navigating Recalbox

When you boot Recalbox this is a typical image of what you will see:‎

boot_11

Move the joystick up and down to choose between different emulators. Press the ‘A [Select]’ ‎button to pick the one you want to use. Once the list of games is shown, use the same ‎actions to navigate the list and start a game.‎

Hotkey Combinations

On the right-hand side of the Picade Max is a black button called the ‘Hotkey’, which can be ‎used in combination with other buttons to control RecalBox. You will find the following ‎button combinations helpful.‎

  • ‎‘Hotkey’ + ‘R3 [Main]’ to return to the home screen

  • ‎‘Hotkey’ + ‘A [Select]’ to bring up the in-game quick menu, allowing you to load and ‎save game states so you can carry on playing later. It also enables you to change the ‎controls used in the game

  • ‎‘Hotkey’ + ‘B [Back]’ to reset the game‎

  • ‎‘Hotkey’ + ‘L1’ to save a screenshot (these are stored in the ‎folder /share/screenshots)‎

Change Recalbox Settings

Recalbox has a lot of different settings. We’re not going to take you through them all ‎because that would take a long time! However, here are some of the most important ones. ‎You can change Recalbox settings from the Main Menu, accessed by pressing the ‘R3 ‎‎[Main]’ button.‎

settings_12

Use the joystick to navigate through the options, and press 'A [Select]' to open a sub-menu ‎or choose an option. To return to the previous menu, just hit the 'B [Back]' button. To find a ‎specific game, just click the 'R1 [Search]' button. Use the onscreen keyboard to spell out ‎the name of the game, using the 'Y [Backspace]' to delete a character if you made a ‎mistake.‎

You can shutdown or restart Recalbox using the Quit menu by pressing the ‘L3 [Quit]’ ‎button.‎

Changing Game Controls

You might find that the default controls don't work well for you for some games you play. In ‎Recalbox, you can change which buttons do what. Open the settings menu using the ‘R3 ‎‎[Main]’ button and use the joystick to move down to Controller Settings.‎

controller_13

Press the ‘A [Select]’ button to open the controller menu:‎

select_14

Press the 'A [Select]' button to select Configure a Controller:‎

select_15

After reading the text, press 'A [Select]' again:

select_16

Recalbox will see that you have two controllers connected, even if you are only using the one ‎player layout and will ask you to choose one to set up. To do this, press and hold the chosen ‎controller’s ‘A [Select]’ button until the setup menu shows up.‎

menu_17

You can now change the buttons for each action by pressing the one you want for each ‎action. Just keep in mind that this will also affect how you move around the Recalbox ‎menus. It might be best to wait until you have everything set up the way you want before ‎making these changes.‎

You can do the same thing for the other controller. You can also set up different controller ‎settings for each emulator, but we won't go into that here. For more information, please ‎check out the Recalbox Wiki.‎

Setting up a Network to add Emulators and Games

If your Picade Max isn't hooked up to your network with a cable, you'll need to use WiFi ‎instead. Start by going to the main menu and choosing Network Settings.‎

network_18

Scroll down to Enable Wi-Fi and enable it by pressing ‘A [Select].’‎

Move to Network Name and use left/right on the joystick to scroll through available ‎networks.‎

Once chosen, scroll down to Wi-Fi Password and hit ‘A [Select].’‎

If you have a keyboard connected, just type in your password. If you don’t, you can use the ‎on-screen keyboard. Move the left and right joysticks to choose a letter. Use the up and ‎down movement to switch between lowercase letters, numbers, and symbols. Press ‘A ‎‎[Select]' to choose a letter, and the ‘R3 [Main Menu]’ button when you have entered the ‎whole password.‎

password_19

Here is an example of the network settings once everything is set up.‎

example_20

You might need to restart your device to connect to Wi-Fi.‎

You can connect remotely to Recalbox in three helpful ways once you have a network ‎connection:‎

  • Shared folder access

  • The Recalbox web manager

  • Login via ssh

Access the web manager from your computer by browsing to http://recalbox (or whatever ‎name you have used as the hostname). From there you can see the installed emulators and ‎games, monitor your Raspberry Pi, and make settings changes.‎

access_21

Adding Emulators and BIOS Files

Some emulators require BIOS files to work - these provide firmware or an OS for specific ‎emulation platforms. Before you look for a BIOS online, check whether Recalbox already ‎has the emulator you want. The emulator won't show up in the list until you've added a ‎game ROM. You can check this from the Main Menu by selecting BIOS Checking or by going ‎to the Recalbox WebManager.

adding_22

You will find a list of emulators that are working and not working, along with details on ‎which ones might need extra BIOS files.‎

files_23

As you go through the list, you'll see that working emulators have a green thumbs-up, not ‎working emulators have a red thumbs-down, and those that work partially have a yellow ‎thumbs-up.

‎After you have located the BIOS files you need, transfer them to your Raspberry Pi. If you're ‎using Windows, open File Explorer, and type \\RECALBOX in the address bar, or you can ‎use the IP address. You'll need to log in with the username root and the ‎password recalboxroot.‎

located_24

On a Linux machine, mount the BIOS folder with:‎

  • mkdir ~/recalboxbios

  • sudo mount -t cifs //recalbox/bios ~/recalboxbios

  • When asked for the root password, use: recalboxroot

  • You can also open the file manager and type smb://RECALBOX/bios in the address ‎bar. You can log in as an anonymous user without a username or password.‎

linux_25

The 'bios' folder has a separate folder for each machine you want to emulate. Just put the ‎additional BIOS files into the right folder.‎

You will need to restart Recalbox for the BIOS files to be recognised.‎

Adding Games (ROMs)‎

Recalbox comes with some games already installed. You can see the list of these ‎games here.‎

You might want to add your favourite games too. Installing games is similar to installing ‎BIOS files. Instead of placing them in the BIOS folder, you need to put them in the roms ‎‎(internal) folder. Just make sure to place them in the specific subfolder that matches the ‎emulator you are using.‎

You will need to restart Recalbox for them to be detected.‎

Configuring the Power Button

To make the power button on the left-hand side of the Picade Max function, we need to ‎make some setting changes.‎

Make sure that the Picade Max is connected to your network. Then, use a program like Putty ‎or a terminal to connect using SSH (Secure Shell) to the Raspberry Pi. For example, if you’re ‎using a Linux terminal, type the following to connect to your Recalbox:‎

Copy Code
ssh root@recalbox

When asked for the password, use ‘recalboxroot’.‎

The ‘boot’ folder must be mounted for writing so you can edit the configuration file. Type in ‎the following:‎

Copy Code
mount -o remount,rw /boot

nano /boot/recalbox-user-config.txt

To make the power button safely turn off your Raspberry Pi, add these lines at the end of the ‎file:‎

Copy Code
dtoverlay=gpio-shutdown,gpio_pin=17,active_low,debounce=2000‎

dtoverlay=gpio-poweroff,gpiopin=4,active_low

The debounce setting is optional but makes it so the button has to be held down for 2 ‎seconds (2000 milliseconds), to avoid accidental presses from turning off your Picade Max ‎during your session.‎

Additionally, add this line to the file to ensure that the devices plugged into your Pi's USB ‎ports receive the most power possible:‎

Copy Code
usb_max_current_enable=1‎

Reboot Recalbox for these to take effect.‎

Setting up Sound

The volume button is on the left side of your Picade Max. You can change the volume by ‎turning the knob, and you can mute or unmute it by pressing the button.‎

If you notice there’s no sound at all (or if the mute button is misbehaving), it could be ‎because Recalbox has the wrong audio settings.‎

From the Main Menu (accessed by 'R3 [Main]'), go down to Sound Settings.

sound_26

Press ‘A [Select]’ to open the sound settings menu:‎

sound_27

Move down to Output Device, and press ‘A [Select]’.

move_28

Scroll to Digital Output (S/PDIF) - PICADE USB AUDIO and select it with ‘A [Select].’‎

scroll_29

Return to the Recalbox platform page using ‘B [Back].’‎

You should now be able to enjoy music and sounds from the speakers of your Picade Max.‎

Moving over to an SSD on your Pimoroni NVMe Base

If you’ve got a Pimoroni NVMe Base with an M.2 SSD you can move everything from the SD ‎card to the SSD.‎

Connect to your Pi using SSH as shown above.‎

To check that your SSD is connected correctly, type:‎

Copy Code
ls /dev/nvme0

If the SSD cannot be found, the terminal will report:‎

Copy Code
ls: cannot access \'/dev/nvme0\': No such file or directory‎

In which case, turn off your Raspberry Pi and recheck the ribbon cable connections and the ‎SSD installation. Remember that the clips on both the NVMe Base and Raspberry Pi 5 need ‎to be folded/pressed back in place for the connections to work. Use this tutorial if you need ‎help.‎

If the SSD is correctly connected, /dev/nvme0 will be repeated back in the terminal. All is ‎good and you are ready to proceed. Perform the copy by typing:‎

Copy Code
dd if=/dev/mmcblk0 of=/dev/nvme0n1‎

Once everything has been copied over to the SSD, shutdown the Pi, remove the SD card, ‎and restart the Pi. Recalbox should now be booting from the SSD. If it does not, you might ‎have an old version of the firmware on your Pi, in which case you will need to prepare ‎another SD card with Raspberry Pi OS Lite, put that in your Pi, boot it and follow the steps in ‎our NVMe Base Learn Guide to update the firmware.‎

RetroPie

RetroPie has been available for a while - it's very customisable, with a great community ‎behind it. It's not included in the Raspberry Pi Imager for the Raspberry Pi 5 right now ‎though, and you can't use the versions designed for older Raspberry Pi models. As such, ‎setting it up takes a bit more effort than using Recalbox.‎

Preparing the Operating System

You're going to start with a basic Raspberry Pi OS image, so fire up Raspberry Pi Imager. ‎We'll be using the Lite version as we're planning on connecting to our Pi 'headlessly' from ‎another computer, but if you'd like to have access to the Raspberry Pi graphical interface ‎you can use the Full/Desktop version instead.‎

preparing_30

Click on Choose Device and pick Raspberry Pi 5.‎

click_31

Click on Raspberry Pi OS (Other):

click_32

Select Raspberry Pi OS Lite (64-bit):‎

select_33

On the next screen, click on Choose Storage:

storage_34

Select your SD card:‎

card_35

Select Next to start writing the OS to the SD card:‎

next_36

But before you start, you need to set up the operating system so you can log in from another ‎computer using SSH. Click on Edit Settings:‎

edit_37

In the General Tab, change the device name to RetroPie, update the password to something ‎new, and set up your WiFi connection.‎

general_38

In the Services section, turn on SSH so you can log in from another location and transfer ‎files using SFTP. Then, click Save.‎

services_38

Then click on Yes. Raspberry Pi OS Lite will be written to the SD card:‎

written_39

Confirm it is okay to overwrite your SD card:‎

confirm_40

And wait for the OS to be written:‎

wait_41

After it's finished writing, you can safely remove the SD card and insert it into your ‎Raspberry Pi in the Picade Max.‎

after_42

Installing RetroPie

Installing RetroPie directly on the Raspberry Pi can take a while, so it's best to connect a ‎keyboard to the Pi and do the installation there. This way, you won't run into issues with ‎remote connections dropping and having to start the installation again.‎

After the Picade Max has started up, log in using the username and password you created ‎earlier. As always, the first thing to do is update the OS to the latest version:‎

Copy Code
sudo apt update

sudo apt dist-upgrade

You need to install git to download RetroPie from GitHub.‎

Copy Code
sudo apt install git

The RetroPie maintainers have set up an installation script for us, so let’s go ahead and ‎download it:‎

Copy Code
cd ~‎

git clone --depth=1 https://github.com/RetroPie/RetroPie-Setup.git

After downloading it, you can begin the installation.‎

Copy Code
cd RetroPie-Setup

sudo ./retropie_setup.sh

This might take a little while! When it’s done, please restart the Pi:‎

Copy Code
sudo reboot

You can find easy-to-follow setup instructions on the RetroPie website here.‎

Changing Settings

Since RetroPie uses the same Emulation Station software as Recalbox, changing settings is ‎exactly the same as for Recalbox. We therefore refer you back to the Controlling ‎Recalbox section. This also includes instructions for setting up the sound card.‎

Installing Emulators and Games

RetroPie includes only a few emulators and doesn't have any games, so you'll need to add ‎those on your own. If you'd like to download a ROM to practice with, the Tanglewood ‎demo for Mega Drive is available for free on itch.io.‎

When you set up the operating system, you turned on SSH, which also means you can use ‎SFTP (Secure FTP). You can use any FTP client to move files, but we suggest ‎using WinSCP if you're on Windows or Filezilla (available for Windows, Mac or Linux) to ‎transfer files to RetroPie.‎

RetroPie and Recalbox can use the same game files and system BIOSs, so you can share ‎them between the two. To set things up, you need to place the system BIOSs in the ‎folder /home/pi/RetroPie/BIOS, and the game files in /home/pi/RetroPie/roms. Make ‎sure to organise the files into folders named after the game consoles they belong to. If you ‎need help figuring out the names of the folders, you can check the RetroPie guide.‎

Hotkey Combinations

On the right-hand side of the Picade Max is a black button, which is called the ‘Hotkey’ - this ‎can be used in combination with other buttons to control RecalBox. You will find the ‎following button combinations helpful.‎

  • ‎‘Hotkey’ + ‘R3 [Main]’ to return to the home screen.‎

  • ‎‘Hotkey’ + ‘A [Select]’ to bring up the in-game quick menu, allowing you to load and ‎save game states so you can carry on playing later. It also enables you to change the ‎controls used in the game.‎

  • ‎‘Hotkey’ + ‘B [Back]’ to reset the game‎

  • ‎‘Hotkey’ + ‘L1’ to save a screenshot (which is stored in the ‎folder /share/screenshots)‎

Configuring the Power Button

To make the power button on the left-hand side of the Picade Max function, we need to ‎make some setting changes.‎

Make sure that the Picade Max is connected to your network. Then, use a program like Putty ‎or a terminal to connect using SSH (Secure Shell) to the Raspberry Pi. For example, if you’re ‎using a Linux terminal, type the following to connect to your RetroPie:‎

Copy Code
ssh pi@retropie

Use the password you set when you wrote the SD card (the default is raspberry).‎

Edit the configuration file:‎

Copy Code
sudo nano /boot/firmware/config.txt

To make the power button safely turn off your Raspberry Pi, add these lines at the end of the ‎file:‎

Copy Code
dtoverlay=gpio-shutdown,gpio_pin=17,active_low,debounce=2000‎

dtoverlay=gpio-poweroff,gpiopin=4,active_low

The debounce setting is optional but makes it so the button has to be held down for 2 ‎seconds (2000 milliseconds), to avoid accidental presses from turning off your Picade Max ‎during your session.‎

Additionally, add this line to the file to ensure that the devices plugged into your Pi's USB ‎ports receive the most power possible:‎

Copy Code
usb_max_current_enable=1‎

Reboot RetroPie for these to take effect.‎

Moving over to an SSD on your Pimoroni NVMe Base

If you’ve got a Pimoroni NVMe Base with an M.2 SSD you can move everything from the SD ‎card to the SSD.‎

Connect to your Pi using SSH as shown above.‎

To check that your SSD is connected correctly, type:‎

Copy Code
ls /dev/nvme0‎

If the SSD cannot be found, the terminal will report:‎

Copy Code
ls: cannot access \'/dev/nvme0\': No such file or directory‎

In which case, turn off your Raspberry Pi and recheck the ribbon cable connections and the ‎SSD installation. Remember that the clips on both the NVMe Base and Raspberry Pi 5 need ‎to be folded/pressed back in place for the connections to work. Use this tutorial if you need ‎help.‎

If the SSD is correctly connected, /dev/nvme0 will be repeated back in the terminal. All is ‎good and you are ready to proceed. Perform the copy by typing:‎

Copy Code
sudo dd if=/dev/mmcblk0 of=/dev/nvme0n1 status=progress‎

Once everything has been copied over to the SSD, shutdown the Pi, remove the SD card, ‎and restart the Pi. Recalbox should now be booting from the SSD. If it does not, you might ‎have an old version of the firmware on your Pi, in which case you will need to prepare ‎another SD card with Raspberry Pi OS Lite, put that in your Pi, boot it and follow the steps in ‎our NVMe Base Learn Guide to update the firmware.‎

Updating the Picade Max Firmware

The Picade Max's USB Audio and USB Controller boards are powered by the Raspberry Pi ‎RP2040. This means we can make our own custom firmware for them! To see if there are ‎any firmware updates available and find how to update the boards, please visit the GitHub ‎pages below:‎

Next Steps

Hopefully, this guide has given you a brief overview of how to get started with Recalbox and ‎Retropie - we hope you have lots of fun with your Picade Max. There's a ton more ‎information on how to customise both systems at the links below (plus info on how you ‎can support their development):‎

If you'd like to discuss Picade Max specifically, check out our forums or the Picade channel ‎on our Discord:‎

That's all folks!‎

制造商零件编号 PIM708
PICADE MAX
Pimoroni Ltd
制造商零件编号 SC1628
MEM CARD MICROSD 32GB CLASS 10
Raspberry Pi
制造商零件编号 SC1432
SBC 2.4GHZ 4 CORE 8GB PI 5
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.