Maker.io main logo

Make it fun to remember relative names by M5Stack for children

27

2022-12-01 | By M5Stack

License: General Public License Bluetooth / BLE Drivers / Controllers Arduino

* Thanks for the source code and project information provided by @Mame Tarou

 

background

I think that the frequency of meeting with relatives has decreased in the flow of self-restraint due to the corona wreck. However, grandparents want their grandchildren to remember their names as soon as possible. Therefore, I developed a product that allows families to remember their relative's names without having to meet.

As a reference for how children learn things, I heard that if you connect pictures and sounds with the child's action, such as "Children's books that learn with sounds and pictures", children will learn things quite quickly.

Therefore, I thought of developing a product that would play the name of the relative when the child tapped a photo of the relative.

parts

  • M5Paper
  • Grove MP3 Module v2.0
  • speaker
  • microSD card

 parts

image preparation

I wanted to display about 6 relative images on the screen. M5Paper is 540x960, so prepare 6 square images of 250x250.

  • create a resources folder
  • Place 1 to 6 png files of 250x250 in the resources folder
  • Execute image2gray.py under resources folder → Create ImageResouce.hfolder<Program>

┣Program.ino
┗Program<resources>
┣1.png
┣2.png
┣3.png
┣4.png
┣5.png
┣6.png
┣image2gray.py
┗ageResource.h

*image2gray.py is located at https://github.com/m5stack/M5EPD/tree/main/tools/image2gray

Preparing the microSD card

  • Create audio corresponding to the designation 1 to 6.png
  • Data will be written to the SD card "in order from 1"

*Grove MP3 module v2.0 can specify the index number in the order in which the audio is written

connection

  • Insert microSD card into Grove MP3 Module v2.0
  • Connect Port.A of M5Paper and Grove MP3 module v2.0 with Grove cable
  • Write program to M5Paper

4

 

How it works

When you touch the face of a relative, the name will be played by voice.

 

 

program

Write the following program to M5Paper.

 

Copy Code
#include <SoftwareSerial.h>
#include <MP3Player_KT403A.h>
#include <M5EPD.h>
#include "./resources/ImageResource.h"

// edp
#define PIC_SIZE 250
#define LEFT_INDEXX 10
#define RIGHT_INDEXX 280
#define UPPER_INDEXY 50
#define MIDDLE_INDEXY 320
#define LOWER_INDEXY 590

#define BUTTON_RESET_MSEC 1000
#define DELAY_MSEC 10

int preIndex = 0;

// mp3
#define swtxPin 25
#define swrxPin 32

// Note: You must define a SoftwareSerial class object that the name must be mp3,
// but you can change the pin number according to the actual situation.
SoftwareSerial mp3(swrxPin, swtxPin);

M5EPD_Canvas canvas(&M5.EPD);

void setup()
{
M5.begin();
M5.EPD.SetRotation(90);
M5.EPD.Clear(true);

// 写真の表示
canvas.createCanvas(540, 960);
canvas.setTextSize(3);
canvas.pushImage(LEFT_INDEXX, UPPER_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_1_250x250);
canvas.pushImage(RIGHT_INDEXX, UPPER_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_2_250x250);
canvas.pushImage(LEFT_INDEXX, MIDDLE_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_3_250x250);
canvas.pushImage(RIGHT_INDEXX, MIDDLE_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_4_250x250);
canvas.pushImage(LEFT_INDEXX, LOWER_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_5_250x250);
canvas.pushImage(RIGHT_INDEXX, LOWER_INDEXY ,PIC_SIZE,PIC_SIZE,ImageResource_6_250x250);
canvas.pushCanvas(0,0,UPDATE_MODE_GC16);

// タッチパネルの準備
M5.TP.SetRotation(90);

// mp3初期設定
pinMode(swrxPin, INPUT);
pinMode(swtxPin, OUTPUT);
mp3.begin(9600);
delay(100);
SelectPlayerDevice(0x02); // Select SD card as the player device.
SetVolume(0x1E); // Set the volume, the range is 0x00 to 0x1E.
}


// 写真番号に応じた動作
void touchAction(int picNumber){
SpecifyMusicPlay(picNumber);
Serial.printf("x:%d\r\n", picNumber);
}

// 領域内をタッチしたかどうか判定
bool InsideSquare(int squareIndexX, int squareIndexY, int picSize, int touchX , int touchY)
{
if(touchX < squareIndexX) return false;
if((squareIndexX + picSize) < touchX) return false;
if(touchY < squareIndexY) return false;
if((squareIndexY + picSize) < touchY) return false;

return true;
}

// どの写真を押したかチェック
int CheckTouchPicture(int touchX , int touchY)
{
int index = 0;

if(InsideSquare(LEFT_INDEXX, UPPER_INDEXY ,PIC_SIZE, touchX, touchY)) index = 1;
else if(InsideSquare(RIGHT_INDEXX, UPPER_INDEXY ,PIC_SIZE, touchX, touchY)) index = 2;
else if(InsideSquare(LEFT_INDEXX, MIDDLE_INDEXY ,PIC_SIZE, touchX, touchY)) index = 3;
else if(InsideSquare(RIGHT_INDEXX, MIDDLE_INDEXY ,PIC_SIZE, touchX, touchY)) index = 4;
else if(InsideSquare(LEFT_INDEXX, LOWER_INDEXY ,PIC_SIZE, touchX, touchY)) index = 5;
else if(InsideSquare(RIGHT_INDEXX, LOWER_INDEXY ,PIC_SIZE, touchX, touchY)) index = 6;

return index;
}

// 0:タッチなし
// 1~6:写真をタッチ
int checkTouch(void){
int index = 0;

if(M5.TP.avaliable()){
if(!M5.TP.isFingerUp()){
M5.TP.update();
tp_finger_t FingerItem = M5.TP.readFinger(0);
index = CheckTouchPicture(FingerItem.x,FingerItem.y);
}

if(index != 0 && preIndex != index){
preIndex = index;
return index;
}else{
// 更新なし
return 0;
}
}
return 0;
}

int totalMsec;

void loop()
{
int picIndex = checkTouch();
if(picIndex != 0){
touchAction(picIndex);
totalMsec = 0;
}

// 押したことを初期化
if(preIndex != 0){
if(totalMsec < BUTTON_RESET_MSEC){
totalMsec = totalMsec + DELAY_MSEC;
}else{
preIndex = 0;
totalMsec = 0;
}
}else{
preIndex = 0;
totalMsec = 0;
}

delay(DELAY_MSEC);
}

 

制造商零件编号 K049-B
M5PAPER ESP32 EINK DEV KIT V1.1
M5Stack Technology Co., Ltd.
制造商零件编号 107020008
GROVE - MP3 V2.0
Seeed Technology Co., Ltd
制造商零件编号 112990066
MEM CARD MICROSD 32GB CLASS 10
Seeed Technology Co., Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.