Maker.io main logo

Keypad Controlled Door Locking System Using Arduino

10

2026-05-19 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Keypad Arduino

In this tutorial, we will learn how to make a locking system using a keypad and Arduino. If you type the correct code within a time limit of 5 seconds, the door will open; in our case, the green LED will glow. After the 5 seconds, it will lock back; in our case, the red LED will glow.

To develop this project further, you can easily connect a relay with a lock connected to it (see the schematic below).

Watch the video!

Also, check out this tutorial: Arduino Nano Matrix Keypad With Visuino

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

What You Will Need photo 9

The Circuit

  • Connect Keypad pin 1 to Arduino digital pin 2

  • Connect Keypad pin 2 to Arduino digital pin 3

  • Connect Keypad pin 3 to Arduino digital pin 4

  • Connect Keypad pin 4 to Arduino digital pin 5

  • Connect Keypad pin 5 to Arduino digital pin 6

  • Connect Keypad pin 6 to Arduino digital pin 7

  • Connect Keypad pin 7 to Arduino digital pin 8

  • Connect Keypad pin 8 to Arduino digital pin 9

  • Connect Arduino pin [GND] to breadboard pin GND Line

  • Connect Arduino digital pin [11] to the breadboard Resistor1

  • Connect Arduino digital pin [12] to the breadboard Resistor2

  • Connect Resistor1 to the green LED's positive pin [+]

  • Connect the Green LED negative pin [-] to the breadboard pin GND Line

  • Connect Resistor2 to Red LED positive pin [+]

  • Connect the red LED negative pin [-] to the breadboard pin GND Line

To add a relay and a solenoid:

  • Connect Relay VCC pin(+) to Arduino 5V pin

  • Connect Relay GND pin(-) to Arduino GND pin or to breadboard pin GND Line

  • Connect Relay signal pin(S) to Arduino Digital pin 11

  • Connect power supply 12V (+) to solenoid red wire(+)

  • Connect power supply 12V (-) to solenoid pin(com)

  • Connect solenoid black wire (-) to relay pin(NO)

The Circuit

The Circuit photo 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, Add Components

  • Add "Keypad" component

  • Add "Char Multi Source" component

  • Add "Char To Text" component

  • Add "Compare Text Value" component

  • Add "Toggle(T) Flip-Flop" component

  • Add 2X "Delay" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Add Components photo 5

In Visuino Set Components

  • Double-click on "Keypad1" and in the "Keys" window, drag "Character Key Group" to the left side. In the properties window, select "Keys" and click on the 3-dot button. Now, in a "Keys" window, drag 16X "Char Key" to the Left side, and for each key set "Character" in the properties window, set "Character" for each in the order as you see in picture 6, for

  • "Char Key1" the "Character" will be 1

  • for "Char Key2" the "Character" will be 4

  • for "Char Key3" the "Character" will be 7

  • for "Char Key4" the "Character" will be *

  • for "Char Key5" the "Character" will be 2

  • and so on until the end

  • Close All the Windows

  • Select "Delay1" and in the properties window, set "Interval (uS)" to 5000000

  • Select "Delay2" and in the properties window, set "Interval (uS)" to 5000000

  • Select "CharToText1" and in the properties window, set "Update On Each Char" to True

To Set the Keypad Code: Select "CompareValue1" and in the properties window set the "Value"; in this example, it is 34571

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Set Components photo 5

In Visuino Set Components photo 6

In Visuino Set Components photo 7

In Visuino Set Components photo 8

In Visuino Set Components photo 9

In Visuino Connect Components

  • Connect Arduino Digital Pin[6] to "Keypad1" > Rows Pin [0]

  • Connect Arduino Digital Pin[7] to "Keypad1" > Rows Pin [1]

  • Connect Arduino Digital Pin[8] to "Keypad1" > Rows Pin [2]

  • Connect Arduino Digital Pin[9] to "Keypad1" > Rows Pin [3]

  • Connect "Keypad1" > Columns Pin [0] to Arduino Digital Pin[2]

  • Connect "Keypad1" > Columns Pin [1] to Arduino Digital Pin[3]

  • Connect "Keypad1" > Columns Pin [2] to Arduino Digital Pin[4]

  • Connect "Keypad1" > Columns Pin [3] to Arduino Digital Pin[5]

  • Connect "Keypad1" > "CharacterKeyGroup16" pin [Out] to "CharMultiSource1" pin[In]

  • Connect "CharMultiSource1" pin [0] to "CharToText1" pin [In]

  • Connect "CharMultiSource1" pin [1] to "Delay1" pin [Start]

  • Connect "Delay1" pin [Out] to "CharToText1" pin [Clear]

  • Connect "CharToText1" pin [Out] to "CompareValue1" pin [In]

  • Connect "CharToText1" pin [Out] to "Delay2" pin [Start]

  • Connect "CompareValue1" pin [Out] to "TFlipFlop1" pin[Set]

  • Connect "Delay2" pin [Out] to "TFlipFlop1" pin[Reset]

  • Connect "TFlipFlop1" pin [Out] to Arduino Digital Pin[11]

  • Connect "TFlipFlop1" pin [Inverted] to Arduino Digital Pin[12]

In Visuino Connect Components

In Visuino Connect Components photo 2

In Visuino Connect Components photo 3

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the Arduino module, the red LED will glow, and if you enter the correct code, the green LED will glow for 5 seconds. If you do not enter the right code, the entered code will reset in 5 seconds, and you can try it again.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.