Maker.io main logo

INA219 DC Current Sensor Using Visuino & Arduino

229

2025-05-20 | By Ron Cutts

License: General Public License Displays LED / Display Drivers Voltage Arduino

Download Project File

Step 1: What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

What You Will Need

image

  1. Arduino UNO or any other Arduino board

  2. Breadboard

  3. OLED Display

  4. INA219 DC Current Sensor

  5. Jumper wires

  6. Power Supply

  7. Some load, like a light bulb or DC motor

  8. Visuino software: Download here

Step 2: The Circuit

The Circuit

  1. Connect INA219 pin [SCL] to Arduino pin [SCL]

  2. Connect INA219 pin [SDA] to Arduino pin [SDA]

  3. Connect INA219 pin [VCC] to Arduino pin [5v]

  4. Connect INA219 pin [GND] to Arduino pin [GND]

  1. Connect OLED Display pin [SCL] to Arduino pin [SCL]

  2. Connect OLED Display pin [SDA] to Arduino pin [SDA]

  3. Connect OLED Display pin [VCC] to Arduino pin [5v]

  4. Connect OLED Display pin [GND] to Arduino pin [GND]

  1. Connect Power Supply (+) to INA219 pin [Vin -]

  2. Connect Light Bulb (+) to INA219 pin [Vin +]

  3. Connect Light Bulb (-) to Connect Power Supply (-)

Step 3: Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type

The Visuino: https://www.visuino.com also needs to be installed. You can download the free version or register for a free trial.

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2.


Step 4: In Visuino Add, Set & Connect Components

In Visuino Add, Set & Connect Components

In Visuino Add, Set & Connect Components

In Visuino Add, Set & Connect Components

In Visuino Add, Set & Connect Components

In Visuino Add, Set & Connect Components

imageimage

Add "INA219" component

  1. Add "OLED I2C" component

  1. Double click on the "DisplayOLED1" component and in the Elements window drag "Text Field" to the left side and in the properties window set "Size" to 2, "Width" to 10, and "Y" to 15

  2. In the Elements window, drag "Draw Text" to the left side and in the properties window set "Size" to 2, "Text" to mA, "X" to 100 and "Y" to 15

  3. Close the Elements window

  1. Connect "VoltageCurrentPower1" pin [Current mA] to "DisplayOLED1" > "Text Field1" pin [In]

  2. Connect "VoltageCurrentPower1" Control pin [I2C] to Arduino pin [I2C]

  3. Connect "DisplayOLED1" pin [I2C] to Arduino pin [I2C]

Step 5: Generate, Compile, and Upload the Arduino Code

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Step 6: Play

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created. You can download it and open it in Visuino: https://www.visuino.com

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.