Maker.io main logo

How to Use PCF8574 GPIO Extender With Arduino or ESP32

104

2026-03-31 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Arduino ESP32

If you require more pins for your project to connect more buttons, sensors, or LEDs, GPIO expanders can help. Essentially, these expanders offer additional GPIOs when your board doesn't provide enough pins.

In this tutorial, we will learn how to use the PCF8574 I2C GPIO Expander with Arduino UNO or ESP32

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

  • Arduino UNO or ESP32 (Or any other Board)

  • PCF8574 I2C GPIO Expander

  • To do the test experiment:

  • 2x 1k ohm resistor

  • LED

  • Jumper wires

  • Breadboard

  • Visuino program: Download Visuino

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

What You Will Need photo 9

The Circuit Using Arduino UNO

Connecting LED:

  • Connect PCF8574 pin [0] to a 1K ohm resistor on the breadboard

  • Connect the other side of the resistor to the LED pin [positive +]

  • Connect the LED pin [negative -] to the breadboard negative pin [Black line]

Connecting Button:

  • Connect PCF8574 pin [1] to the button on the breadboard and to the resistor.

  • Connect the other side of the resistor to the breadboard pin [GND]

  • Connect the other pin of the button to the breadboard positive pin [5V]

  • Connect Arduino pin [5V] to breadboard positive pin [Red line]

  • Connect Arduino pin [GND] to breadboard negative pin [Black line]

Connecting PCF8574:

  • Connect PCF8574 pin [VCC] to breadboard positive pin [Red line]

  • Connect PCF8574 pin [GND] to breadboard positive pin [Black line]

  • Connect PCF8574 pin [SCL] to Arduino pin [SCL]

  • Connect PCF8574 pin [SDA] to Arduino pin [SDA]

The Circuit Using Arduino UNO

The Circuit Using Arduino ESP32

Connecting LED:

  • Connect PCF8574 pin [0] to a 1K ohm resistor on the breadboard

  • Connect the other side of the resistor to the LED pin [positive +]

  • Connect the LED pin [negative -] to the breadboard negative pin [Black line]

Connecting Button:

  • Connect PCF8574 pin [1] to the button on the breadboard and to the resistor.

  • Connect the other side of the resistor to the breadboard pin [GND]

  • Connect the other pin of the button to the breadboard positive pin [5V]

  • Connect the ESP32 pin [5V] to the breadboard positive pin [Red line]

  • Connect the ESP32 pin [GND] to the breadboard negative pin [Black line]

Connecting PCF8574:

  • Connect PCF8574 pin [VCC] to breadboard positive pin [Red line]

  • Connect PCF8574 pin [GND] to breadboard positive pin [Black line]

  • Connect PCF8574 pin [SCL] to ESP32 GPIO pin [22]

  • Connect PCF8574 pin [SDA] to ESP32 GPIO pin [21]

The Circuit Using Arduino ESP32

Start Visuino, and Select the Arduino UNO or ESP32 Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2 or "ESP32 Development Board" as shown in Picture 3

Start Visuino, and Select the Arduino UNO or ESP32 Board Type

Start Visuino, and Select the Arduino UNO or ESP32 Board Type photo 2

Start Visuino, and Select the Arduino UNO or ESP32 Board Type photo 3

Experiment No.1 - in Visuino Add & Set Components

  • Add "PCF8574" component

  • Add "Pulse Generator" component

  • Select the "GPIO1" component, and in the properties window, set the I2C "Address". My module I2C address was 32. You can check the pins on the module and compare them to the table, as shown in Picture 4, or check Step 7.

  • Connect "PulseGenerator1" pin [Out] to "GPIO1" pin Channel 0 [In]

  • Connect "GPIO1" pin I2C [Out] to the Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Experiment No.1 - in Visuino Add & Set Components

Experiment No.1 - in Visuino Add & Set Components photo 2

Experiment No.1 - in Visuino Add & Set Components photo 3

Experiment No.1 - in Visuino Add & Set Components photo 4

Experiment No.1 - in Visuino Add & Set Components photo 5

Experiment No.1 - in Visuino Add & Set Components photo 6

Experiment No.1 - in Visuino Add & Set Components photo 7

How to Find the I2C Address of the Module With Visuino

Make sure that the module is connected to the board correctly (pins VCC, GND, SCL, SDA)

  • In Visuino, select the board and in the properties window expand "I2C Channels" > "I2C" > "Elements" and click on the 3 dots button

  • In the "Elements" window, drag "I2C Scan" to the Left side

  • Close the "Elements" window

  • Add "Start" component

  • Connect "Start1" component to the board pin [Scan]

  • Connect board pin [Address] to the board Serial pin 0 [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

  • Select the "Serial" tab, click the "Connect" button, and you should see the I2C Address of your module

How to Find the I2C Address of the Module With Visuino

How to Find the I2C Address of the Module With Visuino photo 2

How to Find the I2C Address of the Module With Visuino photo 3

How to Find the I2C Address of the Module With Visuino photo 4

How to Find the I2C Address of the Module With Visuino photo 5

How to Find the I2C Address of the Module With Visuino photo 6

Experiment No.2 - in Visuino Add & Set Components

  • Add "Debounce Button" component

  • Add "Toggle Flip Flop" component

  • Connect "GPIO1" pin Channel 2 [Out] to "Button1" pin [In]

  • Connect "Button1" pin [Out] to "TFlipFlop1" pin [Clock]

  • Connect "TFlipFlop1" pin [Out] to "GPIO1" pin Channel 1 [In]

  • Connect "GPIO1" pin I2C [Out] to the Board pin I2C [In]

  • Upload the Project to the board; see the "Generate, Compile, and Upload the Arduino Code" Step on how to upload the project

Experiment No.2 - in Visuino Add & Set Components

Experiment No.2 - in Visuino Add & Set Components photo 2

Experiment No.2 - in Visuino Add & Set Components photo 3

Experiment No.2 - in Visuino Add & Set Components photo 4

Experiment No.2 - in Visuino Add & Set Components photo 5

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Note: If you are using an ESP32 dev board, then hold the "BOOT" when uploading the project

Generate, Compile, and Upload the Arduino Code

Play

If you power the board in Experiment No. 1, the LED will blink, and in Experiment No.2, the LED will turn on or off if you press the button.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

Downloads

制造商零件编号 A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.