Maker.io main logo

Getting Started with Rainbow HAT

17

2021-10-21 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

This tutorial will show you how to install the Rainbow HAT Python library, and then walk through its functionality.

Installing the Software

We always recommend using the most up-to-date version of Raspbian, as this is what we test our boards and software against, and it often helps to start with a completely fresh install of Raspbian, although this isn't necessary.

As with most of our boards, we've created a really quick and easy one-line-installer to get your Rainbow HAT set up. We'd suggest that you use this method to install the Rainbow HAT software.

Open a new terminal, and type the following, making sure to type 'y' or 'n' when prompted:

Copy Code
curl https://get.pimoroni.com/rainbowhat | bash

Once that's done, it probably a good idea to reboot your Pi to let the changes propagate.

Using the Software

Open a new terminal and type python to open a new Python prompt.

To import the Rainbow HAT library, type the following in your Python prompt that you just opened:

Copy Code
import rainbowhat as rh

Notice that we said as rh. That just saves us from typing rainbowhat every time we want to use something from the library.

The Rainbow

Rainbow HAT's rainbow is a single sweep of 7 APA102 RGB LED pixels that can be controlled individually through the Rainbow HAT Python library. As is the convention in Python, the seven pixels are numbered from 0 to 6, and arranged from right to left (pixel 0 is the rightmost, pixel 6 is the leftmost).

There are two methods that we can use to control the rainbow pixels - set_pixel and set_all - the former allows per-pixel control of colour, and the latter sets all of the pixels to the same colour.

We'll begin by lighting the first pixel red. The set_pixel function needs to be passed four pieces of information - the pixel number, and a red, green, and blue brightness value (from 0 to 255). Once pixel values have been set, you have call the show function to update the pixels and show the colours that you've set.

Type the following:

Copy Code
rh.rainbow.set_pixel(0, 255, 0, 0)
rh.rainbow.show()

The rightmost pixel should just have lit red. Notice that we typed rh.rainbow.set_pixel(0, 255, 0, 0). All of the functions related to the Rainbow are collected together into a module called rainbow, hence why we had to type rh.rainbow before the name of the function we wanted to use.

rainbow_1

Now, let's get a little more advanced and try making our red pixel scan across from right to left. We'll use a while loop and a for loop to do this.

Type the following, pressing control-c to break out:

Copy Code
import time

while True:
for pixel in range(7):
rh.rainbow.clear()
rh.rainbow.set_pixel(pixel, 255, 0, 0)
rh.rainbow.show()
time.sleep(0.1)

The red pixel should now be scanning across from right to left.

We introduced a couple of new functions here - time.sleep(0.1) and rh.rainbow.clear(). The time.sleep(0.1) allows us to introduce a small pause of 0.1 seconds between lighting each pixel and therefore to set the animation speed (decrease the number to speed it up, increase it to slow it down). The rh.rainbow.clear() clears any set pixels, and we call this function each time at the top of our for loop so that only a single pixel is lit at any one time.

Now, we'll use the set_all function to control all of the pixels at once and then make them scan through all the colours of the rainbow. Because this function controls all of the pixels we don't have to pass a pixel number in, just the RGB values.

To scan through the colours of the rainbow, we're going to use HSV colour and convert it to RGB before passing it to the set_all function. HSV colour is handy for this because the H of the HSV controls the hue of the colour and represents a position around the colour wheel. This means that we can just cycle around and transition between all of the colours of the rainbow.

Type the following, pressing control-c to break out:

Copy Code
import colorsys
import time

rh.rainbow.clear()

while True:
for i in range(101):
h = i / 100.0
r, g, b = [int(c * 255) for c in colorsys.hsv_to_rgb(h, 1.0, 1.0)]
rh.rainbow.set_all(r, g, b)
rh.rainbow.show()
time.sleep(0.02)

This is pretty complex, so let's look at each step. First, we had to import the colorsys library to use its hsv_to_rgb function to convert our HSV colour to RGB.

Again, we're using a while True loop that will run continuously and then a for loop inside that. The for loop is what will cycle through the hues in the colour wheel. Conveniently, 0 and 1 are both at the same position on the wheel, so we just have to go from 0 up to 1 then start again at 0. We're just using a range of numbers from 0 to 100 and dividing them by 100 to get 101 values between 0 and 1 (where it says h = i / 100.0).

The line that says r, g, b = [int(c * 255) for c in colorsys.hsv_to_rgb(h, 1.0, 1.0)] converts our HSV colours to RGB. Because the hsv_to_rgb function both accepts and returns colour values between 0 and 1, and we need numbers between 0 and 255, we're using a list comprehension to multiply the RGB values we get back by 255 and also convert them back into integers (where it says int(c * 255)). List comprehensions are really handy ways to run the same operation on several things at once and take the form [function(x) for x in y]. They return a list. We're also using list unpacking (r, g, b =) to assign the resulting list of three values straight to three variables r, g, and b.

Finally, we're just using set_all to set the RGB values on all of the pixels, and the show function to update the pixels and show the colour, with a small delay of 0.02 seconds so that the rainbow cycles once every two seconds (since we have about 100 values).

set_2

The 14-segment Displays

Because we've used 14-segment displays on Rainbow HAT rather than the more commonly-used 7-segment displays, we can display both numbers and upper and/or lower-case text on them. There's also four decimal points that come in handy when displaying floating point numbers.

All of the display functions are collected together into the display module, and be accessed under rh.display. The two functions we'll be looking at here are print_str and print_float, which print strings and floating-point numbers respectively, as you may have guessed!

We're going to print the string AHOY to the displays. Similar to the rainbow pixels, the displays have a show method, so after you've used print_str you also have call show to update the displays with your string.

Type the following:

Copy Code
rh.display.print_str('AHOY')
rh.display.show()

print_3

As well as being able to display text and numbers, there's support for most of the commonly-used special characters like @ and such.

Now, we'll use the print_float function to display some floating-point numbers, inside a while loop that adds 0.01 each time, in effect creating a counter.

Type the following, pressing control-c to break out:

Copy Code
i = 0.0

while i < 999.9:
rh.display.clear()
rh.display.print_float(i)
rh.display.show()
i += 0.01

This starts at 0.0, clears the display, then uses the print_float method and show to display the current value of i, and finally increments i by 0.01.

You can also control the four decimal points, which is especially handy if you want to do something like make a clock. The set_decimal function takes two arguments - the position of the decimal point you want to toggle on, and a True or False value depending on whether you want to turn it on or off. The decimal points are numbered 0-3 from left to right.

Type the following to toggle on the first decimal point

Copy Code
rh.display.clear()
rh.display.set_decimal(0, True)
rh.display.show()

Touch Pads and LEDs

Rainbow HAT has three capacitive touch pads, marked A, B, and C, each with a coloured LED above. The touch pads can be used with decorator functions to link a touch and/or release event to a function. Decorators in Python are added directly before your function definition, allowing the function to be called automatically when the decorator is triggered, and can pass data into the function as well.

The LEDs associated with the touch pads can be controlled independently. Here, we'll link the LED above touch pad A to the touch pad, so that when the touch pad is pressed the LED lights up.

Type the following:

Copy Code
@rh.touch.A.press()
def touch_a(channel):
print('Button A pressed')
rh.lights.rgb(1, 0, 0)

@rh.touch.A.release()
def release_a(channel):
print('Button A released')
rh.lights.rgb(0, 0, 0)

You'll see that the touch pads - A, B, and C - are referred to in the decorator line as @rh.touch.A, @rh.touch.B, and @rh.touch.C, and that they have both press() and release() methods. Our two functions - touch_a and release_a are triggered by the generator when the pad is touched or released, and we light the LED with rh.lights.rgb(1, 0, 0).

touch_4

To control the LEDs above the pads, you pass either a 1 (to switch on) or a 0 (to switch off) to the rh.lights.rgb function. The three numbers passed correspond to each of the three LEDs in turn, meaning that you can toggle several on or off at the same time.

Type the following to turn all three LEDs on:

Copy Code
rh.lights.rgb(1, 1, 1)

And type the following to switch them off again:

Copy Code
rh.lights.rgb(0, 0, 0)

Temperature and Pressure

The BMP280 sensor on Rainbow HAT measures both temperature and pressure. It's really simple to read the current temperature and pressure. Both are under the rh.weather module, so temperature can be read with rh.weather.temperature() and pressure with rh.weather.pressure().

Type the following, pressing control-c to break out:

Copy Code
while True:
t = rh.weather.temperature()
p = rh.weather.pressure()
print(t, p)
time.sleep(0.5)

That should print the temperature in degrees Celsius and the pressure in Pascals (divide by 100 to get the more commonly-used hectoPascals) every half second.

You could easily modify that code to display the temperature on the 14-segment displays, using the print_float method, as follows:

Copy Code
while True:
t = rh.weather.temperature()
rh.display.clear()
rh.display.print_float(t)
rh.display.show()
time.sleep(0.5)

code_5

Piezo Buzzer

The piezo buzzer allows you to play notes of specific frequencies, or midi note numbers. Let's begin by playing a note of a specific frequency, middle C which has a frequency of 261Hz. The buzzer methods are under the buzzer module, rh.buzzer, and the note method takes a frequency in Hz and a note length in seconds.

Type the following:

Copy Code
rh.buzzer.note(261, 1)

That should play middle C for 1 second. Next, we'll do that same but with the midi_note function that allows you to use midi note numbers. Middle C is midi note 60, so we'll play that now.

Type the following:

Copy Code
rh.buzzer.midi_note(60, 1)

To play a tune, you could make a list of the notes, and then loop through them, with a short pause after each one.

Type the following:

Copy Code
song = [68, 68, 68, 69, 70, 70, 69, 70, 71, 72]

for note in song:
rh.buzzer.midi_note(note, 0.5)
time.sleep(1)

It's worth noting that if you want a half second note and then a half second pause, you'll add your note length to the length of your pause, e.g. 0.5 + 0.5 = 1 in the example above.

Also, the notes we've used are all of the same length and ideally, you'd want to vary the note length to make the tune sound correct.

Did you guess what song that was?

Project Ideas

The variety of different inputs and outputs on Rainbow HAT makes it ideal for all sorts of projects, combining the inputs and outputs in interesting ways and applying what you've learned above.

Here are some ideas we've had:

Weather Station

Use the temperature and pressure sensor and display the values on the 14-segment displays. You could even use the rainbow LEDs to display a bar chart of the temperature or pressure with the colour indicating cold or warm temperatures, or low or high pressure. Why not make it internet-connected and tweet the values, or log the values to a Google Sheet?

Tiny, Three-Note Piano

There are plenty of tunes you can play with three notes! Here’s one to get you started - Mary Had a Little Lamb. The piezo buzzer uses PWM (pulse width modulation) to generate different frequencies of sound, and it’s easy to map these frequencies to notes. You could even use chording to get up to eight notes!

Reaction Time Game

Use the buttons to make a reaction time game for up to three players. Press a button to start, and when the rainbow lights change from red to green the first player to hit their button is the winner. Display the winning time on the 14-segment displays.

Stopwatch or Countdown Timer

Use the buttons as controls for starting or stopping a stopwatch and display the time on the 14-segment displays. You could use the rainbow LEDs to display the seconds ticking. Or use the buttons to set the seconds and minutes on a countdown timer, displaying the countdown on the displays, and then buzz the buzzer when the time is up!

Mood Light

Set your mood with the rainbow LEDs, using the 3 buttons to select and adjust each colour channel, fade through the hue, or switch between lighting effects.

制造商零件编号 PIM242
RAINBOW HAT FOR ANDROID THINGS
Pimoroni Ltd
制造商零件编号 SC0193(11)
SBC 1.5GHZ 4 CORE 2GB PI 4 MOD B
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.