Maker.io main logo

Getting Started with PicoSystem and C++

16

2022-04-12 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

This guide will show you how to get started programming your PicoSystem ‎using our PicoSystem C++ API. PicoSystem is a pocket-sized handheld ‎games console, built around Raspberry Pi's RP2040 chip (that's the little fella ‎that's the core of a Raspberry Pi Pico).‎

The PicoSystem C++ API is intentionally designed to be lightweight and get ‎out of your way when you're developing games for PicoSystem. It has around ‎‎40 functions to provide access to the hardware and help with drawing, audio, ‎and user input. It's separate from the rest of our Pico drivers/libraries, to keep ‎it super slimline.‎

Once you're familiar with the process of building your project for PicoSystem ‎you may find our PicoSystem API Cheatsheet a useful reference to keep ‎handy.‎

Before We Start

First of all, we need to install the Pico SDK from Raspberry Pi. This provides ‎all of the useful bits and pieces needed to make the most of the RP2040 ‎processor.‎

We've found that setting up the Pico build chain is most straightforward on a ‎Raspberry Pi or other Linux computer. The instructions below assume you're ‎using a Raspberry Pi running Raspberry Pi OS, but if your setup is Linux based ‎the process should be very similar. For more detailed instructions and how to ‎build Pico/RP2040 projects using other platforms we'd suggest taking a look ‎at the Raspberry Pi Getting Started Guide (or, for more technical info, the ‎C/C++ SDK docs).‎

If you're building on a Pi, we'd recommend using a fresh image of Raspberry ‎Pi OS and doing a sudo apt update before starting to make sure your package ‎lists are up to date.

‎‎1.‎ Install the build tools:‎

‎sudo apt install cmake gcc-arm-none-eabi libnewlib-arm-none-eabi libstdc++-arm-none-eabi-newlib

2.‎ Download the Pico SDK:

‎‎git clone https://github.com/raspberrypi/pico-sdk.git ~/pico-sdk

3.‎ Set the PICO_SDK_PATH environment variable on your system:

echo 'export PICO_SDK_PATH="~/pico-sdk"' >> ~/.bashrc

‎‎4.‎ Log out, log in (or sudo reboot your Pi) and you're done!‎

Installing the PicoSystem SDK

Now we have everything ready we can download the PicoSystem SDK and ‎build the example projects to prove that everything is working.

‎‎1.‎ Download our PicoSystem SDK:

‎‎git clone https://github.com/pimoroni/picosystem.git ~/picosystem

‎2.‎ Create a build folder:‎‎

mkdir ~/picosystem/build‎

3.‎ Build the examples (if you're using a Pi 4, you can make -j4 to use all the ‎cores and make things go a little faster).

‎‎cd ~/picosystem/build

‎‎cmake ..‎‎

make‎

4.‎ You will now have the example projects built in ~/picosystem/build/examples. ‎You can copy the .uf2 files in this directory directly to your PicoSystem ‎while it is in DFU (Device Firmware Update) mode.‎

BOOTING PICOSYSTEM INTO DFU MODE

If it's not plugged in already, connect your PicoSystem to your computer. Hold ‎down the X action button and toggle the power. PicoSystem will boot into ‎DFU mode and appear as a disk on your computer, called RPI-RP2.‎

If you're using a GUI, you should be able to drag a .uf2 file onto the ‎PicoSystem disk and it will be uploaded and launch immediately.‎

If you're using a Raspberry Pi and are logged in via SSH you might find that ‎your PicoSystem doesn't mount as a drive automatically - section 3.2.2 of ‎the Getting Started guide will show you how to mount it manually.‎

Creating your first PicoSystem project

Examples are all well and good but the real fun starts with creating our own ‎games and demos.‎

We've created a boilerplate template to make setting up a new C++ project ‎super simple.‎

Download the boilerplate into a new directory, to keep things tidy:‎

Copy Code
git clone https://github.com/pimoroni/picosystem-boilerplate.git ~/ourproject
cd ~/ourproject

‎(we're calling our directory ourproject but call yours what you will!).‎

This new project directory will contain a few different files, but the ones you'll ‎be primarily concerned with are:‎

  • CMakeLists.txt contains instructions to the compiler and linker about how ‎to build the project. You will need to change the options in here if you ‎want to change the project name or set high level options like ‎resolution or turning the splash screen on or off. By default, PicoSystem ‎will build the project in pixel_double mode, which gives us a resolution of ‎‎120x120 pixels and will mean we get lovely retro-vibe graphics.‎
  • main.cpp contains the source code for our project - this is where your ‎game code will go and where the magic will happen!

Open up main.cpp in an editor (on a Pi, you can nano main.cpp) and add some ‎simple code to draw on the screen.‎

Copy Code
#include "picosystem.hpp"

using namespace picosystem;

void init() {
}

void update(uint32_t tick) {
}

void draw(uint32_t tick) {
pen(0, 0, 0);
clear();

pen(15, 15, 15);
text("Hello, world!", 0, 0);
}

Then, as we did with the examples, create a build directory for the compiler to ‎output into and tell it to build our project.‎

Copy Code
mkdir ~/ourproject/build
cd ~/ourproject/build
cmake ..
make

Once completed there will be a .uf2 file in your build directory (by default it's ‎called my_project.uf2). Put your PicoSystem into DFU mode and copy it over.

‎That's all folks!‎

制造商零件编号 PIM559
PICOSYSTEM
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.