Maker.io main logo

Create a Simple Gaming System with the Atmel SAM4S Xplained Pro

62

2017-05-19 | By All About Circuits

License: See Original Project

Courtesy of All About Circuits

This article provides teaches some code development, hardware configuration, and the OLED interface for SAM4S Xplained Pro.

 

Required Hardware/Software

Supporting Information

A (Very) Simple Display Driver

Let's take what we've learned about using the SAM4S Xplained Pro to develop a primitive video game, consisting of a moving square target and a laser beam that fires when you press pushbutton 2. If your laser beam hits the target, you win. If your laser beam misses the target, you keep shooting until you win.

The first thing we'll need is a simple display driver for our simple video game. This gives us a convenient way to set and clear pixels anywhere within our OLED screen. We want to maintain memory in our microcontroller corresponding to the current state of the screen. This will allow us to check the pixels' state without reading data from the OLED controller. This is especially important for our hardware configuration because we’re talking to the OLED module via SPI, and the OLED controller’s SPI interface (unlike its parallel interface) does not support read operations.

Pages and Columns

We first need to understand how the OLED pixels are arranged. Take a look at the following diagrams from the SSD1306 datasheet.

Pages and Columns

Pages and Columns

What we have here are 8 "pages" of vertical pixels and 128 columns of horizontal pixels. Each page consists of 8 vertical pixels, making the total resolution 64 vertical pixels by 128 horizontal pixels. However, the display's physical size is only 32 vertical pixels by 128 horizontal pixels. So, the OLED controller has enough pixel memory for 8 vertical pages, but can only display 4 pages at one time.

We can modify the OLED display by writing a byte via SPI. This controls the 8 vertical pixels corresponding to the page and column address that are currently chosen. The second diagram shows the relationship between the pixels in a page and the bits within a written byte - the least significant bit in the byte corresponds to the highest pixel in the page, and the most significant bit corresponds to the lowest pixel.

Individual Pixels vs. All the Pixels

It’s possible to modify only one column of one page; you can do this by setting the column and page address and then writing a single data byte. The ASF functions for this are ssd1306_set_page_address() and ssd1306_set_column_address(), followed by ssd1306_write_data(). I prefer to modify pixels in a display buffer before updating the entire screen. It may seem rather inefficient, but it’s actually not too bad because the OLED’s SPI interface supports fairly high clock rates. The scope trace below shows the SPI clock signal, which is configured to run at 5 MHz (the maximum supported by the OLED controller is 10 MHz).

Individual Pixels vs. All the Pixels

So it only takes 1.6 µs to write one byte. You’d think that we could update the entire screen in about (1.6 µs) × (128 columns) × (4 pages) ≈ 0.8 ms, but it actually takes much longer because there’s about 10 µs of dead time between successive bytes. This dead time is incorporated intentionally into the ssd1306_write_data() function to accommodate the SSD1306's latency. A comment in the function indicates that the dead time can be as low as 3 µs, so I’m not sure why Atmel chose 10 µs. You can try to reduce the delay in ssd1306_write_data() if you want to speed things up. With the current delay it should take about (11.6 µs) × (128 columns) × (4 pages) ≈ 5.9 ms to update the entire screen, and the scope reading confirms that this is the case:

Individual Pixels vs. All the Pixels

We can see that the amount of time needed to update the entire screen isn't excessive by any means, especially when you consider that even at 30 frames per second, we’d have 33 ms between screen updates.

Driver Code

I use the following two-dimensional array as the display buffer:

Copy Code
                  //Preprocessor definitions
#define OLED_HEIGHT_BYTES 32/8
#define OLED_WIDTH_PIXELS 128

//Global variables
unsigned char OLED_Pixels[OLED_HEIGHT_BYTES][OLED_WIDTH_PIXELS];

These two functions modify a single pixel in the display buffer:

Copy Code
                  /*This function sets one OLED pixel identified by the Row and Column parameters.
Keep in mind that the OLED array rows are addressed as bytes (of 8 pixels), whereas
the Row parameter passed to this function is a pixel address.*/
static inline void Set_OLED_Pixel(unsigned char Row, unsigned char Column)
{
if (Row < 8)
{
OLED_Pixels[0][Column] |= (0x01 << Row);
}

else if (Row < 16)
{
OLED_Pixels[1][Column] |= (0x01 << (Row - 8));
}

else if (Row < 24)
{
OLED_Pixels[2][Column] |= (0x01 << (Row - 16));
}

else if (Row < 32)
{
OLED_Pixels[3][Column] |= (0x01 << (Row - 24));
}
}

/*This function clears one OLED pixel identified by the Row and Column parameters.
Keep in mind that the OLED array rows are addressed as bytes (of 8 pixels), whereas
the Row parameter passed to this function is a pixel address.*/
static inline void Clear_OLED_Pixel(unsigned char Row, unsigned char Column)
{
if (Row < 8)
{
OLED_Pixels[0][Column] &= ~(0x01 << Row);
}

else if (Row < 16)
{
OLED_Pixels[1][Column] &= ~(0x01 << (Row - 8));
}

else if (Row < 24)
{
OLED_Pixels[2][Column] &= ~(0x01 << (Row - 16));
}

else if (Row < 32)
{
OLED_Pixels[3][Column] &= ~(0x01 << (Row - 24));
}
}

I declared these as "inline" functions so they will execute more quickly.

Here's the function I used to clear all the pixels in the display buffer:

Copy Code
                  static void Clear_OLED_Array(void)
{
unsigned char x, y;

for (x = 0; x < OLED_HEIGHT_BYTES; x++)
{
for (y = 0; y < OLED_WIDTH_PIXELS; y++)
{
OLED_Pixels[x][y] = 0;
}
}
}

These three functions don't actually update the OLED screen; they merely modify the buffer. The screen updates by copying the display buffer's contents to the OLED controller's memory:

Copy Code
                  static void Update_OLED_Display(void)
{
unsigned char Row, Column;

ssd1306_set_page_address(0);
ssd1306_set_column_address(0);

for (Row = 0; Row < OLED_HEIGHT_BYTES; Row++)
{
for (Column = 0; Column < OLED_WIDTH_PIXELS; Column++)
{
ssd1306_write_data(OLED_Pixels[Row][Column]);
}
}
}

This function writes all the bytes from the display buffer to the OLED controller via SPI, according to the pattern below. These bytes are written one after another, with no intervening memory-address information. So, we need to make sure that our OLED controller interprets this data correctly. To accomplish this, we configure it for "horizontal addressing mode":

horizontal addressing mode

When the OLED controller operates in this mode, it will automatically update its address pointer in a way consistent with how we are sending out the contents of the display buffer.

A Moving Target

The target is a 4 by 4 pixel square that repeatedly moves from left to right, as follows:

 

There's a delay of 30 ms between the one-pixel-to-the-right target movements. The scope capture below shows the data packets transmitted to the OLED controller; as we saw earlier, the packets (The data bytes for updating the entire screen) are about 6 ms wide, and now we have 30 ms between packets.

A Moving Target

The code excerpt below gives you the entire main() function. The moving-target functionality is in the infinite while loop. Refer to the comments in the code for important details.

Copy Code
int main (void)
{
//clock configuration and initialization
sysclk_init();

/*Disable the watchdog timer and configure/initialize
port pins connected to various components incorporated
into the SAM4S Xplained development platform, e.g., the
NAND flash, the OLED interface, the LEDs, the SW0 pushbutton.*/
board_init();

//initialize SPI and the OLED controller
ssd1306_init();

/*These two statements configure the OLED module for
"horizontal addressing mode."*/
ssd1306_write_command(SSD1306_CMD_SET_MEMORY_ADDRESSING_MODE);
ssd1306_write_command(0x00);

Configure_Pushbutton2();

/*This function clears all the pixels in the array; it does not
update the OLED display.*/
Clear_OLED_Array();

Update_OLED_Display();

/*These variables hold the row and column address
corresponding to the top-left pixel of the
4-pixel-by-4-pixel square target. The row address
is set to 14 because we want the target to be in the
middle of the display, and the column address is set
to 0 so that the target starts from the left-hand
edge of the screen.*/
TargetRow = 14;
TargetColumn = 0;

while (1)
{
//form the 4-pixel-by-4-pixel square target
Set_OLED_Pixel(TargetRow, TargetColumn);
Set_OLED_Pixel(TargetRow, TargetColumn+1);
Set_OLED_Pixel(TargetRow, TargetColumn+2);
Set_OLED_Pixel(TargetRow, TargetColumn+3);
Set_OLED_Pixel(TargetRow+1, TargetColumn);
Set_OLED_Pixel(TargetRow+1, TargetColumn+1);
Set_OLED_Pixel(TargetRow+1, TargetColumn+2);
Set_OLED_Pixel(TargetRow+1, TargetColumn+3);
Set_OLED_Pixel(TargetRow+2, TargetColumn);
Set_OLED_Pixel(TargetRow+2, TargetColumn+1);
Set_OLED_Pixel(TargetRow+2, TargetColumn+2);
Set_OLED_Pixel(TargetRow+2, TargetColumn+3);
Set_OLED_Pixel(TargetRow+3, TargetColumn);
Set_OLED_Pixel(TargetRow+3, TargetColumn+1);
Set_OLED_Pixel(TargetRow+3, TargetColumn+2);
Set_OLED_Pixel(TargetRow+3, TargetColumn+3);

Update_OLED_Display();

delay_ms(30);

//clear the previous target
Clear_OLED_Pixel(TargetRow, TargetColumn);
Clear_OLED_Pixel(TargetRow, TargetColumn+1);
Clear_OLED_Pixel(TargetRow, TargetColumn+2);
Clear_OLED_Pixel(TargetRow, TargetColumn+3);
Clear_OLED_Pixel(TargetRow+1, TargetColumn);
Clear_OLED_Pixel(TargetRow+1, TargetColumn+1);
Clear_OLED_Pixel(TargetRow+1, TargetColumn+2);
Clear_OLED_Pixel(TargetRow+1, TargetColumn+3);
Clear_OLED_Pixel(TargetRow+2, TargetColumn);
Clear_OLED_Pixel(TargetRow+2, TargetColumn+1);
Clear_OLED_Pixel(TargetRow+2, TargetColumn+2);
Clear_OLED_Pixel(TargetRow+2, TargetColumn+3);
Clear_OLED_Pixel(TargetRow+3, TargetColumn);
Clear_OLED_Pixel(TargetRow+3, TargetColumn+1);
Clear_OLED_Pixel(TargetRow+3, TargetColumn+2);
Clear_OLED_Pixel(TargetRow+3, TargetColumn+3);

/*Move the target one pixel to the right. If the
right edge of the target has reached the last
display column, return the target to the left-hand
edge of the screen.*/
TargetColumn++;
if ( (TargetColumn+3) == OLED_WIDTH_PIXELS)
{
TargetColumn = 0;
}
}
}

Firing the Laser

You can fire the laser by pressing pushbutton 2. The pushbutton functionality is interrupt-driven, so we need to enable the port pin connected to pushbutton 2 and configure its interrupt

Copy Code
static void Configure_Pushbutton2(void)
{
/*Enable the clock for PIOC, which is one of the parallel
input/output controllers. The pushbutton 2 signal is connected
to a pin included in PIOC.*/
pmc_enable_periph_clk(ID_PIOC);

/*Configure the integrated debounce functionality for the pin
connected to pushbutton 2.*/
pio_set_debounce_filter(PIOC, PIN_PUSHBUTTON_2_MASK, 10);

/*This assigns an interrupt handler function for the pushbutton 2
interrupt. The third parameter consists of attributes used in the
process of configuring the interrupt. In this case the attributes
parameter indicates that the pin's internal pull-up is active, that
the pin's debounce filter is active, and that the interrupt fires on
the falling edge.*/
pio_handler_set(PIOC, ID_PIOC, PIN_PUSHBUTTON_2_MASK, PIN_PUSHBUTTON_2_ATTR, PushButton2_InterruptHandler);

//enable PIOC interrupts in the NVIC (nested vectored interrupt controller)
NVIC_EnableIRQ((IRQn_Type) ID_PIOC);

//15 is the lowest priority, 0 is the highest priority
pio_handler_set_priority(PIOC, (IRQn_Type) ID_PIOC, 0);

/*Enable the pushbutton 2 interrupt source. Note that it is necessary
to both "enable the interrupt" and "enable the interrupt in the NVIC."*/
pio_enable_interrupt(PIOC, PIN_PUSHBUTTON_2_MASK);
}

The laser is shown as a vertical line that extends upward from the bottom-center of the screen (i.e., row = 31, column = 63). If your laser hits the target, the program will generate the "debris effect," i.e., the square will disappear and be replaced by four pixels expanding outward (one from each corner of the square). This explosion doesn't satisfy conservation of mass, since the original target had a total of 16 pixels; so we’ll just assume that the other 12 pixels were vaporized into invisibly small particles.

Below is the pushbutton 2 interrupt handler, which includes all the functionality for the laser. The comments are essentially a continuation of the information in the article itself, so don't forget about them.

Copy Code
static void PushButton2_InterruptHandler(uint32_t id, uint32_t mask)
{
/*Confirm that the source of the interrupt is pushbutton 2. This seems
unnecessary to me, but it is included in Atmel's example code.*/
if ((id == ID_PIOC) && (mask == PIN_PUSHBUTTON_2_MASK))
{
/*Disable the pushbutton 2 interrupt to prevent spurious
interrupts caused by switch bounce. I probed the pushbutton
signal, and it looks like the spurious transitions occur at the end
of the signal's active-low state, so disabling the interrupt as
soon as we enter the interrupt handler effectively suppresses
the spurious interrupt requests. For some reason I was not able
to completely resolve this problem by means of the pin's integrated
debounce filter.*/
pio_disable_interrupt(PIOC, PIN_PUSHBUTTON_2_MASK);

//these next 8 groups of statements create the laser beam
Set_OLED_Pixel(31, 63);
Set_OLED_Pixel(30, 63);
Set_OLED_Pixel(29, 63);
Set_OLED_Pixel(28, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(27, 63);
Set_OLED_Pixel(26, 63);
Set_OLED_Pixel(25, 63);
Set_OLED_Pixel(24, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(23, 63);
Set_OLED_Pixel(22, 63);
Set_OLED_Pixel(21, 63);
Set_OLED_Pixel(20, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(19, 63);
Set_OLED_Pixel(18, 63);
Set_OLED_Pixel(17, 63);
Set_OLED_Pixel(16, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(15, 63);
Set_OLED_Pixel(14, 63);
Set_OLED_Pixel(13, 63);
Set_OLED_Pixel(12, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(11, 63);
Set_OLED_Pixel(10, 63);
Set_OLED_Pixel(9, 63);
Set_OLED_Pixel(8, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(7, 63);
Set_OLED_Pixel(6, 63);
Set_OLED_Pixel(5, 63);
Set_OLED_Pixel(4, 63);
Update_OLED_Display();
delay_ms(10);

Set_OLED_Pixel(3, 63);
Set_OLED_Pixel(2, 63);
Set_OLED_Pixel(1, 63);
Set_OLED_Pixel(0, 63);
Update_OLED_Display();
delay_ms(10);

/*Does the target currently include the laser-beam column?
If so, clear the OLED array to remove the target and the laser,
then create the debris effect. After that, clear the OLED screen
and return the target to its starting position.*/
if (TargetColumn >= 60 && TargetColumn <= 63)
{
Clear_OLED_Array();

Set_OLED_Pixel(TargetRow-1, TargetColumn-1);
Set_OLED_Pixel(TargetRow-1, TargetColumn+4);
Set_OLED_Pixel(TargetRow+4, TargetColumn-1);
Set_OLED_Pixel(TargetRow+4, TargetColumn+4);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-1, TargetColumn-1);
Clear_OLED_Pixel(TargetRow-1, TargetColumn+4);
Clear_OLED_Pixel(TargetRow+4, TargetColumn-1);
Clear_OLED_Pixel(TargetRow+4, TargetColumn+4);

Set_OLED_Pixel(TargetRow-2, TargetColumn-2);
Set_OLED_Pixel(TargetRow-2, TargetColumn+5);
Set_OLED_Pixel(TargetRow+5, TargetColumn-2);
Set_OLED_Pixel(TargetRow+5, TargetColumn+5);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-2, TargetColumn-2);
Clear_OLED_Pixel(TargetRow-2, TargetColumn+5);
Clear_OLED_Pixel(TargetRow+5, TargetColumn-2);
Clear_OLED_Pixel(TargetRow+5, TargetColumn+5);

Set_OLED_Pixel(TargetRow-3, TargetColumn-3);
Set_OLED_Pixel(TargetRow-3, TargetColumn+6);
Set_OLED_Pixel(TargetRow+6, TargetColumn-3);
Set_OLED_Pixel(TargetRow+6, TargetColumn+6);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-3, TargetColumn-3);
Clear_OLED_Pixel(TargetRow-3, TargetColumn+6);
Clear_OLED_Pixel(TargetRow+6, TargetColumn-3);
Clear_OLED_Pixel(TargetRow+6, TargetColumn+6);

Set_OLED_Pixel(TargetRow-4, TargetColumn-4);
Set_OLED_Pixel(TargetRow-4, TargetColumn+7);
Set_OLED_Pixel(TargetRow+7, TargetColumn-4);
Set_OLED_Pixel(TargetRow+7, TargetColumn+7);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-4, TargetColumn-4);
Clear_OLED_Pixel(TargetRow-4, TargetColumn+7);
Clear_OLED_Pixel(TargetRow+7, TargetColumn-4);
Clear_OLED_Pixel(TargetRow+7, TargetColumn+7);

Set_OLED_Pixel(TargetRow-5, TargetColumn-5);
Set_OLED_Pixel(TargetRow-5, TargetColumn+8);
Set_OLED_Pixel(TargetRow+8, TargetColumn-5);
Set_OLED_Pixel(TargetRow+8, TargetColumn+8);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-5, TargetColumn-5);
Clear_OLED_Pixel(TargetRow-5, TargetColumn+8);
Clear_OLED_Pixel(TargetRow+8, TargetColumn-5);
Clear_OLED_Pixel(TargetRow+8, TargetColumn+8);

Set_OLED_Pixel(TargetRow-6, TargetColumn-6);
Set_OLED_Pixel(TargetRow-6, TargetColumn+9);
Set_OLED_Pixel(TargetRow+9, TargetColumn-6);
Set_OLED_Pixel(TargetRow+9, TargetColumn+9);
Update_OLED_Display();
delay_ms(200);

Clear_OLED_Pixel(TargetRow-6, TargetColumn-6);
Clear_OLED_Pixel(TargetRow-6, TargetColumn+9);
Clear_OLED_Pixel(TargetRow+9, TargetColumn-6);
Clear_OLED_Pixel(TargetRow+9, TargetColumn+9);

Set_OLED_Pixel(TargetRow-7, TargetColumn-7);
Set_OLED_Pixel(TargetRow-7, TargetColumn+10);
Set_OLED_Pixel(TargetRow+10, TargetColumn-7);
Set_OLED_Pixel(TargetRow+10, TargetColumn+10);
Update_OLED_Display();
delay_ms(500);

Clear_OLED_Array();
Update_OLED_Display();
delay_ms(1000);

TargetColumn = 0;
}

/*If the laser beam missed the target, clear the laser beam pixels.
Nothing else needs to be done; the target will continue moving
when execution returns to the infinite loop in main().*/
else
{
OLED_Pixels[0][63] = 0;
OLED_Pixels[1][63] = 0;
OLED_Pixels[2][63] = 0;
OLED_Pixels[3][63] = 0;
}

//reenable the pushbutton 2 interrupt
pio_enable_interrupt(PIOC, PIN_PUSHBUTTON_2_MASK);
}
}

Results

You can download all of the source and project files on All About Circuits.

And here is the code in action. Who needs to buy video games when you can make them yourself?

 

制造商零件编号 ATSAM4S-XSTK
SAM4S XPLAINED PRO ATSAM4SD32C
Microchip Technology
制造商零件编号 ATSAM4S-XPRO
SAM4S XPLAINED PRO ATSAM4SD32C
Microchip Technology
制造商零件编号 ATOLED1-XPRO
XPLAINED PRO 128X32 OLED ADD-ON
Microchip Technology
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.