Maker.io main logo

Arduino Control DC Motor Speed and Direction Using a Potentiometer & But

70

2026-04-23 | By Ron Cutts

License: GNU Lesser General Public License Motors PWM Arduino ESP32

In this tutorial, we will learn how to use a L298N DC MOTOR CONTROL driver and a potentiometer to control a DC motor speed and direction with two buttons.

Watch a demonstration video.

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

What You Will Need photo 5

What You Will Need photo 6

What You Will Need photo 7

What You Will Need photo 8

What You Will Need photo 9

The Circuit

  • Connect Arduino Pin 5V to breadboard positive pin (red line)

  • Connect Arduino Pin GND to the breadboard negative pin (blue line)

  • Connect button1 first pin to breadboard positive pin (red line)

  • Connect button1 second pin to Arduino digital pin 6

  • Connect button1 second pin to resistor1

  • Connect button2 first pin to breadboard positive pin (red line)

  • Connect button2 second pin to Arduino digital pin 7

  • Connect button2 second pin to resistor2

  • Connect resistor1 to the breadboard negative pin (blue line)

  • Connect resistor2 to the breadboard negative pin (blue line)

  • Connect digital pin(2) from Arduino to motor driver pin (IN2)

  • Connect digital pin(3) from Arduino to motor driver pin (IN1)

  • Connect the DC motor to one side of the motor driver

  • Connect the power supply (batteries) pin (gnd) to the motor driver controller pin (gnd)

  • Connect Power supply (batteries) pin (+) to motor driver controler pin (+)

  • Connect GND from the Arduino to the motor driver controller pin (gnd)

  • Connect the potentiometer pin (DTB) to the Arduino Analog pin (A0)

  • Connect the potentiometer pin (VCC) to the Arduino pin (5V)

  • Connect the potentiometer pin (GND) to the Arduino pin (GND)

The Circuit

Start Visuino, and Select the Arduino UNO Board Type

To start programming the Arduino, you will need to have the Arduino IDE installed from here: http://www.arduino.cc/.

Please be aware that there are some critical bugs in Arduino IDE 1.6.6. Make sure that you install 1.6.7 or higher; otherwise, this will not work! If you have not done so, follow the steps to set up the Arduino IDE to program the ESP8266! The Visuino: https://www.visuino.eu also needs to be installed. Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino UNO" as shown in Picture 2

Start Visuino, and Select the Arduino UNO Board Type

Start Visuino, and Select the Arduino UNO Board Type photo 2

In Visuino, add AND Connect Components

  • Add "Dual DC Motor Driver Digital and PWM Pins Bridge (L9110S, L298N)" component

  • Add "Speed and Direction To Speed" component
    In the "Properties window " set "Initial Reverse" to "True"

  • Add "SR Flip-Flop" component

  • Connect Arduino Board digital pin[6] to "SRFlipFlop1" pin[Set]

  • Connect Arduino Board digital pin[7] to "SRFlipFlop1" pin[Reset]

  • Connect Arduino Board AnalogIn pin[0] to "SpeedAndDirectionToSpeed1" pin[Speed]

  • Connect "SRFlipFlop1" pin[Out] to "SpeedAndDirectionToSpeed1" pin[Reverse]

  • Connect "SpeedAndDirectionToSpeed1" pin[Out] to "DualMotorDriver1" > Motors[0] pin [In]

  • Connect "DualMotorDriver1" > Motors[0] pin [Direction(B] to Arduino board digital pin[2]

  • Connect "DualMotorDriver1" > Motors[0] pin [Speed(A)] to Arduino board digital pin[3]

In Visuino Add AND Connect Components

In Visuino Add AND Connect Components photo 2

In Visuino Add AND Connect Components photo 3

In Visuino Add AND Connect Components photo 4

In Visuino Add AND Connect Components photo 5

In Visuino Add AND Connect Components photo 6

Generate, Compile, and Upload the Arduino Code

In Visuino, Press F9 or click on the button shown in Picture 1 to generate the Arduino code, and open the Arduino IDE

In the Arduino IDE, click on the Upload button to compile and upload the code (Picture 2)

Generate, Compile, and Upload the Arduino Code

Generate, Compile, and Upload the Arduino Code photo 2

Play

If you power the Arduino Uno module and add batteries for the motor controller, the DC motor is ready to spin.

By sliding the potentiometer, you can regulate the motor speed and change the direction by pushing the buttons.

Congratulations! You have completed your Project. Also attached is the Visuino project that I created for this. You can download it here and open it in Visuino: https://www.visuino.eu

制造商零件编号 DRI0002
EVAL BOARD FOR L298
DFRobot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.