STM32N6是ST最新一代边缘AI MCU,基于ARM全新的M55内核,带来全新的AI体验,拥有高达600Gops的计算能力。那么,59001型干簧传感器接入STM32N6,能在物理世界和AI之间,带来如何的体验呢?
STM32N6使用了M55内核,主频可达800MHz,内置4.2MB的RAM,无内部flash,可通过QSPI接口扩展外部高速NOR FLASH。N6内置Neural-ART加速器,最高工作频率1GHz。拥有ST最新的Neo-Chrom图形加速器,可带来优异的图像显示。可接入CSI接口的摄像头,能对H264进行编解码模块,带来优质的图形体验。
在IO接口方面,使用5个40p的排针,组合成IO接口,除高速接口的CSI和QSPI,均引出到IO接口上,同时还引出不同的电源引脚,方便后续的修改。同时引出STLINK的接口,引出BOOT调试接口,方便使用。
在电源方面,N6需要三路主电源,电压分别是3V3,1V8,0V8,使用GD的LDO进行滤波供电,将5V转换为对应的电压。VDDIO的电压可通过0R电阻跳线连接到3V3电源中去,方便后续不同模式的使用。
在BOOT方面,使用2.54x3p的排针,通过跳线帽的连接以选择高低电平,高低电平到引脚之前均有10K电阻进行限流。在下载电路方面,使用ST通用的1.27x20p的排针,方便接入外置的STLINK进行下载。在复位电路方面,NRST在STLINK的排针中。
在CSI电路方面,进行50R阻抗调整,等长控制,使用24p的FPC插座,为外接摄像头预留空间。在外挂FLASH上,使用NOR FALSH,因为N6没有内部FLASH,通过外挂FLASH来存储代码,使用等长控制,以便达到最佳速度和读写。在USB接口方面,使用差分对布线,进行阻抗调整,连接到排针上来。为绘制USB扩展板预留空间。
为了方便焊接,电源引脚的阻容选取0402封装的。阻容在空间允许的情况下尽量使用0603封装的。
PCB设计选用6层PCB,L2为GND平面,L3和L4为信号层,L5为电源平面,对不同电源进行了分割。PCB堆叠使用的是6层PCB,1.6的板厚。最后从下单PCB,等PCB到手后准备尝试DIY焊接。