【DigiKey好物畅享】ST STM32MP157D-DK1开发板 搭建应用程序编译环境

测试应用程序搭建环境。

一、安装需要的软件包

hui@hui-virtual-machine:~$ sudo apt-get update

hui@hui-virtual-machine:~$ sudo apt-get install gawk wget git git-lfs diffstat unzip texinfo gcc-multilib  chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libsdl1.2-dev pylint xterm bsdmainutils libusb-1.0-0 bison flex

hui@hui-virtual-machine:~$ sudo apt install libegl1-mesa

hui@hui-virtual-machine:~$ sudo apt-get install build-essential libncurses-dev libyaml-dev libssl-dev

hui@hui-virtual-machine:~$ sudo apt install python-is-python3

hui@hui-virtual-machine:~$ sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html libxml2-utils

二、安装SDK工具

2.1、下载SDK工具包

官网地址:https://www.st.com/en/embedded-software/stm32mp1dev.html

2.2、安装SDK工具包

hui@hui-virtual-machine:~/STM32MPU_workspace$ tar xvf SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz

hui@hui-virtual-machine:~/STM32MPU_workspace$ ./stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/sdk/st-image-weston-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.8-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.sh -d  /home/hui/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/SDK

图片

2.3、测试工具

hui@hui-virtual-machine:~/STM32MPU_workspace$ source STM32MPU-Ecosystem-v6.1.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

hui@hui-virtual-machine:~/STM32MPU_workspace$ $CC –version

图片

三、应用程序测试

3.1、创建文件夹

hui@hui-virtual-machine:~/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp1-openstlinux-25.06.11/sources$ mkdir gtk_hello_world_example

3.2、创建测试文件

hui@hui-virtual-machine:~/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp1-openstlinux-25.06.11/sources/gtk_hello_world_example$ vi gtk_hello_world.c

hui@hui-virtual-machine:~/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp1-openstlinux-25.06.11/sources/gtk_hello_world_example$ vi Makefile

3.2.1、gtk_hello_world.c

#include <gtk/gtk.h>



static void

print_hello (GtkWidget *widget,

             gpointer   data)

{

  g_print ("Hello World\n");

}



static void

activate (GtkApplication *app,

          gpointer        user_data)

{

  GtkWidget *window;

  GtkWidget *button;

  GtkWidget *button_box;



  window = gtk_application_window_new (app);

  gtk_window_set_title (GTK_WINDOW (window), "Window");

  gtk_window_set_default_size (GTK_WINDOW (window), 200, 200);



  button_box = gtk_button_box_new (GTK_ORIENTATION_HORIZONTAL);

  gtk_container_add (GTK_CONTAINER (window), button_box);



  button = gtk_button_new_with_label ("Hello World");

  g_signal_connect (button, "clicked", G_CALLBACK (print_hello), NULL);

  g_signal_connect_swapped (button, "clicked", G_CALLBACK (gtk_widget_destroy), window);

  gtk_container_add (GTK_CONTAINER (button_box), button);



  gtk_widget_show_all (window);

}



int

main (int    argc,

      char **argv)

{

  GtkApplication *app;

  int status;



  app = gtk_application_new ("org.gtk.example", G_APPLICATION_DEFAULT_FLAGS);

  g_signal_connect (app, "activate", G_CALLBACK (activate), NULL);

  status = g_application_run (G_APPLICATION (app), argc, argv);

  g_object_unref (app);



  return status;

}


3.2.2、Makefile

PROG = gtk_hello_world

SRCS = gtk_hello_world.c



CLEANFILES = $(PROG)



# Add / change option in CFLAGS and LDFLAGS

CFLAGS += -Wall $(shell pkg-config --cflags gtk+-3.0)

LDFLAGS += $(shell pkg-config --libs gtk+-3.0)



all: $(PROG)



$(PROG): $(SRCS)

        $(CC) -o $@ $^ $(CFLAGS) $(LDFLAGS)



clean:

        rm -f $(CLEANFILES) $(patsubst %.c,%.o, $(SRCS))

3.3、编译程序

hui@hui-virtual-machine:~/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp1-openstlinux-25.06.11/sources/gtk_hello_world_example$ make

四、程序运行

4.1、复制文件到开发板

hui@hui-virtual-machine:~/STM32MPU_workspace/STM32MPU-Ecosystem-v6.1.0/Developer-Package/stm32mp1-openstlinux-25.06.11/sources/gtk_hello_world_example$ scp gtk_hello_world root@192.168.1.5:/mnt

4.2、在开发板上运行程序

root@stm32mp1-e5-56-d3:/mnt# ./gtk_hello_world

屏幕显示