Page 1
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
XL-TrashSonar™-WR™ Series
IP67 Weather Resistant, Ultrasonic Trash Sensor
MB7137, MB7138, MB71393
Features
• Real-time auto calibration and noise
rejection
• High acoustic power output
• Precise narrow beam
• Object detection includes zero range
objects
• 3V to 5.5V supply with very low
average current draw
• Free run operation can continually
measure and output range
information
• Triggered operation provides the
range reading as desired
• All interfaces are active
simultaneously
• RS232 Serial, 0 to Vcc, 9600 Baud,
81N (MB7138, MB7139)
• I2C Bus operates up to 400KHz with
clock stretching (MB7137)
• Analog, (Vcc/1024) / cm (MB7138,
MB7139)
• Sensor operates at 42KHz
Benefits
• Acoustic and electric noise
resistance
• Reliable and stable range data
• Robust, low cost IP67 standard
sensor
• Narrow beam characteristics
• Very low power excellent for battery
based systems
• Ranging can be triggered externally
or internally
• Sensor reports the range reading
directly, frees up user processor
• Easy hole mounting or mating with
standard electrical fittings
• Filtering allows very reliable
operation in most environments
Applications & Uses
• Tank level measurement
• Bin level measurement
• Trash level measurement
• Environments with acoustic and
electrical noise
• Distance measuring
• Long range object detection
• Industrial sensor
• -40C to +65C operation1
Notes:
1Please reference page 15 for minimum operating
voltage verses temperature information.
2Minimum distance is 25cm for the MB7138 pipe
and compact only.
3 Please reference page 20 for part number key.
The XL-TrashSonar-WR sensor series provide users with robust range
information in air. These sensors also feature high-power acoustic output along
with real-time auto calibration for changing conditions (supply voltage sag,
acoustic noise, or electrical noise), operation with supply voltage from 3.0V to
5.5V, object detection from 0-cm to 350-cm, and sonar range information from
20-cm out to 350-cm with 1-cm resolution. Objects from 0-cm to 20-cm typically
range as 20-cm. (25cm for the MB7138 Pipe and Compact only2 ) The sensor is housed in a
robust PVC housing, designed to meet the IP67 water intrusion standard. This sensor line is available in the
following package types — 3/4” PVC threading, 1” NPS pipe threading, 1” BSPP pipe threading, and 30mm
1.5 pipe threading. The user interface formats included are pulse-width, analog voltage output, RS232 serial
output, and I2C (MB7137).
Close Range Operation
Applications requiring 100% reading-to-reading reliability should not use MaxSonar sensors at a distance closer than
20cm. Although most users find MaxSonar sensors to work reliably from 0 to 20cm for detecting objects in many
applications, MaxBotix™ Inc. does not guarantee operational reliability for objects closer than the minimum reported
distance. Because of ultrasonic physics, these sensors are unable to achieve 100% reliability at close distances.
25cm for the MB7138 pipe and compact only 2
_______________________________________________________________________________________________________________________________________
Warning: Personal Safety Applications
We do not recommend or endorse this product be used as a component in any personal safety applications. This product is
not designed, intended or authorized for such use. These sensors and controls do not include the self-checking redundant
circuitry needed for such use. Such unauthorized use may create a failure of the MaxBotix™ Inc. product which may result
in personal injury or death. MaxBotix™ Inc. will not be held liable for unauthorized use of this component.
www maxtmux cam
Page 2
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7137 Pinout
For I2C information please skip to page 12
Pin 1 - Temporary Default: This pin is internally pulled high. On power up, the state of this pin is checked. If the pin is
left high or disconnected the sensor will use the address stored in memory for I2C communication. If pulled low, the
sensor will use its default address for the current power cycle.
Pin 2 - Address Announce / Status: While the sensor is performing a range reading. During non-ranging operation, this
pin is held low and the sensor is listening for incoming I2C communication. Operationally, users may poll this pin to
determine if the sensor has finished its ranging cycle and is ready to report the latest range information.
During power-up this pin will provide a pulse width representation of the sensor’s current address with a length of ~100
microseconds per digit. (The default address of 224 will announce with a pulse of 22,400 microseconds in length)
Pin 3 - Not Used: This pin is not used.
Pin 4 - SDA (I2C Data): This is the data line for I2C communications. These sensors operate as I2C slave devices.
Pin 5 - SCL (I2C Clock): This is the clock line for I2C communications. These sensors support I2C clock frequencies up
to 400KHz provided clock stretching is supported by the master devices. Without clock stretching the devices can run at
speeds up to 50KHz.
V+ Operates on 3V - 5.5V. The average (and peak) current draw for 3.3V operation is 2.7mA (50mA peak) and 5V
operation is 4.4mA (100mA peak) respectively. Peak current is used during sonar pulse transmit. Please reference page 15
for minimum operating voltage verses temperature information.
GND: Return for the DC power supply. GND (& V+) must be ripple and noise free for best operation.
_______________________________________________________________________________________________________________________________________
MB7138 & MB7139 Pinout
Pin 1 - BW: Leave open (or high) for serial output on the Pin 5 output. When Pin 1 is held low the Pin 5 output sends a
pulse (instead of serial data), suitable for low noise chaining.
Pin 2 - PW: This pin outputs a pulse-width representation of range. To calculate the distance, use a scale factor of 58uS
per cm.
Pin 3 - AN: This pin outputs analog voltage with a scaling factor of (Vcc/1024) per cm. A supply of 5V yields ~4.9mV/
cm., and 3.3V yields ~3.2mV/cm. The output is buffered and corresponds to the most recent range data.
Pin 4 - RX: This pin is internally pulled high. If Pin-4 is left unconnected or held high, the sensor will continually
measure the range. If Pin-4 is held low the sensor will stop ranging. Bring high 20uS or more to command a range
reading.
Pin 5 - TX: When Pin 1 is open or held high, the Pin 5 output delivers asynchronous serial data in an RS232 format,
except the voltages are 0-Vcc. The output is an ASCII capital “R”, followed by ASCII character digits representing the
range in centimeters up to a maximum of 350, followed by a carriage return (ASCII 13). The baud rate is 9600, 8 bits, no
parity, with one stop bit. Although the voltages of 0V to Vcc are outside the RS232 standard, most RS232 devices have
sufficient margin to read the 0V to Vcc serial data. If standard voltage level RS232 is desired, invert, and connect an
RS232 converter such as a MAX232.When Pin 1 is held low, the Pin 5 output sends a single pulse, suitable for low noise
chaining (no serial data).
V+ Operates on 3V - 5.5V. The average (and peak) current draw for 3.3V operation is 2.1mA (50mA peak) and 5V
operation is 3.4mA (100mA peak) respectively. Peak current is used during sonar pulse transmit. Please reference page 15
for minimum operating voltage verses temperature information.
GND-Return for the DC power supply. GND (& V+) must be ripple and noise free for best operation.
_______________________________________________________________________________________________________________________________________
About Ultrasonic Sensors
Our ultrasonic sensors are designed for use in air, non-contact object detection and ranging sensors that detect objects
within a defined area. These sensors are not affected by the color or other visual characteristics of the detected object.
Ultrasonic sensors use high frequency sound to detect and localize objects in a variety of environments. Ultrasonic sensors
measure the time of flight for sound that has been transmitted to and reflected back from nearby objects. Based upon the
time of flight, the sensor then outputs a range reading.
www maxtmux cam
Page 3
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Supply Voltage Compensation
During power up, the XL-TrashSonar-WR sensor line will calibrate itself for the supply voltage. Additionally, the sensor
will compensate if the supplied voltage gradually changes.
If the average voltage applied to the sensor changes faster than 0.5V per second, it is best to remove and reapply power to
the sensor.
For best operation, the sensor requires noise free power. If the sensor is used with noise on the supplied power or ground,
the accuracy of the readings may be affected. Typically, adding a 100uF capacitor at the sensor between the V+ and GND
pins will correct most power related electrical noise issues.
_______________________________________________________________________________________________________________________________________
MB7139
The MB7139 is the base model of the XL-TrashSonar-WR sensor line. This sensor is recommended for general purpose
use. The additional features are mentioned below.
The MB7139 reports the range to the first detectable target. Unless the target is barely detectable, this sensor will have a
very stable output. If a smaller object is in front of the target, the sensor may report the range to the object depending on
the object’s size and position.
_______________________________________________________________________________________________________________________________________
MB7137
The MB7137 communicates using the I2C bus protocol. This sensor reports the range to the first detectable target in
real-time. This sensor is capable of outputting new range readings with speeds up to 40Hz if the status pin is being
monitored. The recommended refresh rate is 10Hz or slower.
_______________________________________________________________________________________________________________________________________
MB7138
The XL-TrashSonar-WRM sensors prioritize large targets over both small targets and noise. These sensors report the
target that gives the largest acoustic reflection. This stands in contrast to other units such as the MB7139 which are
designed to report the distance to the first detectable target. If the largest target is removed from the field of view, the
MB7138 will switch to the target that gives the next largest detectable return. 25cm for the MB7138 pipe and compact only 2
The XL-TrashSonar-WRM sensors are designed for applications where users are concerned with ranging the distance to
flat targets (such as water and fuel tanks).
When targets are of similar amplitude reflections, preference is given to the closer target. The sensor expects to see a
target by 3.5 meters. If no target is found, the sensor will increase in sensitivity until a target is found, or until no targets
can be found.
In addition to the most-likely filtering, the MB7052 and MB7092 come equipped with a three-reading filter and reading
hold which requires three consecutive range readings within 1cm of the most recent reading to be considered a valid range
reading. If readings are found to be outside 1cm, or no target can be found by the sensor, then the sensor will report the
last valid range reading. Upon power-up the sensor will default to reporting 3.5 meters unit a valid range reading is found.
The last reading hold is designed for users operating in environments with intermittent high noise who desire to poll the
MB7138 at intermittent times. This allows the sensor to report the previously valid reading until the sensor’s environment
improves. If no valid range reading is found for ~1.5 hours, the sensor will send a fail-safe output “000” on all interfaces.
9:0;
Page 4
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Sensor Integration
The XL-TrashSonar-WR sensors are designed to be mounted at the top of a trash receptacle near the center. For best
operation, it is recommended that end users conduct filtering of the sensor data to achieve the most reliable results.
Filtering Examples
• History Filter — Verifies the reading is accurate when compared to the previous ranges.
• Mode Filter — Output the sensor’s reported range that is shown the most.
• Median filter — Output the reported range that is in the center of a range set.
Sensor Mounting
Trash bins that are lined with plastic bags may detect false reflections if there is air trapped behind the plastic bag.
If the sensor is mounted in a trash bin with stepping sides that get narrower from top down, shown in Diagram 1, the
sensor will typically not range properly to the trash. In this installation the sensor may report the range to the highest side
step.
For trash bins with internal side braces, shown in Diagram 2, the sensor will not report the range past the internal brace.
Like the side steps, this brace creates an ultrasonic echo that the sensor may report the range to.
For installations with that get wider from the top of the bin to the base, shown in Diagram 3, the sensor will typically
report the trash level properly. Testing is recommended for this configuration if side steps get dramatically wider as they
may be detected by the XL-TrashSonar-WR.
Diagram 4 shows the ideal sensor mounting for the XL-TrashSonar-WR sensor line. It is recommended that the sensor is
mounted in a trash bin with smooth sides. This either eliminates or dramatically reduces the secondary reflections that
may return to the sensor.
As the bin increases in size, the less likely the installation is going to detect unwanted objects and noise.
Testing is recommended for any sensor mounting method and bin size.
Diagram 1 Diagram 2
In both of these configurations
the sensor will range to the first
indentation in the trash bin. The
indentation creates a large
detectable reflection.
Diagram 4
In this configuration
the sensor typically
operates properly. This
is the recommended
mounting method.
Diagram 3
This configuration
typically operates
properly.
1ft
min.
2in
max.
-r
: Ml!
A .
B 2.00" 50.7 mm
C 0.58" 14.4 mm
D 0.31" 7.9 mm
E 0.23" 5.8 mm
F 0.10" 2.54 mm
H 1.032” 26.2 mm .
I 1.37" 34.8 mm
www.mathix.com
Page 5
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Sensor Minimum Distance
The XL-TrashSonar-WR sensors have a minimum reported distance of 20-cm (7.87 inches). However, the
XL-TrashSonar-WR will range and report targets to the front sensor face. Large targets closer than 20-cm will typically
range as 20-cm. For the alternative housings, objects between 4-cm and 25-cm will typically range as 25-cm.
_______________________________________________________________________________________________________________________________________
About Package Types
The XL-TrashSonar-WR sensor line is available in a variety of packages for applications with specific mounting
requirements. The full horn package provides peak accuracy and sensitivity in this sensor line. It is recommended that
testing is completed to ensure that the selected sensor will operate as desired in your application.
Performance Changes when Selecting a Non-Full Horn Package
When selecting a XL-TrashSonar-WR without the full horn the sensor will experience the following performance
changes:
The sensor will have a wider beam shape for the first meter.
The sensor may have a dead zone from 0-6cm.
The sensor may have worse performance to small or soft targets.
The sensor may experience decreased noise immunity when ranging to small, soft, angled, or distant targets.
_______________________________________________________________________________________________________________________________________
Mechanical Dimensions
Full Horn
Package Types Currently Available
Full Horn — 3/4” NPT straight; back mounted thread (best performance)
Compact — 3/4” NPT straight; back mounted thread
Ultra-Compact — PCB with 4 mounting holes
1”NPS — External thread over full sensor body (1”NPS)
1” BSPP — External thread over full sensor body (1”BSPP)
30mm1.5 — External thread over full sensor body (30mm1.5)
All package types have exposed PCB on user end for easy connection.
Users desiring a fully enclosed assembly may purchase the “Shielded
Cable Attach Option” along with their sensor.
A 1.72” dia. 43.8 mm dia.
B 2.00” 50.7 mm
C 0.58” 14.4 mm
D 0.31” 7.9 mm
E 0.23” 5.8 mm
F 0.10” 2.54 mm
G 3/4”-14 NPS
H 1.032” dia. 26.2 mm dia.
I 1.37” 34.8 mm
50 grams Weight
Values Are Nominal
Pin 1
A
B
D
C
E
F
G
I
H
‘__.
‘_—>
A .
. . B 0_70” 179mm
_’| I“ C 0.57” 14'4 mm
D 0.31” 7'9 mm
E 0.23” 5'8 mm
F 0.10» 2.54 mm
H 1.032” 26'2 mm I
.1 I 137v 343mm
A
B 1.30” 33'1““
c 0.20” 5'2 mm
D 0.10” 2'54 mm
F 0.73” 19'8 mm
gillflllllllllllh
W
Page 6
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Mechanical Dimensions Continued
Ultra-Compact
Compact Housing
1” NPS Pipe Threading
A 1.37” dia. 34.7 mm dia.
B 0.70” 17.9 mm
C 0.57” 14.4 mm
D 0.31” 7.9 mm
E 0.23” 5.8 mm
F 0.10” 2.54 mm
G 3/4”-14 NPS
H 1.032” dia. 26.2 mm dia.
I 1.37” 34.8 mm
32 grams Weight
Values Are Nominal
I H
A
B
D
C
E
F
Pin 1
G
A 1.29” dia. 38.2 mm dia.
B 1.30” 33.1 mm
C 0.20” 5.2 mm
D 0.10” 2.54 mm
E 1”— NPS
F 0.78” 19.8 mm
Weight 35 grams
Values Are Nominal
F
A
B C
D
Pin 1
E
All values are nominal F 17.78 mm 0.70 ” L 13.4 mm 0.53 ” R 7.80 mm 0.31 ”
A 30.48 mm 1.20 ” G 30.48 mm 1.20 ” M 25.0 mm 0.98 ” S 7.62 mm 0.30 ”
B 35.56 mm 1.40 ” H 3.180 mm 0.13 ” N 1.57 mm 0.62 ” T 2.54 mm 0.10 ”
C 12.24 mm 0.60 ” I 25.40 mm 1.00 ” O 6.20 mm 0.24 ” U 1.07 mm 0.04 ”
D 2.540 mm 0.10 ” J 25.27 mm 1.00 ” P 8.00 mm 0.31 ” V 1.27 mm 0.05 ”
E 2.540 mm 0.10 ” K 10.40 mm 0.41 ” Q 13.9 mm 0.55 ” Weight 15.1 gram.
F
I
H
B G
E
D
C
A P
O
Q
R
S T U
V
N
M
J
L
K
A
| B 1 3 33 1mm
C
D 0 10 2 54 mm
i F 0.78 19.8 mm
1 7
A .
|‘ ' B 1.30” 33.1 mm
\ c 0.20” 5.2 mm
1 D 0.10” 2.54 mm T
i F 0.73” 19.8mm l
j
www mmmmmmmmmmm
Page 7
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Mechanical Dimensions Continued
1” BSPP Pipe Threading
30mm1.5 Pipe Threading
_______________________________________________________________________________________________________________________________________
Device Comparison Chart
_______________________________________________________________________________________________________________________________________
Real-time Auto Calibration
The XL-TrashSonar-WR automatically calibrates prior to each range reading. The sensor then uses this data to range ob-
jects. If the temperature, humidity, or applied voltage changes during sensor operation, the sensor will continue to func-
tion normally. (The sensors do not apply compensation for the speed of sound change verses temperature to any range
readings.) Detection has been characterized in the published sensor beam patterns.
Real-Time Noise Rejection
While the XL-TrashSonar-WR is designed to operate in the presence of noise, best operation is obtained when noise
strength is low and desired signal strength is high. Hence, the user is encouraged to mount the sensor in such a way that
minimizes outside acoustic noise pickup. In addition, keep the DC power to the sensor free of noise. This will let the sen-
sor deal with noise issues outside of the users direct control (Even so, in general, the sensor will still function well even if
these things are ignored). Users are encouraged to test the sensor in their application to verify usability.
_______________________________________________________________________________________________________________________________________
Temperature Compensation
The speed of sound in air increases about 0.6 meters per second, per degree centigrade. The XL-TrashSonar-WR sensors
are not equipped with an internal temperature compensation. If temperature compensation is desired, it is recommended
to test an HRXL-MaxSonar-WR. The HRXL-MaxSonar-WR applies compensation for speed of sound changes.
Part
Number
AN
Voltage
Serial
Data
(0 to Vcc level)
Pulse
Width
Stability
Filter
Most
Likely
Filter I2C Bus
MB7137 Yes
MB7138 Yes RS232 Yes Yes Yes
MB7139 Yes RS232 Yes
A 1.17” dia. 29.7 mm dia.
B 1.30” 33.1 mm
C 0.20” 5.2 mm
D 0.10” 2.54 mm
E 30mm 1.5
F 0.78” 19.8 mm
Weight 31 grams
Values Are Nominal
F
A
B C
D
Pin 1
E
A 1.29” dia. 38.2 mm dia.
B 1.30” 33.1 mm
C 0.20” 5.2 mm
D 0.10” 2.54 mm
E 1”— BSPP
F 0.78” 19.8 mm
Weight 34 grams
Values Are Nominal
F
A
B C
D
Pin 1
E
Page 8
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Range “0” Location
The XL-TrashSonar-WR will report the range to the closest detectable object. Target detection has been characterized in
the sensor beam patterns.
The XL-TrashSonar-WR sensors reports the range to distant targets starting from the front of the sensor as shown in the
diagrams below.
The range is measured from the front of the transducer to the target.
Range Zero
Range Zero
The range is measured from the front of the transducer to the target.
Range Zero
The range is measured from the front of the transducer to the target.
Range Zero
The range is measured from the front of the transducer to the target.
Pulse wrath output sensor Operatron
V
R5232 Senal output sensor operatrorr V
V
.lprrrmwmm
Analog voltage output sensor Opennon V
WW m as. mm m. V I m. M W mmwmm V
supvlyVoluw-maomss voVu | supvlyvoluw-maomss voVu
emu “Kareem“ ‘ | emu “Kareem“
A
M M p... W wmu plnmAD mm | w”. an 9... mm W. I
on are met sensor
for :1 least 2W5
men the rest or
tne sensors wlll
man In sequence
wmu plrmmrpu. I
Canned to GNDI ammo GMD|
sweet to cm) I
V V
Pull ax pln hm on
me flnl nun-r! rm :1
least zone men are
mlcvo co wlll
A A
V
nepeex m .44 . mlfly servers I) Auind
w..eunp...mu...pm I wiremyrmrnrwm I
Wire“. Prmtorwu I
Come-.110 anal connect to snul
Connect to snul
hive lo return Al‘s
pm to e mgr.
Imam 5m: so
mat me next lune
mum me n
elm-n mm me last
sensor wlll mk: w:
wrylorne xx orme
m: sensor.
I
:A
A
V
1%
A
A
Reveal to add is minv Sensnls is a
Pull RX pln hlgh
ror .t least mus.
men just strobe
the sensovs‘ RX
plus no me ren
mun plnloADlnpm I wmu plntaADlnvut I
wmn pmloADlnpm I
V V
or the sensors wlll
read the unge
srmuluneuusly,
A A
l
Repeatta add ls manysznsan as desirzd
www maxb x com
Page 9
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7138 - MB7139 Operating Modes
Independent Sensor Operation
The XL-TrashSonar-WR sensors are designed to operate in a single sensor environment. Free-run is the default mode of
operation for all of the MaxBotix Inc., sensors. The XL-TrashSonar-WR sensors have three separate outputs that update
the range data simultaneously: Analog Voltage, Pulse Width1, and RS232 Serial. Below are diagrams on how to connect
the sensor for each of the three outputs.
Using Multiple Sensors in a Single System
When using multiple ultrasonic sensors in a single system, there can be interference (cross-talk) from the other sensors.
MaxBotix Inc., has engineered a solution to this problem for the XL-TrashSonar-WR sensors. The solution is referred to
as chaining. We have 3 methods of chaining that work well to avoid the issue of cross-talk.
The first method is AN Output Commanded Loop. The first sensor will range, then trigger the next sensor to range and so
on for all the sensors in the array. Once the last sensor has ranged, the array stops until the first sensor is triggered to range
again. Below is a diagram on how to set this up.
The next method is AN Output Constantly Looping. The first sensor will range, then trigger the next sensor to range and
so on for all the sensor in the array. Once the last sensor has ranged, it will trigger the first sensor in the array to range
again and will continue this loop indefinitely. Below is a diagram on how to set this up.
The final method is AN Output Simultaneous Operation. This method does not work in all applications and is sensitive to
how the other sensors in the array are physically positioned in comparison to each other. Testing is recommend to verify
this method will work for your application. All the sensors RX pins are connected together and triggered at the same time
causing all the sensor to take a range reading at the same time. Once the range reading is complete, the sensors stop
ranging until triggered next time. Below is a diagram on how to set this up.
Power Up Timing
w.-
Clean, stable power provided In Vac
Pin 6
(V06)
"—
Vac
Pin 5 Mel Driven Bum data output in R5232
gmfifiml Low idle slate
o for R8232
Va _
m5?“ Not Driven Internally sec high or user controlled 5"" Panama 0'
sumac” monitoring
o_ _ begins
'I'Ime OMS -5|1m5 -ll'lm5 -115ms
Real-lime Operation
Vet:
Pin 6 Cleanslable plywer pmvined to vac Power Supply must be free cl noise
"cc, for besl results
a (All signals are referenced In v“ and W.)
Initially set law
\
Pln A \ _ _
"my.“ \ DrIve Ingl- lor >2ous l>o.ozmsl
smnlsmp) \\
l
Pin 3 nus The analog voltage output maintains
(Analog Voltage Range the voltage correspondan to the
output) voltage gel [as avallable) lalest range measurement
Pln 2 Range infomlation is output with a
(pub, ma... high pulse width between 1.16ms and
Dunn") “Ams'
Pln 5 m ”m |
(R5232 Serial R5232
0W3")
_ Low idle state for R8232
Tlnle ans -32.3lns ~7a1nls4 «guns -9lllns
www maxbollx cam
Page 10
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7138 - MB7139 Sensor Timing Diagrams
Power-Up Timing
Sensor Free-Run Timing
Free-Run Operation
Pin 5
(Vac) Clean. slable pow provided to vcc
n(A|| signals Ire referent!!! by Vcc and W.)
Pin 4
[Ranging
Stanlslnp)
Pln 3
(Analog Voltage
Output)
Pin 2
(Pulse mam
culpur)
Pin 5
(Ran-z serial
Output)
Power supply must be free of nolse
for best results
Start ranging or monitoring begins
11|e Analog voltage output holds to
the latest range measurement
Range Information Is output wllh a
high pulse width between 1.16m5
and 44.4m5 (7.65meter models) or
Sims (10.68 meter models)
Law idle state for R5232
www maxlmux cam
Page 11
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7138 - MB7139 Sensor Timing Diagrams Continued
Real-Time Operation
Timing Description
175mS after power-up, the XL-TrashSonar-WR is ready to begin ranging. If Pin-4 is left open or held high (20uS or
greater), the sensor will take a range reading. The XL-TrashSonar-WR checks Pin-4 at the end of every cycle. Range
data can be acquired once every range reading. Each range reading starts by Pin-4 being high or open, after which the
XL-TrashSonar-WR calibrates and calculates for 20.5mS, and after which, thirteen 42KHz waves are sent. The sensor
then determines the range to the target. Next the analog voltage is set. At 99mS, the sensors with a pulse width (PW), Pin
2 is set high for a length of time between 1.16mS and 20.3mS. At 94.3mS, for the next 4.7mS the serial data is sent. The
most accurate range output on the XL-TrashSonar-WR sensors is the PW output.
m ananmn“
SCl i
Is‘anl ADDRESS | u/w | [MACK |
74m Izc address 3
3-bit read/WIRE Izc address
w___._____
—=.
u..__-.
Oms ~7Um m
www maxbohx cam
Page 12
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7137 Default Address
The representation of the sensor address will be different depending on the addressing scheme your master device uses.
The chart below shows the default address for the I2CXL-MaxSonar-WR/WRC sensors under different addressing
implementations. Elsewhere in this datasheet a 8-bit read/write addressing scheme is assumed.
_______________________________________________________________________________________________________________________________________
MB7137 Power-Up Timing
The I2CXL-MaxSonar-WR/WRC starts operating within milliseconds of application of power. The major timing of
power-up events for the I2CXL-MaxSonar-WR/WRC can be seen in the diagram below.
After the sensor is commanded to take a range reading it sends an ultrasonic pulse, waits between ~15ms to ~70ms to
detect a target, and determines the range Then the sensor will resume I2C communications. If the sensor is addressed
while in the middle of a range reading, all requests for communication will be responded with a NACK (not
acknowledge).
In environments that reflect acoustic noise well, sampling faster than 10Hz could cause the sensor to pick up signals from
previous ultrasonic pulses and report false data. It is possible, however, to take range readings at a significantly faster rate
in certain environments.
When changing the part address, ensure that power to the sensor is not disrupted or memory corruption may occur. If the
memory becomes corrupted, the part should automatically use the default shipped address on power up. It is
recommended to avoid changing the address often, as it could cause premature memory failure due to repeated erase/write
cycles.
Addressing
Scheme
Default Address
(decimal)
Default Address
(binary)
Notes
7-bit addressing 112 1110 000X 7-bit addressing handles the address shifting and R/W bit
for the user
8-bit addressing 224 1110 000X 8-bit addressing inserts the R/W bit and only allows for
even number addresses
8-bit read/write
addressing
Write: 224
Read: 225
1110 0000
1110 0001
8-bit R/W addressing schemes require the user to set the
R/W bit directly.
0ms ~70ms ~90ms ~115ms ~135ms
Pin 6 V+
Vcc Power is
applied
Sensor Ready for I2C
Gnd
Pin 2 Address
Announce / Status
Vcc
Pulse Width
between 200uS
Gnd
Pin 1
Temporary Default
Vcc
Pulled high unless grounded by external source
Gnd
Note: external grounding
checked at 70mS
www maxboux cam
Page 13
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7137 Commands
MB7137 Range Cycle Interrupt
If the sensor receives a request to report the last range value while it is taking a range reading the range reading will be
interrupted and a NACK will be sent. If you desire to allow the full range cycle to complete before reading monitor the
status pin for the completion of a range cycle or wait for the full 100ms for the range . If the sensor is interrupted and has
already found a target the sensor will report the range to the target. If the sensor has not yet found a target when it is
interrupted the sensor will send the previous range value. If no range values have been found the distance sent will
alternate between 0cm and 255cm.
Command Sequence of Events Value Used
(decimal)
Value Used
(binary)
Notes
Take a range
reading
1. Initiate a write at the sensor
address
2. Write the range command
byte
224 (default)
81
1110 0000
0101 0001
Commands the sensor to take a
single range reading and save to
distance found for the next range
request. It is best to allow 100ms
between readings to allow for
proper acoustic dissipation.
Report the last
range value
1. Initiate a read at the sensor
address
2a. Read the two bytes from
the sensor starting with the
range high byte.
2b. Read the range low byte.
225 (default)
(Sent by sensor)
(Sent by sensor)
1110 0001
Range High
Byte
Values are
MSB to LSB
The sensor will report the distance
value in cm obtained from its last
range reading. Users requiring
real-time information should
command a range reading ~80ms
before reading the sensor. After
power-up if no range command is
sent the sensor respond with two
part info bytes.
Change the
sensor address
1. Initiate a write at the sensor
address
2a. Write three bytes to the
sensor starting with the
addr_unlock_1 command
2b. Write the addr_unlock_2
command
2c. Write the new sensor
address
224 (default)
170
165
(User Value)
1110 0000
1010 1010
1010 0101
#### ###0
The sensor will only accept even
address values. If an odd numbered
address is sent the sensor will be set
to the next lowest even number. If
the sensor is told to change to one of
the invalid addresses below the
sensor will ignore this command
and stay at its current address.
Invalid Address Values:
0, 80, 164, 170
Page 14
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7137 Wiring Diagram
The I2C bus is a two wire interface that consists of a clock line and data line where each requires a pull-up resistor
attached to V+. Only one pull-up resistor is required each for the SCL and SDA lines per bus – not per sensor.
The I2C specification recommends a resistance value of 4.7 kΩ for 20-100kHz interfaces with good low inductance
routing. However, these specifications are for communication between chips on a singe PCB. If you have longer cable
lengths it is best to use lower value resistor, such as 1kΩ, and also to use properly shielded cables. Often I2C bus
problems can be fixed by doing one of the following: by using properly shielded cable or by decreasing the value of the
pull-up resistors. The I2CXL-TrashSonar-WR/WRC series is capable of sinking more current than the I2C specification
requires (15mA versus 3mA) so a much lower resistance value can be used. The voltage applied to the I2C lines should
be the same voltage that is applied to V+ of the sensor.
MB7137 Multiple Sensor Wiring Diagram
SDA
I2C Bus Master
SCL
GND
V+
I2CXL-TrashSonar-WR Sensors
GND
V+
GND
V+
GND
V+
I2CXL-TrashSonar-WR Sensor
I2C Bus Master
SDA
SCL
GND
V+
GND
V+
Supply Voltage (V)
3.5
125
175
7.5
125
Minimum Operating Voltage vs Temperature
For operation to 40°C voltage
shall be 3.2V or higher
40 10 o 20 up so
Temperature (°C)
www maxboilx corn
Page 15
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Voltage vs Temperature
The graph below shows minimum operating voltage of the sensor verses temperature.
Background Information Regarding our Beam Patterns
Each XL-TrashSonar-WR sensor has an individually calibrated beam pattern, and is matched to provide the approximate
detection pattern shown in this datasheet. This allows end users to select the part number that matches their given sensing
application. Each part number has a consistent field of detection so additional units of the same part number will have
similar beam patterns. The beam plots are provided to help identify an estimated detection zone for an application based
on the acoustic properties of a target versus the plotted beam patterns.
Each beam pattern is a 2D representation of the detection area of the sensor. The beam pattern is
actually shaped like a 3D cone (having the same detection pattern both vertically and horizontally).
Detection patterns for dowels are used to show the beam pattern of each sensor. Dowels are long
cylindered targets of a given diameter. The dowels provide consistent target detection characteristics
for a given size target which allows easy comparison of one MaxSonar sensor to another MaxSonar
sensor.
For each part number, the four patterns (A, B, C, and D) represent the detection zone for a given
target size. Each beam pattern shown is determined by the sensor’s part number and target size.
The actual beam angle changes over the full range. Use the beam pattern for a specific target at any
given distance to calculate the beam angle for that target at the specific distance. Generally, smaller
targets are detected over a narrower beam angle and a shorter distance. Larger targets are detected
over a wider beam angle and a longer range.
People Sensing:
For users that
desire to detect
people, the
detection area to
the 1-inch
diameter dowel, in
general, represents
the area that the
sensor will
reliably detect
people.
MB7137-1XX MB7138-1XX
MB7139-1XX
_ 1050 cm
XL—TrashSonar‘"—WR"' Beam Pattern (“3‘ “’
Sample results for measured beam pattern are shown on a 30-cm grid The detection
pattern is shown for dowels of varying diameters that are placed in front of the sensor _ 900 cm
A 6.1-mm (0.25—ilch) diameter dawel D 11 -inch wide hoard moved left to riglt with (~30 fl)
B 254cm (1-inch) diameter dowel the board parallel to Ihe from snsor face.
C 8‘89-cm (15-inch) diameter dowel This shows the sensor's range capabiity.
Home; For peolie detection the pattern _ 750 cm
typicaly falls between charts A and B. (~25 ft)
- - Partial Detection c 600
cm
_ 5-0 V (~20 fl)
. 3.3 V
_450 cm
A (~15 fl)
_ 300 cm
(~10 fl)
_ 150 an
("5 R»)
30 cm
‘ (-1 n.)
Beam Characteristics are Approximate
Beam Pattern drawn to a 1:95 scie for easy comparison to our otha products.
www.maxbolix.com
Page 16
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB7137, MB7138, MB7139 XL-TrashSonar™-WR™ Beam Pattern & Uses
The XL-TrashSonar-WR sensors are the recommended sensor for trash level measurement. These sensors reject
electrical noise and outside acoustic noise.
MB7137, MB7138, MB7139
Features and Benefits
• Real-time calibration, noise
rejection and additional filtering
provides stable range information
• Excellent for applications that
require consistently accurate
outputs
• Impressive acoustic and electrical
noise resistance
MB7137, MB7138, MB7139
Applications and Uses
• Autonomous Navigation
• Environments with acoustic and
electrical noise
• Bin Level Measurement
• Tank Level Measurement
• Trash Level measurement
MB7137-2XX MB7138-2XX MB7139—2XX
MB7137-5XX MB7138—5XX MB7139—5XX
MB7137-6XX MB7138-6XX MB7139~6XX
MB7137-7XX MB7138-7XX MB7139—7XX
XL-‘l'lashSonar "- Beam Pattern
Sample resins for measuned beam pattern are shown on a 30-cm grid. The deleclion
patlem is shown for dowels of vzying diameters lhal are placed in from oflhe sensor
A 6.1-mm (0.25-irch) diameter dowel D 11-inch wide board moved lefl lo vigil wilh
B 2.54-cm (1-ilch) diameter dowel lhe board parallel to lhe front sensor face.
C 8.8941m (3.5-irch) diameter dowel This shows the sensor's range capability.
Mole: For people deledion the paIern
lypicalyfalls between charts Aard B.
C
Beam Charaderislics are Approximale
Beam Pauan drawn in a 1:95 scale for easy comparison to our olher products.
_1050 cm
(~34 to
www.maxba|ix.com
Page 17
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB713X XL-TrashSonar™-WR™ Beam Pattern & Uses
The XL-TrashSonar-WR product line is available in alternative housings that include a WRC housing, 1” NPS pipe
threading, 1” BSPP pipe threading, and 30mm 1.5 pipe threading.
MB713X
Features & Benefits
• Can be flush mounted in an
application
• Same resolution as the full horn
equivalent
• Available in both metric and
imperial housing sizes
MB713X
Applications & Uses
• Autonomous Navigation
• Environments with acoustic and
electrical noise
• Bin Level Measurement
• Tank Level Measurement
• Trash Level measurement
M37137-300 M37137-320
M37138-300 M37138-320 D
M371 39-300 M371 39-320 _ 1050 cm
XL-TrashSonar "- Beam Pattern ("3‘“)
Sample results for measured beam pattern are shown on a Elli-cm grid. The detection
pattern is shown for dowels of varying diameters that are placed in front of the sensor. _ 900 cm
A 6.1-mm (0.25-ilch) diameter dime! D 11 -inch wide boad moved lefl to riylt wilh (~30 it.)
B 2.5442m (1-inch) dameter Mel the board parallel to the front sensor facet
C 8789-cm (3.5—inch) iiameter dowel This shows the sensor's range capabiity
Note: For peofle detection the paltern _ 750 cm
typicaly falls between charts Aard 3. (~25 it.)
- - Partial Detection c 600
cm
_ 5-0 V (~20 n)
O 3.3 v
_450 cm
A (~15 '1)
_ 300 cm
(-10 n)
_ 150 cm
(“5 fl-)
_ 30 cm
('“1 fl-)
Beam Characteristics are Approximate
Beam Pattern drawn no a 1 :95 scale for easy oompxlson to our other products.
www.maxbaiix.com
Page 18
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB713X XL-TrashSonar™-WR™ Beam Pattern & Uses
The XL-TrashSonar-WR product line is available in an UltraCompact alternative housing. The UltraCompact housing is
designed for users creating a custom horn mount. The recommended horn can be downloaded from
http://www.maxbotix.com/Ultrasonic_Sensors/TrashSonar-Sensors.htm
MB713X
Features & Benefits
• Capable of being flush mounted in
an application
• Same resolution as the full horn
equivalent
• Gives the ability to create custom
mounts
MB713X
Applications & Uses
• Autonomous Navigation
• Environments with acoustic and
electrical noise
• Bin Level Measurement
• Tank Level Measurement
• Trash Level measurement
M37137-400 M371 37-420
M37138-400 M371 38-420
M37139-400 M371 39-420
XL-TrashSonar "- Beam Pattern
Sample results for measured beam pmern we shown on a 30-cm grid. The detection
pattern is shown for doweb of vary'ng diameters that are placed in front of the sensor.
A 6‘1—mm (0.25-ilch) diameter dowel D 11 inch wide bold moved left to rig“ wilh
B 2,54-cm (1-inch) dameter dowel the board paralel I: the from sensor face.
C 818942m (3.5-inch) dameter dowel This shows the sensor's range capabiliy.
Nae: For people detection the pattern
typicaly fals between charts A and B.
C
Beam Characteristics are Approximate
Beam Pattern drawn to a 1 :95 scale for easy comparison to our other products.
www.maxba|ix.com
Page 19
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
MB713X XL-TrashSonar™-WR™ Beam Pattern & Uses
The XL-TrashSonar-WR product line is available in an UltraCompact alternative housing. The UltraCompact housing is
designed for users creating a custom flush mount.
MB713X
Features & Benefits
• Capable of being flush mounted in
an application
• Same resolution as the full horn
equivalent
• Gives the ability to create custom
mounts
MB713X
Applications & Uses
• Autonomous Navigation
• Environments with acoustic and
electrical noise
• Bin Level Measurement
• Tank Level Measurement
• Trash Level measurement
www maxboux cam
Page 20
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
Part Numbers
All part numbers are a combination of a six-character base followed by a dash and a three-digit product code.
Please review the following table for more information on the three-digit product code.
Note: Active part numbers listed on page 21.
M B 7 1 3 X - 1 0 0
Base Housing Options Wire
0 Not Applicable
1 3/4” NPS WR
2 3/4” NPS WRC
3 Ultra Compact
4 Ultra Compact Flush Mount
5 1” NPS
6 1” BSPP
7 30MM 1.5
8 Extended Horn
0 No Options (Bagged)
1 F-Option
2 P-Option
3 F-Option and P-Option
4 No Options (Trayed)
5 TTL (Bagged)
6 TTL (Trayed)
0 No Wire
1 Wire Attached
www maxboux cam
Page 21
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
The following tables display all of the active and valid part numbers for these products.
Active Part Numbers for MB7137
MB7137-100 MB7137-101 MB7137-110 MB7137-111 MB7137-120 MB7137-121 MB7137-130 MB7137-131
MB7137-200 MB7137-201 MB7137-210 MB7137-211 MB7137-220 MB7137-221 MB7137-230 MB7137-231
MB7137-300 MB7137-320 MB7137-400 MB7137-420 MB7137-500 MB7137-501 MB7137-510 MB7137-511
MB7137-520 MB7137-521 MB7137-530 MB7137-531 MB7137-600 MB7137-601 MB7137-610 MB7137-611
MB7137-620 MB7137-621 MB7137-630 MB7137-631 MB7137-700 MB7137-701 MB7137-710 MB7137-711
MB7137-720 MB7137-721 MB7137-730 MB7137-731
Active Part Numbers for MB7138
MB7138-100 MB7138-101 MB7138-110 MB7138-111 MB7138-120 MB7138-121 MB7138-130 MB7138-131
MB7138-200 MB7138-201 MB7138-210 MB7138-211 MB7138-220 MB7138-221 MB7138-230 MB7138-231
MB7138-300 MB7138-320 MB7138-400 MB7138-420 MB7138-500 MB7138-501 MB7138-510 MB7138-511
MB7138-520 MB7138-521 MB7138-530 MB7138-531 MB7138-600 MB7138-601 MB7138-610 MB7138-611
MB7138-620 MB7138-621 MB7138-630 MB7138-631 MB7138-700 MB7138-701 MB7138-710 MB7138-711
MB7138-720 MB7138-721 MB7138-730 MB7138-731
Active Part Numbers for MB7139
MB7139-100 MB7139-101 MB7139-110 MB7139-111 MB7139-120 MB7139-121 MB7139-130 MB7139-131
MB7139-200 MB7139-201 MB7139-210 MB7139-211 MB7139-220 MB7139-221 MB7139-230 MB7139-231
MB7139-300 MB7139-320 MB7139-400 MB7139-420 MB7139-500 MB7139-501 MB7139-510 MB7139-511
MB7139-520 MB7139-521 MB7139-530 MB7139-531 MB7139-600 MB7139-601 MB7139-610 MB7139-611
MB7139-620 MB7139-621 MB7139-630 MB7139-631 MB7139-700 MB7139-701 MB7139-710 MB7139-711
MB7139-720 MB7139-721 MB7139-730 MB7139-731
Technical Suggort
Sensor Selection Hell;
F
s
Fullv Calibrated Beam Patterns
Understanding Range Readings
How to Use Multigle Ultrasonic Sensors
l 165 [Dmaxbotixxom
www maxautlx com
Page 22
Web: www.maxbotix.com
PD13516h
MaxBotix® Inc.
Copyright 2005 - 2015 MaxBotix Incorporated
Patent 7,679,996
XL-TrashSonar™-WR™ Series
MaxBotix Inc., products are engineered and assembled in the USA
After reviewing this datasheet, do you have any more questions?
We offer Technical Support on all of our products even if you purchased them through one of our many vendors
worldwide.
You can fill out a Technical Support form for assistance on a sensor here --> Technical Support
Not sure which sensor you need for your application?
We offer Sensor Selection Assistance, click the link here to fill out a form for support --> Sensor Selection Help
Looking for tutorials to help you get started?
Frequently Asked Questions about Our Sensors
We receive many questions about our products and services. This resource offers answers to common inquiries
we receive about our product lines and their application.
Fully Calibrated Beam Patterns
All of our sensors are factory calibrated to provide consistent beam patterns, detection zones, to fit into a wide
variety of applications. In our product lines, each model number comes with a different beam pattern that reflects
the sensitivity and the detection zone of how it sees a target. Additionally, we strive to maintain consistency be-
tween our finished products, and you will see little to no deviation between sensors of the same model. This al-
lows you to have confidence in your final application when using multiple sensors.
Understanding Range Readings
The success of an application may hinge upon knowing the exact location of a target. However, a sensor may
report one meter even if the target is not exactly one meter away from the sensor. Sensor specifications, such as
resolution, precision, and accuracy, help you to understand sensor performance.
How to Use Multiple Ultrasonic Sensors
This guide covers three ways to run your sensors in a Multiple Sensor environment and issues you may face.
Contact us now with any questions at sales@maxbotix.com or call +1-218-454-0766.
Please call during our preferred business hours of 8:00 am – 4:30 pm EST on Monday through Thursday and 8:00 am –
2:00 pm EST on Friday, or you may leave us a voicemail anytime.
Products related to this Datasheet
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENS 42KHZ TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR
ULTRASONIC SENSOR XL-TRASHSONAR