Parallax Serial LCD 规格书
Dx‘R‘IL.
\/
/\
:INI
Web Site: www.parallax.com
Forums: forums.parallax.com
Sales: sales@parallax.com
Technical: support@parallax.com
Office: (916) 624-8333
Fax: (916) 624-8003
Sales: (888) 512-1024
Tech Support: (888) 997-8267
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 1 of 11
Parallax Serial LCD
2 rows x 16 characters, Non-backlit, with Piezospeaker (#27976)
2 rows x 16 characters, Backlit, with Piezospeaker (#27977)
4 rows x 20 characters, Backlit, with Piezospeaker (#27979)
The Parallax Serial LCDs are very functional, low-cost liquid crystal displays that can be easily interfaced
to and controlled by a microcontroller using a I/O pin. The LCD displays provide basic text wrapping so
that your text looks correct on the display. Full control over all of their advanced LCD features allows you
to move the cursor anywhere on the display with a single instruction and turn the display on and off in
any configuration. They support visible ASCII characters Dec 32-127, and in addition you may define up
to eight of your own custom characters to display anywhere on the LCD.
NOTE: If your Serial LCD Display does not have a speaker on the back, use the specifications
and information in the Product Change Notice: Revision E and Earlier section on page 11.
Features
Clear 40-pixel characters (8 H x 5 W)
Supports ASCII DEC characters 32-127
Define up to eight custom characters
Automatic text wrapping
Single command cursor placement
Single command clears the display
Define up to eight custom characters
Select 2400, 9600, or 19,200 baud with switches on
the back of the device
Display type: STN, YG, positive transflective LCD
Adjustable contrast knob on the back of the device
YG LED for backlit model displays
Key Specifications
Power requirements:
o Non-backlit: +5 VDC, 20 mA
o Backlit: +5 VDC, 20 mA (light off), ~ 80 mA typical (light on)
Communication: Selectable asynchronous serial baud rates: 2400, 9600, 19200
Operating temperature: -4 to +158 °F (-20 to +70°C)
Dimensions: NOTE - Board and LCD size and style may vary
o 2x16: Approx. 1.42 x 3.15 in (36 x 80 mm)
o 4x20: Approx. 2.37 x 3.86 in (60.2 x 98.1 mm)
PROVTDE A SIGNAL TO THE ‘RX‘ PIN BEFORE APPLYING 5 VDC TO THE ‘SV‘ PIN
—=-Rx
5V
(3ND
Parallax LCD
MODE SW1 SW2
Test OFF OFF
2,400 ON OFF
9,600 OFF ON
19,200 ON ON
lsel
NO 140 was
450 NO can
No NO nnz‘sL
130 110
ms ms 300w
@©®@®®@®®®®®®@®E
PmHax "'
.u Sena‘ LCD
0 A
mm
E WW 0
fl EVF cwmv G
WSW , e E“
9434le Z
.4 y‘
O
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 2 of 11
Quick-Start Circuit
The Serial LCDs should be powered from an external regulated 5 V power supply. Make sure the power
supply has an adequate current rating to power the Serial LCD and the BASIC Stamp, Propeller chip, or
whichever microcontroller and other devices you are using.
CAUTION
DO NOT PROVIDE A SIGNAL TO THE 'RX' PIN BEFORE APPLYING 5 VDC TO THE '5V' PIN.
Baud Rate Setup
After connecting the Serial LCD, you will need to select the baud rate at which you are going to send it
data. You have three choices: 2400, 9600, and 19,200 baud. To set the baud rate, move the dip switches
on the back of the LCD into the correct positions according to the table next to the switches, which is also
repeated below:
MODE SW1 SW2
Test OFF OFF
2,400 ON OFF
9,600 OFF ON
19,200 ON ON
As you can see from the table, there is also a fourth choice called Test. Use this Test mode to confirm
that the power and ground to the LCD are hooked up correctly before you send it any data. Move the dip
switches to the Test setting and turn on the power. The LCD display should turn on with the backlight on
(models 27977, 27979) and display the following text:
Parallax, Inc.
www.parallax.com
If you don’t see the text at first, try adjusting the LCD contrast by turning the pot labeled “Increase
Contrast” with a screwdriver. Turn it in the direction of the arrow to make the characters show up more
clearly. If you still don’t see the characters, go back and check your electrical connections and try again.
Once you’ve successfully completed test mode, move the dip switches to the correct positions to select
the baud rate you want to use for your application.
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 3 of 11
Displaying Text
Now that the LCD is set up, it’s time to start sending text to the display. To display a character of text on
the Serial LCD, simply send the ASCII code of that character to the Serial LCD over the serial port at the
correct baud rate.
When a character is received, the Serial LCD displays that character at the current cursor position and
then moves the cursor one position to the right. When you first turn on the LCD, the cursor is in the
leftmost position on the top line, as you might expect. The short bar on the bottom of the character
shows where the cursor is positioned currently.
Once you’ve sent a full line characters to the LCD, you will notice that the cursor automatically wraps
around to the leftmost position of the second line, just like the text in a book. The text will wrap like this
at the end of every line, with the end of the bottom line wrapping back around to the top line of the LCD.
The text will never “run off” the display; you’ll always see all of the characters you send.
Example code is provided below. You may download the example code files from the 27976, 27977, or
27979 product pages at www.parallax.com; just enter any of these product numbers in the “search” field
on the home page
BASIC Stamp® 2 Example Code
You may download the example code from the 27976, 27977, or 27979 product pages at
www.parallax.com; just enter any of these product numbers in the “search” field on the home page. Try
the following code on your BASIC Stamp 2 to send a text string to the LCD display. First, set the baud
rate on your Serial LCD to 19,200. Then, load the code below into your BASIC Stamp 2 and run it.
You will see the text string show up and wrap to the second line of the display.
In all of your Serial LCD code, you should pause for 100 ms at start-up to give time for the Serial LCD to
initialize. You should also set the serial port pin on the BASIC Stamp to HIGH before the 100 ms start-up
delay, as this is the normal state of a serial port when it isn’t sending any data.
' {$STAMP BS2}
' {$PBASIC 2.5}
TxPin CON 0
Baud19200 CON 32
HIGH TxPin ' Set pin high to be a serial port
PAUSE 100 ' Pause for Serial LCD to initialize
SEROUT TxPin, Baud19200, ["Hello, this text will wrap."]
Propeller P8X32A Example Code
Try the following code on your Propeller to send a text string to the LCD display. First, set the baud rate
on your Serial LCD to 19,200. Then, load the code below into your Propeller and load RAM or EEPROM.
You will see the text string show up and wrap to the second line of the display.
In all of your Serial LCD code, you should wait for 100 ms after starting the FullDuplexSerial.spin object,
to give the object and the Serial LCD time to initialize. The FullDuplexSerial.spin object is included with
the Propeller Tool.
SerialiLEDilJemo‘ spin
ixlnfr‘eq = Siflflfliflflfl
TXJIN = fl
UBJ
LCD.start(TX7PIN. TXJIN, Zlflflfl. 1972M)
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 4 of 11
{{
Serial_LCD_Demo.spin
For Parallax Serial LCDs 27976, 27977, 27979
}}
CON
_clkmode = xtal1 + pll16x
_xinfreq = 5_000_000
TX_PIN = 0
BAUD = 19_200
OBJ
LCD : "FullDuplexSerial.spin"
PUB Main
LCD.start(TX_PIN, TX_PIN, %1000, 19_200)
waitcnt(clkfreq / 100 + cnt) ' Pause for FullDuplexSerial.spin to initialize
LCD.str(string("Hello, this text will wrap."))
Moving the Cursor
When you send a character to the Serial LCD, it always displays at the current cursor position. There are
a few different ways to move the cursor on the Serial LCD display. After each character you send, the
cursor automatically moves over one position. Along with this, there is a standard set of cursor move
commands including Backspace, Carriage Return, and Line Feed.
The Backspace/Left command (Dec 8) moves the cursor one place to the left and the Right command
(Dec 9) moves the cursor one place to the right. These can be useful for moving the cursor around to
overwrite existing text. These commands wrap to the next line of the display, if necessary. The Line Feed
command (Dec 10) moves the cursor to the next line of the display without changing the horizontal
position of the cursor. The Carriage Return command (Dec 13) also moves the cursor to the next line, but
it moves the cursor to the leftmost position on that line as well. The Form Feed command (Dec 12) clears
the entire display and moves the cursor to the leftmost position on line 0, just like when you first turn on
the display. You will need to pause for 5mS in your code after sending the Form Feed command, to give
the Serial LCD time to clear the display. Except for Form Feed, none of these move commands affects the
characters on the display.
There are also direct move commands that you can use to move the cursor to any position on the display
with a single command. The commands in the range Dec 128 to 143 and Dec 148 to 163 move the cursor
to the 16 different positions on each of the two lines of the model 27976 and 27977 LCDs. The
commands in the range Dec 128 to 207 move the cursor to the 20 different positions on each of the four
lines of the model 27979 LCD.
Controlling the Display
You also have control over the various display modes of the Serial LCD. The display-off command (Dec
21) turns off the display so that all of the characters disappear. The characters aren’t erased from the
display, though, and you can even keep writing new characters to the display when it is turned off. A
trick to make a lot of text show up all at once, even at a slow baud rate, is to turn off the display and
then send all of your text. Then, when you turn the display on again, all of the text appears instantly.
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 5 of 11
The display-on commands (Dec 22 to 25) turn the display back on and also control whether you want to
display the cursor and/or make the cursor character blink. The cursor is the short bar that shows up
below the character at the current cursor position. The blink option makes that character blink on and off
repeatedly. You can turn the cursor and blink options on or off, in any combination, as listed in the
command set table. You can change the cursor and blink mode even if the display is already on; you
don’t need to turn it off and then back on again.
With models 27977 and 27979, you can also control the backlight of the display. The backlight lights up
the display so that it is easier to see in the dark. There are commands to turn the backlight on (Dec 17)
and off (Dec 18).
Custom Characters
The Serial LCD has the capability to store up to eight user-defined custom characters. The custom
characters are stored in RAM and so they need to be redefined if you turn off the power. You can display
the custom characters by sending the commands Dec 0 to 7, as shown in the command set table. The
custom character will display at the current cursor position.
The custom characters are five pixels wide by eight pixels high. Each of the characters is stored as a
series of eight data bytes where the low five bits of each byte represent a row of pixels in the character.
The high three bits of each byte are ignored. A bit value of one turns that pixel on (i.e. makes it black).
The bottom row of pixels is often left blank (all zeros) to make it easier to see the cursor.
To define a custom character, you will send a total of 9 bytes to the Serial LCD. The first byte needs to
be a valid define-custom-character command (Dec 248 to 255) and must be followed by eight data bytes
that define the pixels of the character. The Serial LCD will always use the next eight bytes it receives to
set the pixels of the character. The data bytes define the character starting at the topmost row of pixels,
as shown in the example code.
BASIC Stamp 2 Custom Character Example
Define a custom character using the code example below. First, set the baud rate on your Serial LCD to
19,200. Then, load the code below into your BASIC Stamp 2 and run it. You will see a diamond character
appear on the screen.
' {$STAMP BS2}
' {$PBASIC 2.5}
TxPin CON 0
Baud19200 CON 32
HIGH TxPin ' Set pin high to be a serial port
PAUSE 100 ' Pause for Serial LCD to initialize
SEROUT TxPin, Baud19200, [250] ' Define custom character 2
' Now send the eight data bytes
SEROUT TxPin, Baud19200, [%00000] ' %00000 =
SEROUT TxPin, Baud19200, [%00100] ' %00100 = *
SEROUT TxPin, Baud19200, [%01110] ' %01110 = * * *
SEROUT TxPin, Baud19200, [%11111] ' %11111 = * * * * *
SEROUT TxPin, Baud19200, [%01110] ' %01110 = * * *
SEROUT TxPin, Baud19200, [%00100] ' %00100 = *
SEROUT TxPin, Baud19200, [%00000] ' %00000 =
SEROUT TxPin, Baud19200, [%00000] ' %00000 =
SEROUT TxPin, Baud19200, [2] ' Display the new custom character 2
((
))
iclkmode = xtall , pllle
TX7PIN = a
LCD : "FullDuplexSer1a1.sp1n"
PUB Main
waltcnthlkfreq / 1mm 4 cnt
LCD.” (25%)
LCD. xx (Zflfllflfl)
LCD . Kx(Z@111@)
LCD. xx (KNEW)
' Define
' Zflfllflfl
' Zfllllfl
' Zflflflflfl
' Pause for FullDuplexSerial‘spin xo
custom characxer 2
u
«
inlxlallze
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 6 of 11
Propeller™ P8X32A Example Code
Define a custom character using the code example below. First, set the baud rate on your Serial LCD to
19,200. Then, load the code below into your Propeller and load RAM or EEPROM. You will see a diamond
character appear on the screen. Note: the FullDuplexSerial.spin object is included with the Propeller Tool
software.
{{
Serial_LCD_Custom_Character.spin
For Parallax Serial LCDs 27976, 27977, 27979
}}
CON
_clkmode = xtal1 + pll16x
_xinfreq = 5_000_000
TX_PIN = 0
BAUD = 19_200
OBJ
LCD : "FullDuplexSerial.spin"
PUB Main
LCD.start(TX_PIN, TX_PIN, %1000, 19_200)
waitcnt(clkfreq / 100 + cnt) ' Pause for FullDuplexSerial.spin to initialize
LCD.tx(250) ' Define custom character 2
' Now send the eight data bytes
LCD.tx(%00000) ' %00000 =
LCD.tx(%00100) ' %00100 = *
LCD.tx(%01110) ' %01110 = * * *
LCD.tx(%11111) ' %11111 = * * * * *
LCD.tx(%01110) ' %01110 = * * *
LCD.tx(%00100) ' %00100 = *
LCD.tx(%00000) ' %00000 =
LCD.tx(%00000) ' %00000 =
LCD.tx(2) ' Display the new custom character 2
Playing Music
The Serial LCD has a built-in piezoelectric speaker which can play musical notes. The LCD includes a
sophisticated music player enabling users to program songs and tunes. You can play musical notes by
sending three types of note commands (Dec 214 to 232), as shown in the command set table.
Set Length
The “set length” commands (Dec 208 to 214) determines the length of time each note will play for. This
value remains the same until another “set length” command is received. A note’s length can range from
a 1/64th note to a whole note. A whole note is 2 seconds long.
Backspace / Left , The cursor is moved one position to the left The
Right , The cursor is moved one position to the right The
command doesn't erase the character
Line Feed , The cursor is moved down one line. For the two i
LCD model, if on line 0 it goes to line 1. If on line 1, it wraps
around to line 0. The horizontal position remains the same.
Form Feed ,
entire displa
commandi
Carriage Return , For
is moved to position
position 0 on line 0‘
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 7 of 11
Set Scale
The “set scale” commands (Dec 215 to 219) determines the octave each note will play in. This value
remains the same until another “set scale” command is received. The current octave can be set to a
value between 3 and 7, and each octave consists of 12 notes. The frequency for each note and scale
combination is shown in the table below.
Scale A A# B C C# D D# E F F# G G#
3 220 233 247 262 277 294 311 330 349 370 392 415
4 440 466 494 523 554 587 622 659 698 740 784 831
5 880 932 988 1047 1109 1175 1245 1319 1397 1480 1568 1661
6 1760 1865 1976 2093 2217 2349 2489 2637 2794 2960 3136 3322
7 3520 3729 3951 4186 4435 4699 4978 5274 5588 5920 6272 6645
Play Note
The “play note” commands (Dec 220 to 232) play a single note for the currently set time and in the
currently set octave.
Command Set
The tables on the following pages list all of the valid Serial LCD commands. Commands marked as N/A
are invalid and are ignored. The lines of the LCD display are numbered starting from 0, with line 0 being
the top line. The character positions on each line are numbered starting from 0, with position 0 being the
leftmost position on the line.
Dec Hex Action
0 00 Display custom character 0
1 01 Display custom character 1
2 02 Display custom character 2
3 03 Display custom character 3
4 04 Display custom character 4
5 05 Display custom character 5
6 06 Display custom character 6
7 07 Display custom character 7
8 08
Backspace / Left - The cursor is moved one position to the left. The
command doesn’t erase the character.
9 09
Right - The cursor is moved one position to the right. The
command doesn’t erase the character.
10 0A Line Feed - The cursor is moved down one line. For the two line
LCD model, if on line 0 it goes to line 1. If on line 1, it wraps
around to line 0. The horizontal position remains the same.
Dec Hex Action
11 0B N/A
12 0C Form Feed - The cursor is moved to position 0 on line 0 and the
entire display is cleared. Users must pause 5mS after this
command.
13 0D
Carriage Return – For the two line LCD model, if on line 0 the cursor
is moved to position 0 on line 1. If on line 1, it wraps around to
position 0 on line 0.
14 - 16 0E - 10 N/A
17 11 Turn backlight on (only on models 27977, 27979)
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 8 of 11
Dec Hex Action
18 12 Turn backlight off (Default)
19 - 20 13 - 14 N/A
21 15 Turn the display off
22 16 Turn the display on, with cursor off and no blink
23 17 Turn the display on, with cursor off and character blink
24 18 Turn the display on, with cursor on and no blink (Default)
25 19 Turn the display on, with cursor on and character blink
26 - 31 1A - 1F N/A
32 - 127 20 - 7F Display ASCII characters. See the ASCII character set table.
128 80 Move cursor to line 0, position 0
129 81 Move cursor to line 0, position 1
130 82 Move cursor to line 0, position 2
131 83 Move cursor to line 0, position 3
132 84 Move cursor to line 0, position 4
133 85 Move cursor to line 0, position 5
134 86 Move cursor to line 0, position 6
135 87 Move cursor to line 0, position 7
136 88 Move cursor to line 0, position 8
137 89 Move cursor to line 0, position 9
138 8A Move cursor to line 0, position 10
139 8B Move cursor to line 0, position 11
140 8C Move cursor to line 0, position 12
141 8D Move cursor to line 0, position 13
142 8E Move cursor to line 0, position 14
143 8F Move cursor to line 0, position 15
144 90 Move cursor to line 0, position 16 (only on model 27979)
145 91 Move cursor to line 0, position 17 (only on model 27979)
146 92 Move cursor to line 0, position 18 (only on model 27979)
147 93 Move cursor to line 0, position 19 (only on model 27979)
148 94 Move cursor to line 1, position 0
149 95 Move cursor to line 1, position 1
150 96 Move cursor to line 1, position 2
151 97 Move cursor to line 1, position 3
152 98 Move cursor to line 1, position 4
153 99 Move cursor to line 1, position 5
154 9A Move cursor to line 1, position 6
155 9B Move cursor to line 1, position 7
156 9C Move cursor to line 1, position 8
Dec Hex Action
157 9D Move cursor to line 1, position 9
158 9E Move cursor to line 1, position 10
159 9F Move cursor to line 1, position 11
160 A0 Move cursor to line 1, position 12
161 A1 Move cursor to line 1, position 13
162 A2 Move cursor to line 1, position 14
163 A3 Move cursor to line 1, position 15
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 9 of 11
Dec Hex Action
164 A4 Move cursor to line 1, position 16 (only on model 27979)
165 A5 Move cursor to line 1, position 17 (only on model 27979)
166 A6 Move cursor to line 1, position 18 (only on model 27979)
167 A7 Move cursor to line 1, position 19 (only on model 27979)
168 A8 Move cursor to line 2, position 0 (only on model 27979)
169 A9 Move cursor to line 2, position 1 (only on model 27979)
170 AA Move cursor to line 2, position 2 (only on model 27979)
171 AB Move cursor to line 2, position 3 (only on model 27979)
172 AC Move cursor to line 2, position 4 (only on model 27979)
173 AD Move cursor to line 2, position 5 (only on model 27979)
174 AE Move cursor to line 2, position 6 (only on model 27979)
175 AF Move cursor to line 2, position 7 (only on model 27979)
176 B0 Move cursor to line 2, position 8 (only on model 27979)
177 B1 Move cursor to line 2, position 9 (only on model 27979)
178 B2 Move cursor to line 2, position 10 (only on model 27979)
179 B3 Move cursor to line 2, position 11 (only on model 27979)
180 B4 Move cursor to line 2, position 12 (only on model 27979)
181 B5 Move cursor to line 2, position 13 (only on model 27979)
182 B6 Move cursor to line 2, position 14 (only on model 27979)
183 B7 Move cursor to line 2, position 15 (only on model 27979)
184 B8 Move cursor to line 2, position 16 (only on model 27979)
185 B9 Move cursor to line 2, position 17 (only on model 27979)
186 BA Move cursor to line 2, position 18 (only on model 27979)
187 BB Move cursor to line 2, position 19 (only on model 27979)
188 BC Move cursor to line 3, position 0 (only on model 27979)
189 BD Move cursor to line 3, position 1 (only on model 27979)
190 BE Move cursor to line 3, position 2 (only on model 27979)
191 BF Move cursor to line 3, position 3 (only on model 27979)
192 C0 Move cursor to line 3, position 4 (only on model 27979)
193 C1 Move cursor to line 3, position 5 (only on model 27979)
194 C2 Move cursor to line 3, position 6 (only on model 27979)
195 C3 Move cursor to line 3, position 7 (only on model 27979)
196 C4 Move cursor to line 3, position 8 (only on model 27979)
197 C5 Move cursor to line 3, position 9 (only on model 27979)
198 C6 Move cursor to line 3, position 10 (only on model 27979)
199 C7 Move cursor to line 3, position 11 (only on model 27979)
200 C8 Move cursor to line 3, position 12 (only on model 27979)
201 C9 Move cursor to line 3, position 13 (only on model 27979)
202 CA Move cursor to line 3, position 14 (only on model 27979)
Dec Hex Action
203 CB Move cursor to line 3, position 15 (only on model 27979)
204 CC Move cursor to line 3, position 16 (only on model 27979)
205 CD Move cursor to line 3, position 17 (only on model 27979)
206 CE Move cursor to line 3, position 18 (only on model 27979)
207 CF Move cursor to line 3, position 19 (only on model 27979)
208 D0 Set note length to 1/64 note
Se‘ect the 3’d
Se‘ect the 4‘“
Se‘ect the 5‘“
Se‘ect the 6‘“
Se‘ect the 7‘“
Defme custom character 0‘ Thws command must be foHowed by
ewght data bytes
Defme custom cha
ewght data bytes
ewght data bytes
Defme custom cha
ewght data bytes
Defme custom cha
ewght data bytes
Defme custom character 6‘ Thws command must be foHowed by
Defme custom character 7‘ Thws command must be foHowed by
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 10 of 11
Dec Hex Action
209 D1 Set note length to 1/32 note
210 D2 Set note length to 1/16 note
211 D3 Set note length to 1/8 note
212 D4 Set note length to 1/4 note
213 D5 Set note length to 1/2 note
214 D6 Set note length to whole note (2 seconds)
215 D7 Select the 3rd scale (A = 220 Hz)
216 D8 Select the 4th scale (A = 440 Hz)
217 D9 Select the 5th scale (A = 880 Hz)
218 DA Select the 6th scale (A = 1760 Hz)
219 DB Select the 7th scale (A = 3520 Hz)
220 DC Play A note
221 DD Play A# note
222 DE Play B
223 DF Play C
224 E0 Play C#
225 E1 Play D
226 E2 Play D#
227 E3 Play E
228 E4 Play F
229 E5 Play F#
230 E6 Play G
231 E7 Play G#
232 E8 Pause for current note length (no sound)
233 - 247 E9 – F7 N/A
248 F8 Define custom character 0. This command must be followed by
eight data bytes.
249 F9 Define custom character 1. This command must be followed by
eight data bytes.
250 FA Define custom character 2. This command must be followed by
eight data bytes.
251 FB Define custom character 3. This command must be followed by
eight data bytes.
252 FC Define custom character 4. This command must be followed by
eight data bytes.
253 FD Define custom character 5. This command must be followed by
eight data bytes.
254 FE Define custom character 6. This command must be followed by
eight data bytes.
255 FF Define custom character 7. This command must be followed by
eight data bytes.
@©®®@®®®®®®®@@®E‘
.. ”GREASE g _,
6
7.. g CWT
3 EEO m: E
El iii'éxiv‘via'éfi? El
3| 2.550 8? 8:: s .. .. "Jamaal, E
fiéggn 35' 3x PAMLgx a“ E
0 As A M6 o
w
P0 D RX
5V
6ND Parallax LCD
Vss
Copyright © Parallax Inc. Parallax Serial LCDs (#27976, 27977, 27979) v3.1 3/11/2013 Page 11 of 11
Product Change Notice: Revision E and Earlier
If your Serial LCD Display does not have a piezospeaker on the back and looks similar to the image
above, please use the following information and specifications when using this product. All connections,
test code and commands remain the same, except for commands controlling the piezospeaker.
Key Specifications
Power requirements:
o Non-backlit: +5 VDC, 20 mA
o Backlit: +5 VDC, 20 mA (light off), 80 mA (light on)
Communication: Selectable asynchronous serial baud rates: 2400, 9600, 19200
Operating temperature: -4 to +158 °F (-20 to +70°C)
Dimensions: Board and LCD size and style may vary
o 2x16: Approx. 1.5 x 3.15 in (38 x 80 mm)
o 4x20: Approx. 2.4 x 3.9 in (60 x 100 mm)
REV E CAUTION: DO NOT PROVIDE A SIGNAL TO THE ‘RX’ PIN BEFORE APPLYING 5 VDC TO THE ‘5V’
PIN.
Revision History
Version 3.1: corrected current draw specification on Page 1 from 50 mA to 80 mA.