EPC 的 EPC9114 Quick Start Guide 规格书
EFFICIENT POWER CONVERSION l
Demonstration System
EPC9114
Quick Start Guide
EPC2107 and EPC2036
6.78 MHz, ZVS Class-D Wireless Power System
QUICK START GUIDE Demonstration System EPC9114
2 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
DESCRIPTION
The EPC9114 wireless power demonstration system is a high efficiency,
A4WP compatible, Zero Voltage Switching (ZVS), Voltage Mode class-D
wireless power transfer demonstration kit capable of delivering up to
10 W into a DC load while operating at 6.78 MHz (Lowest ISM band).
The purpose of this demonstration system is to simplify the evaluation
process of wireless power technology using eGaN® FETs.
The EPC9114 wireless power system comprises the three boards
(shown in Figure 1) namely:
1) A Source Board (Transmitter or Power Amplifier) EPC9510
2) A Class 2 A4WP compliant Source Coil (Transmit Coil)
3) A Category 3 A4WP compliant Device Coil with rectifier and DC
smoothing capacitor.
The amplifier board features the enhancement-mode half-bridge
field effect transistor (FET), the 100 V rated EPC2107 eGaN FET with
integrated synchronous bootstrap FET. The amplifier is configured for
single ended operation and includes the gate driver/s, oscillator, and
feedback controller for the pre-regulator that ensures operation for
wireless power control based on the A4WP standard. This allows for
testing compliant to the A4WP class 2 standard over the entire load
range of ±35j Ω. The pre-regulator features the 100 V rated 65 mΩ
EPC2036 as the main switching device for a SEPIC converter.
The amplifier is equipped with a pre-regulator controller that adjusts
the voltage supplied to the ZVS class D amplifier based on the limits
of 3 parameters; coil current, DC power delivered and maximum
voltage. The coil current has the lowest priority followed by the power
delivered with the amplifier supply voltage having the highest priority.
Changes in the device load power demand, physical placement of the
device on the source coil and other factors such as metal objects in
proximity to the source coil all contribute to variations in coil current,
DC power and amplifier voltage requirements. Under any conditions,
the controller will ensure the correct operating conditions for the ZVS
class D amplifier based on the A4WP standard.
The pre-regulator can be bypassed to allow testing with custom control
hardware. The board further allows easy access to critical measurement
nodes that allow accurate power measurement instrumentation
hookup. A simplified diagram of the amplifier board is given in Figure 2.
The Source and Device Coils are Alliance for Wireless Power (A4WP)
compliant and have been pre-tuned to operate at 6.78 MHz with the
EPC9510 amplifier. The source coil is Class 2 and the device coil is
Category 3 compliant.
The device board includes a high frequency schottky diode based full
bridge rectifier and output filter to deliver a filtered unregulated DC
voltage. The device board comes equipped with two LED’s, one green
to indicate the power is being received with an output voltage equal
or greater than 4 V and a second red LED that indicates that the output
voltage has reached the maximum and is above 37 V.
For more information on the EPC2107 and EPC2036 eGaN FETs please
refer to the datasheet available from EPC at www.epc-co.com. The
datasheet should be read in conjunction with this quick start guide.
The Source coil used in this wireless power transfer demo system is
provided by NuCurrent (nucurrent.com). Reverse Engineering of the
Source coil is prohibited and protected by multiple US and international
patents. For additional information on the source coil, please contact
NuCurrent direct or EPC for contact information.
MECHANICAL ASSEMBLY
The assembly of the EPC9114 Wireless Demonstration kit is simple and
shown in Figure 1. The source coil and amplifier have been equipped
with SMA connectors. The source coil is simply connected to the amplifier.
The device board does not need to be mechanically attached to the
source coil.
DETAILED DESCRIPTION
The Amplifier Board (EPC9510)
Figure 2 shows the system block diagram of the EPC9510 ZVS class-D
amplifier with pre-regulator and Figure 3 shows the details of the ZVS
class-D amplifier section. The pre-regulator is used to control the ZVS
class-D wireless power amplifier based on three feedback parameters
1) the magnitude of the coil current indicated by the green LED, 2) the
DC power drawn by the amplifier indicated by the yellow LED and 3)
a maximum supply voltage to the amplifier indicated by the red LED.
Only one parameter at any time is used to control the pre-regulator
with the highest priority being the maximum voltage supplied to the
amplifier followed by the power delivered to the amplifier and lastly the
magnitude of the coil current. The maximum amplifier supply voltage
is pre-set to 66 V and the maximum power drawn by the amplifier is
pre-set to 10 W. The coil current magnitude is pre-set to 580 mARMS,
but can be made adjustable using P25. The pre-regulator comprises a
SEPIC converter that can operate at full power from 17 V through 24 V.
50 mm
80 mm
Amplifier Board
Source Coil
Device Board
150 mm
103 mm
57 mm
47 mm
Figure 1: EPC9114
Demonstration System
h—n-i
The prerregulamr can be bypassed by connecting khe posikive
aving
sikive
aced
by
nce
er.
d
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 3
The pre-regulator can be bypassed by connecting the positive
supply directly to the ZVS class-D amplifier supply after removing
the jumper at location JP1 and connecting the main positive
supply to the bottom pin. JP1 can also be removed and replaced
with a DC ammeter to directly measure the current drawn by
the amplifier. When doing this observe a low impedance
connection to ensure continued stable operation of the controller.
Together with the Kelvin voltage probes (TP1 and TP2) connected
to the amplifier supply, an accurate measurement of the power
drawn by the amplifier can be made.
The EPC9510 is also provided with a miniature high efficiency
switch-mode 5 V supply to power the logic circuits on board such as
the gate drivers and oscillator.
The amplifier comes with its own low supply current oscillator that is
pre-programmed to 6.78 MHz ± 678 Hz. It can be disabled by placing
a jumper into JP70 or can be externally shutdown using an externally
controlled open collector / drain transistor on the terminals of JP70
(note which is the ground connection). The switch needs to be capable
of sinking at least 25 mA. An external oscillator can be used instead
of the internal oscillator when connected to J70 (note which is the
ground connection) and the jumper (JP71) is removed.
The pre-regulator can also be disabled in a similar manner as the oscillator
using JP50. However, note that this connection is floating with respect to
the ground so removing the jumper for external connection requires a
floating switch to correctly control this function. Refer to the datasheet of
the controller IC and the schematic in this QSG for specific details.
The EPC9510 is provided with 3 LED’s that indicate the mode of
operation of the system. If the system is operating in coil current limit
mode, then the green LED will illuminate. For power limit mode, the
yellow LED will illuminate. Finally, when the pre-regulator reaches
maximum output voltage the red LED will illuminate indicating that
the system is no longer A4WP compliant as the load impedance
is too high for the amplifier to drive. When the load impedance
is too high to reach power limit or voltage limit mode, then the current
limit LED will illuminate incorrectly indicating current limit mode. This
mode also falls outside the A4WP standard and by measuring the
amplifier supply voltage across TP1 and TP2 will show that it has nearly
reach the maximum value limit.
ZVS Timing Adjustment
Setting the correct time to establish ZVS transitions is critical
to achieving high efficiency with the EPC9510 amplifier. This
can be done by selecting the values for R71 and R72 or P71
and P72 respectively. This procedure is best performed using a
potentiometer installed at the appropriate locations that is used to
determine the fixed resistor values. The timing MUST initially be set
WITHOUT the source coil connected to the amplifier. The timing
diagrams are given in Figure 10 and should be referenced when
following this procedure. Only perform these steps if changes have
been made to the board as it is shipped preset. The steps are:
1. With power off, remove the jumper in JP1 and install it into JP50 to
place the EPC9510 amplifier into Bypass mode. Connect the main input
power supply (+) to JP1 (bottom pin – for bypass mode) with ground
connected to J1 ground (-) connection.
2. With power off, connect the control input power supply bus (19 V) to
(+) connector J1. Note the polarity of the supply connector.
3. Connect a LOW capacitance oscilloscope probe to the probe-hole of
the half-bridge to be set and lean against the ground post as shown in
Figure 9.
4. Turn on the control supply – make sure the supply is approximately 19 V.
5. Turn on the main supply voltage starting at 0 V and increasing to the
required predominant operating value (such as 24 V but NEVER exceed
the absolute maximum voltage of 66 V).
6. While observing the oscilloscope adjust the applicable
potentiometers to so achieve the green waveform of Figure 10.
7. Replace the potentiometers with fixed value resistors if required.
Remove the jumper from JP50 and install it back into JP1 to revert the
EPC9510 back to pre-regulator mode.
Table 2: Performance Summary (TA = 25 °C) Category 3 Device Board
Symbol Parameter Conditions Min Max Units
VOUT Output Voltage Range 0 38 V
IOUT Output Current Range 0 1.5# A
# Actual maximum current subject to operating temperature limits
* Maximum current depends on die temperature – actual maximum current will be subject to switching
frequency, bus voltage and thermals.
Table 1: Performance Summary (TA = 25°C) EPC9510
Symbol Parameter Conditions Min Max Units
VIN
Bus Input Voltage Range – Pre-
Regulator Mode
Also used in
bypass mode
for logic supply
17 24 V
VIN
Amp Input Voltage Range – Bypass
Mode 0 80 V
VOUT Switch Node Output Voltage 66 V
IOUT Switch Node Output Current (each) 0.8* A
Vextosc External Oscillator Input Threshold Input ‘Low’ -0.3 0.8 V
Input ‘High’ 2.4 5 V
VPre_Disable
Pre-regulator Disable
Voltage Range Floating -0.3 5.5 V
IPre_Disable
Pre-regulator Disable
Current Floating -10 10 mA
VOsc_Disable
Oscillator Disable
Voltage Range
Open Drain/
Collector -0.3 5 V
IOsc_Disable
Oscillator Disable
Current
Open Drain/
Collector -25 25 mA
VSgnDiff Differential or Single Select Voltage Open Drain/
Collector -0.3 5.5 V
ISgnDiff Differential or Single Select Current Open Drain/
Collector -1 1 mA
QUICK START GUIDE Demonstration System EPC9114
4 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
LZVS = ∆tvt
8 ∙ fsw∙ COSSQ + Cwell
COSSQ =
VAMP
∙
∫
0
VAMP
COSS (v) ∙ dv
1
Determining component values for LZVS
The ZVS tank circuit is not operated at resonance, and only provides the
necessary negative device current for self-commutation of the output
voltage at turn off. The capacitor CZVS1 is chosen to have a very small
ripple voltage component and is typically around 1 µF. The amplifier
supply voltage, switch-node transition time will determine the value of
inductances for LZVS1 and LZVS2 which needs to be sufficient to maintain
ZVS operation over the DC device load resistance range and coupling
between the device and source coil range and can be calculated using
the following equation:
(1)
Where:
Δtvt = Voltage transition time [s]
ƒSW = Operating frequency [Hz]
COSSQ = Charge equivalent device output capacitance [F].
Cwell = Gate driver well capacitance [F]. Use 20 pF for the LM5113
NOTE. the amplifier supply voltage VAMP is absent from the equation as it
is accounted for by the voltage transition time. The COSS of the EPC2107
eGaN FETs is very low and lower than the gate driver well capacitance
Cwell which as a result must be now be included in the ZVS timing
calculation. The charge equivalent capacitance can be determined using
the following equation:
(2)
To add additional immunity margin for shifts in coil impedance, the value
of LZVS can be decreased to increase the current at turn off of the devices
(which will increase device losses). Typical voltage transition times range
from 2 ns through 12 ns.
The Source Coil
Figure 4 shows the schematic for the source coil which is Class 2 A4WP
compliant. The matching network includes both series and shunt tuning.
The matching network series tuning is differential to allow balanced
connection and voltage reduction for the capacitors.
The Device Board
Figure 5 shows the basic schematic for the device coil which is Category
3A4WP compliant. The matching network includes both series and
shunttuning. The matching network series tuning is differential to
allow balanced connection and voltage reduction for the capacitors.
The device board comes equipped with a kelvin connected output
DC voltage measurement terminal and a built in shunt to measure the
output DC current. Two LEDs have been provided to indicate that the
board is receiving power with an output voltage greater than 4 V (green
LED) and that the board output voltage limit has been reached (greater
than 36 V using the red LED).
QUICK START PROCEDURE
The EPC9114 demonstration system is easy to set up and evaluate the
performance of the eGaN FET in a wireless power transfer application.
Refer to Figure 1 to assemble the system and Figures 6 through 8 for
proper connection and measurement setup before following the
testing procedures.
The EPC9510 can be operated using any one of two alternative
methods:
a. Using the pre-regulator.
b. By-passing the pre-regulator.
a. Operation using the pre-regulator
The pre-regulator is used to supply power to the amplifier in this mode
and will limit the coil current, power delivered or maximum supply
voltage to the amplifier based on the pre-determined settings.
The main 19 V supply must be capable of delivering 2 ADC. DO NOT
turn up the voltage of this supply when instructed to power up
the board, instead simply turn on the supply. The EPC9510 board
includes a pre-regulator to ensure proper operation of the board
including start up.
1. Make sure the entire system is fully assembled prior to making
electrical connections and make sure jumper JP1 is installed. Also
make sure the source coil and device coil with load are connected.
2. With power off, connect the main input power supply bus to J1 as
shown in Figure 7. Note the polarity of the supply connector.
3. Make sure all instrumentation is connected to the system.
4. Turn on the main supply voltage to the required value (19 V).
5. Once operation has been confirmed, observe the output voltage,
efficiency and other parameters on both the amplifier and
device boards.
6. For shutdown, please follow steps in the reverse order.
b. Operation bypassing the pre-regulator
In this mode, the pre-regulator is bypassed and the main power is
connected directly to the amplifier. This allows the amplifier to be
operated using an external regulator. In this mode there is no protection
for ensuring the correct operating conditions for the eGaN FETs.
1. Make sure the entire system is fully assembled prior to making
electrical connections and make sure jumper JP1 has been removed
and installed in JP50 to disable the pre-regulator and place the
EPC9510 in bypass mode. Also make sure the source coil and device
coil with load are connected.
2. With power off, connect the main input power supply bus to the
bottom pin of JP1 and the ground to the ground connection of J1 as
shown in Figure 7.
3. With power off, connect the control input power supply bus to J1.
Note the polarity of the supply connector. This is used to power the
gate drivers and logic circuits.
4. Make sure all instrumentation is connected to the system.
5. Turn on the control supply – make sure the supply is 19 V range.
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 5
6. Turn on the main supply voltage to the required value (it is
recommended to start at 0 V and do not exceed the absolute
maximum voltage of 80 V).
7. Once operation has been confirmed, adjust the main supply voltage
within the operating range and observe the output voltage, efficiency
and other parameters on both the amplifier and device boards.
8. For shutdown, please follow steps in the reverse order. Start by
reducing the main supply voltage to 0 V followed by steps 6 through 2.
NOTE.
1. When measuring the high frequency content switch-node (Source Coil Voltage), care
must be taken to avoid long ground leads. An oscilloscope probe connection (preferred
method) has been built into the board to simplify the measurement of the Source Coil
voltage (shown in Figure 9).
2. You may experience audible noise emanating from the inductor of the SEPIC converter.
This is due to a minor instability. This minor instability does not impact the performance
of the power amplifier or the protection circuitry of the system.
3. AVOID using a Lab Benchtop programmable DC as the load for the category 3 device
board. These loads have low control bandwidth and will cause the EPC9114 system to
oscillate at a low frequency and may lead to failure. It is recommended to use a fixed low
inductance resistor as an initial load. Once a design matures, a post regulator, such as a
Buck converter, can be used.
THERMAL CONSIDERATIONS
The EPC9114 demonstration system showcases the EPC2107 and
EPC2036 eGaN FETs in a wireless energy transfer application. Although
the electrical performance surpasses that of traditional silicon devices,
their relatively smaller size does magnify the thermal management
requirements. The operator must observe the temperature of the gate
driver and eGaN FETs to ensure that both are operating within the
thermal limits as per the datasheets.
NOTE. The EPC9114 demonstration system has limited current protection only when
operating off the Pre-Regulator. When bypassing the pre-regulator there is no current
protection on board and care must be exercised not to over-current or over-temperature
the devices. Excessively wide coil coupling and load range variations can lead to increased
losses in the devices.
Pre-Cautions
The EPC9114 demonstration system has no enhanced protection
systems and therefore should be operated with caution. Some specific
precautions are:
1. Never operate the EPC9114 system with a device board that is A4WP
compliant as this system does not communicate with the device to
correctly setup the required operating conditions and doing so can
lead to failure of the device board. Contact EPC should operating
the system with an A4WP compliant device is required to obtain
instructions on how to do this. Please contact EPC at info@epc-co.com
should the tuning of the coil be required to change to suit specific
conditions so that it can be correctly adjusted for use with the ZVS
class-D amplifier.
2. There is no heat-sink on the devices and during experimental
evaluation it is possible present conditions to the amplifier that may
cause the devices to overheat. Always check operating conditions and
monitor the temperature of the EPC devices using an IR camera.
3. Never connect the EPC9510 amplifer board into your VNA in an
attempt to measure the output impedance of the amplifier. Doing so
will severely damage the VNA.
Figure 3: Diagram of EPC9510 amplifier circuit
+
V
AMP
Q1
Q2
CZVS
LZVS
Coil
Connection
Pre-
Regulator
Pre-Regulator
Jumper
JP1
J1
VIN
Bypass Mode
Connection
Figure 2: Block diagram of the EPC9510 wireless power amplifier
X
IAMP P
AMP
VAMP
Icoil
|Icoil |
19 V
SEPIC
Pre-Regulator
ZVS Class-D
Amplifier
Control Reference Signal
Combiner
DC
C
Coil
S
1 V –
DC
66 VDC
Amplifier
women, image;
5 sores‘o
QUICK START GUIDE Demonstration System EPC9114
6 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
Source Coil
Coil
Connection
Matching
Impedance
Network
Class 2
Coil
Figure 4: Basic schematic of the A4WP Class 2 Source Coil
Un-Regulated
DC output
Matching
Impedance
Network
Cat. 3
Coil
Device Board
Figure 5: Basic Schematic of the A4WP Category 3 Device Board
Figure 6: Proper Connection and Measurement Setup for the Amplifier Board
17-24 VDC
VIN Supply
(Note Polarity)
Source Coil
Connection
External
Oscillator
Switch-node Main
Oscilloscope Probe
Ground Post
Voltage
Source Jumper
Disable
Oscillator
Jumper
Disable Pre-Regulator
Jumper
Coil Current Setting
Amplifier
Timing Setting
(Not Installed)
+
Pre-Regulator Jumper
Bypass Connection
Operating Mode LED
Indicators
Ground Post
Amplifier
Supply Voltage
(0 V – 80 Vmax.)
V
Switch-node
Pre-Regulator
Oscilloscope probe
Internal Oscillator
Selection Jumper
Makdlin
; W m
Erna Nu uc mm mm
>5VLED
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 7
Figure 8: Proper connection and measurement setup for the device board
Standoffs for Mechanical
attachment to Source Coil
to these locations (x5)
Device Output
Voltage
(0 V – 38 V
max
)
A
V
mV
External Load
Connection
Matching
Device Output
Current
(300 m Shunt)
Output Voltage
> 5 V LED
Output Voltage
> 37 V LED
Load Current
(See Notes for details)
* ONLY to be used with
Shunt removed
Source Board
Connection
Matching with
trombone tuning
Figure 7: Proper connection for the source coil
Do not use
probe ground lead
A: "
, - ‘ I—
Illtpc‘fi‘kofémfi?:53thU
QUICK START GUIDE Demonstration System EPC9114
8 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
Figure 9: Proper Measurement of the Switch Nodes using the hole and ground post
Do not use
probe ground lead
Ground
probe
against
post
Place probe tip
in large via Minimize
loop
Figure 10: ZVS Timing Diagrams
Shoot-
through
Q2 turn-on
Q1 turn-off
VAMP
0
time
ZVS
Partial
ZVS
ZVS + Diode
Conduction
Shoot-
through
Q1 turn-on
Q2 turn-off
VAMP
0
time
ZVS
Partial
ZVS
ZVS + Diode
Conduction
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 9
Table 3: Bill of Materials - Amplifier Board
Item Qty Reference Part Description Manufacturer Part #
1 2 C1, C80 1 µF, 10 V TDK C1005X7S1A105M050BC
2 8 C2, C4, C51, C70, C71, C72, C81, C130 100 nF, 16 V Würth 885012205037
3 2 C3, C95 22 nF, 25 V Würth 885012205052
4 1 C5 DNP (100 nF, 16 V) Würth 885012205037
5 1 C20 DNP (10 nF, 50 V) Murata GRM155R71H103KA88D
6 1 C45 DNP (10 nF, 100 V) Murata C1005X7S2A103K050BB
7 1 C73 DNP (22 pF, 50 V) Würth
8 1 C133 DNP (1 nF, 50 V) Murata
9 1 R20 DNP (10k) Panasonic ERJ-2GEJ103X
10 1 R45 DNP (1.5k) Panasonic ERJ-2RKF1501X
11 5 C6, C7, C31, C44, C82 22 pF, 50 V Würth 885012005057
12 2 C11, C12 10 nF, 100 V TDK C1005X7S2A103K050BB
13 3 C15, C64, C65 2.2 µF, 100 V Taiyo Yuden HMK325B7225KN-T
14 1 C21 680 pF, 50 V Murata GRM155R71H681KA01D
15 1 C22 1 nF, 50 V Murata GRM155R71H102KA01D
16 2 C30, C50 100 nF, 100 V Murata GRM188R72A104KA35D
17 1 C32 47 nF, 25 V Murata GRM155R71E473KA88D
18 2 C43, C53 10 nF, 50 V Murata GRM155R71H103KA88D
19 1 C52 100 pF Murata GRM1555C1H101JA01D
20 2 C61, C62 4.7 µF, 50 V
Taiyo Yuden UMK325BJ475MM-T
21 1 C63 10 µF, 35 V
Taiyo Yuden GMK325BJ106KN-T
22 3 C90, C91, C92 1 µF, 25 V Würth
885012206076
23 1 C131 1 nF, 50 V
Murata GRM1555C1H102JA01D
24 1 Czvs1 1 µF, 50 V
Würth 885012207103
25 2 D1, D95 40 V, 300 mA
ST BAT54KFILM
26 7 D2, D21, D40, D41, D42, D71, D72 40 V, 30 mA
Diodes Inc. SDM03U40
27 2 D3, D20 DNP (40 V, 30 mA)
Diodes Inc. SDM03U40
28 1 D4 5 V1, 150 mW
Bournes CD0603-Z5V1
29 1 D35 LED 0603 Yellow
Lite-On LTST-C193KSKT-5A
30 1 D36 LED 0603 Green
Lite-On LTST-C193KGKT-5A
31 1 D37 LED 0603 Red
Lite-On LTST-C193KRKT-5A
32 1 D60 100 V, 1A
On-Semi MBRS1100T3G
33 1 D90 40 V, 1A Diodes Inc. PD3S140-7
34 2 GP1, GP60 .1" mAle Vert. Würth 61300111121
35 1 J1 .156" mAle Vert. Würth 645002114822
36 1 J2 S mA Board Edge Linx CONSAM003.062
37 5 J70, JP1, JP50, JP70, JP71 .1" mAle Vert. Würth 61300211121
38 1 L60 100 µH, 2.2A CoilCraft MSD1260-104ML
39 1 L80 10 µH, 150 mA Taiyo Yuden LBR2012T100K
40 1 L90 47 µH, 250 mA Würth 7440329470
41 1 Lsns 110 nH CoilCraft 2222SQ-111JE
42 2 Lzvs1, Lzvs2 390 nH CoilCraft 2929SQ-391JE
43 1 P25 DNP (10k) Murata PV37Y103C01B00
44 2 P71, P72 DNP (1k) Murata PV37Y102C01B00
45 1 Q1 100 V, 220 mΩ with SB EPC EPC2107
46 1 Q60 100 V, 65 mΩ EPC EPC2036
47 1 Q61 DNP (100 V, 6A, 30mΩ) EPC EPC2007C
48 2 R2, R82 20 Ω Stackpole RMCF0402JT20R0
49 1 R3 27 k Panasonic ERJ-2GEJ273X
50 1 R4 4.7 Ω Panasonic ERJ-2GEJ4R7X
51 1 R21 100k Panasonic ERJ-2GEJ104X
52 2 R25, R133 6.8k, 1% Panasonic ERJ-2RKF6801X
53 1 R26 2.8k, 1% Panasonic ERJ-2RKF2801X
54 1 R30 100 Ω Panasonic ERJ-3EKF1000V
55 1 R31 71k5, 1% Panasonic ERJ-6ENF7152V
(continued on next page)
QUICK START GUIDE Demonstration System EPC9114
10 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
Table 3: Bill of Materials - Amplifier Board (continued)
Item Qty Reference Part Description Manufacturer Part #
56 1 R32 8.2k, 1% Panasonic ERJ-2RKF8201X
57 1 R33 75k Panasonic ERJ-2GEJ753X
58 2 R35, R36 634 Ω Panasonic ERJ-2RKF6340X
59 1 R37 150k, 1% Panasonic ERJ-2RKF1503X
60 2 R38, R91 49.9k, 1% Panasonic ERJ-2RKF4992X
61 2 R40, R130 261k Panasonic ERJ-3EKF2613V
62 2 R41, R131 6.04k Panasonic ERJ-2RKF6041X
63 1 R42 24.9k Panasonic ERJ-2RKF2492X
64 1 R43 10.5k Panasonic ERJ-2RKF1052X
65 2 R44, R90 100k, 1% Panasonic ERJ-2RKF1003X
66 1 R50 10 Ω Panasonic ERJ-3EKF10R0V
67 1 R51 124k, 1% Panasonic ERJ-2RKF1243X
68 1 R52 71.5k, 1%
Panasonic ERJ-2RKF7152X
69 1 R53 1.00k Panasonic
ERJ-2RKF1001X
70 1 R54 0 Ω
Yageo RC0402JR-070RL
71 1 R60 80 mΩ, 0.4 W Vishay Dale
WSLP0603R0800FEB
72 1 R61 300 mΩ, 0.125 W
Vishay Dale RL0805FR-070R3L
73 1 R70 47k
Panasonic ERJ-2RKF4702X
74 1 R71 430 Ω
Panasonic ERJ-2RKF4300X
75 1 R72 180 Ω
Panasonic ERJ-2RKF1800X
76 1 R73 10k
Panasonic ERJ-2GEJ103X
77 1 R80 2.2 Ω
Yageo RC0402JR-072R2L
78 1 R92 9.53k 1%
Panasonic ERJ-2RKF9531X
79 1 R132 18k 1% Panasonic ERJ-2RKF1802X
80 1 R134 470k Panasonic ERJ-2RKF4703X
81 2 TP1, TP2 SMD Probe Loop Keystone 5015
82 1 Tsns 10 µH, 1:1, 96.9% CoilCraft PFD3215-103ME
83 1 U1 100 V, eGaN Driver
Texas Instruments LM5113TM
84 1 U30 Power & Current Monitor
Linear LT2940IMS#PBF
85 1 U50 Boost Controller
Texas Instruments LM3478MAX/NOPB
86 1 U70 Programmable Oscillator
KDS Daishinku DSO221SHF 6.780
87 1 U71 2 In NAND
Fairchild NC7SZ00L6X
88 1 U72 2 In AND Fairchild NC7SZ08L6X
89 1 U80 Gate Driver with LDO Texas Instruments UCC27611DRV
90 1 U90 1.4 MHz, 24 V, 0.5 A Buck MPS MP2357DJ-LF
91 1 U130 Comparator Texas Instruments TLV3201AIDBVR
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 11
Table 4: Bill of Materials - Source Coil
Item Qty Reference Part Description Manufacturer Part #
1 1 Ctrombone 470 pF, 300 V Vishay VJ1111D471KXLAT
2 1 C1 3.3 pF, 1500 V Vishay VJ1111D3R3CXRAJ
3 1 C2 3.3 pF, 1500 V Vishay VJ1111D3R3CXRAJ
4 1 C3 390 pF, 630 V Vishay VJ1111D391KXLAT
5 1 PCB1 Class 2 Coil Former NuCurrent R42DMTxD1
6 1 J1 SMA PCB Edge Linx CONREVSMA003.031
Table 5: Bill of Materials - Device Board
Item Qty Reference Part Description Manufacturer Part #
1 1 C84 100 nF, 50 V Murata GRM188R71H104KA93D
2 1 C85 10 µF, 50 V Murata GRM32DF51H106ZA01L
3 1 PCB1 Cat3PRU Coastal Circuits Cat3DeviceBoard
4 2 CM1, CM11 470 pF Vishay VJ1111D471KXLAT
5 4 CM2, CM12, CMP1, CMP2 DNP
– –
6 4 CM5, CM7, CMP3, CMP4 DNP
– –
7 1 CM6 56 pF Vishay VJ0505D560JXPAJ
8 1 CM8 68 pF Vishay VJ0505D680JXPAJ
9 4 D80, D81, D82, D83 40 V, 1 A Diodes Inc. PD3S140-7
10 1 D84 LED 0603 Green Lite-On LTST-C193KGKT-5A
11 1 D85 2.7 V 250 mW NXP BZX84-C2V7,215
12 1 D86 LED 0603 Red Lite-On LTST-C193KRKT-5A
13 1 D87 33 V, 250 mW NXP BZX84-C33,215
14 2 J81, J82 .1" Male Vert. Würth 61300211121
15 2 LM1, LM11 82 nH Würth 744912182
16 1 R80 300 mΩ, 1 W Stackpole CSRN2512FKR300
17 1 R81 4.7k Ω Stackpole RMCF1206FT4K70
18 1 R82 422 Ω Yageo RMCF0603FT422R
19 4 TP1, TP2, TP3, TP4 SMD Probe Loop Keystone 5015
20 1 JPR1 Wire Jumper at CM11
– –
EPC would like to acknowledge Würth Electronics (www.we-online.com/web/en/wuerth_elektronik/start.php), Coilcraft (www.coilcraft.com), and KDS Daishinku America (www.kdsamerica.com) for their support of this project.
QUICK START GUIDE Demonstration System EPC9114
12 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
Figure 11: EPC9510-ZVS class-D schematic
19 V 1 Amax
VIN
5 V
VOUT
GND
Icoil
PreRegulator
EPC9510PR_R1_0.SchDoc
VIN
5 V
VOUT
Pre-Regulator
SDM03U40
40 V 30 mA
D71
5 V
5 V
5 V
Deadtime Fall
Deadtime Rise
1k
P71
A
B
U71
NC7SZ00L6X
A
B
Y
U72
NC7SZ08L6X
5 V
DSO221SHF 6.780
4
2
GND
OUT3
OE
1VCC
U70
5 V
5 V
Oscillator
IntOsc
5 V
5 V
Logic Supply Regulator
VIN
OSC
OSC
OSC
.1" Male Vert.
1
2
JP70
Oscillator Disable
OSCIntOsc
.1" Male Vert.
1
2
J70
External Oscillator
Internal / External Oscillator
SDM03U40
40 V 30 mA
D72
1k
P72
TBD
1 2
R72
OSC
H_Sig1
L_S ig1
OSC
.1" Male Vert.
1
2
JP71
OutA
ZVS Tank Circuit
1
2
.156" Male Vert.
J1
VIN
Main SupplyVAMP
VOUT
SMA Board Edge
J2
Pre-Regulator Disconnect
SMD probe loop
1
TP1
SMD probe loop
1
TP2
VAMP
VAMP
5 V
GND
LIN
OUTHIN
a
EPC9510_SE_ZVSclassD_Rev1_0.S chDoc
TBD
Lzvs1
VAMP
H_Sig1
L_S ig1
5 V
Jumper 100
JP10
110 nH
Lsns
Coil Current Sense
100k
1 2
R21
680 pF, 50 V
C21
SDM03U40
40 V 30 mA
D20
SDM03U40
40 V 30 mA
D21
Icoil
Icoil
TBD
1 2
R71
10 nF, 50 V
C20
10 nF, 50 V
C22
10k
12
R73
47k
1
2
R70
10k
12
R20
100 nF, 16 V
C72
100 nF, 16 V
C71
22 pF, 50 V
C73
EMPTY
1 µF, 25 V
C90
C92
1 µF 50 V
Czvs1
100 nF, 16 V
C70
Jumper 100
JP72
.1" Male Vert.
1
2
JP1
4
3
5
2
1
6
OSC
Reg
0.81V
GND
IN
FB
EN
DRV
CNTL
U90
MP2357DJ-LF
9.53k 1%
1
2
R92
49.9k 1%
12
R91
5 V
22 nF, 25 V
C95
47µH 250 mA
L90
100k 1%
1
2
R90
VIN
D95
BAT54KFILM
PD3S140-7
40 V 1 A
D90
1µF, 25 V 1µF, 25 V
C91
TBD
1
2
R26
TBD
1
2
R25
10k
P25
Current Adjust
1
2
10µH 1:1 96.9%
3
4
Tsns
FD1
Local Fiducials
FD2 FD3
L
g
F
a»
D A A
1H1; U‘u
H
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 13
Figure 12: EPC9510- Gate driver and power devices schematic
GU
5 VHS
5 VHS
5 V
GL
Gate Driver
U1
LM5113 TM
OUT
GU
GL
D1
BAT54KFILM
5 V
4.7 V
4.7 V
GL
20 Ω
12
R2
SDM03U40
D3
EMPTY Synchronous Bootstrap Power Supply
1µF, 10 V
C1
D4
CD0603-Z5 V1
Gbtst
27k
12
R3
D2
SDM03U40
22 nF, 25 V
C3
GND
5 V
OUT
VAMP
Out
GU
GL
Out
2.2µF, 100 V
C15
10 nF, 100 V
C11
10 nF, 100 V
C12
VAMP
VAMP
VAMP
VAMP
GND
HIN
LIN
HIN
LIN
1
Probe Hole
PH1
Ground Post
1
.1" Male Vert.
GP1
100 V, 220 mΩ with BS
Q1A
EPC2107
Q1B
EPC2107
4.7 Ω
1 2
R4
100 nF, 16 V
C2
100 nF, 16 V
C4
100 nF, 16 V
C5
EMPTY
22 pF
, 50 V
C6
22 pF, 50 V
C7
QUICK START GUIDE Demonstration System EPC9114
14 | | EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016
Figure 13: Pre-regulator schematic
100k 1%
12
R44
VIN
Isns
100 pF
C52
.1" Male Vert.
1
2
JP50
Pre-Regulator Disable
FA/SD
VOUT
VIN
Vsepic
5 V 5 VGD
5 VGD
GLPH
GLPL
Gate Driver
2.2 Ω
1 2
R80
GLPLGLPH
12
80 mΩ, 0.4 W
R60
SW
VIN
VIN
5 V
VOUT
GND
PreDR PWM
71.5k 1%
12
R52
124k 1%
1
2
R51
5 V
10 nF, 50 V
C53
Ground Post
4.7µF, 50 V
C62
4.7µF, 50 V
C61
2.2µF, 100 V
C64
5
4
UVLO
Osc
3
6
Pgnd
1.26 V
Cnt
FA/SD
FB
Comp
8
7
Agnd
Isens
VIN
2
1
DR
U50
LM3478 MAX/NOPB
0 Ω
1 2
R52
100 V, 1A
D60
MBRS110 0T3G
Vfdbk VIN
Isns
10µF, 35 V
C63
1
6
D
3
2
1.24V
12
8
7
9
CLR LE
Q
V-
V+
I-
I+
4
5
11
10
VCC
GND
UVLC
Latch Hi
Lo
CMPOUT
CMPOUT
Pmon
Imon
CMP+
U30
LT2940 IMS #PBF
1 2
300 mΩ, 0.125 W
R61
6
2
3EP
4
5
LDO
VREF
VSS
1VDD
U80
UCC27611DRV
75k
1 2
R33
D36
D35
Current Mode
Power Mode
Pmon
Imon
Vsepic VOUT
634 Ω
1 2
R35 5 V
8.2k 1%
1
2
R32
V+
Vsepic
Pcmp
DC Power Monitor
Isns
Isns
Isns
Pmon
Output Voltage Limit
Output Power Limit
Output Current Limit
SDM03U40
40 V, 30 mA
D40
SDM03U40
40 V, 30 mA
D41
24.9k
1 2
R42
Isns
2.2µF, 100V
C65
10 µH, 150 mA
L80
Isns
VOUT
Comp
100 Ω
1 2
R30
Icoil
100 nF, 100 V
C50
10 Ω
1 2
R50
1
.1" Male Vert.
GP60
1
ProbeHole
PH60
20 Ω
1 2
R82
100 nF, 16 V
C81
100 nF, 100 V
C30
22 pF, 50 V
C44
22 pF, 50 V
C82
22 pF, 50 V
C31
5 VGD
5 VGD
1µF, 10 V
C80
Pcmp
49.9k 1%
1
2
R38
6.04k
12
R41
10.5k
1
2
R43
150k 1%
12
R37
261k
1 2
R40
SDM03U40
40 V, 30 mA
D42
4
3
1
52
U130
TLV3201AIDBVR
100 nF, 16 V
C130
D37
634 Ω
1 2
R36
5 V
5 V
Voltage Mode
VOUT
Vom
Pled
Iled
100 V, 65 mΩ
Q60
EPC2036
EP C2007C
100 V, 6 A, 30 mΩ
Q61
GLPL
10nF, 50 V
C43
12
71k5 1%
R31
1
3
100 µH, 2.2 A
4
2
L60
1.5k
1 2
R45
EMPTY
10 nF, 100 V
C45
EMPTY
47nF, 25 V
C32
18k 1%
12
R132
6.8k 1%
12
R133
470k
1 2
R134
5 V
6.04k
12
R131
261k
12
R130
1nF, 50 V
C131
1nF, 50 V
C133
EMPTY
1.00k
1 2
R53
100 nF, 16 V
C51
VOUT
Vfdbk
QUICK START GUIDE Demonstration System EPC9114
EPC – EFFICIENT POWER CONVERSION CORPORATION | WWW.EPC-CO.COM | COPYRIGHT 2016 | | 15
Figure 14: Class 2 Source Board Schematic
Figure 15: Category 3 device board schematic
C1
3.3 pF 1111
C2
3.3 pF 1111
SMA PCB
Edge
J1
Ctrombone
Adjust on trombone
Amplifier
Connection
470 pF 1111
390 pF 1111
C3
Coil Matching Cl1
Cls2PTU
40 V, 1 A
D80
40 V, 1A
D82
40 V, 1 A
D81
40 V, 1 A
D83
10 µF, 50 V
C85
VRECT
100 nF, 50V
C84
VRECT VRECT VOUT
VOUT
1 2
300 mΩ,1W
R80
.1" Male Vert.
1
2
J81
RX Coil
SMD probe loop
1
TP1
SMD probe loop
1
TP2
Kelvin Output Current
SMD probe loop
1
TP3
SMD probe loop
1
TP4
VOUT
.1" Male Vert.
1
2
J82
Output
Cat3PRU
Cl1
DNP
CMP1
CM1
470 pF
470 pF
CM 11
CM 2
DNP
DNP
CM 12
DNP
CMP2
Kelvin Output Voltage
Shunt Bypass
LM 1
LM 11
82 nH
82 nH
Matching
CMP3
DNPCM P4
DNP pF
CM 5
DNP
CM 6
56 pF
CM 7
DNP
CM 8
68 pF
4.7k
12
R81
Receive Indicator Over-Voltage Indicator
422 Ω
12
R82
LED 0 603
Green
D84
LED 0 603 Red
D86
VOUT > 4 V VOUT > 36 V
2.7 V, 250 mW 250 mW
D85
33 V,
D87
EFFIEIENT POWER (ONVERSION l
Demonstration Board Notification
The EPC9114 board is intended for product evaluation purposes only and is not intended for commercial use. Replace components on the Evaluation Board only with those parts shown on
the parts list (or Bill of Materials) in the Quick Start Guide. Contact an authorized EPC representative with any questions.
This board is intended to be used by certified professionals, in a lab environment, following proper safety procedures. Use at your own risk.
As an evaluation tool, this board is not designed for compliance with the European Union directive on electromagnetic compatibility or any other such directives or regulations. As board
builds are at times subject to product availability, it is possible that boards may contain components or assembly materials that are not RoHS compliant. Efficient Power Conversion
Corporation (EPC) makes no guarantee that the purchased board is 100% RoHS compliant.
The Evaluation board (or kit) is for demonstration purposes only and neither the Board nor this Quick Start Guide constitute a sales contract or create any kind of warranty, whether express
or implied, as to the applications or products involved.
Disclaimer: EPC reserves the right at any time, without notice, to make changes to any products described herein to improve reliability, function, or design. EPC does not assume any liability
arising out of the application or use of any product or circuit described herein; neither does it convey any license under its patent rights, or other intellectual property whatsoever, nor the
rights of others.
EPC Products are distributed through Digi-Key.
www.digikey.com
For More Information:
Please contact info@epc-co.com
or your local sales representative
Visit our website:
www.epc-co.com
Sign-up to receive
EPC updates at
bit.ly/EPCupdates
or text “EPC” to 22828