Silicon Labs 的 EFM32 Getting Started Appl Note 规格书
SILIEEIN LABS
#‘fi' E'Hflmw"
mam-an m
Khruogmuplomm} nag V=D “D
. gumrwmmflwwmm‘ a , ‘
,, QM“, - :gkfugumm k
- i: mam ammo" :x-v
D Em - gm." mm m,
1) 9mm ‘ 9mm. 1 u
I, m 17mm ‘ 9mm um.
- «mm (awnam 2m. mm m, rm Milkmmqm
- mam" is mm «0 mm N «his mum m .ny WM.
- mm": mm .1 mummy”; .nd «a an" n and m inrilm: a.
‘ mm, mm m m mm. mumm-
‘ 1. m my" a m; Wm M m n. mm W. m m
‘ m... m: m m. w. my“) ”mm.
- 2. mm mm mm .5. a: m...» mm .5 m, m m m h!
- mama .5 m: m: mm. m".
- 3. m mm may m k mm w mm (w. my mm “mm“...
- msnnnn a; wwlefl-lm w mum 5mm uh, m m
‘ mum“. H, mm m; Wm” mm." L.“ x; mm". m
‘ WW. as 15-, m m mm; m Mug "mm; a. .ny um,
‘ “(1-4an m m mm m, my mm mmm w
‘ M mm; m m, vir‘uzular mm w “mm” mm Mun-Fm
- w my menmnj mm; w . mm party.
- Dulce :1 1; Oulline \ = n In Frau-m: mwsemn \a-cm Hwevavchy a mum V = D
'smzxxa-EEJWW .
. q, ”Varanmmm Iran-bran Ram-u M Ivar-m Tm
p Managua-mlnlmrm)
4 ‘
‘wmhu ‘WM ‘1,
AN0009.0: Getting Started with EFM32 and
EZR32 Series 0
This application note introduces the software examples, libraries,
documentation, and software tools available for EFM32 and
EZR32 Series 0.
In addition to providing a basic introduction to the tools available for these devices, this
document includes several basic firmware exercises to familiarize the reader with the
Starter Kit hardware, the emlib firmware library, and the Simplicity Studio software
tools.
Note that this document focuses on the MCU portion of the devices. For wireless prod-
ucts (EZR32), see the additional wireless getting started information available in the
user guide specifically for the product. More information on the hardware for any prod-
uct can be found in the kit user guide. More information about Simplicity Studio in gen-
eral can be found in AN0822: Simplicity Studio™ User Guide. Application notes can be
found on the Silicon Labs website (www.silabs.com/32bit-appnotes) or in Simplicity
Studio.
KEY POINTS
• Simplicity Studio contains everything
needed to develop with EFM32 and
EZR32 Series 0.
• Things you will learn:
• Basic register operation
• Using emlib functions
• Blinking LEDs and reading buttons
• LCD controller
• Energy Modes
• Real-Time Counter operation
silabs.com | Building a more connected world. Rev. 1.22
1. Device Compatibility
This application note supports multiple device families, and some functionality is different depending on the device.
MCU Series 0 consists of:
• EFM32 Gecko (EFM32G)
• EFM32 Giant Gecko (EFM32GG)
• EFM32 Wonder Gecko (EFM32WG)
• EFM32 Leopard Gecko (EFM32LG)
• EFM32 Tiny Gecko (EFM32TG)
• EFM32 Zero Gecko (EFM32ZG)
• EFM32 Happy Gecko (EFM32HG)
Wireless MCU Series 0 consists of:
• EZR32 Wonder Gecko (EZR32WG)
• EZR32 Leopard Gecko (EZR32LG)
• EZR32 Happy Gecko (EZR32HG)
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Device Compatibility
silabs.com | Building a more connected world. Rev. 1.22 | 2
2. Introduction
2.1 Prerequisites
The examples in this application note require access to a supported Silicon Labs device. Supported devices include the EFM32 Series
0 Starter Kit. Before working on this tutorial, ensure a compatible IDE is available by either:
• Installing Simplicity Studio from Silabs.com (http://www.silabs.com/simplicity), or
• If IAR is preferred, install the latest Segger J-Link drivers to support the kit (https://www.segger.com/jlink-software.html)
In Simplicity Studio, ensure that all the available packages are installed and up to date by clicking on the [Update Software] button at
the top-left of the main window:
Note: While Simplicity Studio includes a fully-functional integrated IDE, it also supports some third party IDEs, including IAR. For this
reason, it is recommended to install Simplicity Studio regardless of the preferred IDE for easy access to these examples as well as the
full suite of features provided to facilitate development of EFM32 and EZR32 Series 0 solutions.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Introduction
silabs.com | Building a more connected world. Rev. 1.22 | 3
EFM32 Giant Gecko Starter Kit (EFM3ZGG-STK3700)
“maximum “autumn-[Wm
M Mm Mcu
SDI-Isl
unpu- Fimwul Vanni: Mlpmsn No mama-m with W
Gotflng seam
Baum-Mon Compatible Tools mares
Demos Em Sam-m Examples mu Dona-mm Ina-x m [i
6.4-: swan
sumo. m G S'I‘mjimk I
m; dtm «mm.» (mum: man “u mmv‘: 9mm M WEN” CMSIS U [W W
human of cnoma ("a human Dona m; mm»; "W6 and M bond wwm why
STKIM Nanak
G)
513700)“!!!
.
1m: mm W use 0.: mm was "new?“ word IM (WEI (MES-Mm:
mum «an. ”'60-: boardsuwon when Iflilb pcnykdll Ilhuly m dammnm-m um 91
STEM N“ G 1‘ “ijulk E
"m HAM mm um mm was new
uni-0 emu hum lo «mm m w 0!
Mn eumpk mm... use at me mum.)
new Cumin mam kavp mun-m (Ink
out» soK o-xumm
vAppu-uonuu-
manna-WW
m: ammo" m .s 4mm luv
mun Gwyn" m mun: w m."
2.2 How to Use this Application Note
The source code for this application note is placed in the root folder an0009_efm32_getting_started.
The easiest way to access the example source code and projects is through the [Application Notes] dialogue box under [Getting Star-
ted] tab in Simplicity Studio. Simply click one of the application notes to open the [Application Notes] dialog.
Click any
Application Note
to open dialog
Figure 2.1. Application Notes in Simplicity Studio
Within the [Application Notes] dialog, navigate to and select the [AN0009 Getting Started with EFM32] entry, then click the [Import
Project...] button to view the list of available example projects. Use the project names to identify examples compatible with the kit and
select one to import that project into the IDE (by default, this is the Simplicity IDE, but this configuration can be changed to an
alternative IDE, if desired).
Alternatively, projects for multiple IDEs are stored in separate folders (iar, arm, etc.) in the filesystem that hosts these examples, ac-
cessible with the [Open Folder] button in the Simplicity Studio [Applications Notes] dialog. These projects can be manually loaded in
the appropriate IDE. All of the IAR projects are also collected in one common workspace called efm32.eww. Since the projects are
slightly different for the various kits, make sure to open the project that is prefixed with the name of the kit in use.
Note: The code examples in this application note are not complete, and the reader is required to fill in small pieces of code throughout
the exercises. A completed code file (postfixed with *_solution.c) also exists for each example.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Introduction
silabs.com | Building a more connected world. Rev. 1.22 | 4
3. Register Operation
This chapter explains the basics of how to write C-code for the EFM32 and EZR32 Series 0 devices using the defines and library func-
tions supplied in the [CMSIS] and [emlib] software libraries.
3.1 Address
The EFM32 and EZR32 Series 0 devices consist of several different types of peripherals (CMU, RTC, ADC...). Some peripherals in the
device exist only as one instance, such as the Clock Management Unit (CMU). Other peripherals like Timers (TIMERn) exist as several
instances and the name is postfixed by a number (n) denoting the instance number. Usually, two instances of a peripheral are identical,
but are placed in different regions of the memory map. However, some peripherals have a different feature set for each of the instan-
ces. For example, USART0 can have an IrDA interface, while USART1 cannot. Such differences will be explained in the device data
sheet and the reference manual.
EFM32 and EZR32 Series 0 peripherals are memory mapped, meaning each peripheral instance has a dedicated address region which
contains registers that can be accessed by read/write operations. The peripheral instances and memory regions are found in the device
data sheet. The starting address of a peripheral instance is called the base address. The reference manual for the device series con-
tains a complete description of the registers within each peripheral. The address for each register is given as an offset from the base
address for the peripheral instance.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 5
M11 IMALCTH. - W m
WEI EHFDSND"
m Sggfifigflfiflfififi‘iets9:95:2aosoovnn—o
m 2 e as: E 9:09
4M- E E 255 E 52%?
E
a .0
lun- E 2’ :
é‘ E N W
SSE 35
En Name Reset Access Descnpnon
31:1“ m
mmmmmmmmwnummh 1.20am
3:” ma.
M
W ”mason-rum
mmmmbm.mmsum
Va! m W
0 PRSOH) PRSCMIIGIOW.
| WI Pfismim.
2 m man-mam.
3 Pam PRSCWSW.
4 meow mam—4M.
5 PRSCHS maul-15mm.
G PRSCHS men-unclean“.
1 m7 PRSMTM,
8 m Pusan-mam.
9 m PRSWSM‘
l0 PM") flotsam-om.
II mu menu-nun W.
3.2 Register Description
The EFM32 and EZR32 Series 0 devices use a 32-bit bus for write/read access to the peripherals, and each register in a peripheral
contains 32 bits, numbered 0-31. Unused bits are marked as reserved and should not be modified. The bits used by the peripheral can
either be single bits (e.g. OUTEN bit in the figure below) or grouped together in bitfields (e.g. PRSSEL bitfield in the figure below). Each
bitfield is described with the following attributes:
• Bit position
• Name
• Reset value
• Access type
• Description
Figure 3.1. Example Register Description
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 6
3.3 Access Types
Each register has a set access type for all of the bit fields within that register. The access type describes the reaction to read or write
operations to the bit field. The different access types found for the registers in the devices are described in the table below.
Table 3.1. Register Access Types
Access Type Description
R Read only. Writes are ignored
RW Readable and writable
RW1 Readable and writable. Only writes to 1 have effect
(R)W1 Sometimes readable. Only writes to 1 have effect. Currently only used for IFC registers
W1 Read value undefined. Only writes to 1 have effect
W Write only. Read value undefined.
RWH Readable, writable, and updated by hardware
RW(nB), RWH(nB), etc. "(nB)" suffix indicates that register explicitly does not support peripheral bit set or clear
RW(a), R(a), etc. "(a)" suffix indicates that register has actionable reads
3.4 CMSIS and emlib
The Cortex Microcontroller Software Interface Standard (CMSIS) is a common coding standard for all ARM Cortex devices. The CMSIS
library provided by Silicon Labs contains header files, defines (for peripherals, registers and bitfields), and startup files for all devices. In
addition, CMSIS also includes functions that are common to all Cortex devices, like interrupt handling, intrinsic functions, etc. Although
it is possible to write to registers using hard coded address and data values, it is recommended to use the defines to ensure portability
and readability of the code.
In order to use these defines, projects must include em_device.h in the c-file. This is a common header file for all EFM32 and EZR32
Series 0 devices. Within this file, the header file content for the appropriate device is included in the project builds according to the
preprocessor symbols defined for the project.
To simplify the programming of EFM32 and EZR32 Series 0 devices, Silicon Labs developed and maintains a complete C-function li-
brary called [emlib] that provides efficient, clear, and robust access to and control of all peripherals and core functions in the device.
This library resides within the em_xxx.c (e.g. em_dac.c) and em_xxx.h (e.g. em_dac.h) files in the emlib folder under path below
(where v1.1 is the Gecko SDK Suite version number).
C:\SiliconLabs\SimplicityStudio\v4\developer\sdks\gecko_sdk_suite\v1.1\platform\emlib
In the source files included with this application note, the em_chip.h is included in each and a call to CHIP_Init() exists near the
beginning of every main() function. Like the content of em_device.h, the actions taken within the CHIP_Init() function depends on
the specific part in use, but will include correcting for known errata and otherwise ensuring consistent behavior across devices. For this
reason, do not run any code in the main function prior to running the CHIP_Init() function.
3.4.1 CMSIS Documentation
Complete Doxygen documentation for the EFM32 and EZR32 Series 0 [CMSIS] library and [emlib] is available via the [Gecko SDK
Documentation] box under [Documentation] in the Simplicity Studio main window when the corresponding device or kit is selected.
This documentation is also available on the Silicon Labs website at http://devtools.silabs.com/dl/documentation/doxygen/ or on GitHub
at https://siliconlabs.github.io/Gecko_SDK_Doc/.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 7
3.4.2 Peripheral Structs
In the emlib header files, the register defines for each peripheral type are grouped in structs as defined in the example below:
typedef struct
{
__IO uint32_t CTRL;
__I uint32_t STATUS;
__IO uint32_t CH0CTRL;
__IO uint32_t CH1CTRL;
__IO uint32_t IEN;
__I uint32_t IF;
__O uint32_t IFS;
__O uint32_t IFC;
__IO uint32_t CH0DATA;
__IO uint32_t CH1DATA;
__O uint32_t COMBDATA;
__IO uint32_t CAL;
__IO uint32_t BIASPROG;
} DAC_TypeDef;
Recall that a register address consists of a base address for the peripheral instance plus an additional offset. The peripheral structs in
[emlib] simplify writing to a register and abstract away these underlying addresses and offsets. Hence, writing to CH0DATA in the
DAC0 peripheral instance can then be done like this:
DAC0->CH0DATA = 100;
Similarly, reading a register can be done like this:
myVariable = DAC0->STATUS;
3.4.3 Bit Field Defines
Every device has relevant bit fields defined for each peripheral. These definitions are found within the efm32xx_xxx.h (e.g. efm32tg_da
c.h) files and are automatically included with the appropriate [emlib] peripheral header file.
#define _DAC_CTRL_REFRSEL_SHIFT 20
#define _DAC_CTRL_REFRSEL_MASK 0x300000UL
#define _DAC_CTRL_REFRSEL_DEFAULT 0x00000000UL
#define _DAC_CTRL_REFRSEL_8CYCLES 0x00000000UL
#define _DAC_CTRL_REFRSEL_16CYCLES 0x00000001UL
#define _DAC_CTRL_REFRSEL_32CYCLES 0x00000002UL
#define _DAC_CTRL_REFRSEL_64CYCLES 0x00000003UL
#define DAC_CTRL_REFRSEL_DEFAULT (_DAC_CTRL_REFRSEL_DEFAULT << 20)
#define DAC_CTRL_REFRSEL_8CYCLES (_DAC_CTRL_REFRSEL_8CYCLES << 20)
#define DAC_CTRL_REFRSEL_16CYCLES (_DAC_CTRL_REFRSEL_16CYCLES << 20)
#define DAC_CTRL_REFRSEL_32CYCLES (_DAC_CTRL_REFRSEL_32CYCLES << 20)
#define DAC_CTRL_REFRSEL_64CYCLES (_DAC_CTRL_REFRSEL_64CYCLES << 20)
For every register bitfield, associated shift, mask and default value bit fields are also defined.
#define DAC_CTRL_DIFF (0x1UL << 0)
#define _DAC_CTRL_DIFF_SHIFT 0
#define _DAC_CTRL_DIFF_MASK 0x1UL
#define _DAC_CTRL_DIFF_DEFAULT 0x00000000UL
#define DAC_CTRL_DIFF_DEFAULT (_DAC_CTRL_DIFF_DEFAULT << 0)
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 8
11.5.4 GHO_Px_DOU‘f - Pm Dal: 011 mm
En FOSIQIOn
o
m“ E
Amos E
._
’“"" §
El Name Reset Access Descnpt
31:16 Rwewed Towwmmummmem,mwmemmamehmmmt2mn
(ions
15:0 DOUT 0m RW DIaOII
Daanllpulonp’n.
3.4.4 Register Access Examples
When setting a bit in a control register, it is important to make sure firmware does not unintentionally clear other bits in the register. To
ensure this, the mask containing the bit firmware needs to set can be OR'ed with the original contents, as shown in the example below:
DAC0->CTRL = DAC0->CTRL | DAC_CTRL_LPFEN;
A more compact version is:
DAC0->CTRL |= DAC_CTRL_LPFEN;
Clearing a bit is done by ANDing the register with a value with all bits set except for the bit to be cleared:
DAC0->CTRL = DAC0->CTRL & ~DAC_CTRL_LPFEN; // or
DAC0->CTRL &= ~DAC_CTRL_LPFEN;
When setting a new value to a bit field containing multiple bits, a simple OR function will not do, since this will risk that the original bit
field contents OR'ed with the mask will give a wrong result. Instead, make sure to clear the entire bit field (and only the bit field) before
ORing in the new value:
DAC0->CTRL = (DAC0->CTRL & ~_DAC_CTRL_REFRSEL_MASK) | DAC_CTRL_REFRSEL_16CYCLES;
3.4.5 Grouped Registers
Some registers are grouped together within each peripheral. An example of such a group is the registers associated with each GPIO
port, like the Data Out Register (DOUT) in the figure below. Each GPIO port (A, B, C, ...) contains a DOUT register and the description
below is common for all of these. The x in GPIO_Px_DOUT indicates the port wild card.
Figure 3.2. Grouped Registers in GPIO
In the CMSIS defines, the port registers are grouped in an array P[x]. When using this array, we must index it using numbers instead of
the port letters (A=0, B=1, C=2, ...). Accessing the DOUT register for port C can be done like this:
GPIO->P[2].DOUT = 0x000F;
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 9
4. Example 1 — Register Operation
This example will show how to write and read registers using the CMSIS defines. This tutorial also shows how to observe and manipu-
late register contents through the debugger in Simplicity Studio or IAR Embedded Workbench. While the examples are shown only for
Simplicity Studio and IAR, the tasks can also be completed in other supported IDEs.
For Simplicity Studio:
1. Connect the kit to the PC and open Simplicity Studio.
2. Once the kit appears, click on the kit (e.g. EFM32 Giant Gecko Starter Kit (EFM32GG-STK3700)) in [Device] window.
3. Click one of the application notes under [Getting Started] tab to open [Application Notes] dialog.
4. Search for [AN0009 Getting Started with EFM32] and click the document in the list, then click the [Import Project...] button.
5. Select the [<kit_name>_1_registers.slsproj] option in the dialog and click [OK].
6. Double-click on the 1_registers.c file to open it in the editor view. There's a marker where custom code should be added.
For IAR:
1. Open up the efm32 workspace (an\an0009_efm32_getting_started\iar\efm32.eww).
2. Select the [<kit_name>_1_registers] project in IAR Embedded Workbench.
3. In the main function in the 1_registers.c (inside Source Files), there's a marker where custom code should be added.
4.1 Step 1 — Enable Timer Clock
In this example, we are going to use TIMER0. The high frequency RC oscillator (HFRCO) is running at default frequency band, but all
peripheral clocks are disabled, so we must turn on the clock for TIMER0 before we use it. If we look in the CMU chapter of the refer-
ence manual, we see that the clock to TIMER0 can be switched on by setting the TIMER0 bit in the HFPERCLKEN0 register in the
CMU peripheral.
4.2 Step 2 — Start Timer
Starting the Timer is done by writing a 1 to the START bit in the CMD register in TIMER0.
4.3 Step 3 — Wait for Threshold
Create a while-loop that waits until the counter is 1000 before proceeding.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 1 — Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 10
n: m 5.“. m... hrd. M m... u!
a» N as; q: lvt OJm-Hmsav‘o‘
cva-w
. a x n mm 0an E
g-u v=a
m- vinaml-s
\-. Breakpomls
mam
um
>mm
mm:
mm
w“
“Miomllnem‘ waiving v= n
.. .//.. . u «M .
mm m mm H mm
rm. mm“, u mm
mumv : my»:
my nun; M...
u m
[A 1. nm N m m. wag: .5 mm :. WW W: A, E .- mum“
”Jkamwo; .v “m WWW}
“a“ m "m m m . - H WIN-mm
é; (suiiilflamjhmm(wilwés, I 1.09)) an): m ; . . WMMHW M 7
‘ , . mmumLuwm ,
Ennis-ale :2 Exam \ n Memory M2 mum \oamnaues
hwmnmpmnzmk
x‘aifltdmavnv=a
4.4 Observation
For Simplicity IDE, make sure the [<kit_name>_1_registers] project is active by clicking the project in the left-hand [Project] view.
Then, press the [Debug] button to automatically build and download the code to the device. Click the [Registers] view and find the
STATUS register in TIMER0. After expanding the register, notice that the RUNNING bit set to 0.
In the code view, double-click the left pane to place a breakpoint before firmware starts the timer and click the [Resume] button. Then,
watch the RUNNING bit get set to 1 in the [Registers] view when single stepping over the expression using the [Step Over] button.
Continue to single step and note that the content of the CNT registers is increasing. Try writing a different value to the CNT register by
entering it directly in the [Registers] view.
Build and Debug Registers View
Resume Step Over
Disconnect Reset
Expressions View
Double-click to
add a breakpoint
Figure 4.1. Debug View in Simplicity IDE
For IAR, make sure the [<kit_name>_1_registers] project is active by pressing the corresponding tab at the bottom of the Workspace
window. Then, press the [Download & Debug] button and go to [View]->[Register] and find the STATUS register in TIMER0. After
expanding the register, notice that the RUNNING bit is set to 0.
Place the cursor in front of the line where firmware starts the timer and press [Run to Cursor]. Then, watch the RUNNING bit get set to
1 in the [Register] view when clicking the [Step Into] button to move over the expression. Continue to click the [Step Into] button to
see the content of the CNT registers increasing. Try writing a different value to the CNT register by entering it directly in the [Register]
view.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 1 — Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 11
5(ep mm Em debug
“my,“ WWW“ n. . mm .
mm m. :2 WW mm mm
Run k) Cursor 9-! m1 nay-em As, lle/m nag-m man- Is - nxnnnnnnn 33535an - nxnnnnnnnn
AM” u m, w m __ nu mm, M w mm“
MM _'m. “an, "a k. m a "a “:3; an men-nu
.m, m, ,D u. Wm MW,“ ., . mm..." . 52
.., m a. m m.“ .u, m “WM m. .u, n11 . human“
. .m. m mm m M.” mm
.. mm m m, .m k m, m u "A, .m k 5, _
:, :mi:r:=;;xzz:':;mm mm”
www.mmmmmmm my
: "mum-n m m...” v @
fimmmnfinggmmm a? mm; W
A ”3:2“:ng _: 1:3“,uml‘3m‘m um. um, m... m, m, m.
. MM, m .1; mm m, .., mm m...“ a: “In.” amt] Dxflflfld MW: R5- N
w, m. m a... WWW“ a. mu" M, Mm...” . v. ;
.g, a... mm m." a. m m. m m5,
man“ M m m m “mm, mm, M m.
”M M“, a, ..,.L_. m, u m a”..- w M m, m m
Hm. In. w m ,I m Wm. [W WWW
mu. mm H. m m
mm. mm _
m .ns,
‘enngufiUJI 2‘! $gmf “a“ my . mum. “mu .xnxmncauum.
r...” m .mm , , 2:22: 2512:: 325;“ :z- LEC- ”-
x Manny Fu-
WWW" “WWW
mem
. Inn-w fl
mm ., .M
Reset Download and DebugExit debugStep Into
Run to cursor Run
Figure 4.2. Debug View in IAR
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 1 — Register Operation
silabs.com | Building a more connected world. Rev. 1.22 | 12
EFM32 Giant Gecko Software Documentation
SILIEDII [ABS
efm32gg-do:4.4.u
u...n m: mm in: mm“... m. sum“... mm
V WW 0 Functions ‘
. m wwwmm,.,..n.. mummnm m
mmmmmmm I
w mum“.“um",mmmywdm
’ m suwarnin bandandAhemmnguahebndnnmavahemlhedmtanm uuemmmmmm Mara
mm hmmmuHKydmmumprcoemfi
KW mm“. W. .
m mummwwmmm u.m,.y..mmmmwymum
. nus mmmmbm m.
, W ,mmuw a.“ mmwmm
mummmmmmm W.
-_ mm M, ummca mm}
. (WW “mnmmuumm .
,m ,mmwm m,=.........mm
Mama“ .
' DEG JAT‘QNUNEVHH clllll : hms‘wmzd)
, m WWW“ mm
m ”emu.“ mumm mmmmm
' m an mmrlmmmr. Mm.
. M w
, am .
mugum¢ [murckkjyp-ovfdurk. murzlkbujyp-Mfiw]
gumuwmwm- um
5. Example 2 — Blinking LEDs with an STK
In this example, the aim is to use the GPIO pins to light up the LEDs on the STK and change the LED configuration every time a button
is pressed. Instead of accessing the registers directly, use the emlib functions to configure the peripherals.
The AN0009 application note includes a [<kit_name>_2_leds] project in Simplicity Studio and the IAR efm32 workspace, which will be
used in this example. The emlib C-files are included in the project. The corresponding header files are included at the beginning of the
C-files.
For details on which emlib functions exist and how to use them, open the API documentation through Simplicity Studio using the
[Gecko SDK Documentation] under [Documentation] (or by going to http://devtools.silabs.com/dl/documentation/doxygen/). After
clicking on the software documentation link for the correct device (e.g. Giant Gecko), open up [Modules->EMLIB] and select the [CMU]
peripheral. Find a list of functions for this peripheral by clicking on the [Functions] link at the top-right of the window. These functions
can be used to to easily operate the Clock Management Unit.
Figure 5.1. Documentation for the CMU-specific emlib Functions
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 2 — Blinking LEDs with an STK
silabs.com | Building a more connected world. Rev. 1.22 | 13
($9 EFM32 Giant Gecko Software Documentation e‘mgg'dw‘A'”
SILIEDII LAES
Maln Page names ill: Dncumenuflun name sllihsxam a- sum
, emjmu I o ‘ m mmmmumgunww (m A
m .m.
» emraau
1
» mam
ensign” Enauw‘smumk
, emrbumx In general. mm. dudmg .; damn 3A5 . m; n . mm. duck .1 dubkd, “E "pawn“ mm. .ye nmam‘bk m m.“ rm m. Wm",
m... underledvdues m.“ In mgmx «(mummy "mm have w flag on. a...“ mlyavod was.“ mum, lying :1. Mum..." . :1:ng
v Emmi [M
mummmmam "we
mummmmam
0“szme
mummmamz
mumnmmumm
(Mufimnm
(Mu (mama
Marianna/damn; 2 LF thKSVnmvunlzmun mm mm hwilequsw-ydannn s mum. mm m? mm 5 mmmed mm: was mm has mum:
ms mm‘nmwll slal urml m2 mssyummnman haswmnlm mm mferm (unjmnaflb‘loiw a sum m flown) rummflwe mm m sons
I
humans
mu cladK Th: am in Anabkld‘same Nunavut m al mm (M Dunn: have Swarm enahludvsabk mmL flu)! mm mu memew m Hymn:
manual
my all“:
. m. , enamewmzd am.
. fa‘se , mm: shamed (m.
momma" al x.» In: mm! mm“
5.1 Step 1 — Turn on GPIO clock
In the list of CMU functions we find the following function to turn on the clock to the GPIO:
void CMU_ClockEnable(CMU_Clock_TypeDef clock, bool enable)
If we click on the function, we are shown a description of how to use the function. Clicking on the [CMU_Clock_TypeDef] link goes to a
list of the allowed enumerators for the clock argument. To turn on the GPIO, add the following:
CMU_ClockEnable(cmuClock_GPIO, true);
Figure 5.2. CMU_ClockEnable Function Description
5.2 Step 2 — Configure GPIO Pins for LEDs
The User Manual for a kit is available in Simplicity Studio under the [Documentation] when the corresponing kit is selected in the De-
vice or Solutions window. This document describes the usage of all the pins, including the user LED(s). These LED(s) are connected as
follows on these EFM32 Series 0 kits:
• EFM32-Gxxx-STK: 4 LEDs on port C, pins 0-3
• EFM32TG-STK3300: 1 LED on port D, pin 7
• EFM32GG-STK3700: 2 LEDs on port E, pins 2-3
• EFM32ZG-STK3200: 2 LEDs on port C, pins 10-11
Consult the user manual for information specific to the kit in use.
Looking into the available functions for the GPIO, the following function can be used to configure the mode of the GPIO pins:
void GPIO_PinModeSet(GPIO_Port_TypeDef port, unsigned int pin,
GPIO_Mode_TypeDef mode, unsigned int out)
Use this function to configure the LED pin(s) as Push-Pull outputs with the initial DOUT value set to 0.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 2 — Blinking LEDs with an STK
silabs.com | Building a more connected world. Rev. 1.22 | 14
5.3 Step 3 — Configure a GPIO Pin for a Button
Look at the User Manual for the STK to find where Push Button 0 (PB0) is connected on the kit in use. This button is connected on
several example kits as follows:
• EFM32-Gxxx-STK: Port B, pin 9
• EFM32TG-STK3300: Port D, pin 8
• EFM32GG-STK3700: Port B, pin 9
• EFM32ZG-STK3200: Port C, pin 8
Configure this pin as an input to be able to detect the button state.
5.4 Step 4 — Change LED Status when a Button is Pressed
Write a loop that toggles the LED(s) every time PB0 is pressed. Make sure to not only check that the button is pressed, but also that it
is released, so that the LED(s) only toggle once for each button press. PB0 is pulled high by an external resistor.
5.5 Extra Task — LED Animation
Experiment with creating different blinking patterns on the LED(s), like fading and running LEDs (if there are multiple LEDs). Because
the device typically runs in the HFRCO frequency band by default, add a delay function to be able to see the LEDs changing in real-
time. Using the code for TIMER0 in Example 1, create the following function:
void Delay(uint16_t milliseconds)
Use the PRESC bitfield in TIMER0_CTRL to reduce the clock frequency to a desired value.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 2 — Blinking LEDs with an STK
silabs.com | Building a more connected world. Rev. 1.22 | 15
6. Example 3a — Segment LCD Controller
This example requires an STK with a Segment LCD. This example will demonstrate how to use the Segment LCD controller and display
information on the LCD display. The LCD controller includes an autonomous animation feature which will also be demonstrated. The
AN0009 application note includes a [<kit_name>_3_lcd] project in Simplicity Studio and the IAR efm32 workspace, which will be used
in this example.
6.1 Step 1 — Initialize the LCD controller
The LCD controller driver is located in the starter kit library. First, run the initialize function SegmentLCD_Init()found in segmentlcd.h
to set up the LCD controller.
6.2 Step 2 — Write to the LCD display
By default, all LCD segments are switched off after initialization. The LCD controller driver includes several functions to control the dif-
ferent segment groups on the display. A few examples are:
void SegmentLCD_Number(int value)
void SegmentLCD_Write(char *string)
void SegmentLCD_Symbol(lcdSymbol s, int on);
Experiment with putting custom text, numbers, or symbols on the display and try to make things move about a bit. Use the Delay func-
tion from Example 2. A Delay function can also be found in the solution file.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 3a — Segment LCD Controller
silabs.com | Building a more connected world. Rev. 1.22 | 16
99%?
E4:
43?
6.3 Step 3 — Animate Segments
Seg7
AREGB7
AREGA7
ALOGSEL
Seg6
AREGB6
AREGA6
Seg0
AREGB0
AREGA0
Barrel shift right/left
Barrel shift right/left
Figure 6.1. Animation Function
The LCD controller contains an animation feature which can animate up to 8 segments (8-segment ring on the LCD display) autono-
mously. The data displayed in the animated segments is a logic function (AND or OR) of two register bits for each segment. The two
register arrays (LCD_AREGA, LCD_AREGB) can then be set up to be barrel shifted either left or right every time the Frame Counter
overflows. The Frame Counter can be set up to overflow after a configurable number of frames. The firmware manipulates the LCD
registers by doing direct register writes. The following registers must be set up:
LCD_BACTRL:
• Set Frame Counter Enable bit
• Configure Frame Counter period by setting the FCTOP field
• Set Animation Enable bit
• Select either AND or OR as logic function
• Configure AREGA and AREGB shift direction
• For the Giant Gecko STK (STK3700), also set the ALOC bit to SEG8TO15
LCD_AREGA/LCD_AREGB:
• Write data used for animation to these registers.
Play around a bit with the configuration of the animated segments and watch the results on the LCD display.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 3a — Segment LCD Controller
silabs.com | Building a more connected world. Rev. 1.22 | 17
EFM32 Giant Gecko Software Documentation
efm32gg-doc4.4.u
SI LI E D N LA BS
mm. m..." m“ ”(Minimum “hm... q...
. as» o‘ , MmMHNNMMWMM A
.W 3-3:“
. my
. m
. M Ma Detailed Descnption
m ”SJK Displaykllize dnvaszm litany. Su manly Bum: Dmcr Slukvw m: mlnrmamu
. 9pm
, m
, zen-om
, Mkrybaam
, msm
, magma
, umsa
yum V
Display Device Driver Stack
m mm fiiesfurm: DiSPuwoa-(e dwufiam iihrary isms w. the hS/mmmun/dmus nmvryam mm; in: mm"; mmemmn:
aspmammmm
Mucllm
“In! sun-d
mm m Driver M’amnl'ns
. nus-m mammmumruumm
7. Example 3b — Memory LCD
This example requires an STK equipped with a Memory LCD (e.g. Happy Gecko, Zero Gecko, Pearl Gecko, and EFR32xG Wireless
STKs). This example shows how to configure the Memory LCD driver and write text on the Memory LCD. The software project called
[<kit_name>_3_lcd_mem] will be used in this example.
The Gecko SDK includes a driver for the memory LCD. Documentation for this display driver is found in the [Display] under the [Kit
Drivers] section in corresponding kit [Software Documentation].
Figure 7.1. Documentation for the Display Driver
7.1 Step 1 — Configure the Display Driver
First, initialize the DISPLAY driver with DISPLAY_Init().
The display driver includes TEXTDISPLAY, which is an interface for printing text to a dispaly device. Use TEXTDISPLAY_New() to create
a new TEXTDISPLAY interface.
7.2 Step 2 — Write Text to the Memory LCD
TEXTDISPLAY implements basic functions for writing text to the Memory LCD. Try TEXTDISPLAY_WriteString() and TEXTDISPLAY_W
riteChar().
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 3b — Memory LCD
silabs.com | Building a more connected world. Rev. 1.22 | 18
8. Example 4 — Energy Modes
This example shows how to enter different Energy Modes (EMx) and wake up using an RTC or RTCC interrupt. The project called
[<kit_name>_4_energymodes] is used in this example.
8.1 Advanced Energy Monitor with STK
The Starter Kits include current measurement of the VMCU power domain, which is used to power the device and the LCD display in
addition to other components in the application part of the starter kit. The real-time current measurement can be monitored on a PC
using the Energy Profiler available in Simplicity Studio.
8.2 Step 1 — Enter EM1
To enter EM1, execute a Wait-For-Interrupt instruction with the SLEEPDEEP bit in the SCB_SCR register clear. An intrinsic function for
this instruction (part of CMSIS) is shown below:
SCB->SCR &= ~SCB_SCR_SLEEPDEEP_Msk;
__WFI();
After executing this instruction, observe that the current consumption drops.
In addition, the EMU emlib functions include functions for entering Energy Modes, which firmware can use instead of clearing the
SLEEPDEEP bit and executing the WFI-instruction manually:
void EMU_EnterEM1()
8.3 Step 2 — Enter EM2
Entering EM2 is also done by executing the WFI-instruction, except with the SLEEPDEEP bit in the SCB_SCR register also set, and
with a low frequency oscillator enabled. To enter EM2, first enable a low frequency oscillator (either LFRCO or LFXO) before going to
deep sleep. In this example, enable the LFRCO and wait for it to stabilize by using the following emlib function:
void CMU_OscillatorEnable(CMU_Osc_Typedef osc, bool enable, bool wait)
Now, enter EM2 by setting SLEEPDEEP and executing the WFI-instruction:
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
__WFI();
In addition, the EMU emlib functions include functions for entering Energy Modes, which firmware can use instead of setting the
SLEEPDEEP bit and executing the WFI-instruction manually:
void EMU_EnterEM2(bool restore)
It is strongly recommended to take advantage of this function. This emlib function will also avoid or workaround any errata issues affect-
ing the Energy Modes operation.
Note: When in an active debug session, the device will not be allowed to go below EM1. To measure the current consumption in EM2,
end the debugging session and reset the device with the reset button on the STK.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 4 — Energy Modes
silabs.com | Building a more connected world. Rev. 1.22 | 19
8.4 Step 3 — Enter EM3
To enter EM3, first disable all low frequency oscillators before going to deep sleep (which is accomplished by using the same technique
as for EM2). Disable the LFRCO originally enabled in Step 2 by using the following emlib function:
void CMU_OscillatorEnable(CMU_Osc_Typedef osc, bool disable, bool wait)
Now, enter EM3 by setting SLEEPDEEP and executing the WFI-instruction:
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
__WFI();
In addition, the EMU emlib functions include functions for entering Energy Modes, which firmware can use instead of disabling LF oscil-
lators, setting the SLEEPDEEP bit, and executing the WFI-instruction manually:
void EMU_EnterEM3(bool restore)
It is strongly recommended to take advantage of this function. This emlib function will also avoid or workaround any errata issues affect-
ing the Energy Modes operation.
Note: When in an active debug session, the device will not be allowed to go below EM1. To measure the current consumption in EM3,
end the debugging session and reset the device with the reset button on the STK.
8.5 Step 4 — Configure the Real-Time Counter (RTC) of MCU Series 0
To wake up from EM2, configure the Real-Timer Counter (RTC) to give an interrupt after 5 seconds. First, enable the clock to the RTC
by using the CMU emlib functions. To communicate with Low Energy/Frequency peripherals like the RTC, also enable the clock for the
LE interface (cmuClock_HFLE).
The emlib initialization function for the RTC requires a configuration struct as an input:
void RTC_Init(const RTC_Init_TypeDef *init)
The struct is already declared in the code, but firmware must set the 3 parameters in the struct before using it with the RTC_Init func-
tion:
rtcInit.comp0Top = true;
Next, set compare value 0 (COMP0) in the RTC, which will set interrupt flag COMP0 when the compare value matches the counter
value. Chose a value that will equal 5 seconds given that the RTC runs at 32.768 kHz:
void RTC_CompareSet(unsigned int comp, uint32_t value)
Now the RTC COMP0 flag will be set on a compare match, but the corresponding enable bit must also be set to generate an interrupt
request from the RTC:
void RTC_IntEnable(uint32_t flags)
The RTC interrupt request is enabled on a comparator match, but to trigger an interrupt, the RTC interrupt request line must be enabled
in the Cortex-M. The IRQn_Type to use is RTC_IRQn.
NVIC_EnableIRQ(RTC_IRQn);
An interrupt handler for the RTC is already included in the code (RTC_IRQHandler), but it is empty. In this function, add a function call
to clear the RTC COMP0 interrupt flag. If firmware does not do this, the Cortex-M will be stuck in the interrupt handler, since the inter-
rupt is never deasserted. Look for the RTC emlib function to clear the interrupt flag.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 4 — Energy Modes
silabs.com | Building a more connected world. Rev. 1.22 | 20
8.6 Extra Task — Segment LCD Controller in EM2
As an extra task, enable the LCD controller (assuming there's a Segment LCD on the kit in use) and write something on the LCD dis-
play before going to EM2. Use the segment animation from the previous example in EM2.
Note: Since the RTC or RTCC is used by the Memory LCD display driver, this extra task does not apply to the kits that feature a Memo-
ry LCD instead of a segment LCD.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Example 4 — Energy Modes
silabs.com | Building a more connected world. Rev. 1.22 | 21
EFM32 Giant Gecko Starter Kit (EFMSZGG-STK3700)
panama-mum“: camuwmmm
om Mm mu my.
umuF-man-m Mlpmw mwmmm W
m a
‘ \ Gd- sax m
51‘an e ‘ 51W)!“
"magma «mugs that-numbing" mummuemw ummmmss , Mm“
lwawn :21 (mm ma human hand. "all ‘ "KM-"y Mb I"! me how! mum put-g: W 7 W ,_
‘ ‘ Id.- sou Dunn-flan I
51m “It rmlw sex Mum-w.
IMWWmummcm
mum mom-k Q
«mm an» and m In»: mm mug-
1
s-mmum. Q)
VinwmwflMfl(m§-Mml
amen-nu llbmnn mum-khan“
m sample any“! um [max cm; m m
(Iv-lab WI! lllflly lo magnum. m a
mum
vm gawk dummy“ use ammw
mummnn bukuundmdxk
”WM
WWMWI
"m ammhon rm 13-min
mm mmmmwnnmmu ..
9. Summary
Congratulations! You now know the basics of Energy Friendly Programming, including register and GPIO operation, use of basic func-
tions on the STK and LCD, in addition to handling different Energy Modes in the device and the emlib/CMSIS functions. The [Software
Examples] and [Application Notes] under [Getting Started] tab in Simplicity Studio provide more examples and Application Notes to
explore.
Figure 9.1. Software Examples and Application Notes in Simplicity Studio
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Summary
silabs.com | Building a more connected world. Rev. 1.22 | 22
10. Revision History
Revision 1.22
January 2018
• Removed references to EFM32PG13/EFM32JG13
• Added examples for EFM32TG11 starter kit.
Revision 1.21
June 2017
• Split AN0009 into AN0009.0 and AN0009.1 for MCU/Wireless MCU Series 0 and MCU/Wireless SoC Series 1, respectively.
• Removed RTC configuration instructions from Example 4 text.
• Added examples for EFM32PG12, EFM32GG11, EFR32MG1, EFR32MG12, and EFR32MG13 starter kits.
Revision 1.20
January 2017
• Updated for Simplicity Studio V4.
• Removed example for EFM32G development kit.
• Added example for EFM32PG1 starter kit.
Revision 1.19
November 2017
• Added support for EFM32 Gemstones and the EFR32 Wireless Gecko portfolio.
Revision 1.18
May 2014
• Updated example code to CMSIS 3.20.5
• Changed to Silicon Labs license on code examples
• Added example projects for Simplicity IDE
• Removed example makefiles for Sourcery CodeBench Lite
Revision 1.17
October 2013
• Added missing header file
Revision 1.16
October 2013
• New cover layout
• Added support for the Zero Gecko Starter Kit (EFM32ZG-STK3200)
• New text in the Bit field defines chapter
• Fixed issue with STK3700 and LCD animation
Revision 1.15
May 2013
• Added software projects for ARM-GCC and Atollic TrueStudio.
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Revision History
silabs.com | Building a more connected world. Rev. 1.22 | 23
Revision 1.14
November 2012
• Added support for the Giant Gecko Starter Kit(EFM32GG-STK3700)
• Adapted software projects to new kit-driver and bsp structure
Revision 1.13
April 2012
• Adapted software projects to new peripheral library naming and CMSIS_V3
Revision 1.12
March 2012
• Added efm32lib file efm32_emu.c to LED projects
• Fixed makefile-error for CodeSourcery projects
Revision 1.11
October 2011
• Updated IDE project paths with new kits directory
Revision 1.10
September 2011
• Added support for Tiny Gecko Starter Kit (EFM32TG-STK3300)
Revision 1.03
May 2011
• Updated projects to align with new bsp version
Revision 1.02
November 2010
• Corrected solution c-files for new EFM32LIB functions
• Corrected pdf document for new EFM32LIB functions
Revision 1.01
November 2010
• Changed software/documentation to use the segmentlcd.c functions, lcdcontroller.c is deprecated
• Added section about CMSIS Doxygen documentation
• Changed example folder structure, removed build and src folders
• Updated chip init function to newest efm32lib version
Revision 1.00
September 2010
• Initial revision
AN0009.0: Getting Started with EFM32 and EZR32 Series 0
Revision History
silabs.com | Building a more connected world. Rev. 1.22 | 24
Q
SILICON LABS
http://www.silabs.com
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
USA
Simplicity Studio
One-click access to MCU and
wireless tools, documentation,
software, source code libraries &
more. Available for Windows,
Mac and Linux!
IoT Portfolio
www.silabs.com/IoT
SW/HW
www.silabs.com/simplicity
Quality
www.silabs.com/quality
Support and Community
community.silabs.com
Disclaimer
Silicon Labs intends to provide customers with the latest, accurate, and in-depth documentation of all peripherals and modules available for system and software implementers using or
intending to use the Silicon Labs products. Characterization data, available modules and peripherals, memory sizes and memory addresses refer to each specific device, and "Typical"
parameters provided can and do vary in different applications. Application examples described herein are for illustrative purposes only. Silicon Labs reserves the right to make changes
without further notice and limitation to product information, specifications, and descriptions herein, and does not give warranties as to the accuracy or completeness of the included
information. Silicon Labs shall have no liability for the consequences of use of the information supplied herein. This document does not imply or express copyright licenses granted
hereunder to design or fabricate any integrated circuits. The products are not designed or authorized to be used within any Life Support System without the specific written consent of
Silicon Labs. A "Life Support System" is any product or system intended to support or sustain life and/or health, which, if it fails, can be reasonably expected to result in significant personal
injury or death. Silicon Labs products are not designed or authorized for military applications. Silicon Labs products shall under no circumstances be used in weapons of mass
destruction including (but not limited to) nuclear, biological or chemical weapons, or missiles capable of delivering such weapons.
Trademark Information
Silicon Laboratories Inc.® , Silicon Laboratories®, Silicon Labs®, SiLabs® and the Silicon Labs logo®, Bluegiga®, Bluegiga Logo®, Clockbuilder®, CMEMS®, DSPLL®, EFM®, EFM32®,
EFR, Ember®, Energy Micro, Energy Micro logo and combinations thereof, "the world’s most energy friendly microcontrollers", Ember®, EZLink®, EZRadio®, EZRadioPRO®,
Gecko®, ISOmodem®, Micrium, Precision32®, ProSLIC®, Simplicity Studio®, SiPHY®, Telegesis, the Telegesis Logo®, USBXpress®, Zentri and others are trademarks or registered
trademarks of Silicon Labs. ARM, CORTEX, Cortex-M3 and THUMB are trademarks or registered trademarks of ARM Holdings. Keil is a registered trademark of ARM Limited. All
other products or brand names mentioned herein are trademarks of their respective holders.