Digi-Key Announces Exclusive Stock of GeneSiC Semiconductor SiC 3300 V Schottky Rectifiers
THIEF RIVER FALLS, Minnesota, USA - 2013 年 06 月 13 日
Global electronic components distributor Digi-Key Corporation, the industry leader in electronic component selection, availability and delivery, today announced an agreement to serve as exclusive distributor of the latest low-capacitance silicon carbide (SiC) Schottky rectifiers from GeneSiC Semiconductor. These innovative rectifiers are specifically targeted towards voltage multiplier circuits and high voltage assemblies used in a wide range of x-ray, laser, and particle generator power supplies.
GeneSiC's 3300 V/0.3 A Schottky rectifiers feature zero reverse recovery current that does not change with temperature. This relatively high voltage in a single device allows a reduction in voltage multiplication stages required in typical high voltage generator circuits, through use of higher AC input voltages. The near-ideal switching characteristics allow the elimination/dramatic reduction of voltage balancing networks and snubber circuits.
3300 V/0.3 A SiC Rectifier Technical Highlights
- On-state Drop of 1.7 V at 0.3 A
- Positive temperature coefficient on VF
- Tjmax = 175°C
- Capacitive charge 52 nC (typical)
"This product offering comes from years of sustained efforts at GeneSiC. We believe the 3300 V rating is a key differentiator for the high voltage generator market, and will allow significant benefits to our customers. GeneSiC's low VF, low capacitance SiC Schottky Rectifiers enable this breakthrough product," said Dr. Ranbir Singh, President of GeneSiC Semiconductor.
All devices are 100% tested to full voltage/current ratings and housed in halogen-free, RoHS-compliant, industry-standard TO-220FP (Full Pack) packages.
These advanced devices, as well as the rest of GeneSiC Semiconductor's portfolio of quality products, are available for immediate shipment by visiting any of Digi-Key's global websites.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com