Digi-Key Corporation Now Offers NXP’s CMOS Multiplexer/Demultiplexer
THIEF RIVER FALLS, Minnesota, USA - 2011 年 06 月 13 日
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced the addition of NXP's CMOS 2-to-1 multiplexer/demultiplexer switch for PCI Express Generation 3 (Gen3). The part number for this device is CBTL02043.
This particular multiplexer/demultiplexer can switch two different signals to one of two locations, and is the industry's first 10 Gbps switch. By utilizing a unique design technique, NXP has minimized the impedance of the switch resulting in negligible attenuation. Minimization of channel-to-channel skew and channel-to-channel crosstalk is also observed.
Benefits of this product include high-speed signal switching, high bandwidth, and low insertion loss, as well as a shutdown pin for power-saving mode offering a standby current of less than 1µA.
NXP's CBTL02043 is available for purchase now on Digi-Key's global websites.
Digi-Key Corporation focuses on providing customers with superior service, which includes product selection and availability, on-time delivery, and responsiveness. Using leading-edge processes and state-of-the-art technologies, Digi-Key serves a global customer base from its 600,000 square foot facility in Thief River Falls, Minnesota, USA.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com