Digi-Key Corporation Announces Stock of New Molex LED Array Holders
THIEF RIVER FALLS, Minnesota, USA - 2011 年 08 月 29 日
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced availability of the Molex Incorporated solderless LED array holders.
Molex has simplified the LED mounting process by offering array holders which eliminate the need for hand or SMT soldering. These LED array holders install quickly into fixtures, enabling replacements in the field and allowing for easy upgrades to current applications.
Features of these high-temperature LED array holders include screw-mount attachment method for securing the array to a heat sink, optional snap-lock optics that provide light source adjustment, and compression contacts that will power the array and eliminate soldering during installation. Serviceability is greatly improved by the releasable wire trap. The array’s small form factor, less than 50.00 mm (1.96”) in diameter for ES arrays and 70.00 by 71.00 mm (2.75 by 2.80”) for RS arrays, makes these array holders ideal for use in lamps and small-fixture applications.
These LED array holders are available for purchase on Digi-Key's global websites.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
About Molex Incorporated
Providing more than connectors, Molex delivers complete interconnect solutions for a number of markets including data communications, telecommunications, consumer electronics, industrial, automotive, medical, military, lighting and solar. Established in 1938, the company operates 39 manufacturing locations in 16 countries. The Molex website is www.molex.com. Follow Molex at www.twitter.com/molexconnectors, watch their videos at www.youtube.com/molexconnectors, connect with them at www.facebook.com/molexconnectors and read their blog at www.connector.com.
Molex is a registered trademark of Molex Incorporated.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com