Digi-Key Corporation Announces Stock on New IP67 SEAL-D Connectors from NorComp
THIEF RIVER FALLS, Minnesota, USA - 2010 年 07 月 28 日
Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, today announced it has stock on NorComp's new line of IP67 sealed D-Sub connectors.
These new products are now available for purchase on Digi-Key's global websites and will be featured in future print and online catalogs.
The IP67 SEAL-D connector utilizes a proprietary sealing technology that maintains the same physical size and footprint as standard D-Sub products. This reduces space on new designs and eliminates the need to redesign enclosures and PC boards when implementing IP67 design upgrades.
These connectors are designed for applications that require protection from heavy spray or are exposed to short-term submersion. Typical applications include handheld computers, scanners, and printers that are used outdoors; remote sensors, gauges, and data loggers that are exposed to the elements; industrial and medical equipment routinely subjected to washdown; transmitters and emergency beacons that are subjected to short-term immersion; gas, electric, and water metering systems with embedded Smart Grid electronics; and consumer and commercial shipboard electronics, meters, and sensors.
The IP67 connectors are available in vertical and right angle board mount versions as well as a solder cup version for panel mount cable applications. Standard D-Subs are available in 9, 15, and 25 positions. The high-density models are available in 15, 26, and 44 positions.
Digi-Key Corporation focuses on providing customers with superior service, which includes product selection and availability, on-time delivery, and responsiveness. Using leading-edge processes and state-of-the-art technologies, Digi-Key serves a global customer base from its 600,000 square foot facility in Thief River Falls, Minnesota, USA.
About Digi-Key Corporation
Digi-Key Corporation, based in Thief River Falls, Minn., is a global, full-service provider of both prototype/design and production quantities of electronic components, offering more than three million products from over 650 quality name-brand manufacturers. With over one million products in stock and an impressive selection of online resources, Digi-Key is committed to stocking the broadest range of electronic components in the industry and providing the best service possible to its customers. Additional information and access to Digi-Key's broad product offering is available on the Digi-Key website.
- Editorial Contact
- Laura Stengrim
- DigiKey
- (218) 681-8000 ext. 14489
- laura.stengrim@digikey.com