CA Proposition 规格书

Proposition 65 Declaration
Name of Manufacturer: CIT RELAY & SWITCH
Address of Manufacturer: 14680 James Rd.
Rogers, MN 55374
CIT & Relay & Switch declares that some of its products may contain chemicals
which are listed on the state of California’s Safe Drinking Water and Toxic
Enforcement Act of 1986.
A complete list of chemicals known to the State of California to cause cancer or
reproductive toxicity, listed by the State of California Environmental Protection
Agency Office of Environmental Health and Hazard Assessment, in accordance
with Proposition 65 (the Safe Drinking Water and Toxic Enforcement Act of 1986)
can be found at https://oehha.ca.gov/proposition-65/proposition-65-list
CIT will continue to monitor additions to the complete list of chemicals found on
the above referenced list and update the chart below as needed:
Chemical CAS Number
Cadmium Compounds
used in internal electrical
contacts.
1306-19-0
Nickel used in internal
electrical contacts and
plated on internal parts.
7440-02-0
Lead: Copper containing up
to 0.1% (1000ppm) Lead
by weight
7439-92-1
Updated: July 11
th
, 2018
Ivan Lee
QA Engineering Manager
CIT RELAY & SWITCH
TM