TE Connectivity Raychem Cable Protection 的 RPS Series Spec 规格书
-:.' TE
connectivity
Markers
System Eguigmem
SPECIFICATION: RW-2510
THIS ISSUE: ISSUE 2
DATE: February 2014
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
SPECIFICATION RW-2510
Document Number 108-121013
RPS
1. SCOPE
This specification covers the requirements and performance of the RPS Marker System. This
system is an automatic method of identifying wire and cable. The mark is permanent upon
printing.
1.1 CLASSIFICATION
1.1.1 Markers
The markers shall be fabricated from modified radiation cross-linked polymer tubing, flattened
and mounted on a carrier.
1.1.2 System Equipment
The recommended Printer Ribbon Systems for use with RPS are shown in the latest version of
document 411-121005 Identification Printer Product Ribbon Matrix. System performance is
evaluated in this specification
REVISION HISTORY
Revision
Number
Description of change
Date
Incorporated By
1
Replaces RT-1804 issue 8
July 2004
-
2
Format update
February 2014
M Priddle
While TE Connectivity has made every reasonable effort to ensure the accuracy of the information in this specification, TE Connectivity does not
guarantee that it is error-free, nor does TE Connectivity make any other representation, warranty or guarantee that the information is accurate, correct,
reliable or current. TE Connectivity reserves the right to make any adjustments to the information contained herein at any time without notice. TE
Connectivity expressly disclaims all implied warranties regarding the information contained herein, including, but not limited to, any implied warranties of
merchantability or fitness for a particular purpose. The dimensions in this document are for reference purposes only and are subject to change without
notice. Specifications are subject to change without notice. Consult TE Connectivity for the latest dimensions and design specifications.
Qua‘ificalion Tests
Accegtance Tests
Page 2 SPECIFICATION RW 2510 ISSUE 2
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
2. APPLICABLE DOCUMENTS
This specification takes precedence over documents referenced herein. Unless otherwise
specified, the latest issue of the referenced documents applies.
2.1 PUBLICATIONS
ASTM D 2672
Heat Shrinkable Tubing for Electrical use
UL224
Standard for Extruded Insulating Tubing
ISO-846
Plastics – Evaluation of the action of microorganisms
SAE AS5942
Marking of Electrical Insulating Materials
IEWI-012
TE Connectivity: Mark Adherence & Print Permanence testing using
the hand operated Crockmeter.
3. REQUIREMENTS
3.1 MATERIAL
The sleeving shall be fabricated from irradiated, thermally stabilized, modified polyolefin
compound containing no cadmium in the formulation. It shall be homogeneous and essentially
free from flaws, defects, pinholes, bubbles, seams, cracks or inclusions.
3.2 COLOR
The markers shall be white or yellow.
3.3 FORM
The sleeves shall be cut lengths mounted on a carrier in accordance with Figure 1.
3.4 PROPERTIES
The sleeves shall meet the requirements of Table 4.
4. QUALITY ASSURANCE PROVISIONS
4.1 CLASSIFICATION OF TESTS
4.1.1 Qualification Tests
Qualification tests are those performed on finished markers or marker material submitted for
qualification as a satisfactory product and shall consist of all tests listed in this specification.
4.1.2 Acceptance Tests
Acceptance tests are those performed on finished markers submitted for acceptance under the
contract. Acceptance tests shall consist of the following:
Appearance
Dimensions
Longitudinal Change
Qualification Test Samples
Accegtance Test Samgles
Dimensions Dimensional Recovery and Lonqitudinal Chanae
Tensile Strength and Ullimale Elongation
Low Temgerature Flexibility
RPS 22718 to RPS 874
5/16
7.9
RPS 17400 to RPS 40071000
7/16
11.1
SPECIFICATION RW 2510 ISSUE 2 Page 3
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
4.2 SAMPLING INSTRUCTIONS
4.2.1 Qualification Test Samples
Qualification test samples shall consist of 15 m (50 feet) of continuous marker material and the
appropriate number of finished markers necessary to run all tests. Qualification of any one size
shall qualify all sizes.
4.2.2 Acceptance Test Samples
Acceptance test samples shall consist of the appropriate number of finished markers necessary
to run the specified tests.
4.3 TEST PROCEDURES
Unless otherwise specified, the markers shall be removed from the carrier and recovered for
testing. Where required by test method limitations, testing shall be done on expanded tubing
prior to cutting and assembly.
4.3.1 Dimensions, Dimensional Recovery and Longitudinal Change
Test three markers in accordance with ASTM D 2671 for as supplied dimensions, dimensions as
recovered and longitudinal change. Mark two gauge marks 44.5 mm (1.75 ins.) apart on each
sample. When required, recover specimens for 3 minutes at 200 ± 5oC (392 ± 9oF). Remove
the specimens from the oven, and allow to cool to room temperature. The distance between
gauge marks and inside diameter of each shall be measured. The longitudinal change shall be
expressed as a percentage of the original gauge mark distance. The recovered inside diameter
and recovered wall thickness shall be determined.
4.3.2 Tensile Strength and Ultimate Elongation
Test three specimens for tensile strength and ultimate elongation in accordance with ASTM D
2671, using 25 mm (1-inch) benchmarks, a 50 mm (2-inch) initial jaw separation and a jaw
separation speed of 508 mm (20 inches) per minute.
4.3.3 Low Temperature Flexibility
Recover three specimens, sizes RPS 1-400 and smaller, over a stranded AWG wire (nearest
gauge which is larger than the sleeving maximum I.D. nominal after unrestricted shrinkage). For
tubing size RPS 400-1000, cut three 152 mm by 6.4 mm (6 inch by 1/4 inch) strips, longitudinally
from recovered tubing. Condition the specimens for 4 hours at -30 ± 2oC (-22 ± 4oF). While at
this temperature, bend the tubular specimens 90 degrees, in approximately 2 seconds, over a
similarly conditioned mandrel, selected in accordance with Table 1. Bend the strip specimens
360 degrees over a 7.9 mm (5/16-inch) mandrel, similarly conditioned. Examine the specimens
for cracks.
TABLE 1
MANDREL DIMENSIONS FOR
BEND TESTING
Part Number
Diameter of Mandrel
Inches
millimetres
RPS 22-18 to RPS 8-4
5/16
7.9
RPS 10-2 to RPS 6-250
3/8
9.5
RPS 1-400 to RPS 400-1000
7/16
11.1
Prim Performance , Legibiiity and Durabilily
RPS 22*18/200
Arial or Courier 10 Bold
RPS 18*12/200
Arial or Courier 12 Bold
RPS 16*10/200
Arial or Courier 12 Bold
RPS Brit/2.00
Arial or Courier 12 Bold
RPS 1072/200
Arial or Courier 12 Bold
RPS 6*250/200
Arial or Courier 14 Bold
RPS 1,400/200
Arial or Courier 18 Bold
RPS 40071000200
Arial or Courier 18 Bold
Page 4 SPECIFICATION RW 2510 ISSUE 2
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
4.3.4 Print Performance - Legibility and Durability
Mark eighteen finished markers with the recommended Printer / ribbon system as shown in
document 411-121005. Print random characters across the length of each marker to within 6
mm (1/4 inch) of both ends using the font indicated in Table 2. Remove the specimens from the
carrier.
TABLE 2
Character Font and Size for Print Performance Testing
Part Number
Font type and size
RPS 22-18/2.00
Arial or Courier 10 Bold
RPS 18-12/2.00
Arial or Courier 12 Bold
RPS 16-10/2.00
Arial or Courier 12 Bold
RPS 8-4/2.00
Arial or Courier 12 Bold
RPS 10-2/2.00
Arial or Courier 12 Bold
RPS 6-250/2.00
Arial or Courier 14 Bold
RPS 1-400/2.00
Arial or Courier 18 Bold
RPS 400-1000/2.00
Arial or Courier 18 Bold
4.3.4.1 Recover three marked specimens in an oven for 3 minutes at 200 ± 5oC (392 ± 9oF) and
allow them to cool to room temperature.
The test pieces shall be tested for print permanence in accordance with SAE-AS5942 and
IEWI-012. The number of rubs and weight shall be as specified in Table 4.
Examine the marking for legibility at a distance of 356 mm (14 inches).
4.3.4.2 Recover nine marked specimens in an oven for 3 minutes at 200 ± 5°C (392 ± 9°F) and
allow them to cool to room temperature. Prepare three specimens for each of the following
three fluids:
a) One part by volume of isopropyl alcohol, American Chemical Society (ACS) reagent grade, or
isopropyl alcohol in accordance with TT-I-735, grade A or B and three parts by volume mineral
spirits in accordance with TT-T-291, type II, grade A, or in accordance with P-D-680, type I or
three parts by volume of a mixture of 80% by volume of kerosene and 20% by volume ethyl
benzene.
b) A terpene defluxer consisting of a minimum of 90% d-Limonene and 10% surfactant1
c) A mixture consisting of the following:
1) Forty-two parts by volume water, I megohm-cm minimum resistivity
2) One part by volume of propylene glycol mono-methyl ether (glycol ether PM, 1-methoxy-2-
propanol)
3) One part by volume of monoethanolamine 2
4.3.4.3 Obtain a brush of the following description:
It shall be a toothbrush with a handle made of a non-reactive material. The brush is made of at
least three long rows, 28.5 ± 3 mm (1-1/8 ± 1/8 inch) in length, of hard bristles. Each row shall
contain eight to ten tufts, the free ends of which shall lie substantially in the same plane. Each
brush shall be used with a single solvent and when there is any evidence of softening, bending,
wear, or loss of bristles, it shall be discarded.
Maintain all solutions at a temperature of 23 ± 5°C (73 ± 9°F). Completely immerse the
specimens and the bristle portion of the brush for one minute in the specified solution.
Immediately following immersion, brush the specimen with normal hand pressure -
approximately 56 - 85 g (2 - 3 ounce) pressure - for ten unidirectional strokes on the portion of
the specimen where marking has been applied. Immediately after the initial brushing, repeat the
1 A commonly used terpene defluxer is BIOACT EC-7R. “BIOACT” and is a registered Trademark of Petroferm INC.
2 Normal safety precaution for handling this solution based on O.S.H.A. rules for monoethanolamine
Heat Shock
Heat Aging
Mandrel Bend
Print Performance
Dielectric Strength
Corrosive Elfect
Flammability
Water Absorption
Fungus resistance
Tensile Strength
SPECIFICATION RW 2510 ISSUE 2 Page 5
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
immersion and brushing procedure (one minute of immersion followed by ten brush strokes) a
sufficient number of times to provide the total number of strokes specified in Table 4. After
completion of the brushing, rinse the specimens in water and air-blow dry all the surfaces.
Examine the specimens for legibility at a distance of 356 mm (14 inches).
4.3.5 Heat Shock
The test method shall be as specified in UL 224. The test conditions will be 1 hour at 136 ± 2oC
(277 ± 4oF).
4.3.6 Heat Aging
Shrink three specimens, size RPS 1-400 or smaller, on a stranded AWG wire (nearest gauge
which is larger than the sleeving maximum I.D. nominal after unrestricted shrinkage). For tubing
sizes RPS 400-1000, cut three 152 mm by 6.4 mm (6 inch by 1/4 inch) strips, longitudinally from
recovered tubing. Condition the specimens for 168 hours at 158 ± 2oC (316 ± 4oF) in a
convection oven, with an air velocity of 30 - 60 m (100 - 200 ft) per minute past the specimens.
Remove the specimens from the oven, and allow to cool to room temperature. Test the
specimens for mandrel bend in accordance with Section 4.3.6.1. Test an additional three
specimens for print performance in accordance with Section 4.3.6.2.
4.3.6.1 Mandrel Bend
Bend the specimens recovered on the stranded wire 90 degrees around a mandrel specified in
Table 1. Bend the strips 360 degrees around a 7.9 mm (5/16-inch) diameter mandrel. Examine
the specimens for cracks.
4.3.6.2 Print Performance
Mark three specimens in accordance with Section 4.3.4 and recover them in an oven for 3
minutes at 200 ± 5oC (392 ± 9oF). Condition the specimens in the oven for 168 hours at 158 ±
2oC (316 ± 4oF). Cool to room temperature and test for print performance in accordance with
4.3.4.1
4.3.7 Dielectric Strength
The test method shall be as specified in ASTM D 2671.
4.3.8 Corrosive Effect
Test two specimens in accordance with ASTM D 2671, Procedure A for 16 hours at 158 ± 2 °C
(316 ± 4 °F).
4.3.9 Flammability
The test method shall be as specified in UL 224 All Tubing Flame Test.
4.3.10 Water Absorption
The test method shall be as specified in ASTM D 2671. The test conditions shall be 24 hours at
23 ± 3 °C (73 ± 5 °F).
4.3.11.1 Fungus resistance
Fungus resistance testing shall be conducted in accordance with accordance with ISO 846 B
with an incubation time of 56 days.
4.3.11.2 Tensile Strength
After conditioning per section 4.3.12, test for tensile strength in accordance with section 4.3.2.
U‘timate Elongalicn
Dielectric Strength
Fluid Resistance
Page 6 SPECIFICATION RW 2510 ISSUE 2
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
4.3.11.3 Ultimate Elongation
After conditioning per section 4.3.12, test for ultimate elongation in accordance with section
4.3.2.
Dielectric Strength
After conditioning per section 4.3.12, test for dielectric strength in accordance with section 4.3.7.
4.3.12 Fluid Resistance
Prepare 3 markers for each fluid listed in Table 4 by marking them in accordance with section
4.3.4. and recover them in an oven for 3 minutes at 200 ± 5oC (392 ± 9oF). Allow samples to
cool to room temperature. Immerse the samples for 24 hours at 23 ± 3 °C (73 ± 5 °F). The
volume of the fluid shall not be less than 20 times that of the specimens. After immersion, lightly
wipe the specimens and allow them to air dry 30-60 minutes at room temperature. Test the
specimens for print performance in accordance with Section 4.3.4.1.
4.4 REJECTIONS AND RETEST
Failure of any sample to conform to any of the requirements of this specification sheet shall be
cause for rejection of the lot represented. Markers, which have been rejected, may be replaced
or reworked to correct the defects and resubmitted for acceptance.
5. PREPARATION FOR DELIVERY
5.1 FORM
Markers shall be supplied on a carrier, either wound on spools, in strips or fan folded.
5.2 STORAGE CONDITIONS
Markers should be stored in a clean dry location. Maximum storage temp. 40°C (104°F).
5.3 PACKAGING
Packaging shall be in accordance with good commercial practice.
5.4 MARKING
Each container of markers shall be identified with the product designation, size, quantity,
manufacturer's identification and lot number and date of manufacture.
80.52 i 1.52
(3.170 t 0.060}
%
<—>
SLEEVE
WIDTH
1
48.26 MIN
4.83 i 0.25 ¢ TYP
(0.190 : 0.010) 3.05 (0.120)
O .'
TYP
2 E
38.10 i 0.25
(1.500 t 0.010)
_ 0- d} _é_ {5._
|
4.01 DIA i 0.13/fl/‘
(0158:0005)
+
1:1:zz:::::::::::::::::::
1
494040494040
0.56 MAXj
(0.022)
SLEEVE
PROGRESSION
CARRIER
—>
SPECIFICATION RW 2510 ISSUE 2 Page 7
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
FIGURE #1
Dimensions in mm (inches)
3.05 (0.120)
4.83 ± 0.25
(0.190 ± 0.010)
80.52 ± 1.52
(3.170 ± 0.060)
38.10 ± 0.25
(1.500 ± 0.010)
48.26 MIN
(1.900)
12.70
(0.500)
TYP
TYP
4.01 DIA ± 0.13
(0.158 ± 0.005)
CARRIER
SLEEVE
WIDTH
PROGRESSION
SLEEVE
0.56 MAX
(0.022)
(0.125) (0.042) (0.023 +). 0.003) (0.500 +Ir 0.035)
(0.250) (0.083) (0.023 +). 0.003) (0.007 +Ir 0.035)
(0.375) (0.125) (0.024 +). 0.003) (1.000 +Ir 0.045)
(0.500) (0.100) (0.024 +). 0.003) (1.107 +Ir 0.045)
(0.750) (0.250) (0.024 +). 0.003) (1.007 +Ir 0.045)
(1.000) (0.333) (0.025 +). 0.003) (2.000 +Ir 0.045)
(1.500) (0.750) (0.020 +). 0.003) (2.833 +Ir 0.045)
Page 8 SPECIFICATION RW 2510 ISSUE 2
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
TABLE 3
DIMENSIONAL REQUIREMENTS
IN mm, (INCHES)
Part Number
Minimum
Maximum
Recovered wall
thickness
Sleeve
progression
Nominal
Expanded
Recovered
Sleeve
Inside Dia.
Inside Dia.
Weight (g)
RPS 22-18
3.18
(0.125)
1.07
(0.042)
0.58 +/- 0.08
(0.023 +/- 0.003)
12.70 +/- 0.89
(0.500 +/- 0.035)
0.203
RPS 18-12
4.75
(0.187)
1.57
(0.062)
0.58 +/- 0.08
(0.023 +/- 0.003)
12.70 +/- 0.89
(0.500 +/- 0.035)
0.268
RPS 16-10
6.35
(0.250)
2.11
(0.083)
0.58 +/- 0.08
(0.023 +/- 0.003)
16.94 +/- 0.89
(0.667 +/- 0.035)
0.351
RPS 8-4
9.53
(0.375)
3.18
(0.125)
0.61 +/- 0.08
(0.024 +/- 0.003)
25.40 +/- 1.14
(1.000 +/- 0.045)
0.504
RPS 10-2
12.70
(0.500)
4.22
(0.166)
0.61 +/- 0.08
(0.024 +/- 0.003)
29.64 +/- 1.14
(1.167 +/- 0.045)
0.681
RPS 6-250
19.05
(0.750)
6.35
(0.250)
0.61 +/- 0.08
(0.024 +/- 0.003)
42.34 +/- 1.14
(1.667 +/- 0.045)
1.023
RPS 1-400
25.40
(1.000)
8.46
(0.333)
0.64 +/- 0.08
(0.025 +/- 0.003)
50.80 +/- 1.14
(2.000 +/- 0.045)
1.353
RPS 400-1000
38.10
(1.500)
19.05
(0.750)
0.51 +/- 0.08
(0.020 +/- 0.003)
71.96 +/- 1.14
(2.833 +/- 0.045)
2.198
mm In accordance with Table 3 Section 4.3.1
(inches) In accordance with Table 3 ASTM D 2671
Longitudinal Change Section 4.3.1
3 min. at 200° 1 suc (392° 1 9UP)
508 mm/min. (20 in./min) (psi) (1200) minimum ASTM D 2671
508 mm/min. (20 in./min) ASTM D 2671
Low Temperature Flexibility ,, No cracking Section 4.3.3
4 hours at 730° 1 200 (722° 1 40F)
Solvent/ Brush 1 30 strokes ,, Legible at 356 mm (14 inches) Section 4.3.4.3
Heat Shock 1, No dripping, flowing, Section 4.3.5
1 hr. at 136° 1 2°C (277 : 4”F)
Heat Aging
168 hrs. at 158“ 1 270 (316 : 4”F)
Followed by test for: Mandrei Bend 1, No cracking Section 4.3.6.1
Eraser Rub . 20 rubs ,, Legible at 356 mm (14 inches) Section 4.3.6.2
(Volts/mil) (500 minimum) ASTM D 2671
Procedure A
flowing.
Water Absorption
24 hours at 23° 1 3°C (73° 1 5°F)
Section 4.3.10
Followed by test for:
(Vclts / mil)
(500) minimum
ISO 846 B
ISO 846 B
SPECIFICATION RW 2510 ISSUE 2 Page 9
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
TABLE 4
Requirements
PROPERTY
UNIT
REQUIREMENT
TEST METHOD
Dimensions
mm
In accordance with Table 3
Section 4.3.1
(inches)
In accordance with Table 3
ASTM D 2671
Longitudinal Change
Section 4.3.1
3 min. at 200° ± 5oC (392° ± 9oF)
Percent
0 to -20
ASTM D 2671
Tensile Strength
508 mm/min. (20 in./min)
MPa
(psi)
8.27 minimum
(1,200) minimum
Section 4.3.2
ASTM D 2671
Ultimate Elongation
508 mm/min. (20 in./min)
Percent
150 minimum
Section 4.3.2
ASTM D 2671
Low Temperature Flexibility
---
No cracking
Section 4.3.3
4 hours at -30° ± 2oC (-22° ± 4oF)
Print Performance
Eraser Rub - 20 rubs, 2lbs
Solvent / Brush - 30 strokes
---
---
Legible at 356 mm (14 inches)
Legible at 356 mm (14 inches)
Section 4.3.4.1
Section 4.3.4.3
Heat Shock
---
No dripping, flowing,
Section 4.3.5
1 hr. at 136° ± 2oC (277 ± 4oF)
or cracking
UL 224
Heat Aging
168 hrs. at 158° ± 2oC (316 ± 4oF)
---
Section 4.3.6
Followed by test for: Mandrel Bend
---
No cracking
Section 4.3.6.1
Followed by: Print Performance
Eraser Rub - 20 rubs
---
Legible at 356 mm (14 inches)
Section 4.3.6.2
Dielectric Strength
MV/m
(Volts/mil)
19.7 minimum
(500 minimum)
Section 4.3.7
ASTM D 2671
Corrosive Effect
16 hours at 158 ± 2oC (316° ± 4oF)
---
5% transparent area maximum
Section 4.3.8
ASTM D 2671
Procedure A
Flammability
---
Burn time shall not exceed one
minute, and not more than 25%
of indicator flag shall be burned
or charred. No dripping or
flowing.
Section 4.3.9
UL 224 - All
Tubing Flame
Test
Water Absorption
Section 4.3.10
24 hours at 23° ± 3oC (73° ± 5oF)
Percent
0.5 maximum
ASTM D 2671
Fungus Resistance
56 day incubation
Section 4.3.11
ISO 846 B
Followed by test for:
Tensile Strength
MPa (psi)
8.27 (1,200) minimum
Section 4.3.11.1
ISO 846 B
Ultimate Elongation
Percent
150 minimum
Section 4.3.11.2
ISO 846 B
Dielectric Strength
Kv / mm
(Volts / mil)
19.7 minimum
(500) minimum
Section 4.3.11.3
ISO 846 B
Fluid Resistance
24 hours a123° 1 3°C (73° : 5 F)
HydroFlouroCarbon Solvent Vertrel XF
lsopropyl Alcohol
Gasoline (unleaded)
Diesel Fuel, DFZ
Motor Vehicle Brake Fluid, SAE J 1703
Ethylene Glycol
Eraser Rub . 20 rubs
Legible a1356 mm (14 inches)
Seclion 4.3.4.1
Page 10 SPECIFICATION RW 2510 ISSUE 2
©2014 Tyco Electronics Corporation, a TE Connectivity Ltd. Company
RW-2510 Issue 2
*Trademark. TE Connectivity, TE connectivity (logo), and TE (logo) are trademarks. Other logos, product and/or company names may be trademarks of
their respective owners.
If this document is printed it becomes uncontrolled.
TABLE 4
REQUIREMENTS cont.
Fluid Resistance
24 hours at 23° ± 3oC (73° ± 5oF)
---
---
Section 4.3.12
HydroFlouroCarbon Solvent Vertrel XF
Isopropyl Alcohol
Gasoline (unleaded)
Diesel Fuel, DF2
Auto Engine Oil, SF
10W-40 (SAE J 183, SAE J 300)
Motor Vehicle Brake Fluid, SAE J 1703
Ethylene Glycol
Followed by: Print Performance
Eraser Rub - 20 rubs
---
Legible at 356 mm (14 inches)
Section 4.3.4.1