Vizmonet Pte Ltd
About
The Horizon of Wireless Connectivity Solutions is expanding at a faster pace encompassing several new market segments. Thanks to rapid technology developments over the past two decades, several new wireless standards like WiFi, WiMAX, MIMO, ZigBee, LORA, M-BUS, Wi-SUN have emerged enabling man-to-man and machine-to-machine communications to deliver wireless data bandwidth in various capacities. This had opened up abundant opportunities across geographies for companies to come out with creative applications in Industrial IOT (IIOT) space. Applications like Industry 4.0 have emerged to create new wave of cloud-managed smart factories automating process and machines. However, these use cases have posed a great challenge to the companies in adopting new wireless technology as they have to go through painful long learning curve of acquiring RF design expertise.
This is where Vizmonet comes in to aid the companies plagued by these limitations, by taking care of the entire Wireless product development and offering complementary solutions to the OEM customers. Vizmonet’s innovative Built-to-customize™ Solutions add value to OEMs to shorten time-to-market by eliminating several man months in product development cycle. Vizmonet offers wide range of Software Configurable wireless solutions for hassle-free adoption into OEM systems.
Since inception, Vizmonet has designed, manufactured and shipped to OEMs that represent a variety of industry verticals covering wide frequency spectrum from 300 MHz to 6 GHz across several countries in Asia, America, Canada and Europe. At Vizmonet, Innovation is the key and the company invest in R&D on a continuous basis to develop wireless solution based on emerging technologies. The company is offering complete end-to-end wireless solutions to OEM customers. During execution of the projects, engineers work closely with OEM Customers’ engineering teams in delivering timely solutions with highest level of Quality-Of-Service.
Vizmonet’s manufacturing processes are stream lined to achieve highest level of scalability and quick ramp-up of new product volumes. With a lean organizational structure and work culture based on multi-task environment, operational efficiency of the company is maximized with the help of ERP systems to automate the processes from design to shipment.
The company aspires to become the default choice of go-to-vendor, when it comes to custom-design of Wireless communication modules and systems.