The Significance of the Intrinsic Body Diodes Inside MOSFETs

投稿人:DigiKey

Figure 1 shows a cross-section of an N-channel enhancement-mode MOSFET with the intrinsic body diodes indicated symbolically.  These MOSFETs have diodes in them pointing from the body to the drain and source.  The body to source diode is usually irrelevant, because it is shorted out by an internal body to source connection.

These diodes are appropriately named body diodes, and with the exception of JFETs, they are intrinsic to any FET type.  There are P-N junctions in the FET structure between the substrate and the doped regions.

Current typically flows from the drain to the source in N-channel FET applications because of the body diode polarity.  Even if a channel has not been induced, current can still flow from the source to the drain via the shorted source to body connection and the body to drain diode.  Because of this, a typical N-channel FET cannot block current flow from its source to its drain.

In some applications, such as certain DC-to-DC converters, the body diode is actually relied upon for normal circuit operation.  In contrast, it doubles the number of FETs necessary in other applications, such as certain power source selectors, where current must be blocked in both directions.

The two back-to-back P-N junctions also result in an intrinsic BJT (Bipolar Junction Transistor) within the FET; however, with a shorted body to source connection it effectively ceases to exist.

More considerations regarding MOSFET construction and operation are available here.

Cross-section of an N-channel enhancement-mode MOSFET

Figure 1: Cross-section of an N-channel enhancement-mode MOSFET with the intrinsic body diodes indicated symbolically.

免责声明:各个作者和/或论坛参与者在本网站发表的观点、看法和意见不代表 DigiKey 的观点、看法和意见,也不代表 DigiKey 官方政策。

关于此出版商

DigiKey

DigiKey 总部设在美国明尼苏达州锡夫里弗福尔斯市,是一个同时针对原型开发/设计提供小批量供应、针对生产提供大批量供应的全球电子元件综合服务提供商,在 DigiKey 上提供 750 多家优质制造商品牌、六百多万种产品。