E i.
SILIEEIN LABS
EFM32 Gecko
EFM32G Errata
This document contains information on the errata of EFM32G. The latest available revision of this device is revision E.
For errata on older revisions, please refer to the errata history section for the device. The device revision is typically the first letter on
the line immediately under the part number on the package marking. This is typically the second or third line.
Errata effective date: March 1st, 2017.
silabs.com | Building a more connected world. Rev. 2.20
1. Active Errata Summary
These tables lists all known errata for the EFM32G and all unresolved errata in revision E of the EFM32G.
Table 1.1. Errata History Overview
Designator Title/Problem Exists on Revision:
ABCDE
ACMP_E101 ACMP Mode — X — — —
ADC_E101 ADC Temperature Sensor X — — — —
ADC_E102 ADC SCANGAIN X — — — —
ADC_E104 ADC 1 Msample/s X X — — —
ADC_E105 ADC Output X — — — —
ADC_E106 ADC Reference Settling X X — — —
ADC_E108 ADC Temperature Sensor — X — — —
ADC_E110 ADC VDD Reference Gives Half Resolution — X — — —
ADC_E111 ADC References Doubled X X — — —
ADC_E112 ADC Accuracy X X — — —
ADC_E113 ADC Variability X X — — —
ADC_E114 Incorrect ADC Calibration Register Reset Value X X — — —
ADC_E115 Incorrect ADC Temperature Sensor Calibration Data X X X — —
ADC_E118 Requirements for ADC_CLK > 7 MHz X X X X X
AES_E101 BYTEORDER Does Not Work in Combination with DATA-
START/XORSTART
XXXXX
BOD_E101 BOD Threshold X — — — —
CMU_E101 Peripheral Clocks Active In EM2/EM3 During Debug X — — — —
CMU_E102 LFRCO/HFRCO Frequency Change During EM2/3 X — — — —
CMU_E103 Wrong RCO Frequency X — — — —
CMU_E104 Energy Mode Transitions Cause HFRCO Overshoot X X — — —
CMU_E105 AUXHFRCO Active in EM2/EM3 X — — — —
CMU_E106 LFXO Digital External Mode X X X X X
CMU_E107 Disabled Low Frequency Clocks X X — — —
CMU_E108 LFxCLKEN Write X X X — —
CMU_E109 LFXO Configuration Incorrect X X X — —
DAC_E101 DAC Sample-Hold X X — — —
DAC_E102 DAC Enabling X X — — —
DAC_E103 DAC Ringing X X — — —
DAC_E104 DAC Sample-Hold/Sample-Off X X — — —
DAC_E105 DAC Startup X X — — —
DAC_E107 DAC Accuracy X X — — —
EFM32G Errata
Active Errata Summary
silabs.com | Building a more connected world. Rev. 2.20 | 1
Designator Title/Problem Exists on Revision:
ABCDE
DAC_E108 Incorrect DAC Calibration Register Reset Value X X — — —
DAC_E109 DAC Output Drift Over Lifetime X X X X X
DMA_E101 EM2 with WFE and DMA X X X X X
EBI_E101 EBI Lines X X — — —
EMU_E101 EM Transition Brown Out X X — — —
EMU_E102 DMA Clock EM2/EM3 X — — — —
EMU_E103 EM4 current — X X X X
EMU_E104 Sequencing of Analog and Digital Power X X X X X
EMU_E105 Debug Unavailable During DMA Processing from EM2 X X X — —
EMU_E106 SWO Line Pulled Low in EM2 X X X — —
EMU_E107 Interrupts During EM2 Entry X X X X —
HFRCO_E101 HFRCO Calibration X — — — —
I2C_E101 I2C RX Overflow X ————
I2C_E102 I2C Disabled After EM2/EM3 X X — — —
LCD_E101 LCD Com Line X — — — —
LCD_E102 LCD Voltage Boost Current X X — — —
LETIMER_E101 Buffered Top Value X X — — —
LEUART_E101 LEUART + DMA X — — — —
LEUART_E102 LEUART Baudrate X X — — —
LEUART_E103 LEUART RXOF X X — — —
LFRCO_E101 LFRCO Frequency X X — — —
LFXO_E102 LFXO Temperature Sensitivity X X — — —
PCNT_E101 PCNT0 TOP Register X X — — —
PCNT_E102 PCNT Pulse Width Filtering Does Not Work X X X X X
RTC_E101 RTC PRS Output X X X X X
TIMER_E101 TIMER Up/Down Mode X X — — —
TIMER_E102 Timer Capture and Debugger X X X X X
USART_E101 U(S)ART Double Buffer X X X X X
USART_E102 U(S)ART RXOF X X — — —
USART_E103 U(S)ART Slave TXUF Causes Shift X X — — —
USART_E104 U(S)ART AUTOTRI One Cycle Late X X — — —
USART_E105 U(S)ART Fractional Baudrate X X — — —
USART_E106 U(S)ART Slave TX Tristate X X — — —
USART_E107 U(S)ART TXC X X — — —
USART_E108 U(S)ART Slave TX Data Required Early X X — — —
USART_E109 U(S)ART Slave TXUF Artifacts X X — — —
EFM32G Errata
Active Errata Summary
silabs.com | Building a more connected world. Rev. 2.20 | 2
Designator Title/Problem Exists on Revision:
ABCDE
USART_E110 U(S)ART Slave TX Data Lost X X — — —
USART_E111 U(S)ART RX DMA Request After TX X X — — —
VCMP_E101 VCMP Mode — X — — —
VCMP_E102 VCMP Current X X — — —
WDOG_E101 WDOG in EM2/EM3 X — — — —
WDOG_E102 WDOG Does Not Freeze in EM2/EM3 X X X — —
WDOG_E103 WDOG EM2 Detection with LFXO Digital/Sine Input X X X X X
Table 1.2. Active Errata Status Summary
Errata # Designator Title/Problem Workaround
Exists
Affected
Revision
Resolution
1 ADC_E118 Requirements for ADC_CLK > 7 MHz Yes E —
2 AES_E101 BYTEORDER Does Not Work in Combination with
DATASTART/XORSTART
Yes E —
3 CMU_E106 LFXO Digital External Mode Yes E —
4 DAC_E109 DAC Output Drift Over Lifetime Yes E —
5 DMA_E101 EM2 with WFE and DMA Yes E —
6 EMU_E103 EM4 current Yes E —
7 EMU_E104 Sequencing of Analog and Digital Power Yes E —
8 PCNT_E102 PCNT Pulse Width Filtering Does Not Work No E —
9 RTC_E101 RTC PRS Output Yes E —
10 TIMER_E102 Timer Capture and Debugger Yes E —
11 USART_E101 U(S)ART Double Buffer Yes E —
12 WDOG_E103 WDOG EM2 Detection with LFXO Digital/Sine Input Yes E —
EFM32G Errata
Active Errata Summary
silabs.com | Building a more connected world. Rev. 2.20 | 3
2. Detailed Errata Descriptions
2.1 ADC_E118 — Requirements for ADC_CLK > 7 MHz
Description of Errata
If operating the ADC_CLK at frequencies greater than 7 MHz, the ADC BIASPROG bitfield must be set to a value of 0xF4B in order to
meet specified performance. Operating the ADC_CLK at frequencies of 7 MHz or lower can use the default ADC BIASPROG value of
0x747.
Affected Conditions / Impacts
Devices operating the ADC_CLK at frequencies greater than 7 MHz while using the default ADC BIASPROG value of 0x747 may
experience performance outside data sheet limits.
Workaround
For systems requiring an ADC_CLK rate > 7 MHz, set the ADC BIASPROG bitfield to 0xF4B.
For systems requiring an ADC_CLK rate ≤ 7 MHz, set the ADC BIASPROG bitfield to 0x747.
Resolution
The revision 2.0 data sheet has been updated to reflect the new recommendations.
2.2 AES_E101 — BYTEORDER Does Not Work in Combination with DATASTART/XORSTART
Description of Errata
When the BYTEORDER bit in AES_CTRL is set, an encryption or decryption should not be started through DATASTART or XOR-
START.
Affected Conditions / Impacts
If BYTEORDER is used in combination with DATASTART or XORSTART, the AES data and key are interpreted in the wrong order.
Workaround
Do not use BYTEORDER in combination with DATASTART or XORSTART.
Resolution
There is currently no resolution for this issue.
2.3 CMU_E106 — LFXO Digital External Mode
Description of Errata
LFXO ready flags are never set when LFXO is configured in Digital External Clock mode.
Affected Conditions / Impacts
When LFXOMODE in CMU_CTRL is set to DIGEXTCLK, the LFXORDY flag in CMU_STATUS and CMU_IF will not be set when the
number of cycles set in LFXOTIMEOUT in CMU_CTRL has elapsed. Thus, polling of this flag will not work. However, the clock propa-
gates as normal. It is only the flag that is not set.
Workaround
To detect that the clock has propagated through the ripple counter, write to any Asynchronous Register in Low Energy peripheral and
wait for SYNCBUSY for that register field to go low. Remember to enable the LE core clockand the clock for the LE peripheral you
choose. For example, write 0xA5 to RTC_COMP0 and wait for COMP0 in RTC_SYNCBUSY to go low.
Resolution
There is currently no resolution for this issue.
EFM32G Errata
Detailed Errata Descriptions
silabs.com | Building a more connected world. Rev. 2.20 | 4
2.4 DAC_E109 — DAC Output Drift Over Lifetime
Description of Errata
The voltage output of the DAC might drift over time.
Affected Conditions / Impacts
When the device is powered and the DAC is disabled, stress on an internal circuit node can cause the output voltage of the DAC to
drift over time, and in some cases may violate the VDACOFFSET specification. If the DAC is always enabled while the device is pow-
ered, this condition cannot occur.
Workaround
Both in the startup initialization code and prior to disabling the DAC in application code, set the OPAnSHORT bit in DACn_OPACTRL
to a '1' for the corresponding DAC(s) used by the application. This will prevent the output voltage drift over time effect.
Resolution
There is currently no resolution for this issue.
2.5 DMA_E101 — EM2 with WFE and DMA
Description of Errata
WFE does not work for the DMA in EM2.
Affected Conditions / Impacts
In EM2, when sleeping with WFE (Wait for Event), an interrupt from the DMA will not wake up the system.
Workaround
Use WFI (Wait for Interrupt) or EM1 instead.
Resolution
There is currently no resolution for this issue.
EFM32G Errata
Detailed Errata Descriptions
silabs.com | Building a more connected world. Rev. 2.20 | 5
2.6 EMU_E103 — EM4 current
Description of Errata
In EM4 the device may consume 700nA instead of 20nA.
Affected Conditions / Impacts
If EM4 is issued within a 10 µs - 12 µs window after the 1 kHz RC oscillator rising edge transition, the device will permanently con-
sume 700 nA.
Workaround
There are two possible workarounds for this issue:
1. The first workaround is using the WDOG to identify the rising edge transition and add a delay before going into EM4. Write on the
WDOG_CTRL register (for instance WDOG->CTRL|=WDOG_CTRL_CLKSEL_ULFRCO) and wait for the SYNCBUSY to be released. The
release of the SYNCBUSY happens on a rising edge transition of the 1 kHz clock. After that, insert a number of __NOP(); to
cause a delay of 20 µs (12 µs plus margin). The number of __NOP(); will depend on the processor frequency. After the delay,
EM4 can be entered safely.
Note: To implement this workaround, the WDOG cannot be locked; otherwise, the registers will not be written.
2. The second workaround option is to output the ULFRCO on a pin (CMU_CLK0) using CMU_CTRL and CMU_ROUTE registers.
That pin should then be configured as push pull with interrupt enable on rising edge, so the device can go to EM2 while it waits
for the ULFRCO rising edge transition. When the interrupt occurs, clear it and add a number of __NOP(); before entering EM4, as
described in the first workaround.
Note: The pin used to output the ULFRCO should not be driven by an external source.
Resolution
There is currently no resolution for this issue.
2.7 EMU_E104 — Sequencing of Analog and Digital Power
Description of Errata
Power-on Reset might fail if power is applied to IOVDD_x or VDD_DREG before AVDD_x.
Affected Conditions / Impacts
The device might lock up if power is applied to IOVDD_x or VDD_DREG pins before AVDD_x pins during power up. This lock-up state
can be exited by removing power to the device followed by a power up sequence according to what is described in the workaround.
Workaround
Make sure that the power on the AVDD_x pins ramp earlier or at the same time as the power on IOVDD_x and VDD_DREG during
power up. Practical schematic recommendations for this workaround are given in the EFM32 Application Note AN0002: Hardware De-
sign Considerations.
Resolution
There is currently no resolution for this issue.
EFM32G Errata
Detailed Errata Descriptions
silabs.com | Building a more connected world. Rev. 2.20 | 6
2.8 PCNT_E102 — PCNT Pulse Width Filtering Does Not Work
Description of Errata
PCNT pulse width filtering does not work.
Affected Conditions / Impacts
The PCNT pulse width filter does not work as intended.
Workaround
Do not use the pulse width filter, i.e. ensure FILT = 0 in PCNTn_CTRL.
Resolution
There is currently no resolution for this issue.
2.9 RTC_E101 — RTC PRS Output
Description of Errata
The RTC PRS output might cause false triggers
Affected Conditions / Impacts
If the RTC is selected as a PRS producer, there might occur glitches which will accidentally cause false triggers.
Workaround
Do not use the RTC as a PRS producer; instead, use one of the other timer sources (e.g. TIMER0).
Resolution
There is currently no resolution for this issue.
2.10 TIMER_E102 — Timer Capture and Debugger
Description of Errata
Timer capture triggered when timer is halted by debugger.
Affected Conditions / Impacts
When DEBUGRUN is disabled and the capture input is HIGH, it is possible to wrongly trigger a capture event by halting the MCU and
starting it again (for instance by setting a breakpoint).
Workaround
Enable DEBUGRUN when using a debugger.
Resolution
There is currently no resolution for this issue.
EFM32G Errata
Detailed Errata Descriptions
silabs.com | Building a more connected world. Rev. 2.20 | 7
2.11 USART_E101 — U(S)ART Double Buffer
Description of Errata
Transmission control through TXDATAX and TXDOUBLEX does not work with data double buffering.
Affected Conditions / Impacts
When a frame is loaded into the transmission shift register, transmission control bits always taken from outer buffer element. If only
one frame is in the U(S)ART buffer, the content of the buffer elements is equivalent, and transmission control bits work as specified. If
two frames are in the buffer however, the control bits for the frame in the outer buffer are used for transmitting the frame in inner
buffer. This is not a problem for frames consisting of more than 9 bits, since these large frames occupy both the inner and outer buffer
elements.
Workaround
If using transmission control bits in registers TXDATAX or TXDOUBLEX, make sure there is not more than one frame in the U(S)ART
buffer at a time, or that the control bits are equal. When TXBL in U(S)ARTn_CTRL is cleared, the TXBL status and interrupt flags in
U(S)ARTn_STATUS and U(S)ARTn_IF respectively tell when the buffer is empty. When using transmission control bits, a single
frame can then be loaded into the USART for transmission.
Resolution
There is currently no resolution for this issue.
2.12 WDOG_E103 — WDOG EM2 Detection with LFXO Digital/Sine Input
Description of Errata
The WDOG will mistake EM2 for EM3 if using LFXO with digital or sine input.
Affected Conditions / Impacts
When the WDOG is using LFXO with digital or sine input as a clock source, it will mistake EM2 for EM3. The EM2RUN and EM3RUN
bits of WDOG_CTRL will behave accordingly.
Workaround
When using LFXO with digital/sine input, EM3RUN must be set to keep the WDOG running in EM2.
Resolution
There is currently no resolution for this issue.
EFM32G Errata
Detailed Errata Descriptions
silabs.com | Building a more connected world. Rev. 2.20 | 8
3. Errata History
This section contains the errata history for EFM32G devices.
For errata on latest revision, please refer to the beginning of this document. The device data sheet explains how to identify chip revi-
sion, either from package marking or electronically.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 9
3.1 Errata History Summary
This tables lists all resolved errata for the EFM32G.
Table 3.1. Errata History Status Summary
Errata # Designator Title/Problem Workaround
Exists
Affected
Revision
Resolution
1 ACMP_E101 ACMP Mode Yes B C
2 ADC_E101 ADC Temperature Sensor No A B
3 ADC_E102 ADC SCANGAIN Yes A B
4 ADC_E104 ADC 1 Msample/s Yes B C
5 ADC_E105 ADC Output Yes A B
6 ADC_E106 ADC Reference Settling Yes B C
7 ADC_E108 ADC Temperature Sensor Yes B C
8 ADC_E110 ADC VDD Reference Gives Half Resolution Yes B C
9 ADC_E111 ADC References Doubled Yes B C
10 ADC_E112 ADC Accuracy Yes B C
11 ADC_E113 ADC Variability Yes B C
12 ADC_E114 Incorrect ADC Calibration Register Reset Value Yes B C
13 ADC_E115 Incorrect ADC Temperature Sensor Calibration Data Yes C D
14 BOD_E101 BOD Threshold Yes A B
15 CMU_E101 Peripheral Clocks Active In EM2/EM3 During Debug Yes A B
16 CMU_E102 LFRCO/HFRCO Frequency Change During EM2/3 Yes A B
17 CMU_E103 Wrong RCO Frequency Yes A B
18 CMU_E104 Energy Mode Transitions Cause HFRCO Overshoot Yes B C
19 CMU_E105 AUXHFRCO Active in EM2/EM3 Yes A B
20 CMU_E107 Disabled Low Frequency Clocks Yes B C
21 CMU_E108 LFxCLKEN Write Yes C D
22 CMU_E109 LFXO Configuration Incorrect Yes C D
23 DAC_E101 DAC Sample-Hold Yes B C
24 DAC_E102 DAC Enabling Yes B C
25 DAC_E103 DAC Ringing Yes B C
26 DAC_E104 DAC Sample-Hold/Sample-Off Yes B C
27 DAC_E105 DAC Startup Yes B C
28 DAC_E107 DAC Accuracy No B C
29 DAC_E108 Incorrect DAC Calibration Register Reset Value Yes B C
30 EBI_E101 EBI Lines Yes B C
31 EMU_E101 EM Transition Brown Out Yes B C
32 EMU_E102 DMA Clock EM2/EM3 Yes A B
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 10
Errata # Designator Title/Problem Workaround
Exists
Affected
Revision
Resolution
33 EMU_E105 Debug Unavailable During DMA Processing from
EM2
Yes C D
34 EMU_E106 SWO Line Pulled Low in EM2 Yes C D
35 EMU_E107 Interrupts During EM2 Entry Yes D E
36 HFRCO_E101 HFRCO Calibration Yes A B
37 I2C_E101 I2C RX Overflow Yes A B
38 I2C_E102 I2C Disabled After EM2/EM3 Yes B C
39 LCD_E101 LCD Com Line Yes A B
40 LCD_E102 LCD Voltage Boost Current Yes B C
41 LEUART_E101 LEUART + DMA No A B
42 LEUART_E102 LEUART Baudrate Yes B C
43 LEUART_E103 LEUART RXOF Yes B C
44 LETIMER_E101 Buffered Top Value Yes B C
45 LFRCO_E101 LFRCO Frequency Yes B C
46 LFXO_E102 LFXO Temperature Sensitivity Yes B C
47 PCNT_E101 PCNT0 TOP Register Yes B C
48 TIMER_E101 TIMER Up/Down Mode Yes B C
49 USART_E102 U(S)ART RXOF Yes B C
50 USART_E103 U(S)ART Slave TXUF Causes Shift Yes B C
51 USART_E104 U(S)ART AUTOTRI One Cycle Late Yes B C
52 USART_E105 U(S)ART Fractional Baudrate Yes B C
53 USART_E106 U(S)ART Slave TX Tristate Yes B C
54 USART_E107 U(S)ART TXC Yes B C
55 USART_E108 U(S)ART Slave TX Data Required Early Yes B C
56 USART_E109 U(S)ART Slave TXUF Artifacts Yes B C
57 USART_E110 U(S)ART Slave TX Data Lost Yes B C
58 USART_E111 U(S)ART RX DMA Request After TX Yes B C
59 VCMP_E101 VCMP Mode Yes B C
60 VCMP_E102 VCMP Current No B C
61 WDOG_E101 WDOG in EM2/EM3 Yes A B
62 WDOG_E102 WDOG Does Not Freeze in EM2/EM3 Yes C D
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 11
3.2 Detailed Errata Descriptions
3.2.1 ACMP_E101 — ACMP Mode
Description of Errata
The ACMP only works in the low power reference mode.
Affected Conditions / Impacts
The ACMP only works in the low power reference mode. When the low power reference mode is disabled (by not setting the LPREF
bit in ACMPn_INPUTSEL), the ACMP does not work and its output is always 1.
Workaround
When using the ACMP, put it in its low power reference mode by setting the LPREF bit in ACMPn_INPUTSEL (which is the default
setting). In this mode, the power consumption in the reference buffer (VDD and bandgap) is lowered at the cost of accuracy.
Resolution
This issue is resolved in revision C devices.
3.2.2 ADC_E101 — ADC Temperature Sensor
Description of Errata
The temperature sensor in the ADC does not work.
Affected Conditions / Impacts
The temperature values read when sampling the temperature sensor in the ADC are not correct.
Workaround
Do not use the ADC temperature sensor.
Resolution
This issue is resolved in revision B devices.
3.2.3 ADC_E102 — ADC SCANGAIN
Description of Errata
SCANGAIN in ADCn_CAL affects the gain setting for single conversions.
Affected Conditions / Impacts
When SCANGAIN and SINGLEGAIN in ADCn_CAL have different values, single conversions will be affected by the SCANGAIN val-
ue.
Workaround
Configure SCANGAIN and SINGLEGAIN in ADCn_CAL to the same value. This requires the same reference to be used for both sin-
gle and scan conversions.
Resolution
This issue is resolved in revision B devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 12
3.2.4 ADC_E104 — ADC 1 Msample/s
Description of Errata
1 Msample/s is not achieved for default ADC bias settings.
Affected Conditions / Impacts
At default ADC bias settings the ADC conversion results are wrong when running the ADC_CLK at 13 MHz, which is required to reach
the 1 Msample/s performance. Under typical conditions wrong conversions have been observed for ADC_CLK speeds of 8 MHz and
higher.
Workaround
Increase the ADC performance by programming increased ADC bias, for example by using value 0xF0F for register ADCn_BIA-
SPROG.
Resolution
This issue is resolved in revision C devices.
3.2.5 ADC_E105 — ADC Output
Description of Errata
The ADC does not always sample a voltage at (or close to) the middle of its range correctly (e.g. when sampling 1.25V when using
the 2.5V internal reference).
Affected Conditions / Impacts
When the ADC is sampling voltages at (or close to) the middle of its range, the ADC output code can be off by a large value (e.g.
returning value 1023 or 3072 instead of the expected value of 2048). This effect happens for all ADC reference selections.
Workaround
Perform multiple (e.g. 3) ADC measurements for each ADC sample required and use the median value. Do not average the ADC
results, throw away the 1023 or 3072 sample instead.
Resolution
This issue is resolved in revision B devices.
3.2.6 ADC_E106 — ADC Reference Settling
Description of Errata
The ADC internal references, i.e. 1V25, 2V5 and VDD have a settling time of about 500 µs.
Affected Conditions / Impacts
Measurements done using one of the internal references will not be correct before the reference has settled. This effect appears when
switching between references and when the references have been off between samples.
Workaround
When using the internal references, set WARMUPMODE=3 in ADCn_CTRL and wait until the references have settled before taking
the first sample.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 13
3.2.7 ADC_E108 — ADC Temperature Sensor
Description of Errata
The temperature sensor in the ADC does not work out of reset.
Affected Conditions / Impacts
Temperature measurements done using the temperature sensor in the ADC will be wrong without the fix described below.
Workaround
To enable the temperature sensor, set *0x400C6018 = 0x6. This fix can not be used at the same time as the fix for CMU_E104.
Resolution
This issue is resolved in revision C devices.
3.2.8 ADC_E110 — ADC VDD Reference Gives Half Resolution
Description of Errata
When using the internal VDD reference, the ADC resolution is reduced to 11 bits.
Affected Conditions / Impacts
Measurements done with the VDD reference will appear to have been divided by 2.
Workaround
Double each measurement to give the measurements the correcamplitude, sacrificing one bit of resolution. This workaround will not
be compatible with devices of later revisions where this erratum is corrected.
Resolution
This issue is resolved in revision C devices.
3.2.9 ADC_E111 — ADC References Doubled
Description of Errata
In single-ended mode, external and differential references are doubled internally.
Affected Conditions / Impacts
The reference doubling results in a decrease of the ADC resolution by one bit. As an example, when using an external reference of 1
V in single ended mode, a signal with values from 0 V to 1 V will result in adc codes from 0 to 2047 instead of the full 0 to 4095.
Workaround
A temporary fix for the external references is to halve the reference voltage. This will give full resolution, but will not be compatible
with devices of later revisions where this erratum has been corrected.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 14
3.2.10 ADC_E112 — ADC Accuracy
Description of Errata
The ADC does not meet the specified accuracy of 11.7 effective bits. The ADC is monotonic and although within specification, the hit
frequency for some codes such as 3071 and 3072 is such that DNL is distinctly different from the average DNL (but there are no
missing codes). The gain of the 2XVDD reference is larger than 1.0.
Affected Conditions / Impacts
The ADC accuracy may vary depending on the ADC configuration and may in some cases be down to 10 effective bits. The DNL/INL
anomalies will cause low level spurs in the output spectra. The gain error for the 2XVDD reference is over 20 LSBs and gain for this
reference cannot be calibrated.
Workaround
ADC accuracy can be increased by using hardware oversampling to increase resolution and/or by increasing the ADC bias current.
The ADC oversampling rate can be programmed in the OVSRSEL field of the ADCn_CTRL register; the oversampling can be enabled
by using the OVS value in the RES field of the ADCn_SINGLECTRL or ADCn_SCANCTRL register. The ADC bias current can be
programmed via the ADCn_BIASPROG register.
Resolution
This issue is resolved in revision C devices.
3.2.11 ADC_E113 — ADC Variability
Description of Errata
The PSRR, CMRR and variability over temperature for the ADC do not meet the specification.
Affected Conditions / Impacts
With a DC input voltage, the ADC output will vary depending on changes in VDD level, input common mode level, and temperature.
The temperature related variation particularly applies to the 5VDIFF reference. For a DC level input, variability of the ADC output code
over VDD is 2, 32, 7 LSBs for the VDD, 5VDIFF, and external references respectively. With external references, there is about 8 LSBs
variation in ADC output code depending on the input common mode level.
Workaround
With external references, adjust the common mode level of the differential external reference to a lower level. For the external differ-
ential references, performance is better with the lower external reference negative input level at 0V.
Resolution
This issue is resolved in revision C devices.
3.2.12 ADC_E114 — Incorrect ADC Calibration Register Reset Value
Description of Errata
The ADC calibration register (ADCn_CAL) are not updated with calibration values from production test during reset.
Affected Conditions / Impacts
The ADC will be uncalibrated out of reset and can show offset and gain error outside of specification.
Workaround
Copy the gain and offset values for the selected ADC reference from the Device Information (DI) page in flash to the corresponding
ADCn_CAL register fields before starting a conversion.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 15
3.2.13 ADC_E115 — Incorrect ADC Temperature Sensor Calibration Data
Description of Errata
The ADC temperature sensor calibration value stored in the DI page is not correct.
Affected Conditions / Impacts
Devices with PROD_REV values of 9 or 10 does not have correct ADC temperature sensor reading stored in the
ADC0_TEMP_0_READ_1V25 register of the Device Information Page, and using this value for calculating the temperature will yield
wrong results.
Workaround
Instead of using the value stored in the Device Information table, use ADC0_TEMP_0_READ_1V25 = 0x906 and CAL_TEMP_0 =
0x19 when calculating the temperature. These values are gathered from production data, and will give an accuracy where 3x the
standard deviation correspond to 5.2 degrees celsius.
Resolution
This issue is resolved in revision D devices.
3.2.14 BOD_E101 — BOD Threshold
Description of Errata
The Brown-Out Detector (BOD) threshold voltage is calibrated to a too high value.
Affected Conditions / Impacts
The high BOD threshold voltage may create sporadic BOD resetswhile the EFM32 is running in Energy Mode 2. Also, the BOD may
cause a reset at higher voltages than specified as the threshold voltage in the Electrical Characterisitics.
Workaround
Download Development Kit Board Support Library and Example Code (rev 1.1.1 or later) and include efm32_chip.h in your project.
In the start of the application code, call void CHIP_Init(void). This procedure will re-program the device to a safe BOD threshold.
Resolution
This issue is resolved in revision B devices.
3.2.15 CMU_E101 — Peripheral Clocks Active In EM2/EM3 During Debug
Description of Errata
When a debug session has been active since the last reset, EM1 is entered when trying to enter EM2 or EM3.
Affected Conditions / Impacts
The device cannot enter EM2/3 if a debug session has been entered since the last reset. When attempting to go to either EM2 or
EM3, the system goes to EM1, and the peripheral clocks keep running, even though they should have been turned off in EM2/EM3.
This is only an issue when debugging a system.
Workaround
If the debugger is running, clear HFPERCLKEN in CMU_HFPERCLKDIV before going to EM2/EM3 and set it when going back to
EM0.
Resolution
This issue is resolved in revision B devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 16
3.2.16 CMU_E102 — LFRCO/HFRCO Frequency Change During EM2/3
Description of Errata
RCO oscillator frequency can become unstable on transitions between EM2/3 and EM0.
Affected Conditions / Impacts
When switching between EM0 and EM2/3, the following events can happen occasionally:
1. The frequency of LFRCO becomes off by up to 14%.
2. The frequency of HFRCO becomes off by up to 6%.
The frequency will be off for a shorter or longer period.
Workaround
Make this line of code part of your startup code, typically in the start of main():
*(volatile unsigned int*) 0x400C600CUL = 0x00020100;
As a result of this workaround, the current consumption in EM2/3 will go up by 450 nA. This fix is not compatible with devices of later
revisions where this erratum has been corrected.
Resolution
This issue is resolved in revision B devices.
3.2.17 CMU_E103 — Wrong RCO Frequency
Description of Errata
The HFRCO, AUCHFRCO and LFRCO oscillators has wrong frequency when running with default settings.
Affected Conditions / Impacts
The oscillator frequency has not been programmed with correct calibration values, and the frequencies are not within the expected
frequency ranges.
Workaround
The oscillator frequency can be calibrated in the Clock Management Unit, which is described in the CMU chapter of the EFM32G
Reference Manual.
Resolution
This issue is resolved in revision B devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 17
3.2.18 CMU_E104 — Energy Mode Transitions Cause HFRCO Overshoot
Description of Errata
Transitions between energy modes may cause an overshoot in the HFRCO frequency.
Affected Conditions / Impacts
When switching between energy modes, there is a slight chance that HFRCO will temporarily overshoot its configured frequency and
in some cases cause a BOD reset. This overshoot may be up to 50% and may take the system out of its allowed operating conditions
by having a system clock higher than 32 MHz. Note that when the MSC is configured to use zero waitstates when accessing flash, the
maximum core frequency is 16 MHz.
Workaround
To workaround this issue, set *0x400C6018 = 0xC201. This gives better HFRCO stability at the cost of an increased current consump-
tion in EM0 and EM1 of 10 uA. This fix is not compatible with the fix for ADC_E108. This fix is not compatible with devices of later
revisions where this erratum has been corrected.
Resolution
This issue is resolved in revision C devices.
3.2.19 CMU_E105 — AUXHFRCO Active in EM2/EM3
Description of Errata
AUXHFRCO is not disabled automatically when entering EM2/EM3.
Affected Conditions / Impacts
If AUXHFRCO is running while in EM2/EM3 and the EMVREG bit in EMU_CTRL is cleared, this may result in an unstable system.
Workaround
Disable AUXHFRCO by writing a 1 to AUXHFRCODIS in CMU_OSCENCMD before going to EM2/EM3. When waking up, enable the
AUXHFRCO again if needed by writing a 1 to AUXHFRCOEN in CMU_OSCENCMD.
Resolution
This issue is resolved in revision B devices.
3.2.20 CMU_E107 — Disabled Low Frequency Clocks
Description of Errata
Disabled Low Frequency Clocks tick once every second.
Affected Conditions / Impacts
The LFA and LFB clocks tick with a frequency equal to the source clock divided by 32768 when the correspondingenable bit in
CMU_LFACLKEN0/CMU_LFBCLKEN0 is not set. So, for example, if the RTC is enabled and RTC in CMU_LFACLKEN0 is 0,the RTC
will tick once every second. Notice that it is not possible to write to a Low Energy Peripheral when the clock tothe peripheral is not
enabled. Thus, the effects of this issue is only seen when the clock to an active Low Energy Peripheralis turned off.
Workaround
Disable the Low Energy Peripheral before disabling the clock to the Low Energy Peripheral to avoid unexpected behaviour.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 18
3.2.21 CMU_E108 — LFxCLKEN Write
Description of Errata
First write to LFxCLKEN can be missed.
Affected Conditions / Impacts
For devices with PROD_REV < 15, enabling the clock for LFA/LFB after reset and then immediately writing LFACLKEN/LFBCLKEN
may cause the write to miss its effect.
Workaround
For devices with PROD_REV < 15, make sure CMU_SYNCBUSY is not set before writing LFACLKEN/LFBCLKEN. Can temporarily
switch to HFCORECLKLEDIV2 to speed up clearing synchbusy.
Resolution
This issue is resolved in revision D devices.
3.2.22 CMU_E109 — LFXO Configuration Incorrect
Description of Errata
LFXO configuration incorrect.
Affected Conditions / Impacts
For devices with PROD_REV < 15, the default value for LFXOBOOST in CMU_CTRL is wrong.
Workaround
On devices with PROD_REV < 15, change LFXOBOOST to 0.
Resolution
This issue is resolved in revision D devices.
3.2.23 DAC_E101 — DAC Sample-Hold
Description of Errata
When the DAC is in sample/hold mode, the DAC output is not correctly held, but drifts faster than specified.
Affected Conditions / Impacts
The DAC output starts drifting in the order of 10 mV/µs after two DAC clock cycles.
Workaround
Put the DAC in continuous mode by setting the CONVMODE field in the DACn_CTRL register to CONTINUOUS. The DAC channels
will then drive their outputs continuously with the data in the DACn_CHxDATA registers. This mode will maintain the output voltage
and refresh is therefore not needed. As the DAC cores are not turned off between samples in continuous mode, the power consump-
tion is somewhat increased compared to sample/hold mode.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 19
3.2.24 DAC_E102 — DAC Enabling
Description of Errata
DAC conversions done closely after enabling the DAC channel are incorrect.
Affected Conditions / Impacts
The DAC output takes about 600 µs (under typical conditions) to settle after a DAC channel has been enabled via setting field CH0EN
in DACn_CH0CTRL (or CH1EN in DACn_CH1CTRL for channel 1). The effect is most visible for the 1.25V and 2.5V internal referen-
ces.
Workaround
After enabling a DAC channel, wait 600 µs before programming the channel data (via DACn_CH0DATA, DACn_CH1DATA, or
DACn_COMBDATA).
Resolution
This issue is resolved in revision C devices.
3.2.25 DAC_E103 — DAC Ringing
Description of Errata
Ringing effects can be observed on the DAC output.
Affected Conditions / Impacts
When applying large steps to the DAC, ringing can be observed on the output (up to 100 mV peak-to-peak depending on load). The
oscillations will last no longer than 1 µs.
Workaround
Add a filter on the DAC output or don't apply large steps.
Resolution
This issue is resolved in revision C devices.
3.2.26 DAC_E104 — DAC Sample-Hold/Sample-Off
Description of Errata
When a sample/refresh is done while in the sample-hold and sample-offmodes, a dip in the DAC output voltage occurs.
Affected Conditions / Impacts
The voltage-dip causes noise.
Workaround
Use the DAC in continuous mode by setting the CONVMODE field in the DACn_CTRL register to CONTINUOUS.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 20
3.2.27 DAC_E105 — DAC Startup
Description of Errata
When enabling a DAC channel, there may be a transient on the channel output. This transient may be up to 800 mV and last about 1
µs on an unloaded DAC.
Affected Conditions / Impacts
The DAC output is incorrect a short while after enabling the DAC channel.
Workaround
To prevent the transient on the DAC output, make sure the DAC output is disabled by clearing OUTMODE in DACn_CTRL when ena-
bling a DAC channel.
Resolution
This issue is resolved in revision C devices.
3.2.28 DAC_E107 — DAC Accuracy
Description of Errata
The DAC does not meet the specified accuracy of 11.5 effective bits. The DAC linearity does not meet the specification for all input
codes.
Affected Conditions / Impacts
The DAC accuracy may vary depending on the DAC configuration and may in some cases be down to 9 effective bits (which is pri-
marily caused by the SFDR without external filtering being limited to about 55 dB in case of the 1V25 reference). For some input co-
des, e.g. 1024, 2048, 3072, an increase/decrease of one input code will result in an output change equal to up to 3 input codes.
Workaround
No workaround.
Resolution
This issue is resolved in revision C devices.
3.2.29 DAC_E108 — Incorrect DAC Calibration Register Reset Value
Description of Errata
The DAC calibration register (DACn_CAL) is not updated with calibration values from production test during reset.
Affected Conditions / Impacts
The DAC will be uncalibrated out of reset and can show offset and gain error outside of specification.
Workaround
Copy the gain and offset values for the selected DAC reference from the Device Information (DI) page in flash to the corresponding
DACn_CAL register fields before starting a conversion.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 21
3.2.30 EBI_E101 — EBI Lines
Description of Errata
When the EBI is idle, the 16 address/data lines are left floating.
Affected Conditions / Impacts
The floating address/data lines may cause an increase in current consumption since the schmitt triggers of the GPIO inputs are still
on.
Workaround
Apply external pull-ups to the address-data lines, or make sure to control the address/data lines from software when not used.
Resolution
This issue is resolved in revision C devices.
3.2.31 EMU_E101 — EM Transition Brown Out
Description of Errata
In rare situations, transitioning between energy modes may cause a Brown Out (BO).
Affected Conditions / Impacts
When switching between energy modes, there is a chance that the system will experience a BO. In that case, the system will be reset
and the error condition can be detected by reading the RMU_RSTCAUSE register, which will then show that an internal BO was the
reason for the reset.
Workaround
To fix issue, set *0x400C6020 |= 0x6000. This prevents the BO, but results in an increase of current consumption in EM0 and EM1 by
about 4%. This fix is not compatible with devices of later revisions where this erratum has been corrected.
Resolution
This issue is resolved in revision C devices.
3.2.32 EMU_E102 — DMA Clock EM2/EM3
Description of Errata
When the DMA clock is disabled, the EFM32 is not able to go to Energy Modes 2 or 3.
Affected Conditions / Impacts
The DMA will prevent the system to go to EM2/EM3 as long as the DMA clock is disabled.
Workaround
Make sure the DMA clock is enabled when going to EM2/EM3. The DMA clock can be enabled in the CMU.
Resolution
This issue is resolved in revision B devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 22
3.2.33 EMU_E105 — Debug Unavailable During DMA Processing from EM2
Description of Errata
The debugger cannot access the system processing DMA request from EM2.
Affected Conditions / Impacts
DMA requests from the LEUART can trigger a DMA operation from EM2. While waiting for the DMA to fetch data from the respective
peripheral, the debugger cannot access the system. If such a DMA request is not handled by the DMA controller, the system will keep
waiting for it while denying debug access.
Workaround
Make sure DMA requests triggered from EM2 are handled.
Resolution
This issue is resolved in revision D devices.
3.2.34 EMU_E106 — SWO Line Pulled Low in EM2
Description of Errata
SWO pulled low in EM2.
Affected Conditions / Impacts
The SWO line is pulled low in EM2. This can be interpreted as garbage by an outside observer.
Workaround
Before entering EM2, disable pin-enable by clearing SWOPEN in GPIO_ROUTE and set the SWO pin output high. After exiting EM2,
the SWO pin should be re-enabled.
Resolution
This issue is resolved in revision D devices.
3.2.35 EMU_E107 — Interrupts During EM2 Entry
Description of Errata
An interrupt from a peripheral running from the high frequency clock that is received during EM2 entry will cause the EMU to ignore
the SLEEPDEEP flag.
Affected Conditions / Impacts
During EM2 entry, the high frequency clocks that are disabled during EM2 will run for some clock cycles after WFI isissued to allow
safe shutdown of the peripherals. If an enabled interrupt is requested from one of these non-EM2 peripherals during this shutdown
period, the attempt to enter EM2 will fail, and the device will enter EM1 instead. As a result, the pending interrupt will immediately
wake the device to EM0.
Workaround
Before entering EM2, disable all high frequency peripheral interrupts in the core.
Resolution
This issue is resolved in revision E devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 23
3.2.36 HFRCO_E101 — HFRCO Calibration
Description of Errata
The Device Information page does not contain calibration values for the 1 MHz, 7 MHz, 11 MHz, and 21 MHz frequency bands.
Affected Conditions / Impacts
The HFRCO frequency will be outside the expected frequency range when applying the calibration value from the device information
page.
Workaround
The oscillator frequency can be calibrated in the Clock Management Unit, which is described in the CMU chapter of the EFM32G
Reference Manual.
Resolution
This issue is resolved in revision B devices.
3.2.37 I2C_E101 — I2C RX Overflow
Description of Errata
If reception of a byte by the RX shift register is completed while there is still a byte in the RX buffer, the byte in the shift register is
silently discarded.
Affected Conditions / Impacts
If a received byte is acknowledged before it is read out of the RXDATA, all new bytes received before the read operation are discar-
ded. A new byte is not discarded if the read operation is performed before the new byte is fully received.
Workaround
Make sure to read the RX buffer before the reception of the next byte completes. One way to ensure this is to always read a received
byte before acknowledging it.
Resolution
This issue is resolved in revision B devices.
3.2.38 I2C_E102 — I2C Disabled After EM2/EM3
Description of Errata
If the USART0 clock is disabled, the I2C will not work when waking up from EM2/EM3.
Affected Conditions / Impacts
When waking up from EM2/EM3 with the USART0 clock disabled, the I2C module will be in a disabled state until the USART0 clock
has been enabled again.
Workaround
Make sure the USART0 clock is enabled when using the I2C. Alternatively, enable the USART0 clock for a short while after exiting
EM2/EM3.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 24
3.2.39 LCD_E101 — LCD Com Line
Description of Errata
Artifacts are seen on the LCD com lines (LCD_COM0-LCD_COM3).
Affected Conditions / Impacts
The LCD com lines (LCD_COM0-LCD_COM3) show intermediate voltage levels before settling to their correct values. The artifact
depends on the LCD contrast settings.
Workaround
Always adjust the LCD contrast relative to VDD (VLCD) by setting CONCONF field to 0 in LCD_DISPCTRL. This is its default value.
Use any contrast level other than the maximum value, so keep CONLEV in LCD_DISPCTRL in the range 0-30. The default value of
CONLEV is okay.
Resolution
This issue is resolved in revision B devices.
3.2.40 LCD_E102 — LCD Voltage Boost Current
Description of Errata
When the LCD boost target voltage is close to or lower than VDD, the voltage boost function draws an excessive amount of current
Affected Conditions / Impacts
If voltage boost is enabled when the boost target voltage, given by VBLEV in LCD_DISPCTRL is lower than or close to VDD, the
current consumption of the LCD driver increases by about 500 µA.
Workaround
Make sure the voltage boost is not enabled before VDD is below the boost target voltage. This can be done by using the VCMP mod-
ule to monitor VDD and enable/disable voltage boost when VDD goes below/above a given voltage, or by using the ADC to regularly
sample VDD.
Resolution
This issue is resolved in revision C devices.
3.2.41 LEUART_E101 — LEUART + DMA
Description of Errata
EM2 cannot be entered when transmitting the last byte using LEUART and DMA.
Affected Conditions / Impacts
When using the LEUART with DMA in EM2, TXDMAWU in LEUARTn_CTRL must be cleared when the DMA has no more data to
transmit. Otherwise the LEUART will keep the system awake waiting for data from the DMA. The way to do this is to clear TXDMAWU
in the DMA DONE interrupt for the channel feeding the LEUART with data. In this device revision, the DMA DONE interrupt will not
trigger a wakeup from EM2, and software will thus not be able to clear TXDMAWU immediately when a transmission has been com-
pleted, causing the system to be awake more than necessary.
Workaround
Use the TX complete interrupt (TXC) in the LEUART to clear TXDMAWU, or clear TXDMAWU in the DMA DONE interrupt and make
sure the TXC interrupt is triggered. The system will then be awake with a higher power consumption while the last byte is transmitted
by the LEUART, but will be allowed to go back to EM2 once TXDMAWU has been cleared.
Resolution
This issue is resolved in revision B devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 25
3.2.42 LEUART_E102 — LEUART Baudrate
Description of Errata
The LEUART baudrate generator should have an integral baudrate error no larger than ±0.5 clock cycles. However, the error may be
up to 1 clock cycle.
Affected Conditions / Impacts
For some baudrate settings, the jitter will be higher than ±0.5 clock cycles, and the average baudrate value will also not be as expec-
ted. For ~9600 b/s @ 32.768 kHz oscillator frequency, CLKDIV=0x268 and CLKDIV=0x270 for instance gives significantly different
baudrates. For lower baudrates, there should be no problem when using a 32 kHz oscillator.
Workaround
For 9600 b/s @ 32.768 kHz, use CLKDIV=0x270, which gives a baudrate of ~9534 b/s. This workaround will not be compatible with
devices of later revisions where this erratum has been corrected.
Resolution
This issue is resolved in revision C devices.
3.2.43 LEUART_E103 — LEUART RXOF
Description of Errata
In rare situations, the RX overflow interrupt can be set even though RX data is not lost.
Affected Conditions / Impacts
RXOF is set one cycle too early with the consequence that if RX buffer is read in the same internal clock cycle as RXOF is set, the
frame causing RX data is actually loaded into the RX buffer. Thus, the overflow interrupt does not guarantee that data has been lost.
Workaround
Consider RXOF as an indication that an overflow might have occurred.
Resolution
This issue is resolved in revision C devices.
3.2.44 LETIMER_E101 — Buffered Top Value
Description of Errata
CNT is updated with LETIMERn_COMP0 instead of LETIMERn_COMP1 when REP0 goes to zero.
Affected Conditions / Impacts
In Buffered Mode, both CNT and LETIMERn_COMP0 shall be updated with new LETIMERn_COMP1 value when REP0 goes to zero.
Instead, CNT gets the previous LETIMERn_COMP0 value, while LETIMERn_COMP0 is correctly updated. Thus, the first period in the
next repeat-sequence is the previous top value (LETIMERn_COMP0) and not the new top value (LETIMERn_COMP1) as one would
expect.
Workaround
No workaround.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 26
3.2.45 LFRCO_E101 — LFRCO Frequency
Description of Errata
The frequency of the LFRCO changes with up to 30% between EM0/EM1 and EM2/EM3.
Affected Conditions / Impacts
Calibrating the LFRCO for a given frequency in EM0/EM1 will not guarantee the same frequency in EM2/EM3.
Workaround
Use LFXO if an accurate clock frequency is important.
Resolution
This issue is resolved in revision C devices.
3.2.46 LFXO_E102 — LFXO Temperature Sensitivity
Description of Errata
LFXO may not start.
Affected Conditions / Impacts
On some devices the LFXO may not start, on others the LFXO may stop when temperature approaches -40C. In the latter case, the
LFXO will start up again when the temperature rises.
Workaround
Place a resistor in parallel with the LFXO crystal. The resistor should be approximately 50 MΩ.
Resolution
This issue is resolved in revision C devices.
3.2.47 PCNT_E101 — PCNT0 TOP Register
Description of Errata
The reset value of the TOP register of PCNT0 is incorrect.
Affected Conditions / Impacts
When counting downwards, the pulse counter underflows to an incorrect value. When counting upwards, no interrupt flag is set when
counting beyond the maximum value of 0xFF.
Workaround
Before enabling PCNT0, write the desired top value to the TOPB register. Then load this value into the TOP register by setting
LTOPBM in the CMD register.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 27
3.2.48 TIMER_E101 — TIMER Up/Down Mode
Description of Errata
In up/down mode, TIMERn_CCV and TIMER_TOP are updated on both overflow and underflow.
Affected Conditions / Impacts
Up/down mode may generate pulses that are not centered around the TIMERn_TOP value.
Workaround
Correct PWM operation can be ensured by updating TIMERn_CCx_CCVB after the timer overflow flag (TIMERn_IF_OF) is set. When
using the DMA overflow/underflow trigger to update TIMERn_CCx_CCVB, the CCV samples in the source buffer must duplicated
once. For example, if the CCV sequence is {0x24, 0x100, 0x99}, the buffer the DMA reads from must be {0x24, 0x24, 0x100, 0x100,
0x99, 0x99}. The first sample is written on the underflow event, and the second (duplicate) is written on the overflow event. The DMA
work-around is not compatible with the revision C fix.
Resolution
This issue is resolved in revision C devices.
3.2.49 USART_E102 — U(S)ART RXOF
Description of Errata
In rare situations, the RX overflow interrupt can be set even though RX data is not lost.
Affected Conditions / Impacts
RXOF is set one cycle too early with the consequence that if RX buffer is read in the same internal clock cycle as RXOF is set, the
frame causing RX data is actually loaded into the RX buffer. Thus, the overflow interrupt does not guarantee that data has been lost.
In addition, this frame will have its LSB cleared when transmitting LSB first, and its MSB cleared if MSB is transmitted first.
Workaround
On RX overflow, the last frame received may contain a bit error. Disregard this frame.
Resolution
This issue is resolved in revision C devices.
3.2.50 USART_E103 — U(S)ART Slave TXUF Causes Shift
Description of Errata
Slave TXUF may take TX out of sync with master.
Affected Conditions / Impacts
When in sync slave mode, an underflow may take the slave TX out of sync with the master clock, and data received at the master will
be shifted.
Workaround
Make sure the TX does not underflow when in slave mode.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 28
3.2.51 USART_E104 — U(S)ART AUTOTRI One Cycle Late
Description of Errata
The AUTOTRI feature enables output one cycle late.
Affected Conditions / Impacts
When output enable is controlled by AUTOTRI, the output will be enabled one clock cycle after the first data is output. The largest
effect of this will occur when the U(S)ART clock is close to the U(S)ART baudrate.
Workaround
If the timing of AUTOTRI is not sufficient, use the TXTRIEN/TXTRIDIS commands to enable and disable the USART output.
Resolution
This issue is resolved in revision C devices.
3.2.52 USART_E105 — U(S)ART Fractional Baudrate
Description of Errata
Fractional baudrate is wrong for divisors 1.25, 1.50, and 1.75.
Affected Conditions / Impacts
The fractional baudrate generated by the U(S)ART is wrong for the divisors 1.25, 1.50, and 1.75. This corresponds to the CLKDIV
values 0x40, 0x80, and 0xC0.
Workaround
Avoid using the erroneous divisors.
Resolution
This issue is resolved in revision C devices.
3.2.53 USART_E106 — U(S)ART Slave TX Tristate
Description of Errata
TXTRIEN/TXTRIDIS do not work in half-duplex synchronous slave mode.
Affected Conditions / Impacts
In slave mode, the TXTRIEN and TXTRIDIS commands have no effect on the enabled state of the MISO output. The MISO output is
controlled solely by whether the slave is selected by the master or not. This affects half-duplex communication when using the USART
in synchronous slave mode.
Workaround
To explicitly control output-enable in slave mode, use GPIO to control the mode of the MISO pin.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 29
3.2.54 USART_E107 — U(S)ART TXC
Description of Errata
TXC may be set even though data is in the TX buffer.
Affected Conditions / Impacts
If data is written to the U(S)ART at the same time as the previous transmission completes, the TXC status flag may be set even
though new data has been written to the USART and the USART starts transmission of this data.
Workaround
Qualify the TXC status with the status of TXBL to know whether the U(S)ART is idle and empty.
Resolution
This issue is resolved in revision C devices.
3.2.55 USART_E108 — U(S)ART Slave TX Data Required Early
Description of Errata
For CLKPHA=0, slave TX data is required too early.
Affected Conditions / Impacts
When operating with CLKPHA=0 and the slave TX is empty when CS is asserted or on the last edge of a frame, the slave underflows.
In this case, no data will be clocked out on the next frame.
Workaround
Make sure the slave TX has data in time or use CLKPHA=1 in synchronous slave mode.
Resolution
This issue is resolved in revision C devices.
3.2.56 USART_E109 — U(S)ART Slave TXUF Artifacts
Description of Errata
MISO toggling and TXUF set multiple times on slave TX underflow.
Affected Conditions / Impacts
When underflowing, a U(S)ART slave may give a pulse on MISO on every setup-edge of the SPI clock. The underflow interrupt flag
may also be set multiple times during a frame where the slave underflows.
Workaround
Make sure the slave TX has data in time.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 30
3.2.57 USART_E110 — U(S)ART Slave TX Data Lost
Description of Errata
For CLKPHA=0, a frame is cleared from TX buffer on CS deassert.
Affected Conditions / Impacts
When operating as a slave with CLKPHA=0, a frame is cleared from the TX buffer when CS is asserted by the SPI master.
Workaround
Use CLKPHA=1 or make sure to not write more data to the slave TX than what is intended to transmit during a transmission.
Resolution
This issue is resolved in revision C devices.
3.2.58 USART_E111 — U(S)ART RX DMA Request After TX
Description of Errata
For CLKDIV less than 0x100 RX DMA double requests come after the TX DMA double request.
Affected Conditions / Impacts
When operating with LOOPBK=1 writing and reading 16-bits at a time to the USART using DMA on a loaded system, this will result in
TX requests being handled before RX requests, which may result in TX transmitting frames too fast for RX to handle, leading to RX
overflows.
Workaround
Keep the system load under control and handle the U(S)ART overflows.
Resolution
This issue is resolved in revision C devices.
3.2.59 VCMP_E101 — VCMP Mode
Description of Errata
The VCMP only works in the low power reference mode.
Affected Conditions / Impacts
The VCMP only works in the low power reference mode. When the low power reference mode is disabled (by not setting the LPREF
bit in VCMP_INPUTSEL), the VCMP does not work and its output is always 1.
Workaround
When using the VCMP, put it in its low power reference mode by setting the LPREF bit in VCMP_INPUTSEL (which is the default
setting). In this mode, the power consumption in the reference buffer (VDD and bandgap) is lowered at the cost of accuracy.
Resolution
This issue is resolved in revision C devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 31
3.2.60 VCMP_E102 — VCMP Current
Description of Errata
The current consumption of the VCMP is too high in low power reference mode.
Affected Conditions / Impacts
When the VCMP is enabled in low power reference mode, the current consumption is higher than specified. The current is the same
independent of whether the low power reference mode is enabled or not.
Workaround
No workaround.
Resolution
This issue is resolved in revision C devices.
3.2.61 WDOG_E101 — WDOG in EM2/EM3
Description of Errata
When the watchdog (WDOG) triggers a reset while the EFM32 is in EM2 or EM3, the resulting behaviour is undefined.
Affected Conditions / Impacts
After a watchdog reset from EM2/EM3, the EFM32 may go directly to hard fault or may not start at all.
Workaround
Do not use the watchdog in EM2/EM3 by disabling WDOG before entering EM2/EM3. Note that the EM2RUN and EM3RUN bits can-
not be used (see WDOG_E102 erratum description).
Resolution
This issue is resolved in revision B devices.
3.2.62 WDOG_E102 — WDOG Does Not Freeze in EM2/EM3
Description of Errata
The WDOG keeps running in EM2 and EM3, even though the EM2RUN and EM3RUN bits in WDOG_CTRL are programmed to 0.
Affected Conditions / Impacts
If the WDOG is enabled when entering EM2 or EM3, a WDOG reset will occur unless the system wakes up from EM2/EM3 (by inter-
rupt) and clears the WDOG timer before the WDOG times out.
Workaround
Disable WDOG before entering EM2/EM3 by writing EN bit in WDOG_CTRL to 0. This requires that the WDOG configuration is un-
locked (LOCK bit in WDOG_CTRL = 0). If the WDOG configuration is locked, the WDOG will remain enabled in EM2/EM3, and the
system must wake up the device from EM2/EM3 and clear the WDOG before the WDOG times out.
Resolution
This issue is resolved in revision D devices.
EFM32G Errata
Errata History
silabs.com | Building a more connected world. Rev. 2.20 | 32
4. Revision History
4.1 Revision 2.20
March 1st, 2017
Added ADC_E118, DAC_E109, EBI_E101, and PCNT_E102.
Moved EMU_E107 to fixed for revision E devices.
Updated errata formatting.
Merged all errata documents for EFM32G devices into one document.
Merged errata history and errata into one document.
4.2 Revision 2.10
February 20th, 2015
Added PCNT_E102 and DAC_E109.
Added EMU_E107 for all devices except EFM32G800.
Corrected note on external driver in EMU_E103 for all devices except EFM32G800.
Updated link to errata for older revisions for all devices except EFM32G800.
4.3 Revision 2.00
August 21st, 2013
Updated disclaimer, trademark and contact information.
4.4 Revision 1.90
July 30th, 2013
Added DMA_E101.
Updated errata naming convention.
4.5 Revision 1.80
December 11th, 2012
Removed erratas no longer present for chip revision D: ADC_E115, CMU_E108, CMU_E109, EMU_E105, EMU_E106, WDOG_E102.
Added AES_E101 and TIMER_E102.
4.6 Revision 1.70
January 11th, 2011
Added CMU_E109.
Updated CMU_E108.
4.7 Revision 1.60
November 10th, 2011
Added CMU_E108 and EMU_E106.
EFM32G Errata
Revision History
silabs.com | Building a more connected world. Rev. 2.20 | 33
4.8 Revision 1.50
May 20th, 2011
Added ADC_E115, EMU_E105, and WDOG_E103.
4.9 Revision 1.40
November 17th, 2010
Added EMU_E104.
4.10 Revision 1.30
October 26th, 2010
Added EMU_E103 and RTC_E101.
4.11 Revision 1.20
August 31st, 2010
Removed errata not valid for chip revision C.
Added WDOG_E102.
4.12 Revision 1.10
June 25th, 2010
Removed ADC_E107, DAC_E106, and LCD_E103.
Added ACMP_E101, ADC_E112, ADC_E113, CMU_E106, CMU_E107, DAC_E107, LEUART_E103, LETIMER_E101, TIMER_E101,
USART_E102, USART_E103, USART_E104, USART_E105, USART_E106, USART_E107, USART_E108, USART_E109,
USART_E110, USART_E1011, VCMP_E101, and VCMP_E102.
4.13 Revision 1.00
April 23rd, 2010
Removed ADC_VCM errata.
Updated the errata which are to be fixed in chip revision C.
May 23th, 2011
Initial preliminary release for EFM32G222 devices.
October 15th, 2014
Initial release for EFM32G800 devices.
4.14 Revision 0.90
July 15th, 2011
Initial preliminary release for EFM32G232 and EFM32G842 devices.
4.15 Revision 0.10
April 8th, 2010
Initial preliminary release for EFM32G200, EFM32G210, EFM32G230, EFM32G280, EFM32G290, EFM32G840, EFM32G880, and
EFM32G890 devices.
EFM32G Errata
Revision History
silabs.com | Building a more connected world. Rev. 2.20 | 34
Q
SILICON LABS
http://www.silabs.com
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
USA
Simplicity Studio
One-click access to MCU and
wireless tools, documentation,
software, source code libraries &
more. Available for Windows,
Mac and Linux!
IoT Portfolio
www.silabs.com/IoT
SW/HW
www.silabs.com/simplicity
Quality
www.silabs.com/quality
Support and Community
community.silabs.com
Disclaimer
Silicon Labs intends to provide customers with the latest, accurate, and in-depth documentation of all peripherals and modules available for system and software implementers using or
intending to use the Silicon Labs products. Characterization data, available modules and peripherals, memory sizes and memory addresses refer to each specific device, and "Typical"
parameters provided can and do vary in different applications. Application examples described herein are for illustrative purposes only. Silicon Labs reserves the right to make changes
without further notice and limitation to product information, specifications, and descriptions herein, and does not give warranties as to the accuracy or completeness of the included
information. Silicon Labs shall have no liability for the consequences of use of the information supplied herein. This document does not imply or express copyright licenses granted
hereunder to design or fabricate any integrated circuits. The products are not designed or authorized to be used within any Life Support System without the specific written consent of
Silicon Labs. A "Life Support System" is any product or system intended to support or sustain life and/or health, which, if it fails, can be reasonably expected to result in significant personal
injury or death. Silicon Labs products are not designed or authorized for military applications. Silicon Labs products shall under no circumstances be used in weapons of mass
destruction including (but not limited to) nuclear, biological or chemical weapons, or missiles capable of delivering such weapons.
Trademark Information
Silicon Laboratories Inc.® , Silicon Laboratories®, Silicon Labs®, SiLabs® and the Silicon Labs logo®, Bluegiga®, Bluegiga Logo®, Clockbuilder®, CMEMS®, DSPLL®, EFM®, EFM32®,
EFR, Ember®, Energy Micro, Energy Micro logo and combinations thereof, "the world’s most energy friendly microcontrollers", Ember®, EZLink®, EZRadio®, EZRadioPRO®,
Gecko®, ISOmodem®, Precision32®, ProSLIC®, Simplicity Studio®, SiPHY®, Telegesis, the Telegesis Logo®, USBXpress® and others are trademarks or registered trademarks of Silicon
Labs. ARM, CORTEX, Cortex-M3 and THUMB are trademarks or registered trademarks of ARM Holdings. Keil is a registered trademark of ARM Limited. All other products or brand
names mentioned herein are trademarks of their respective holders.
Products related to this Datasheet
IC MICRO KIT GECKO 32QFN