CY8CKIT-003 Release Notes Datasheet by Cypress Semiconductor Corp
View All Related Products | Download PDF DatasheetE; CYPRESS
RRRRRRR
SRN51793
February 19, 2009 Document No. 001-51793 Rev ** - 1 -
Release Notes srn51793
CY8CKIT-003 PSoC3 FirstTouch™ Kit
Release Date: February 19, 2009
Thank you for your interest in CY8CKIT-003 PSoC3 FirstTouch™ Kit. This document lists the
installation requirements, limitations, and known bugs with Alpha release of the kit.
System Requirements and Recommendations
PSoC Creator™ 1.0 Beta1
PSoC Programmer™ 3.10
The minimum configurations required to run PSoC Creator are:
Windows Operating System: Windows XP SP2 and Windows Vista 32-bit
2 GB Memory
1 GB Hard Disk Space
USB 2.0 (for MiniProg3 connection – Beta1 requirement)
PSoC Creator requires the following software:
Windows Installer 3.1
.Net Framework 2.0 SP1
Keil Compiler
Adobe Reader (optional, but needed to view PDF files)
Installation
Insert the kit CD into your PC's CD-ROM drive. If the installer does not start automatically, start it
manually by clicking autorun.exe in the CD's root directory. After the installation begins, follow the
instructions during installation.
Notes
Do not connect your FirstTouch Kit with the USB port of a PC until all software installations are
complete.
If you have a previous installation of PSoC Creator and/or PSoC Programmer, you must uninstall
them before reinstalling PSoC Programmer and PSoC Creator.
Updates
N/A
[+] Feedback
a; CYPRESS
PERFORM
| | i |
SRN51793
February 19, 2009 Document No. 001-51793 Rev ** - 2 -
Limitations and Known Bugs
The CapSense™ slider and Proximity functions do not work, because CapSense
functionality is not available at the time of this release. CapSense projects are not
included with this release of the kit.
The temperature calibration for the “ThermistorTemperatureSense” project is not done.
The project is calibrated for 25 C only.
VBus sensing is not implemented in the design. The design will not pass USB back
voltage testing.
Suspend handling is not implemented in the design. The design will not pass USB
suspend current testing.
Documentation
Additional Kit documentation is available on the CD, which can be accessed from the
documentation folder of the FirstTouch Kit after installation:
Kit Guide
Release Notes
After installing the PSoC Creator and PSoC Programmer, refer to the documentation as needed:
PSoC Creator > Help > Getting Started
Programmer > User Guide
Other documents are available within PSoC Creator under Help Documentation. You can also
access them from the installation directory at:
C:\Program Files\Cypress\PSoC Creator\Documentation
PSoC Creator Component Author Guide
Warp Verilog Reference Guide
Customization API Reference
PSoC Training
N/A
Silicon Errata
Refer to PSoC Creator Release notes for details on Silicon Errata.
[+] Feedback
:E:
-C—YPRESS
PERFORM
SRN51793
February 19, 2009 Document No. 001-51793 Rev ** - 3 -
Cypress Semiconductor
198 Champion Ct.
San Jose, CA 95134-1709 USA
Tel: 408.943.2600
Fax: 408.943.4730
Application Support Hotline: 425.787.4814
www.cypress.com
© Cypress Semiconductor Corporation, 2009. The information contained herein is subject to change without notice.
Cypress Semiconductor Corporation assumes no responsibility for the use of any circuitry other than circuitry embodied in
a Cypress product. Nor does it convey or imply any license under patent or other rights. Cypress products are not
warranted nor intended to be used for medical, life support, life saving, critical control or safety applications, unless
pursuant to an express written agreement with Cypress. Furthermore, Cypress does not authorize its products for use as
critical components in life-support systems where a malfunction or failure may reasonably be expected to result in
significant injury to the user. The inclusion of Cypress products in life-support systems application implies that the
manufacturer assumes all risk of such use and in doing so indemnifies Cypress against all charges.
Programmable System-on-Chip™, and PSoC Creator™ are trademarks and PSoC® is a registered trademark of Cypress
Semiconductor Corp. All other trademarks or registered trademarks referenced herein are property of the respective
corporations.
This Source Code (software and/or firmware) is owned by Cypress Semiconductor Corporation (Cypress) and is protected
by and subject to worldwide patent protection (United States and foreign), United States copyright laws and international
treaty provisions. Cypress hereby grants to licensee a personal, non-exclusive, non-transferable license to copy, use,
modify, create derivative works of, and compile the Cypress Source Code and derivative works for the sole purpose of
creating custom software and or firmware in support of licensee product to be used only in conjunction with a Cypress
integrated circuit as specified in the applicable agreement. Any reproduction, modification, translation, compilation, or
representation of this Source Code except as specified above is prohibited without the express written permission of
Cypress.
Disclaimer: CYPRESS MAKES NO WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, WITH REGARD TO THIS
MATERIAL, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS
FOR A PARTICULAR PURPOSE. Cypress reserves the right to make changes without further notice to the materials
described herein. Cypress does not assume any liability arising out of the application or use of any product or circuit
described herein. Cypress does not authorize its products for use as critical components in life-support systems where a
malfunction or failure may reasonably be expected to result in significant injury to the user. The inclusion of Cypress’
product in a life-support systems application implies that the manufacturer assumes all risk of such use and in doing so
indemnifies Cypress against all charges.
Use may be limited by and subject to the applicable Cypress software license agreement.
[+] Feedback