dsPIC33FJ(32,64,128)MC(x02,x04) Errata & Datasheet Clarification by Microchip Technology
View All Related Products | Download PDF Datasheet6‘
MICROCHIP
Conflgure>Select Del/Ice
(DebuggebSe/ect T00!
(DebuggebConnect
2009-2015 Microchip Technology Inc. DS80000442K-page 1
dsPIC33FJ32MC302/304,
dsPIC33FJ64MCX02/X04 and
dsPIC33FJ128MCX02/X04
The dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/
X04 and dsPIC33FJ128MCX02/X04 family devices that
you have received conform functionally to the current
Device Data Sheet (DS70291G), except for the
anomalies described in this document.
The silicon issues discussed in the following pages are
for silicon revisions with the Device and Revision IDs
listed in Table 1. The silicon issues are summarized in
Table 2.
The errata described in this document will be addressed
in future revisions of the dsPIC33FJ32MC302/304,
dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/
X04 silicon.
Data Sheet clarifications and corrections start on
Page 13, following the discussion of silicon issues.
The silicon revision level can be identified using the
current version of MPLAB
®
IDE and Microchip’s
programmers, debuggers and emulation tools, which
are available at the Microchip corporate web site
(www.microchip.com).
For example, to identify the silicon revision level using
MPLAB IDE in conjunction with MPLAB ICD 3 or
PICkit™ 3:
1. Using the appropriate interface, connect the device
to the MPLAB ICD 3 programmer/debugger or
PICkit 3.
2. From the main menu in MPLAB IDE, select
Configure>Select Device, and then select the
target part number in the dialog box.
3. Select the MPLAB hardware tool
(Debugger>Select Tool).
4. Perform a “Connect” operation to the device
(Debugger>Connect). Depending on the devel-
opment tool used, the part number and Device
Revision ID value appear in the Output window.
The Device and Revision ID values for the various
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04
and dsPIC33FJ128MCX02/X04 silicon revisions are
shown in Table 1.
Note: This document summarizes all silicon
errata issues from all revisions of silicon,
previous as well as current. Only the
issues indicated in the last column of
Table 2 apply to the current silicon
revision (A5).
Note: If you are unable to extract the silicon
revision level, please contact your local
Microchip sales office for assistance.
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and
dsPIC33FJ128MCX02/X04 Family
Silicon Errata and Data Sheet Clarification
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 2 2009-2015 Microchip Technology Inc.
TABLE 1: SILICON DEVREV VALUES
Part Number Device ID
(1)
Revision ID for Silicon Revision
(2)
A1 A2 A3 A4 A5
dsPIC33FJ32MC302 0x0601
0x3001 0x3002 0x3002 0x3003 0x3004
dsPIC33FJ32MC304 0x0603
dsPIC33FJ64MC202 0x0611
dsPIC33FJ64MC204 0x0613
dsPIC33FJ64MC802 0x0619
dsPIC33FJ64MC804 0x061B
dsPIC33FJ128MC202 0x0621
0x3001 0x3002 0x3002 0x3003 0x3004
dsPIC33FJ128MC204 0x0623
dsPIC33FJ128MC802 0x0629
dsPIC33FJ128MC804 0x062B
Note 1: The Device and Revision IDs (DEVID and DEVREV) are located at the last two implemented addresses in
program memory.
2: Refer to the “dsPIC33F/PIC24H Flash Programming Specification” (DS70152) for detailed information on
Device and Revision IDs for your specific device.
2009-2015 Microchip Technology Inc. DS80000442K-page 3
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
TABLE 2: SILICON ISSUE SUMMARY
Module Feature Item
Number Issue Summary
Affected
Revisions
(1)
A1 A2 A3 A4 A5
UART IR Mode 1. The 16x baud clock signal on the BCLK pin is present
only when the module is transmitting. XXXXX
UART High-Speed
Mode 2. When the UART is in 4x mode (BRGH = 1) and using
two Stop bits (STSEL = 1), it may sample the first Stop
bit instead of the second one.
XXXXX
SPI Transmit
Operation 3. The SPIx Transmit Buffer Full (SPITBF) flag does not
get set immediately after writing to the buffer. XXXXX
SPI Frame Mode 4. The SPIx module will generate incorrect frame
synchronization pulses in Frame Master mode if
FRMDLY = 1.
XXXXX
I
2
CSFR Writes 5. The BCL bit in I2CxSTAT can only be cleared with word
instructions, and can be corrupted with byte instructions
and bit operations.
XXXXX
I
2
C10-Bit
Addressing 6. When the I
2
C module is configured for 10-Bit
Addressing, using the same Address bits (A10 and A9)
as other I
2
C devices, A10 and A9 bits may not work as
expected.
XXXXX
I
2
C10-Bit
Addressing 7. When the I
2
C module is configured as a 10-bit slave
with an address of 0x02, the I2CxRCV register content
for the lower address byte is 0x01 rather than 0x02.
XXXXX
I
2
C—8. With the I
2
C module enabled, the PORT bits and
external interrupt input functions (if any) associated with
the SCLx and SDAx pins will not reflect the actual digital
logic levels on the pins.
XXXXX
I
2
C10-Bit
Addressing 9. The 10-bit slave does not set the RBF flag or load the
I2CxRCV register on address match if the Least
Significant bits (LSbs) of the address are the same as
the 7-bit reserved addresses.
XXXXX
I
2
C—10. After the ACKSTAT bit is set when receiving a NACK, it
may be cleared by the reception of a Start or Stop bit. XXXXX
UART Interrupts 11. The UART error interrupt may not occur, or may occur
at an incorrect time, if multiple errors occur during a
short period of time.
XXXXX
UART IR Mode 12. When the UART module is operating in 8-bit mode
(PDSEL<1:0> = 0x) and using the IrDA
®
encoder/
decoder (IREN = 1), the module incorrectly transmits a
data payload of 80h as 00h.
XXXXX
Comparator Output Pin 13. When the CxOUTEN (CMCON) bit is set, the
comparator output pin cannot be used as a general
purpose I/O pin, even if the comparator is disabled.
XXXXX
Internal
Voltage
Regulator
Sleep Mode 14. When the VREGS bit (RCON<8>) is set to a logic ‘0’, the
device may reset and higher Sleep current may be
observed.
XXXXX
PSV
Operations —15. An address error trap occurs in certain addressing modes
when accessing the first four bytes of any PSV page. XXXXX
ECAN™ Sleep Mode 16. The WAKIF bit in the CiINTF register cannot be cleared
by software instruction after the device is interrupted
from Sleep due to activity on the CAN bus.
XXXXX
Note 1: Only those issues indicated in the last column apply to the current silicon revision.
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 4 2009-2015 Microchip Technology Inc.
ECAN™ Receive
Operation 17. The ECAN™ module may not store the received data in
the correct location. XXX
CPU EXCH
Instruction 18. The EXCH instruction does not execute correctly. X X X X X
PWM Debug Mode 19. PTMR does not keep counting down after halting code
execution in Debug mode. XXXXX
PWM Doze Mode 20. The Motor Control PWM module generates more
interrupts than expected when Doze mode is used and
the output postscaler value is different than 1:1.
XXXXX
SPI Transmit
Operation 21. Writing to the SPIxBUF register as soon as the TBF bit is
cleared will cause the SPIx module to ignore written data. XXXXX
UART Break
Character
Generation
22. The UARTx module will not generate back-to-back
Break characters. XXXXX
QEI Timer Gated
Accumulation
Mode
23. When Timer Gated Accumulation mode is enabled, the
QEI does not generate an interrupt on every falling
edge.
XXXXX
QEI Timer Gated
Accumulation
Mode
24. When Timer Gated Accumulation mode is enabled, and
an external signal is applied, the POSxCNT increments
and generates an interrupt after a match with MAXxCNT.
XXXXX
Audio DAC Voltage
Specifications 25. The audio DAC positive and negative output differential
voltages may not meet the specifications listed in the
data sheet.
XXX
ADC Current
Consumption
in Sleep Mode
26. If the ADC module is in an enabled state when the device
enters Sleep mode, the Power-Down (I
PD
) current of the
device may exceed the device data sheet specifications.
XXXXX
JTAG Boundary
Scan 27. On 28-pin devices, boundary scan does not function
correctly for Pin 7. XXXXX
RTCC Operation
During Reset 28. The RTCC module gets reset on any device Reset,
instead of getting reset only on a POR or BOR. XXXXX
All +150°C
Operation 29. These revisions of silicon only support +140°C
operation instead of +150°C for high-temperature
operating temperature.
XXX
I/O Port Data Direction
Setting 30. When the RB8 pin is in open-drain configuration, the
data direction depends upon the TRISB9 bit instead of
the TRISB8 bit.
XXXXX
CPU Interrupt
Disable 31. When a previous DISI instruction is active (i.e., the
DISICNT register is non-zero), and the value of the
DISICNT register is updated manually, the DISICNT
register freezes and disables interrupts permanently.
XXXXX
CPU div.sd 32. When using the div.sd instruction, the Overflow bit is
not getting set when an overflow occurs. XXXXX
UART TX Interrupt 33. A Transmit (TX) interrupt may occur before the data
transmission is complete. XXXXX
JTAG Flash
Programming 34. JTAG Flash programming is not supported. X X X X X
I
2
CSlave mode 35. Clock stretching may not occur when enabled. X X X X X
TABLE 2: SILICON ISSUE SUMMARY (CONTINUED)
Module Feature Item
Number Issue Summary
Affected
Revisions
(1)
A1 A2 A3 A4 A5
Note 1: Only those issues indicated in the last column apply to the current silicon revision.
Work around
Work around
Allecled Silicon Revisions
Allecled Silicon Revisions
Work around
Alleoled w
can Revisions
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
2009-2015 Microchip Technology Inc. DS80000442K-page 5
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
Silicon Errata Issues
1. Module: UART
When the UARTx is configured for IR interface
operations (UxMODE<9:8> = 11), the 16x baud
clock signal on the BCLK pin is present only when
the module is transmitting. The pin is Idle at all
other times.
Work around
Configure one of the output compare modules to
generate the required baud clock signal when the
UARTx is receiving data or in an Idle state.
Affected Silicon Revisions
2. Module: UART
When the UARTx is in 4x mode (BRGH = 1) and
using two Stop bits (STSEL = 1), it may sample the
first Stop bit instead of the second one.
This issue does not affect the other UARTx
configurations.
Work around
Use the 16x baud rate option (BRGH = 0) and
adjust the baud rate accordingly.
Affected Silicon Revisions
3. Module: SPI
The SPIx Transmit Buffer Full (SPITBF) flag does
not get set immediately after writing to the buffer.
Work around
After a write to the SPIx buffer, poll the SPITBF flag
until the flag gets set, indicating that the transmit
buffer is not full. Afterwards, poll the SPITBF flag
again until the flag gets cleared, indicating that the
transmit has started and that the transmit buffer is
empty, and another write can occur.
Affected Silicon Revisions
4. Module: SPI
The SPIx module will generate incorrect frame
synchronization pulses when configured in Frame
Master mode if the start of data is selected to
coincide with the start of the frame synchronization
pulse (FRMEN = 1, SPIFSD = 0, FRMDLY = 1).
However, the module functions correctly in Frame
Slave mode and also in Frame Master mode if
FRMDLY = 0.
Work around
If DMA is not being used, manually drive the SSx
pin (x = 1 or 2) high, using the associated PORT
register, and then drive it low after the required
1 bit time pulse width. This operation needs to be
performed when the transmit buffer is written.
If DMA is being used, and if no other peripheral
modules are using DMA transfers, use a timer
interrupt to periodically generate the frame
synchronization pulse (using the method
described above) after every 8 or 16-bit period
(depending on the data word size configured using
the MODE16 bit).
If FRMDLY = 0, no work around is needed.
Affected Silicon Revisions
5. Module: I
2
C
The BCL bit in I2CxSTAT can only be cleared with
word instructions, and can be corrupted with byte
instructions and bit operations.
Work around
Use word instructions to clear the BCL bit.
Affected Silicon Revisions
Note: This document summarizes all silicon
errata issues from all revisions of silicon,
previous as well as current. Only the
issues indicated by the shaded column in
the following tables apply to the current
silicon revision (A5).
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 6 2009-2015 Microchip Technology Inc.
6. Module: I
2
C
If there are two I
2
C devices on the bus, one of
them is acting as the master receiver and the other
as the slave transmitter. If both devices are
configured for 10-Bit Addressing mode, and have
the same value in the A10 and A9 bits of their
addresses, then when the slave select address is
sent from the master, both the master and slave
Acknowledge it. When the master sends out the
read operation, both the master and the slave
enter into Read mode and both of them transmit
the data. The resultant data will be the ANDing of
the two transmissions.
Work around
In all I
2
C devices, the addresses, as well as bits,
A10 and A9, should be different.
Affected Silicon Revisions
7. Module: I
2
C
When the I
2
C module is configured as a 10-bit slave
with an address of 0x02, the I2CxRCV register
content for the lower address byte is 0x01, rather
than 0x02; however, the module Acknowledges
both address bytes.
Work around
None.
Affected Silicon Revisions
8. Module: I
2
C
With the I
2
C module enabled, the PORT bits and
external interrupt input functions (if any), associ-
ated with the SCLx and SDAx pins, do not reflect
the actual digital logic levels on the pins.
Work around
If the SDAx and/or SCLx pins need to be polled,
these pins should be connected to other port pins
in order to be read correctly. This issue does not
affect the operation of the I
2
C module.
Affected Silicon Revisions
9. Module: I
2
C
In 10-Bit Addressing mode, some address matches
do not set the RBF flag or load the I2Cx Receive
register, I2CxRCV, if the lower address byte
matches the reserved addresses. In particular,
these include all addresses with the form,
‘xx0000xxxx’ and ‘xx1111xxxx’, with the
following exceptions:
•‘001111000x’
•‘011111001x’
•‘101111010x’
•‘111111011x’
Work around
Ensure that the lower address byte in 10-Bit
Addressing mode does not match any 7-bit
reserved addresses.
Affected Silicon Revisions
10. Module: I
2
C
When the I
2
C module is operating in either Master
or Slave mode, after the ACKSTAT bit is set when
receiving a NACK, it may be cleared by the
reception of a Start or Stop bit.
Work around
Store the value of the ACKSTAT bit immediately
after receiving a NACK from the master.
Affected Silicon Revisions
11. Module: UART
The UARTx error interrupt may not occur, or may
occur at an incorrect time, if multiple errors occur
during a short period of time.
Work around
Read the error flags in the UxSTA register
whenever a byte is received to verify the error
status. In most cases, these bits will be correct,
even if the UARTx error interrupt fails to occur.
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled
can Rev
Work around
Work around
Allecled Silicon Revisions
Work around
Allecled
' can Revisions
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
2009-2015 Microchip Technology Inc. DS80000442K-page 7
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
12. Module: UART
When the UARTx is operating in 8-bit mode
(PDSEL<1:0> = 0x) and using the IrDA encoder/
decoder (IREN = 1), the module incorrectly
transmits a data payload of 80h as 00h.
Work around
None.
Affected Silicon Revisions
13. Module: Comparator
If the CxOUTEN (CMCON) bit is set and the
Comparator x Enable bit, CxEN (CMCON), is
disabled, the remappable Comparator Output
pins, C1OUT and C2OUT, cannot be used as
general purpose I/O pins.
Work around
When the comparator module is disabled, the
CxOUTEN bit should be reset so that the
remappable Comparator Output pins, C1OUT and
C2OUT, are not driven onto the output pad.
Affected Silicon Revisions
14. Module: Internal Voltage Regulator
When the VREGS bit (RCON<8>) is set to a logic
‘0’, the device may reset and a higher Sleep
current may be observed.
Work around
Ensure that the VREGS bit (RCON<8>) is set to a
logic ‘1’ for device Sleep mode operation.
Affected Silicon Revisions
15. Module: PSV Operations
An address error trap occurs in certain addressing
modes when accessing the first four bytes of a
PSV page. This only occurs when using the
following addressing modes:
• MOV.D
• Register Indirect Addressing (Word or Byte
mode) with Pre/Post-Decrement
Work around
Do not perform PSV accesses to any of the first
four bytes using the above addressing modes. For
applications using the C language, MPLAB
®
C30
Version 3.11 or higher provides the following
command-line switch that implements a work
around for the erratum.
-merrata=psv_trap
Refer to the readme.txt file in the MPLAB C30
v3.11 toolsuite for further details.
Affected Silicon Revisions
16. Module: ECAN™
The WAKIF bit in the CiINTF register cannot be
cleared by software instructions after the device is
interrupted from Sleep due to activity on the CAN
bus.
When the device wakes up from Sleep due to CAN
bus activity, the ECAN module is placed in
Operational mode. The ECAN event interrupt
occurs due to the WAKIF flag. Trying to clear the
flag in the Interrupt Service Routine (ISR) may not
clear the flag. The WAKIF bit being set will not
cause repetitive Interrupt Service Routine
execution.
Work around
Although the WAKIF bit does not clear, the device
Sleep and ECAN wake function continue to work
as expected. If the ECAN event is enabled, the
CPU will enter the Interrupt Service Routine due to
the WAKIF flag getting set. The application can
maintain a secondary flag, which tracks the device
Sleep and wake events.
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled Silicon Revisions
Work around
(Pm am > Build
Ognons > Pm'ects > MPLAB 030 > Use Alternate
Settings
Allecled
can Revisions
Work around
Allecled S
ons
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 8 2009-2015 Microchip Technology Inc.
17. Module: ECAN
The ECAN module may not store received data in
the correct location. When this occurs, the receive
buffers will become corrupted. In addition, it is also
possible for the transmit buffers to become
corrupted. This issue is more likely to occur as the
CAN bus speed approaches 1 Mbps.
Work around
Do not use the DMA with ECAN in Peripheral
Indirect mode. Use the DMA in Register Indirect
mode, Continuous mode enabled and Ping-Pong
mode disabled. The receive DMA channel count
should be set to 8 words. The transmit DMA
channel count should be set for the actual
message size (maximum of 7 words for Extended
CAN messages and 6 words for Standard CAN
messages). To simplify application error handling
while using this mode, only one TX buffer should
be used. While message filtering is not affected,
messages will not be stored at distinct RX buffers.
Instead, all messages are stored contiguously in
memory. The start of this memory is pointed to by
the receive DMA channel. The application must
still clear the RXFULx flags and other interrupt
flags. The application must also manage the RX
buffer memory.
Affected Silicon Revisions
18. Module: CPU
The EXCH instruction does not execute correctly.
Work around
If writing source code in assembly, the
recommended work around is to replace:
EXCH Wsource, Wdestination
with:
PUSH Wdestination
MOV Wsource, Wdestination
POP Wsource
If using the MPLAB C30 C compiler, specify the
compiler option: -merrata=exch (Project > Build
Options > Projects > MPLAB C30 > Use Alternate
Settings).
Affected Silicon Revisions
19. Module: PWM
If the PTDIR bit is set (when PTMR is counting
down), and the CPU execution is halted (after a
breakpoint is reached), PxTMR will start counting
up as if PTDIR was zero.
Work around
None.
Affected Silicon Revisions
20. Module: PWM
When the device is operated in Doze mode and the
Motor Control PWM module has a postscaler set to
any value different than 1:1 (PTOPS<3:0> > 0 in the
PxTCON register), the Motor Control PWM module
generates more interrupts than expected.
Work around
Do not use Doze mode with the Motor Control PWM
if the time base output postscaler is different than
1:1 (PTOPS<3:0> > 0 in the PxTCON register).
Affected Silicon Revisions
21. Module: SPI
Writing to the SPIxBUF register as soon as the
TBF bit is cleared will cause the SPIx module to
ignore the written data. Applications which use
SPIx with DMA will not be affected by this erratum.
Work around
After the TBF bit is cleared, wait for a minimum
duration of one SPI clock before writing to the
SPIxBUF register.
Alternatively, do one of the following:
• Poll the RBF bit and wait for it to get set before
writing to the SPIxBUF register
• Poll the SPIx interrupt flag and wait for it to get
set before writing to the SPIxBUF register
• Use an SPI Interrupt Service Routine
•Use DMA
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
2009-2015 Microchip Technology Inc. DS80000442K-page 9
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
22. Module: UART
The UARTx module will not generate consecutive
Break characters. Trying to perform a back-to-
back Break character transmission will cause the
UARTx module to transmit the dummy character,
used to generate the first Break character, instead
of transmitting the second Break character. Break
characters are generated correctly if they are
followed by a non-Break character transmission.
Work around
None.
Affected Silicon Revisions
23. Module: QEI
When the TQCS and TQGATE bits in the
QEIxCON register are set, a QEI interrupt should
be generated after an input pulse on the QEA
input. This interrupt is not generated in the affected
silicon.
Work around
None.
Affected Silicon Revisions
24. Module: QEI
When the TQCS and TQGATE bits in the
QEIxCON register are set, the POSxCNT counter
should not increment, but erroneously does, and if
allowed to increment to match MAXxCNT, a QEI
interrupt will be generated.
Work around
To prevent the erroneous increment of POSxCNT
while running the QEI in Timer Gated Accumulation
mode, initialize MAXxCNT = 0.
Affected Silicon Revisions
25. Module: Audio DAC
The audio DAC positive differential output
voltage and negative differential output voltage
(Parameters DA01 and DA02, respectively) may
not meet the specifications listed in the data sheet.
Work around
None.
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXX
Work around 2:
Work around 1:
Allecled
can Revisions
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 10 2009-2015 Microchip Technology Inc.
26. Module: ADC
If the ADC module is in an enabled state when the
device enters Sleep mode, as a result of executing
a PWRSAV #0 instruction, the device Power-Down
(I
PD
) current may exceed the specifications listed
in the device data sheet. This may happen even if
the ADC module is disabled by clearing the ADON
bit prior to entering Sleep mode.
Work around 1:
In order to remain within the I
PD
specifications listed
in the device data sheet, the user software must
completely disable the ADC module by setting the
ADC module disable bit in the corresponding
Peripheral Module Disable x register (PMDx), prior
to executing a PWRSAV #0 instruction.
Work around 2:
If the ADC module was previously initialized and
enabled before entering Sleep, execute the lines
of code provided in Example 1.
EXAMPLE 1:
Affected Silicon Revisions
Note: The ADC module must be reinitialized by
the user application before resuming ADC
operation.
Note: Unlike Work around 1, the user
application does not need to reinitialize
the ADC module; however, it is necessary
to re-enable the ADC module by setting
the ADON bit after waking from Sleep.
AD1CON1bits.ADON = 0; //Disable the ADC module
__asm__ volatile ("REPEAT #50"); //Wait 50 Tcy
__asm__ volatile ("NOP"); //Repeat NOP 51 times
Sleep(); // Execute PWRSAV #0 and go to Sleep
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
2009-2015 Microchip Technology Inc. DS80000442K-page 11
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
27. Module: JTAG
On 28-pin devices, JTAG boundary scan does not
function correctly for Pin 7. Both Pins 6 and 7
respond to stimulus applied to Pin 7.
Work around
Do not include Pin 7 in the JTAG boundary scan
chain for 28-pin devices.
Affected Silicon Revisions
28. Module: RTCC
The RTCC module gets reset on any device
Reset, instead of getting reset only on a POR or
BOR.
Work around
None.
Affected Silicon Revisions
29. Module: All
The affected silicon revisions listed below are not
warranted for operation at +150°C.
Work around
Only use the affected revisions of silicon for the
high-temperature operating range from -40°C to
+140°C.
Affected Silicon Revisions
30. Module: I/O Port
When the ODCB8 bit (Open-Drain Configuration)
is set to ‘1’, the data direction on the RB8 pin is
controlled by the TRISB9 bit instead of the TRISB8
bit.
Work around
Do not use the RB8 pin in open-drain configuration
while simultaneously using the RB9 pin.
Affected Silicon Revisions
31. Module: CPU
When a previous DISI instruction is active (i.e., the
DISICNT register is non-zero), and the value of the
DISICNT register is updated manually, the DISICNT
register freezes and disables interrupts permanently.
Work around
Avoid updating the DISICNT register manually.
Instead, use the DISI #n instruction with the
required value for ‘n’.
Affected Silicon Revisions
32. Module: CPU
When using the Signed 32-Bit by 16-Bit Division
instruction, div.sd, the Overflow bit does not
always get set when an overflow occurs.
Work around
Test for and handle overflow conditions outside of
the div.sd instruction.
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
Work around
Allecled Silicon Revisions
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 12 2009-2015 Microchip Technology Inc.
33. Module: UART
When using UTXISEL<1:0> = 01 (interrupt when last
character is shifted out of the Transmit Shift Register)
and the final character is being shifted out through
the Transmit Shift Register, the Transmit (TX)
interrupt may occur before the final bit is shifted out.
Work around
If it is critical that the interrupt processing occur
only when all transmit operations are complete,
hold off the interrupt routine processing by adding
a loop at the beginning of the routine that polls the
Transmit Shift Register Empty bit (TRMT) before
processing the rest of the interrupt.
Affected Silicon Revisions
34. Module: JTAG
JTAG Flash programming is not supported.
Work around
None.
Affected Silicon Revisions
35. Module: I
2
C
In Slave mode, clock stretching may not occur
during address detect, even when it has been
enabled (STREN = 1). As a result, the SCLREL bit
may not be cleared upon address reception when
the R/W bit is ‘0’. This is seen in both 7-Bit and
10-Bit Addressing modes.
Work around
User software should read the Acknowledged
address from the receive buffer before the data
byte is received. User software also needs to
configure the slave interrupt priority, such that, the
interrupt latency time should be less (before the
reception of the data byte).
Affected Silicon Revisions
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
A1 A2 A3 A4 A5
XXXXX
2009-2015 Microchip Technology Inc. DS80000442K-page 13
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
Data Sheet Clarifications
The following typographic corrections and clarifications
are to be noted for the latest version of the device data
sheet (DS70291G):
1. Module: Electrical Characteristics
For Parameter DC60d (Base I
PD
) in Table 31-7, the
maximum value is corrected to read as 85 A.
2. Module: Electrical Characteristics
For Parameter DI51d (Input Leakage Current) in
Table 31-9, the maximum value is corrected to
read as ±12 µA.
3. Module: Electrical Characteristics
For Parameter F21 (Internal RC Accuracy) in
Table 31-19, the minimum and maximum values for
the temperature range of -40°C to +85°C are
corrected to read as -30% for minimum and +30%
for maximum.
4. Module: Electrical Characteristics
For Parameter DA01 (Positive Output Differential
Voltage) in Table 31-48, the minimum value is
corrected to read as 0.8V.
5. Module: Electrical Characteristics
Table 31-18: AC Characteristics: Internal RC
Accuracy should be replaced with the following
table.
Note: Corrections are shown in bold. Where
possible, the original bold text formatting
has been removed for clarity.
TABLE 31-18: AC CHARACTERISTICS: INTERNAL RC ACCURACY
AC CHARACTERISTICS Standard Operating Conditions: 3.0V to 3.6V (unless otherwise stated)
Operating temperature -40°C T
A
+85°C for Industrial
-40°C T
A
+125°C for Extended
Param
No. Characteristic Min Typ Max Units Conditions
Internal FRC Accuracy @ 7.3728 MHz
(1,2)
F20 FRC -3 — 3 % -40°C T
A
-10°C V
DD
= 3.0-3.6V
FRC -2 — 2 % -10°C T
A
+85°C V
DD
= 3.0-3.6V
FRC -5 — 5 % +85°C T
A
+125°C V
DD
= 3.0-3.6V
Note 1: Frequency calibrated at +25°C and 3.3V. TUNx bits can be used to compensate for temperature drift.
2: Negative current is defined as current sourced by the pin.
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 14 2009-2015 Microchip Technology Inc.
6. Module: High-Temperature Electrical
Characteristics
A new table, Table 32-8: DC Characteristics: I/O
Pin Input Specifications and Parameter HDI51f
(Input Leakage Current, RB9-RB12), are added to
this chapter under DC Characteristics. They are
shown in Table 32-8 below. The following tables in
this chapter will be renumbered sequentially.
7. Module: High-Temperature Electrical
Characteristics
A new table, Table 32-19: AC Characteristics:
Internal FRC Accuracy, is added to this chapter
under AC Characteristics. Table 32-19 summarizes
the internal oscillator tolerance over the entire
temperature range.
TABLE 32-8: DC CHARACTERISTICS: I/O PIN INPUT SPECIFICATIONS
DC CHARACTERISTICS
Standard Operating Conditions: 3.0V to 3.6V
(unless otherwise stated)
Operating temperature -40°C T
A
+150°C for Extended Temperature
Param
No. Symbol Characteristic Min Typ
(1)
Max Units Conditions
HDI51f I
IL
Input Leakage Current,
RB9 through RB12 ——±15µAV
SS
V
PIN
V
DD
,
pin at high-impedance,
-40°C T
A
+150°C
Note 1:
Negative current is defined as current sourced by the pin.
TABLE 32-19: AC CHARACTERISTICS: INTERNAL FRC ACCURACY
AC CHARACTERISTICS Standard Operating Conditions: 3.0V to 3.6V (unless otherwise stated)
Operating temperature -40°C T
A
+150°C for High Temperature
Param
No. Characteristic Min Typ Max Units Conditions
HF20 FRC
(1,2)
-5 — 5 % -40°C T
A
+150°C V
DD
= 3.0-3.6V
Note 1:
Negative current is defined as current sourced by the pin.
2:
Frequency is calibrated at +25°C and 3.3V. The TUNx bits can be used to compensate for temperature drift.
Rev A Documenl 3/2009
Rev B Documenl 4/2009
Rev C Documenl 8/2009
Rev D Documenl 1/2010
Rev E Documenl 6/2010
Rev F Documenl (10/2010
Rev G Documenl 3/2011
Rev H Documenl 11/2011
Rev J Documenl (11/2013)
Rev K Documenl (11/2015)
2009-2015 Microchip Technology Inc. DS80000442K-page 15
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
APPENDIX A: REVISION HISTORY
Rev A Document (3/2009)
Initial release of this document; issued for revision A1,
A2 and A3 silicon.
Includes silicon issues 1-2 (UART), 3-4 (SPI), 5-10 (I
2
C),
11-12 (UART), 13 (Comparator), 14 (Internal Voltage
Regulator), 15 (PSV Operations), 16-17 (ECAN™), 18
(CPU), 19-20 (PWM) and 21 (SPI).
This document replaces the following errata document:
“dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04
and dsPIC33FJ128MCX02/X04 Rev. A1/A2/A3 Silicon
Errata” (DS80372)
Rev B Document (4/2009)
Corrected part numbers.
Rev C Document (8/2009)
Added silicon issues 22 (UART) and 23-24 (QEI).
Rev D Document (1/2010)
Added Rev. A4 silicon information.
Added silicon issue 25 (Audio DAC).
Rev E Document (6/2010)
Updated silicon issue 18 (CPU).
Added silicon issues 26 (ADC), 27 (JTAG) and 28 (RTCC),
and data sheet clarification 1 (DC Characteristics: I/O Pin
Input Specifications).
Rev F Document (10/2010)
Updated the work around in silicon issue 26 (ADC).
Added silicon issue 29 (All).
Rev G Document (3/2011)
Removed data sheet clarification 1.
Updated the Affected Silicon Revisions for item 29 in
Table 2 and in silicon issue 29 (All).
Added silicon issue 30 (I/O Port).
Rev H Document (11/2011)
Updated the current Device Data Sheet revision to “F”.
Added Rev. A5 silicon information.
Added silicon issues 31 (CPU), 32 (CPU), 33 (UART),
and 34 (JTAG).
Rev J Document (11/2013)
Updated the current Device Data Sheet revision to “G”.
Added data sheet clarifications 1 through 5 (Electrical
Characteristics) and 6 through 7 (High-Temperature
Electrical Characteristics).
Other minor typographic changes to improve table
readability.
Rev K Document (11/2015)
Added silicon issue 35 (I
2
C).
dsPIC33FJ32MC302/304, dsPIC33FJ64MCX02/X04 and dsPIC33FJ128MCX02/X04
DS80000442K-page 16 2009-2015 Microchip Technology Inc.
NOTES:
YSTEM
2009-2015 Microchip Technology Inc. DS80000442K-page 17
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights unless otherwise stated.
Trademarks
The Microchip name and logo, the Microchip logo, dsPIC,
FlashFlex, flexPWR, JukeBlox, K
EE
L
OQ
, K
EE
L
OQ
logo, Kleer,
LANCheck, MediaLB, MOST, MOST logo, MPLAB,
OptoLyzer, PIC, PICSTART, PIC
32
logo, RightTouch, SpyNIC,
SST, SST Logo, SuperFlash and UNI/O are registered
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
The Embedded Control Solutions Company and mTouch are
registered trademarks of Microchip Technology Incorporated
in the U.S.A.
Analog-for-the-Digital Age, BodyCom, chipKIT, chipKIT logo,
CodeGuard, dsPICDEM, dsPICDEM.net, ECAN, In-Circuit
Serial Programming, ICSP, Inter-Chip Connectivity, KleerNet,
KleerNet logo, MiWi, motorBench, MPASM, MPF, MPLAB
Certified logo, MPLIB, MPLINK, MultiTRAK, NetDetach,
Omniscient Code Generation, PICDEM, PICDEM.net, PICkit,
PICtail, RightTouch logo, REAL ICE, SQI, Serial Quad I/O,
Total Endurance, TSHARC, USBCheck, VariSense,
ViewSpan, WiperLock, Wireless DNA, and ZENA are
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
Silicon Storage Technology is a registered trademark of
Microchip Technology Inc. in other countries.
GestIC is a registered trademark of Microchip Technology
Germany II GmbH & Co. KG, a subsidiary of Microchip
Technology Inc., in other countries.
All other trademarks mentioned herein are property of their
respective companies.
© 2009-2015, Microchip Technology Incorporated, Printed in
the U.S.A., All Rights Reserved.
ISBN: 978-1-5224-0056-1
Note the following details of the code protection feature on Microchip devices:
• Microchip products meet the specification contained in their particular Microchip Data Sheet.
• Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
• There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
• Microchip is willing to work with the customer who is concerned about the integrity of their code.
• Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.”
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2009 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC
®
MCUs and dsPIC
®
DSCs, KEELOQ
®
code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
QUALITY MANAGEMENT S
YSTEM
CERTIFIED BY DNV
== ISO/TS 16949 ==
6‘
‘MICRDCHIP
DS80000442K-page 18 2009-2015 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://www.microchip.com/
support
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Austin, TX
Tel: 512-257-3370
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Novi, MI
Tel: 248-848-4000
Houston, TX
Tel: 281-894-5983
Indianapolis
Noblesville, IN
Tel: 317-773-8323
Fax: 317-773-5453
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
New York, NY
Tel: 631-435-6000
San Jose, CA
Tel: 408-735-9110
Canada - Toronto
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2943-5100
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8569-7000
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Chongqing
Tel: 86-23-8980-9588
Fax: 86-23-8980-9500
China - Dongguan
Tel: 86-769-8702-9880
China - Hangzhou
Tel: 86-571-8792-8115
Fax: 86-571-8792-8116
China - Hong Kong SAR
Tel: 852-2943-5100
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8864-2200
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
ASIA/PACIFIC
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4123
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-3019-1500
Japan - Osaka
Tel: 81-6-6152-7160
Fax: 81-6-6152-9310
Japan - Tokyo
Tel: 81-3-6880- 3770
Fax: 81-3-6880-3771
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-5778-366
Fax: 886-3-5770-955
Taiwan - Kaohsiung
Tel: 886-7-213-7828
Taiwan - Taipei
Tel: 886-2-2508-8600
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Dusseldorf
Tel: 49-2129-3766400
Germany - Karlsruhe
Tel: 49-721-625370
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Italy - Venice
Tel: 39-049-7625286
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Poland - Warsaw
Tel: 48-22-3325737
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
Sweden - Stockholm
Tel: 46-8-5090-4654
UK - Wokingham
Tel: 44-118-921-5800
Fax: 44-118-921-5820
Worldwide Sales and Service
07/14/15
Products related to this Datasheet
IC MCU 16BIT 128KB FLASH 44TQFP
IC MCU 16BIT 64KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 28QFN
IC MCU 16BIT 128KB FLASH 44TQFP
IC MCU 16BIT 64KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 44QFN
IC MCU 16BIT 128KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 44QFN
IC MCU 16BIT 128KB FLASH 28SOIC
IC MCU 16BIT 32KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 28QFN
IC MCU 16BIT 64KB FLASH 44TQFP
IC MCU 16BIT 64KB FLASH 28QFN
IC MCU 16BIT 128KB FLASH 28SDIP
IC MCU 16BIT 64KB FLASH 28QFN
IC MCU 16BIT 32KB FLASH 28SOIC
IC MCU 16BIT 128KB FLASH 28SDIP
IC MCU 16BIT 64KB FLASH 28SOIC
IC MCU 16BIT 64KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 44QFN
IC MCU 16BIT 64KB FLASH 44QFN
IC MCU 16BIT 64KB FLASH 44QFN
IC MCU 16BIT 32KB FLASH 44TQFP
IC MCU 16BIT 128KB FLASH 44QFN
IC MCU 16BIT 64KB FLASH 28SOIC
IC MCU 16BIT 32KB FLASH 44QFN
IC MCU 16BIT 64KB FLASH 44TQFP
IC MCU 16BIT 64KB FLASH 28SDIP
IC MCU 16BIT 32KB FLASH 44QFN