PIC18F87J10 Family Revision A4 Errata Datasheet by Microchip Technology
View All Related Products | Download PDF DatasheetG
‘MICROCHIP PIC18F87J10 FAMILY
Work around
Date Codes that pertain to this issue:
oi
ITI
E
N
I
E
,2:
Work around Work around
Date Codes that pertain to this issue:
Date Codes that pertain to this issue:
2010 Microchip Technology Inc. DS80340B-page 1
PIC18F87J10 FAMILY
The PIC18F87J10 family parts you have received
conform functionally to the Device Data Sheet
(DS39663F), except for the anomalies described
below. Any Data Sheet Clarification issues related to
the PIC18F87J10 family will be reported in a separate
Data Sheet errata. Please check the Microchip web site
for any existing issues.
The following silicon errata apply only to
PIC18F87J10 family devices with these Device/
Revision IDs:
1. Module: Flash Program Memory
Writes to program memory address 300000h, that
are not blocked, can cause the program memory
at different locations to be corrupted.
Work around
Do not write to address 300000h. If you wish to
modify the contents of the Configuration registers,
then modify the Configuration Words located at the
end of the user memory and issue a Reset com-
mand. This will reload the Configuration registers
with the new configuration setting.
The end of the user memory is:
• PIC18FX5J10 devices – 7FF4h
• PIC18FX5J10 devices – 3FF4h
For additional information, see the Device Data
Sheet (DS39663), Section 24.1 “Configuration
Bits”.
Date Codes that pertain to this issue:
All engineering and production devices.
2. Module: External Memory Bus
For PIC18F8XJXX devices, the Stack Pointer may
incorrectly increment during a table read operation
if the external memory bus wait states are
enabled.
This is when:
• The Configuration bit, WAIT, is clear
(CONFIG3L<7> = 0)
• The WAITx bits (MEMCON<5:4>) are not equal
to ‘11’
Work around
If using the external memory bus and performing
TBLRD operations with a non-zero wait state –
described by the preceding two bullet points – first
disable interrupts by clearing the GIE/GIEH
(INTCON<7>) and PEIE/GIEL (INTCON<6>) bits.
Date Codes that pertain to this issue:
All engineering and production devices.
3. Module: External Memory Bus
The A<19:16> EMB address lines and read/write
control pins (OE, WRH and WRL) are released to
their respective inactive states at the same time
which violates the timing condition mentioned in
Figure 27-5 and Figure 27-6 in the data sheet.
This may result in the peripheral device on the bus
detecting an address change when write/read is
initiated. The bus capacitance and signal delay on
the address and control lines can affect the
probability of invalid detection.
Work around
Do one of the following:
• Use a latch based on the falling edge of ALE to
hold the A<19:16> signals.
• Add a delay circuit to extend the valid time for
A<19:16> signals to ensure the address is valid
until read/write signals go inactive.
Date Codes that pertain to this issue:
All engineering and production devices.
Part Number Device ID Revision ID
PIC18F65J10 0001 0101 001 0 0101
PIC18F65J15 0001 0101 010 0 0101
PIC18F66J10 0001 0101 011 0 0101
PIC18F66J15 0001 0101 100 0 0101
PIC18F67J10 0001 0101 101 0 0101
PIC18F85J10 0001 0101 111 0 0101
PIC18F85J15 0001 0111 000 0 0101
PIC18F86J10 0001 0111 001 0 0101
PIC18F86J15 0001 0111 010 0 0101
PIC18F87J10 0001 0111 011 0 0101
The Device IDs (DEVID1 and DEVID2) are located at
addresses 3FFFFEh:3FFFFFh in the device’s
configuration space. They are shown in hexadecimal
in the format “DEVID2 DEVID1”.
PIC18F87J10 Family Rev. A4 Silicon Errata
Work around
Date Codes that pertain to this issue:
Work around
TiSYNC
Dale Codes that pert to I sue:
|:|
Date Codes that genain to this issue:
HZI
PIC18F87J10 FAMILY
DS80340B-page 2 2010 Microchip Technology Inc.
4. Module: Timer1
In 16-Bit Asynchronous Counter mode (with or
without use of the Timer1 oscillator), the TMR1H
and TMR3H buffers do not update when TMRxL is
read.
This issue only affects reading the TMRxH regis-
ters. The timers increment and set the interrupt
flags as expected and the Timer registers can be
written as expected.
Work around
1. Use 8-bit mode by clearing the RD16 bit
(T1CON<7>).
2. Use the internal clock synchronization option
by clearing the T1SYNC bit (T1CON<2>).
Date Codes that pertain to this issue:
All engineering and production devices.
5. Module: Master Synchronous Serial Port
(MSSP)
In SPI mode, the following bits are not reset upon
disabling the SPI module (by clearing the SSPEN
bit in SSPxCON1 register):
• Buffer Full bit – BF in SSPxSTAT register
• Write Collision Detect bit – WCOL in
SSPxCON1
• Receive Overflow Indicator bit – SSPOV in
SSPxCON1
For example, if SSPxBUF is full (BF bit is set) and
the MSSP module is disabled and re-enabled, the
BF bit will remain set. In SPI Slave mode, that can
mean:
• A subsequent write to SSPxBUF will result in a
write collision
• A new byte will cause a receive overflow
Work around
Before disabling the MSSP module, ensure that:
•WCOL is clear
• If the buffer is full, SSPxBUF is read (thus
clearing the BF flag)
• If the module was configured in SPI Slave
mode, the SSPOV bit is clear
Date Codes that pertain to this issue:
All engineering and production devices.
6. Module: Master Synchronous Serial Port
(MSSP)
In its current implementation, the Baud Rate Gen-
erator for I2C™ in Master mode is slower than the
rates specified in Table 19-3 of the Device Data
Sheet.
For this revision of silicon:
• For the I2C™ clock rates – use the values
shown in Table 1 in place of those shown in
Table 19-3 of the Device Data Sheet. (The
differences are shown in bold text.)
• For bit description, SSPM<3:0> = 1000, use
the following formula in place of the one shown
in Register 18-2 (SSPxCON1) of the Device
Data Sheet.
Note: The I2C bus is a synchronous protocol, so
the accuracy of the bus frequency is not
critical.
Date Codes that pertain to this issue:
All engineering and production devices.
TABLE 1: I2C™ CLOCK RATE with BRG
SSPADD = INT((FCY/FSCL) – (FCY/1.111 MHz)) – 1
FOSC FCY FCY * 2 BRG Value FSCL
(2 Rollovers of BRG)
40 MHz 10 MHz 20 MHz 0Eh 400 kHz(1)
40 MHz 10 MHz 20 MHz 15h 312.5 kHz
40 MHz 10 MHz 20 MHz 59h 100 kHz
16 MHz 4 MHz 8 MHz 05h 400 kHz(1)
16 MHz 4 MHz 8 MHz 08h 308 kHz
16 MHz 4 MHz 8 MHz 23h 100 kHz
4 MHz 1 MHz 2 MHz 01h 333 kHz(1)
4 MHz 1 MHz 2 MHz 08h 100 kHz
4 MHz 1 MHz 2 MHz 00h 1 MHz(1)
Note 1: The I2C™ interface does not conform to the 400 kHz I2C specification (which applies to rates greater than
100 kHz) in all details, but may be used with care where higher rates are required by the application.
Work around
Date Codes that pertain to t sue:
Work around
Date Codes that pertain to th sue:
Work around
Date Codes that pertain to th issue:
Work around
Date Codes that pertain to th ssue:
2010 Microchip Technology Inc. DS80340B-page 3
PIC18F87J10 FAMILY
7. Module: Master Synchronous Serial Port
(MSSP)
After an I2C transfer is initiated, the SSPxBUF
register may be written for up to 10 TCY before
additional writes are blocked. The data transfer may
be corrupted if SSPxBUF is written during this time.
The WCOL bit is set any time an SSPxBUF write
occurs during a transfer.
Work around
Avoid writing SSPxBUF until the data transfer is
complete, indicated by the setting of the SSP1IF
bit (PIR1<3>).
Verify the WCOL bit (SSPxCON1<7>) is clear after
writing SSPxBUF to ensure any potential transfer
in progress is not corrupted.
Date Codes that pertain to this issue:
All engineering and production devices.
8. Module: Master Synchronous Serial Port
(MSSP)
When the SPI is using Timer2/2 as the clock
source, a shorter than expected SCKx pulse may
occur on the first bit of the transmitted/received
data (see Figure 1).
FIGURE 1: SCKx PULSE VARIATION
USING TIMER2/2
Work around
To avoid producing the short pulse:
1. Turn off Timer2.
2. Clear the TMR2 register.
3. Load the SSPxBUF with the data to be
transmitted.
4. Turn Timer2 back on.
For sample code, see Example 1.
EXAMPLE 1: AVOIDING THE INITIAL
SHORT SCK1 PULSE
(FOR MSSP1)
Date Codes that pertain to this issue:
All engineering and production devices.
9. Module: Master Synchronous Serial Port
(MSSP)
In SPI mode, the SDOx output may change after the
inactive clock edge of the bit ‘0’ output. This may
affect some SPI components that read data more
than 300 ns after the inactive edge of SCKx.
Work around
None.
Date Codes that pertain to this issue:
All engineering and production devices.
10. Module: Master Synchronous Serial Port
(MSSP)
When the MSSP peripherals are configured for
SPI mode, the Buffer Full bit, BF (SSPxSTAT<0>)
should not be polled in software to determine when
the transfer is complete.
Work around
Do one of the following:
• Copy the SSPxSTAT register into a variable
and perform the bit test on the variable.
(Example 2 copies SSP1STAT into the working
register where the bit test is performed.)
EXAMPLE 2: Master Synchronous Serial
Port (MSSP1)
• Poll the Master Synchronous Serial Port
Interrupt Flag bit, SSP1IF (PIR1<3>). This bit
can be polled and will set when the transfer is
complete.
Date Codes that pertain to this issue:
All engineering and production devices.
SDOx
SCKx
Write SSPxBUF
bit 7 =
1
bit 6 =
0
bit 5 =
1
. . . .
LOOP BTFSS SSP1STAT, BF ;Data received?
;(Xmit complete?)
BRA LOOP ;No
MOVF SSP1BUF, W ;W = SSPBUF
MOVWF RXDATA ;Save in user RAM
MOVF TXDATA, W ;W = TXDATA
BCF T2CON, TMR2ON ;Timer2 off
CLRF TMR2 ;Clear Timer2
MOVWF SSP1BUF ;Xmit New data
BSF T2CON, TMR2ON ;Timer2 on
loop_MSB:
MOVF SSP1STAT, W
BTFSS WREG, BF
BRA loop_MSB
Work around
Date Codes that pertain to th sue:
Work around
Work around
Date Codes that pertain to th ssue:
Dale Codes that pert to t su
PIC18F87J10 FAMILY
DS80340B-page 4 2010 Microchip Technology Inc.
11. Module: Enhanced Universal
Synchronous Asynchronous
Receiver Transmitter (EUSART)
In rare situations, one or more extra zero bytes
have been observed in a packet transmitted by the
module operating in Asynchronous mode. The
actual data is not lost or corrupted; only unwanted
(extra) zero bytes are observed in the packet.
This situation has only been observed when the
contents of the transmit buffer, TXREGx, are trans-
ferred to the TSR during the transmission of a Stop
bit. For this to occur, three things must happen in
the same instruction cycle:
• The TXREGx is written to
• The baud rate counter overflows (at the end of
the bit period)
• A Stop bit is transmitted (shifted out of TSR)
Work around
If possible, do not use the module’s double-buffer
capability. Instead, load the TXREGx register
when the TRMT bit (TXSTAx<1>) is set, indicating
the TSR is empty.
If double-buffering is used and back-to-back
transmission is performed, load TXREGx immedi-
ately after TXxIF is set or wait 1-bit time after
TXxIF is set. Both solutions prevent writing
TXREGx while a Stop bit is transmitted. Note that
TXxIF is set at the beginning of the Stop bit
transmission.
If transmission is intermittent, do one of the
following:
• Wait for the TRMT bit to be set before loading
TXREGx.
• Execute the following:
- Use a free timer resource to time the baud
period.
- Set up the timer to overflow at the end of
Stop bit.
- Start the timer when you load the TXREGx.
-Do not load the TXREGx when the timer is
about to overflow.
Date Codes that pertain to this issue:
All engineering and production devices.
12. Module: Enhanced Universal
Synchronous Asynchronous
Receiver Transmitter (EUSART)
In 9-Bit Asynchronous Full-Duplex Receive mode,
the received data may be corrupted if the TX9D bit
(TXSTAx<0>) is not modified immediately after the
RCIDL bit (BAUDCONx<6>) is set.
Work around
Write to TX9D only when a reception is not in prog-
ress (RCIDL = 1). Since there is no interrupt asso-
ciated with RCIDL, it must be polled in software to
determine when TX9D can be updated.
Date Codes that pertain to this issue:
All engineering and production devices.
13. Module: Enhanced Universal
Synchronous Asynchronous
Receiver Transmitter (EUSART)
After the last received byte has been read from the
EUSART Receive Buffer (RCREGx), the value is
no longer valid for subsequent read operations.
Work around
The RCREGx register should be read only once for
each byte received. After each byte is received from
the EUSART, store the byte into a user variable.
To determine when a byte is available to read from
RCREGx, do one of the following:
• Poll the RCIDL bit (BAUDCONx<6>) for a
low-to-high transition
• Use the EUSART Receive Interrupt Flag,
RC1IF (PIR1<5>)
Date Codes that pertain to this issue:
All engineering and production devices.
exther Foss/64, Pose/32 or Fuse/16, Ihe GO/DONE
Work around
: m
Work around
Date Codes that pertain to th Issue:
Date Codes that pertain to t sue:
2010 Microchip Technology Inc. DS80340B-page 5
PIC18F87J10 FAMILY
14. Module: Enhanced Universal
Synchronous Asynchronous
Receiver Transmitter (EUSART)
With the auto-wake-up option enabled by setting
the WUE bit (BAUDCONx<1>), the RC1IF bit
(PIR1<5>) will become set on a high-to-low
transition on the RXx pin. While the WUE bit is set,
reading the receive buffer (RCREGx) will not clear
the RCxIF interrupt flag.
Because of this, RCxIF cannot be automatically
cleared by reading RCREGx until the WUE bit is
cleared.
Work around
Do the following:
1. Poll either the WUE bit or the RXx pin.
2. When WUE is clear or RXx is high, read
RCREGx.
Step 2 clears RCxIF.
Date Codes that pertain to this issue:
All engineering and production devices.
15. Module: 10-Bit Analog-to-Digital (A/D)
Converter
When the A/D conversion clock is selected to be
either FOSC/64, FOSC/32 or FOSC/16, the GO/DONE
bit cannot be set for a second conversion without
first selecting (temporarily) the RC oscillator as the
A/D conversion clock.
The A/D functions normally with the A/D
conversion clock settings of FOSC/2, FOSC/4 and
FRC.
Work around
For A/D conversion clock settings of FOSC/64,
FOSC/32 or FOSC/16, perform the work around
shown in Example 3 prior to setting the GO/DONE
bit for subsequent conversions.
It is recommended that this code be inserted
immediately after the A/D result has been read
from the previous conversion.
Date Codes that pertain to this issue:
All engineering and production devices.
EXAMPLE 3:
Note: RCxIF can only be cleared by reading
RCREGx
MOVF ADCON2, W ;copy the value of ADCON2 to WREG
BSF ADCON2, ADCS0 ;temporarily select RC oscillator as clock
BSF ADCON2, ADCS1
MOVWF ADCON2 ;restore ADCON2 to original value
Work around
Dale Codes that gen to 1 Sn
Work around
Work around
PIC18F87J10 FAMILY
DS80340B-page 6 2010 Microchip Technology Inc.
16. Module: 10-Bit Analog-to-Digital (A/D)
Converter
When FOSC/8 is selected as the A/D conversion
clock, A/D conversion will not be performed.
Work around
None.
Date Codes that pertain to this issue:
All engineering and production devices.
17. Module: Master Synchronous Serial Port
(MSSP)
In extremely rare cases, when configured for I2C
slave reception, the MSSP module may not
receive the correct data. This occurs only if the
Serial Receive/Transmit Buffer Register
(SSPxBUF) is not read within a window after the
SSPxIF interrupt has occurred.
Work around
The issue can be resolved in either of these ways:
• Prior to the I2C slave reception, enable the
clock stretching feature. This is done by setting
the SEN bit (SSPxCON2<0>).
• Each time the SSPxIF is set, read the
SSPxBUF before the first rising clock edge of
the next byte being received.
18. Module: I/O Ports
During a Power-on Reset, the PORTJ pins will not
behave as high-impedance pins.
For the Power-up Timer period (approximately
65.6 ms), PORTJ pins may be driven high or low.
Work around
None.
Rev A Documenl 8/2007
Rev B Documenl 7/2010
2010 Microchip Technology Inc. DS80340B-page 7
PIC18F87J10 FAMILY
REVISION HISTORY
Rev A Document (8/2007)
First release of this document. Includes silicon issues
1 (Flash Program Memory), 2-3 (External Memory
Bus), 4 (Timer1), 5-10 (MSSP), 11-14 EUSART and
15-16 (10-Bit A/D Converter).
Rev B Document (7/2010)
Added silicon issues 17 (Master Synchronous Serial
Port – MSSP) and 18 (I/O Ports).
PIC18F87J10 FAMILY
DS80340B-page 8 2010 Microchip Technology Inc.
NOTES:
QUALITY MANAGEMENT SYSTEM
CERTIFIED BY DNV
= ISO/TS 16949:2002 =
2010 Microchip Technology Inc. DS80340B-page 9
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights.
Trademarks
The Microchip name and logo, the Microchip logo, dsPIC,
KEELOQ, KEELOQ logo, MPLAB, PIC, PICmicro, PICSTART,
PIC32 logo, rfPIC and UNI/O are registered trademarks of
Microchip Technology Incorporated in the U.S.A. and other
countries.
FilterLab, Hampshire, HI-TECH C, Linear Active Thermistor,
MXDEV, MXLAB, SEEVAL and The Embedded Control
Solutions Company are registered trademarks of Microchip
Technology Incorporated in the U.S.A.
Analog-for-the-Digital Age, Application Maestro, CodeGuard,
dsPICDEM, dsPICDEM.net, dsPICworks, dsSPEAK, ECAN,
ECONOMONITOR, FanSense, HI-TIDE, In-Circuit Serial
Programming, ICSP, Mindi, MiWi, MPASM, MPLAB Certified
logo, MPLIB, MPLINK, mTouch, Octopus, Omniscient Code
Generation, PICC, PICC-18, PICDEM, PICDEM.net, PICkit,
PICtail, REAL ICE, rfLAB, Select Mode, Total Endurance,
TSHARC, UniWinDriver, WiperLock and ZENA are
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
All other trademarks mentioned herein are property of their
respective companies.
© 2010, Microchip Technology Incorporated, Printed in the
U.S.A., All Rights Reserved.
Printed on recycled paper.
ISBN:
Note the following details of the code protection feature on Microchip devices:
• Microchip products meet the specification contained in their particular Microchip Data Sheet.
• Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
• There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
• Microchip is willing to work with the customer who is concerned about the integrity of their code.
• Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.”
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2002 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC® MCUs and dsPIC® DSCs, KEELOQ® code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
MICROCHIP
AMERICAS ASIA/PACIFIC ASIA/PACIFIC EUROPE
DS80340B-page 10 2010 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://support.microchip.com
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Farmington Hills, MI
Tel: 248-538-2250
Fax: 248-538-2260
Kokomo
Kokomo, IN
Tel: 765-864-8360
Fax: 765-864-8387
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
Santa Clara
Santa Clara, CA
Tel: 408-961-6444
Fax: 408-961-6445
Toronto
Mississauga, Ontario,
Canada
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2401-1200
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8528-2100
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Chongqing
Tel: 86-23-8980-9588
Fax: 86-23-8980-9500
China - Hong Kong SAR
Tel: 852-2401-1200
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8203-2660
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
ASIA/PACIFIC
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4123
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-2566-1512
Fax: 91-20-2566-1513
Japan - Yokohama
Tel: 81-45-471- 6166
Fax: 81-45-471-6122
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-6578-300
Fax: 886-3-6578-370
Taiwan - Kaohsiung
Tel: 886-7-213-7830
Fax: 886-7-330-9305
Taiwan - Taipei
Tel: 886-2-2500-6610
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
UK - Wokingham
Tel: 44-118-921-5869
Fax: 44-118-921-5820
WORLDWIDE SALES AND SERVICE
07/15/10
Products related to this Datasheet
IC MCU 8BIT 96KB FLASH 80TQFP
IC MCU 8BIT 48KB FLASH 64TQFP
IC MCU 8BIT 128KB FLASH 64TQFP
IC MCU 8BIT 128KB FLASH 80TQFP
IC MCU 8BIT 64KB FLASH 64TQFP
IC MCU 8BIT 128KB FLASH 64TQFP
IC MCU 8BIT 128KB FLASH 80TQFP
IC MCU 8BIT 32KB FLASH 64TQFP
IC MCU 8BIT 64KB FLASH 64TQFP
IC MCU 8BIT 32KB FLASH 80TQFP
IC MCU 8BIT 48KB FLASH 64TQFP
IC MCU 8BIT 64KB FLASH 80TQFP
IC MCU 8BIT 48KB FLASH 64TQFP
IC MCU 8BIT 96KB FLASH 64TQFP
IC MCU 8BIT 48KB FLASH 80TQFP
IC MCU 8BIT 96KB FLASH 80TQFP
IC MCU 8BIT 32KB FLASH 64TQFP
IC MCU 8BIT 64KB FLASH 80TQFP
IC MCU 8BIT 64KB FLASH 64TQFP
IC MCU 8BIT 48KB FLASH 80TQFP
IC MCU 8BIT 96KB FLASH 64TQFP
IC MCU 8BIT 32KB FLASH 80TQFP
IC MCU 8BIT 64KB FLASH 80TQFP
IC MCU 8BIT 48KB FLASH 80TQFP
IC MCU 8BIT 64KB FLASH 64TQFP
IC MCU 8BIT 48KB FLASH 64TQFP