TB-4018 Page 1 of 3 © 2018 DESCO INDUSTRIES, INC.
Employee Owned
3651 Walnut Avenue, Chino, CA 91710
Phone: (909) 627-2453 • Web Site: MendaPump.com
35868 ESD Service Vacuum, 220 VAC, No Power Cord:
35822 Type 2 Filter for Dust and Toner
35825 7 Foot Dissipative Hose
35826 Crevice Tool
35827 Crevice Tool Brush
35828 Wand
35829 Needle Nose Nozzle
35830 Dust Brush
Optional Accessories
35823 Type 1 Filter for Fine Particles
35824 Carrying Strap
Grounding Instructions
The 35867 Vacuum is for use on a nominal 120 volt circuit
and has a grounding plug. The 35868 Vacuum is for use
on a nominal 240 volt circuit. Make sure the vacuum is
connected to an outlet having the same configuration as
the plug. No adapter should be used with this vacuum.
Any service on the vacuum should be performed by an
authorized service representative.
Warning: Improper connection of the equipment-grounding
conductor can result in the risk of electric shock. Check
with a qualified electrician or service person if you are in
doubt as to whether the outlet is properly grounded. Do
not modify the plug provided with the appliance. If the plug
does not fit the outlet, have a proper outlet installed by a
qualified electrician.
Specifications
Electrical
35867
35868
120VAC, 50/60Hz, 6.0amps
220/240VAC, 50/60Hz, 4.25amps
Motor 1 Horsepower
Suction
Dimensions
Approx. 51”/H20
17.8" L x 7.8" W x 9.3" H
(45.2 cm L x 19.7 cm W x 23.5 cm H)
Weight 11 lbs.
ESD Service Vacuum
Operation and Maintenance
January 2018
USER GUIDE TB-4018
Figure 1. ESD Service Vacuum.
Description
The 35867/35868 ESD Service Vacuum is designed
for high-efficiency cleanup of most business equipment
including removing toner and dust. Portability, quick
setup and efficient and safe operation are key features
of this vacuum. It contains a one horsepower, six amp
motor.
This product meets ANSI/ESD S20.20 and is designed
to be used in an ESD protected area. The hose and
accessories are conductive/dissipative so electrostatic
charges will be removed when properly grounded
through the power cord to electrical outlet ground prong.
The ESD Service Vacuum is available in two models:
Item Description
35867 ESD Service Vacuum, 120 VAC, US Plug
35868 ESD Service Vacuum, 220 VAC, No Power Cord
Packaging
35867 ESD Service Vacuum, 120 VAC, US Plug:
Includes 8 Foot Power Cord, US Plug
35822 Type 2 Filter for Dust and Toner
35825 7 Foot Dissipative Hose
35826 Crevice Tool
35827 Crevice Tool Brush
35828 Wand
35829 Needle Nose Nozzle
35830 Dust Brush
Made in the
United States of America
TB-4018 Page 2 of 3 © 2018 DESCO INDUSTRIES, INC.
Employee Owned
3651 Walnut Avenue, Chino, CA 91710
Phone: (909) 627-2453 • Web Site: MendaPump.com
Figure 3. How to replace the ESD Service Vacuum Filter.
1. Release the latches and open the lid .
2. Remove red filter plug or hose. Save the plug for
use later (see WEEE Statement).
3. Grasp the filter on each side by using the circular
indentations . Pull filter straight up by both ends.
4. Insert the red filter plug in the filter.
5. Dispose of the filter in a suitable manner.
6. Remove the red plug from the new filter and position
filter in the vacuum with the filter hole to your left.
Save the red plug for use in disposing of the filter
(see WEEE Statement).
7. Verify that the gasket between the filter and the
motor fits tightly.
8. Insert the red filter plug or hose.
9. Close and latch the lid.
To Store Attachments for Transport
1. Unplug the power cord from the outlet and
vacuum .
2. Open the lid and retrieve the filter plug.
3. Remove the hose from the inlet and insert the
filter plug.
4. Detach the hose nozzle from the base.
5. Place the hose, power cord and attachments into the
lid and close the accessory door.
6. Close the lid and securely fasten the latches .
Safety Information
Warning: TO REDUCE THE RISK OF FIRE, ELECTRIC
SHOCK OR INJURY, FOLLOW THESE SAFETY
RULES:
1. Use only as described in this manual. Use only
manufacturer’s recommended attachments.
2. Do not use this machine to vacuum hazardous dust,
flammable or combustible liquids, such as gasoline.
3. Connect to a properly grounded outlet only. See
Grounding instructions.
4. Do not use without filter in place.
5. Do not leave appliance plugged in when not in use.
Unplug from the outlet when not in use and before
servicing.
6. Turn off all controls before unplugging
7. Do not unplug by pulling on the cord. To unplug,
grasp the plug, not the cord.
To Operate
1. Release latches and open lid .
2. Unfasten accessory door and remove vacuum hose,
electrical cord and hose attachments .
3. Remove filter plug from vacuum inlet (always
replace when repacking for transport) .
4. Attach selected accessory to hose (insert crevice
brush as shown ). Insert other end of hose into
inlet .
5. Place remaining accessory and filter plug in lid.
Close lid.
6. Latch lid securely.
7. Insert hooded end of power cord in power cord
receptacle on vacuum .
8. Plug cord into power outlet.
9. Turn on power switch .
Figure 2. How to operate the ESD Service Vacuum.
To Replace Filter
The ESD Service Vacuum is designed for use with
disposable MENDA Filters. The filters must be replaced
on a regular basis. Frequency of filter replacement
depends on the type and frequency of use of the ESD
Service Vacuum.
IN
TIE-401E
TB-4018 Page 3 of 3 © 2018 DESCO INDUSTRIES, INC.
Employee Owned
3651 Walnut Avenue, Chino, CA 91710
Phone: (909) 627-2453 • Web Site: MendaPump.com
Limited Warranty, Warranty Exclusions, Limit of
Liability and RMA Request Instructions
See the MENDA Warranty -
http://menda.descoindustries.com/Limited-Warranty.aspx
8. Do not handle the plug or appliance with wet hands.
9. Do not use appliance outdoors or on wet surfaces.
Electrical shock could occur.
10. Do not use with damaged cord or plug. If appliance
is not working as it should, has been dropped
or damaged, left outdoors, or dropped in water,
discontinue use.
11. Do not pull or carry by cord, use cord as a handle,
close door on cord or pull cord around sharp edges
and corners. Keep cord away from heated surfaces.
12. Do not put any object into openings. Do not use with
any opening that is blocked.
13. Keep hair, loose clothing, fingers and all body parts
away from openings and moving parts.
14. Do not pick up anything that is burning or smoking,
such as cigarettes, matches or hot ashes.
15. Do not use to pick up flammable or combustible
liquids, such as gasoline, and do not use in areas
where these may be present.
16. Do not allow to be used as a toy. Close attention is
necessary when used near children.
Electric shock could occur if used outdoors or on wet
surfaces.
Caution: To avoid risk of fire, filter must be installed
properly and replaced regularly. Do not open filter, reuse
filter or attempt to replace components within filter.
Regulatory Information
WEEE Statement
The following information is only for EU-member States:
The mark shown to the right is in compliance with Waste
Electrical and Electronic Equipment Directive 2002/96/
EC (WEEE). The mark indicates the requirement NOT to
dispose the equipment as unsorted municipal waste, but
use the return and collection systems according to
local law.
Dispose of filter and vacuum components properly
according to applicable local, state and federal laws.
Products related to this Datasheet
FILTER, TYPE 2, FOR TONER AND DU
FILTER, TYPE 1, FINE PARTICLES
STRAP, VACUUM CARRYING
HOSE ASSEMBLY
NOZZLE, CREVICE, VACUUM
TOOL, BRUSH CREVICE, VACUUM
WAND ASSEMBLY, BENT
NOZZLE, NEEDLE NOSE
BRUSH, DUSTING, STATIC DISSIPATI
VACUUM, ESD SERVICE, 120VAC, US
VACUUM, ESD SERVICE, 220VAC NO P