FTDI Basic Breakout 3.3/5V (Arduino Compatible)
SKU:DFR0065
INTRODUCTION
This is a basic breakout board for the FTDI FT232RL USB to serial IC. The pinout of this board matches the FTDI cable to work
with official Arduino and cloned 3.3V Arduino boards. It can also be used for general serial applications. The major difference
with this board is that it brings out the DTR pin as opposed to the RTS pin of the FTDI cable. The DTR pin allows an Arduino
target to auto-reset when a new Sketch is downloaded. This is a really nice feature to have and allows a sketch to be downloaded
without having to hit the reset button. This board will auto reset any Arduino board that has the reset pin brought out to a 6-pin
connector.
The pins labeled BLK and GRN correspond to the colored wires on the FTDI cable. The black wire on the FTDI cable is GND,
green is DTR. Use these BLK and GRN pins to align the FTDI basic board with your Arduino target.
There are pros and cons to the FTDI Cable vs the FTDI Basic. This board has TX and RX LEDs that allow you to actually see
serial traffic on the LEDs to verify if the board is working, but this board requires a miniB cable. The FTDI Cable is well
protected against the elements, but is large and cannot be embedded into a project as easily. The FTDI Basic uses DTR to cause a
hardware reset where the FTDI cable uses the RTS signal.
This board was designed to decrease the cost of Arduino development and increase ease of use (the auto-reset feature rocks!). We
made some little change with silk-screen, it needs to connect "TX" to "TX"; "RX" to "RX" in programming, Our Arduino Pro
and LilyPad boards use this type of connector.
SPECIFICATION
3.3/5V output(switchable via Jumpers)
Powered By DFRobot © 2008-2017
Products related to this Datasheet
USB 2.0 TO UART MODULE