TIE-9072
TB-9072 Page 1 of 3 © 2018 DESCO INDUSTRIES INC
Employee Owned
SCS - 926 JR Industrial Drive, Sanford, NC 27332
East: (919) 718-0000 | West: (909) 627-9634 • Website: StaticControl.com
497ABG Electronic Service Vacuum, 220 VAC, Euro
Plug:
SV-MPF2 Type 2 Filter
8 Foot Power Cord, Europe
SV-SH33 7 Foot Dissipative Hose
SV-WA2 Wand
SV-CN1 Crevice Tool
SV-CB1 Crevice Tool Brush
SV-DBSD1 Dust Brush
SV-NN Needle Nose Nozzle
497ABG-NO Electronic Service Vacuum, 220 VAC,
No Power Cord:
SV-MPF2 Type 2 Filter
SV-SH33 7 Foot Dissipative Hose
SV-WA2 Wand
SV-CN1 Crevice Tool
SV-CB1 Crevice Tool Brush
SV-DBSD1 Dust Brush
SV-NN Needle Nose Nozzle
Grounding Instructions
The 497AJN Vacuum is for use on a nominal 120 volt
circuit and has a grounding plug. The 497ABG Vacuum
is for use on a nominal 240 volt circuit and has a
grounding plug. Make sure the vacuum is connected to
an outlet having the same configuration as the plug. No
adapter should be used with this vacuum. Any service
on the vacuum should be performed by an authorized
service representative.
Warning: Improper connection of the equipment-
grounding conductor can result in the risk of electric
shock. Check with a qualified electrician or service
person if you are in doubt as to whether the outlet is
properly grounded. Do not modify the plug provided with
the appliance. If the plug does not fit the outlet, have a
proper outlet installed by a qualified electrician.
Specifications
Electrical
497AJN
497ABG
497ABG-NO
120VAC, 50/60Hz, 6.0amps
220/240VAC, 50/60Hz, 4.25amps
220/240VAC, 50/60Hz, 4.25amps
Motor 1 Horsepower
Suction
Dimensions
Approx. 51”/H20
17.8" L x 7.8" W x 9.3" H
(45.2 cm L x 19.7 cm W x 23.5 cm H)
Weight 11 lbs.
Certification cULus, EAC
Electronic Service Vacuum
Operation and Maintenance
March 2018
USER GUIDE TB-9072
Figure 1. Electronic Service Vacuum.
Description
The 497AJN/497ABG Electronic Service Vacuum is
designed for high-efficiency cleanup of most business
equipment including removing toner and dust. Portability,
quick setup and efficient and safe operation are key
features of this vacuum. It contains a one horsepower,
six amp motor.
This product meets ANSI/ESD S20.20 and is designed
to be used in an ESD protected area; The hose and
accessories are conductive/dissipative so electrostatic
charges will be removed when properly grounded
through the power cord to electrical outlet ground prong.
The SCS Electronic Service Vacuum is available in three
models:
Item Description
497AJN Electronic Service Vacuum, 120 VAC,
US Plug
497ABG Electronic Service Vacuum, 220 VAC,
Euro Plug
497ABG-NO Electronic Service Vacuum, 220 VAC,
No Power Cord
Packaging
497AJN Electronic Service Vacuum, 120 VAC, US Plug:
SV-MPF2 Type 2 Filter
SV-PC8 8 Foot Power Cord
SV-SH33 7 Foot Dissipative Hose
SV-WA2 Wand
SV-CN1 Crevice Tool
SV-CB1 Crevice Tool Brush
SV-DBSD1 Dust Brush
SV-NN Needle Nose Nozzle
Made in the
United States of America
TB-9072
TB-9072 Page 2 of 3 © 2018 DESCO INDUSTRIES INC
Employee Owned
SCS - 926 JR Industrial Drive, Sanford, NC 27332
East: (919) 718-0000 | West: (909) 627-9634 • Website: StaticControl.com
Figure 3. How to replace the Electronic Service Vacuum
Filter.
1. Release the latches and open the lid .
2. Remove red filter plug or hose. Save the plug for
use later (see WEEE Statement).
3. Grasp the filter on each side by using the circular
indentations . Pull filter straight up by both ends.
4. Insert the red filter plug in the filter.
5. Dispose of the filter in a suitable manner.
6. Remove the red plug from the new filter and position
filter in the vacuum with the filter hole to your left.
Save the red plug for use in disposing of the filter
(see WEEE Statement).
7. Verify that the gasket between the filter and the
motor fits tightly.
8. Insert the red filter plug or hose.
9. Close and latch the lid.
To Store Attachments for Transport
1. Unplug the power cord from the outlet and
vacuum .
2. Open the lid and retrieve the filter plug.
3. Remove the hose from the inlet and insert the
filter plug.
4. Detach the hose nozzle from the base.
5. Place the hose, power cord and attachments into the
lid and close the accessory door.
6. Close the lid and securely fasten the latches .
Safety Information
Warning: TO REDUCE THE RISK OF FIRE, ELECTRIC
SHOCK OR INJURY, FOLLOW THESE SAFETY
RULES:
1. Use only as described in this manual. Use only
manufacturer’s recommended attachments.
2. Do not use this machine to vacuum hazardous dust,
flammable or combustible liquids, such as gasoline.
3. Connect to a properly grounded outlet only. See
Grounding instructions.
4. Do not use without filter in place.
5. Do not leave appliance plugged in when not in use.
Unplug from the outlet when not in use and before
servicing.
6. Turn off all controls before unplugging
To Operate
1. Release latches and open lid .
2. Unfasten accessory door and remove vacuum hose,
electrical cord and hose attachments .
3. Remove filter plug from vacuum inlet (always
replace when repacking for transport) .
4. Attach selected accessory to hose (insert crevice
brush as shown ). Insert other end of hose into
inlet .
5. Place remaining accessory and filter plug in lid.
Close lid.
6. Latch lid securely.
7. Insert hooded end of power cord in power cord
receptacle on vacuum .
8. Plug cord into power outlet.
9. Turn on power switch .
Figure 2. How to operate the Electronic Service Vacuum.
To Replace Filter
The Electronic Service Vacuum is designed for use with
disposable SCS Filters. The filters must be replaced on
a regular basis. Frequency of filter replacement depends
on the type and frequency of use of the Electronic
Service Vacuum.
IN
TIE-9072
TB-9072 Page 3 of 3 © 2018 DESCO INDUSTRIES INC
Employee Owned
SCS - 926 JR Industrial Drive, Sanford, NC 27332
East: (919) 718-0000 | West: (909) 627-9634 • Website: StaticControl.com
Limited Warranty, Warranty Exclusions, Limit
of Liability and RMA Request Instructions
See the SCS Warranty -
StaticControl.com/Limited-Warranty.aspx
7. Do not unplug by pulling on the cord. To unplug,
grasp the plug, not the cord.
8. Do not handle the plug or appliance with wet hands.
9. Do not use appliance outdoors or on wet surfaces.
Electrical shock could occur.
10. Do not use with damaged cord or plug. If appliance
is not working as it should, has been dropped
or damaged, left outdoors, or dropped in water,
discontinue use.
11. Do not pull or carry by cord, use cord as a handle,
close door on cord or pull cord around sharp edges
and corners. Keep cord away from heated surfaces.
12. Do not put any object into openings. Do not use with
any opening that is blocked.
13. Keep hair, loose clothing, fingers and all body parts
away from openings and moving parts.
14. Do not pick up anything that is burning or smoking,
such as cigarettes, matches or hot ashes.
15. Do not use to pick up flammable or combustible
liquids, such as gasoline, and do not use in areas
where these may be present.
16. Do not allow to be used as a toy. Close attention is
necessary when used near children.
Electric shock could occur if used outdoors or on wet
surfaces.
Caution: To avoid risk of fire, filter must be installed
properly and replaced regularly. Do not open filter, reuse
filter or attempt to replace components within filter.
Regulatory Information
cULus Statement
Meets cULus requirements.
WEEE Statement
The following information is only for EU-member
States: The mark shown to the right is in
compliance with Waste Electrical and Electronic
Equipment Directive 2002/96/EC (WEEE). The mark
indicates the requirement NOT to dispose the equipment
as unsorted municipal waste, but use the return and
collection systems according to local law.
Dispose of filter and vacuum components properly
according to applicable local, state and federal laws.