Polymer Guide for Tantalum Caps Datasheet by Vishay Sprague
View All Related Products | Download PDF DatasheetVISHAY.
gomecmvusnamom
www.v\shay.com/doc?91000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 1Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
Guide for Tantalum Solid Electrolyte Chip Capacitors
with Polymer Cathode
INTRODUCTION
Tantalum electrolytic capacitors are the preferred choice in
applications where volumetric efficiency, stable electrical
parameters, high reliability, and long service life are primary
considerations. The stability and resistance to elevated
temperatures of the tantalum/tantalum oxide/manganese
dioxide system make solid tantalum capacitors an
appropriate choice for today's surface mount assembly
technology.
Vishay Sprague has been a pioneer and leader in this field,
producing a large variety of tantalum capacitor types for
consumer, industrial, automotive, military, and aerospace
electronic applications.
Tantalum is not found in its pure state. Rather, it is
commonly found in a number of oxide minerals, often in
combination with Columbium ore. This combination is
known as “tantalite” when its contents are more than
one-half tantalum. Important sources of tantalite include
Australia, Brazil, Canada, China, and several African
countries. Synthetic tantalite concentrates produced from
tin slags in Thailand, Malaysia, and Brazil are also a
significant raw material for tantalum production.
Electronic applications, and particularly capacitors,
consume the largest share of world tantalum production.
Other important applications for tantalum include cutting
tools (tantalum carbide), high temperature super alloys,
chemical processing equipment, medical implants, and
military ordnance.
Vishay Sprague is a major user of tantalum materials in the
form of powder and wire for capacitor elements and rod and
sheet for high temperature vacuum processing.
THE BASICS OF TANTALUM CAPACITORS
Most metals form crystalline oxides which are
non-protecting, such as rust on iron or black oxide on
copper. A few metals form dense, stable, tightly adhering,
electrically insulating oxides. These are the so-called
“valve”metals and include titanium, zirconium, niobium,
tantalum, hafnium, and aluminum. Only a few of these
permit the accurate control of oxide thickness by
electrochemical means. Of these, the most valuable for the
electronics industry are aluminum and tantalum.
Capacitors are basic to all kinds of electrical equipment,
from radios and television sets to missile controls and
automobile ignitions. Their function is to store an electrical
charge for later use.
Capacitors consist of two conducting surfaces, usually
metal plates, whose function is to conduct electricity. They
are separated by an insulating material or dielectric. The
dielectric used in all tantalum electrolytic capacitors is
tantalum pentoxide.
Tantalum pentoxide compound possesses high-dielectric
strength and a high-dielectric constant. As capacitors are
being manufactured, a film of tantalum pentoxide is applied
to their electrodes by means of an electrolytic process. The
film is applied in various thicknesses and at various voltages
and although transparent to begin with, it takes on different
colors as light refracts through it. This coloring occurs on the
tantalum electrodes of all types of tantalum capacitors.
Rating for rating, tantalum capacitors tend to have as much
as three times better capacitance/volume efficiency than
aluminum electrolytic capacitors. An approximation of the
capacitance/volume efficiency of other types of capacitors
may be inferred from the following table, which shows the
dielectric constant ranges of the various materials used in
each type. Note that tantalum pentoxide has a dielectric
constant of 26, some three times greater than that of
aluminum oxide. This, in addition to the fact that extremely
thin films can be deposited during the electrolytic process
mentioned earlier, makes the tantalum capacitor extremely
efficient with respect to the number of microfarads available
per unit volume. The capacitance of any capacitor is
determined by the surface area of the two conducting
plates, the distance between the plates, and the dielectric
constant of the insulating material between the plates.
In the tantalum electrolytic capacitor, the distance between
the plates is very small since it is only the thickness of the
tantalum pentoxide film. As the dielectric constant of the
tantalum pentoxide is high, the capacitance of a tantalum
capacitor is high if the area of the plates is large:
where
C = capacitance
e = dielectric constant
A = surface area of the dielectric
t = thickness of the dielectric
Tantalum capacitors contain either liquid or solid
electrolytes. In solid electrolyte capacitors, a dry material
(manganese dioxide) forms the cathode plate. A tantalum
lead is embedded in or welded to the pellet, which is in turn
connected to a termination or lead wire. The drawings show
the construction details of the surface mount types of
tantalum capacitors shown in this catalog.
COMPARISON OF CAPACITOR
DIELECTRIC CONSTANTS
DIELECTRIC e
DIELECTRIC CONSTANT
Air or vacuum 1.0
Paper 2.0 to 6.0
Plastic 2.1 to 6.0
Mineral oil 2.2 to 2.3
Silicone oil 2.7 to 2.8
Quartz 3.8 to 4.4
Glass 4.8 to 8.0
Porcelain 5.1 to 5.9
Mica 5.4 to 8.7
Aluminum oxide 8.4
Tantalum pentoxide 26
Ceramic 12 to 400K
CeA
t
-------
=
VISHAY.
pomechfilvlshaxmom
www.vushay.com/doc791000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 2Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
SOLID ELECTROLYTE POLYMER TANTALUM CAPACITORS
Solid electrolyte polymer capacitors utilize sintered tantalum pellets as anodes. Tantalum pentoxide dielectric layer is formed
on the entire surface of anode, which is further impregnated with highly conductive polymer as cathode system.
The conductive polymer layer is then coated with graphite, followed by a layer of metallic silver, which provides a conductive
surface between the capacitor element and the outer termination (lead frame or other).
Molded chip polymer tantalum capacitor encases the element in plastic resins, such as epoxy materials. After assembly, the
capacitors are tested and inspected to assure long life and reliability. It offers excellent reliability and high stability for variety of
applications in electronic devices. Usage of conductive polymer cathode system provides very low equivalent series resistance
(ESR), which makes the capacitors particularly suitable for high frequency applications.
TANTALUM CAPACITOR WITH POLYMER CATHODE TYPE T55
TANTALUM CAPACITOR WITH POLYMER CATHODE TYPE T58
Silver adhesive
Solderable cathode termination
Polymer / carbon / silver coating
Sintered tantalum pellet
Epoxy encapsulation
Lead frame welded to Ta wire
Anode polarity bar
Solderable anode termination
Anode polarity bar
Side anode termination (+)
Side cathode termination (-) Encapsulation
Sintered tantalum pellet
Polymer / carbon / silver coating
Glass reinforced epoxy resin substrate
Bottom cathode termination (-)
Silver adhesive epoxy
Conductive strip
Rating / marking
Bottom anode termination (+)
Copper pad
Anode wire
VISHAY.
pa‘flech@vlshay.com
www.vushay.com/doc791000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 3Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
TANTALUM CAPACITOR WITH POLYMER CATHODE TYPE T52
TANTALUM CAPACITOR WITH POLYMER CATHODE TYPE T54 / T59
Polarity bar
marking
Side anode termination (+)
Side cathode termination (-)
Bottom anode
termination (+)
Silver plated copper substrate
Bottom cathode
termination (-)
Silver adhesive epoxy
Conductive strip
T52 E5 case
Encapsulation
Polymer / carbon / silver coating
Sintered
tantalum pellet
T52 M1 case
Side anode termination (+)
Bottom anode termination (+)
Polarity bar marking
Side cathode termination (-)
Sintered
tantalum pellet
Polymer / carbon / silver coating
Silver plated
copper substrate
Bottom cathode termination (-)
Silver adhesive epoxy
Encapsulation
Anode polarity marking
Side anode termination (+)
Side cathode termination (-)
Encapsulation
Sintered tantalum pellet
Polymer / carbon / silver coating
Top / bottom cathode termination (-)
Silver plated copper substrate
Top / bottom cathode termination (-)
Top / bottom anode termination (+)
Top / bottom anode termination (+)
Conductive strip
Silver adhesive epoxy
VISHAY.
m9. ms) 0 Q Q Q
gomechfilvlshayLom
www.v\shay.com/doc?91000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 4Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
POLYMER CAPACITORS - MOLDED CASE
SERIES T55
PRODUCT IMAGE
TYPE VPolyTanTM, molded case, high performance polymer
FEATURES High performance
TEMPERATURE RANGE -55 °C to +105 °C
CAPACITANCE RANGE 3.3 F to 1000 F
VOLTAGE RANGE 2.5 V to 63 V
CAPACITANCE TOLERANCE ± 20 %
LEAKAGE CURRENT 0.1 CV
DISSIPATION FACTOR 8 % to 10 %
ESR 12 m to 500 m
CASE SIZES J, P, A, T, B, Z, V, D
TERMINATION FINISH
Cases J, P: 100 % tin
Case A: 100 % tin or Ni / Pd / Au
Cases T, B, Z, V, D: Ni / Pd / Au
POLYMER CAPACITORS - LEADFRAMELESS MOLDED CASE
SERIES T52 T58 T59 T54
PRODUCT
IMAGE
TYPE
vPolyTanTM polymer
surface mount chip
capacitors, low profile,
leadframeless molded type
vPolyTanTM polymer surface
mount chip capacitors,
compact, leadframeless
molded type
vPolyTanTM polymer surface
mount chip capacitors,
low ESR, leadframeless
molded type
vPolyTanTM polymer
surface mount chip
capacitors, low ESR,
leadframeless molded type,
hi-rel commercial
off-the-shelf (COTS)
FEATURES Low profile Small case size Multianode Hi-rel COTS, multianode
TEMPERATUR
E RANGE -55 °C to +105 °C -55 °C to +105 °C -55 °C to +105 °C -55 °C to +125 °C
CAPACITANCE
RANGE 47 µF to 1500 µF 1 µF to 330 µF 15 µF to 470 µF 15 µF to 470 µF
VOLTAGE
RANGE 10 V to 35 V 6.3 V to 35 V 16 V to 75 V 16 V to 75 V
CAPACITANCE
TOLERANCE ± 20 % ± 20 % ± 10 %, ± 20 % ± 20 %
LEAKAGE
CURRENT 0.1 CV
DISSIPATION
FACTOR 10 % 8 % to 14 % 10 % 10 %
ESR 25 m to 55 m50 m to 500 m25 m to 150 m25 m to 150 m
CASE SIZES E5, M1 MM, M0, W0, W9,
A0, AA, B0, BB EE EE
TERMINATION 100 % tin 100 % tin / lead
—
VISHAY.
l:l
-l—L
gomecmvusnamom
www.msha .com/d05791000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 5Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
MOLDED CAPACITORS, T55 TYPE
Note
• A reel diameter of 330 mm is also applicable
Note
• A reel diameter of 330 mm is also applicable
PLASTIC TAPE AND REEL PACKAGING DIMENSIONS in millimeters
TAPE WIDTH 8 12
A + 0 / - 3 Ø 180
B + 1 / 0 Ø 60
C ± 0.2 Ø 13
D ± 0.5 Ø 21
E ± 0.5 2.0
W ± 0.3 9.0 13.0
PLASTIC TAPE SIZE DIMENSIONS in millimeters
CASE CODE A ± 0.2 B ± 0.2 W ± 0.3 F ± 0.1 E ± 0.1 P1 ± 0.1 tmax.
J 1.0 1.8 8.0 3.5 1.75 4.0 1.3
P 1.4 2.2 8.0 3.5 1.75 4.0 1.6
A 1.9 3.5 8.0 3.5 1.75 4.0 2.5
T 3.1 3.8 8.0 3.5 1.75 4.0 1.7
B 3.1 3.8 8.0 3.5 1.75 4.0 2.5
Z 4.8 7.7 12.0 5.5 1.75 8.0 2.6
V 4.8 7.7 12.0 5.5 1.75 8.0 2.6
D 4.8 7.7 12.0 5.5 1.75 8.0 3.4
Label
DE
W
B
A
C
Perforation
Direction of tape flow
Inserting direction
t
A
F
P1
W
B
E
Ø 1.5
Pocket
+ 0.1
0
4.0 ± 0.1
2.0 ± 0.1
Perforation
Symbol: R
Marking side (upper)
Mounting terminal side (lower)
—
VISHAY.
V
gomechfilvlshayLom
www.msha .com/d05791000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 6Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
LEADFRAMELESS MOLDED CAPACITORS, ALL TYPES
Notes
• Metric dimensions will govern. Dimensions in inches are rounded and for reference only
(1) A0, B0, K0, are determined by the maximum dimensions to the ends of the terminals extending from the component body and / or the body
dimensions of the component. The clearance between the ends of the terminals or body of the component to the sides and depth of the
cavity (A0, B0, K0) must be within 0.002" (0.05 mm) minimum and 0.020" (0.50 mm) maximum. The clearance allowed must also prevent
rotation of the component within the cavity of not more than 20°
(2) Tape with components shall pass around radius “R” without damage. The minimum trailer length may require additional length to provide
“R” minimum for 12 mm embossed tape for reels with hub diameters approaching N minimum
(3) This dimension is the flat area from the edge of the sprocket hole to either outward deformation of the carrier tape between the embossed
cavities or to the edge of the cavity whichever is less
(4) This dimension is the flat area from the edge of the carrier tape opposite the sprocket holes to either the outward deformation of the carrier
tape between the embossed cavity or to the edge of the cavity whichever is less
(5) The embossed hole location shall be measured from the sprocket hole controlling the location of the embossment. Dimensions of
embossment location shall be applied independent of each other
(6) B1 dimension is a reference dimension tape feeder clearance only
PLASTIC TAPE AND REEL PACKAGING in inches [millimeters]
Tape and Reel Specifications: all case sizes are
available on plastic embossed tape per EIA-481.
Standard reel diameter is 7" [178 mm].
0.004 [0.10]
max.
K0
Tape thickness
B1 (max.) (6)
0.014
[0.35]
max.
10 pitches cumulative
tolerance on tape
± 0.008 [0.200]
Embossment
0.069 ± 0.004
[1.75 ± 0.10]
D1 (min.) for components
0.079 x 0.047 [2.0 x 1.2] and larger (5)
.
Maximum
USER DIRECTION
OF FEED
Center lines
of cavity
A0
P1
FW
0.030 [0.75]
min. (3)
0.030 [0.75]
min. (4)
0.079 ± 0.002
[2.0 ± 0.05]
0.157 ± 0.004
[4.0 ± 0.10]
0.059 + 0.004 - 0.0
[1.5 + 0.10 - 0.0]
B0
Maximum
component
rotation
(Side or front sectional view)
20°
For tape feeder
reference only
including draft.
Concentric around B0
(5)
Deformation
between
embossments
Top
cover
tape
Top cover
tape
cavity size (1)
Cathode (-)
Anode (+)
DIRECTION OF FEED
20° maximum
component rotation
Typical
component
cavity
center line
Typical
component
center line
A0
B0
(Top view)
0.9843 [250.0]
Tape
3.937 [100.0]
0.039 [1.0]
max.
0.039 [1.0]
max.
Camber
Allowable camber to be 0.039/3.937 [1/100]
(Top view)
Non-cumulative over 9.843 [250.0]
VISHAY.
gomecmvusnamom
www.v\shay,com/doc?91000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 7Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
Notes
(1) For reference only
(2) Standard packaging of MM case is with paper tape. Plastic tape is available per request
Note
(1) A0, B0 are determined by the maximum dimensions to the ends of the terminals extending from the component body and / or the body
dimensions of the component. The clearance between the ends of the terminals or body of the component to the sides and depth of the
cavity (A0, B0) must be within 0.002" (0.05 mm) minimum and 0.020" (0.50 mm) maximum. The clearance allowed must also prevent rotation
of the component within the cavity of not more than 20°
CARRIER TAPE DIMENSIONS in inches [millimeters]
CASE CODE TAPE SIZE B1 (MAX.) (1) D1 (MIN.) F K0 (MAX.) P1W
E5 12 mm 0.329 [8.35] 0.059 [1.5] 0.217 ± 0.002
[5.50 ± 0.05] 0.071 [1.8] 0.315 ± 0.004
[8.0 ± 0.10]
0.476 ± 0.008
[12.1 ± 0.20]
MM (2) 8 mm 0.075 [1.91] 0.02 [0.5] 0.138 [3.5] 0.043 [1.10] 0.157 [4.0] 0.315 [8.0]
M1 12 mm 0.32 [8.2] 0.059 [1.5] 0.217 ± 0.002
[5.5 ± 0.05] 0.094 [2.39] 0.315 ± 0.04
[8.0 ± 1.0]
0.472 + 0.012 / - 0.004
[12.0 + 0.3 / - 0.10]
W9 8 mm 0.126 [3.20] 0.030 [0.75] 0.138 [3.5] 0.045 [1.15] 0.157 [4.0] 0.315 [8.0]
W0 8 mm 0.126 [3.20] 0.030 [0.75] 0.138 [3.5] 0.045 [1.15] 0.157 [4.0] 0.315 [8.0]
A0 8 mm - 0.02 [0.5] 0.138 [3.5] 0.049 [1.25] 0.157 [4.0] 0.315 [8.0]
AA 8 mm 0.154 [3.90] 0.039 [1.0] 0.138 [3.5] 0.079 [2.00] 0.157 [4.0] 0.315 [8.0]
B0 12 mm 0.181 [4.61] 0.059 [1.5] 0.217 [5.5] 0.049 [1.25] 0.157 [4.0] 0.315 [8.0]
BB 8 mm 0.157 [4.0] 0.039 [1.0] 0.138 [3.5] 0.087 [2.22] 0.157 [4.0] 0.315 [8.0]
EE 12 mm 0.32 [8.2] 0.059 [1.5] 0.217 ± 0.002
[5.5 ± 0.05] 0.175 [4.44] 0.315 ± 0.04
[8.0 ±1.0]
0.472 + 0.012 / - 0.004
[12.0 + 0.3 / - 0.10]
PAPER TAPE AND REEL PACKAGING DIMENSIONS in inches [millimeters]
CASE
SIZE
TAPE
SIZE A
0
B
0
D
0
P
0
P
1
P
2
EFWT
MM 8 mm 0.041 ± 0.002
[1.05 ± 0.05]
0.071 ± 0.002
[1.8 ± 0.05]
0.06 ± 0.004
[1.5 ± 0.1]
0.157 ± 0.004
[4.0 ± 0.1]
0.157 ± 0.004
[4.0 ± 0.1]
0.079 ± 0.002
[2.0 ± 0.05]
0.069 ± 0.004
[1.75 ± 0.1]
0.0138 ± 0.002
[3.5 ± 0.05]
0.315 ± 0.008
[8.0 ± 0.2]
0.037 ± 0.002
[0.95 ± 0.05]
M0 8 mm 0.049 ± 0.002
[1.25 ± 0.05]
0.081 ± 0.002
[2.05 ± 0.05]
0.06 ± 0.004
[1.5 ± 0.1]
0.157 ± 0.004
[4.0 ± 0.1]
0.157 ± 0.004
[4.0 ± 0.1]
0.079 ± 0.002
[2.0 ± 0.05]
0.069 ± 0.004
[1.75 ± 0.1]
0.0138 ± 0.002
[3.5 ± 0.05]
0.315 ± 0.008
[8.0 ± 0.2]
0.041 ± 0.002
[1.05 ± 0.05]
Ø D
0
T
Bottom cover
tape
F
P
1
A
0
B
0
E
2
P
2
W
P
0
E
1
Cavity size
(1)
Bottom cover tape
USER FEED DIRECTION
Cavity center lines
Top
cover tape
[10 pitches cumulative tolerance on tape ± 0.2 mm]
G
Anode
VISHAY.
T “Cs
V 4
+
+
.7 4.
.7 4.
gomecmvusnamom
www.v\shay,com/doc?91000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 8Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
PACKING AND STORAGE
Polymer capacitors meet moisture sensitivity level rating (MSL) of 3 or 4 as specified in IPC/JEDEC® J-STD-020 and are dry
packaged in moisture barrier bags (MBB) per J-STD-033. MSL for each particular family is defined in the datasheet - either in
“Features” section or “Standard Ratings” table. Level 3 specifies a floor life (out of bag) of 168 hours and level 4 specifies a floor
life of 72 hours at 30 °C maximum and 60 % relative humidity (RH). Unused capacitors should be re-sealed in the MBB with
fresh desiccant. A moisture strip (humidity indicator card) is included in the bag to assure dryness. To remove excess moisture,
capacitors can be dried at 40 °C (standard “dry box” conditions).
For detailed recommendations please refer to J-STD-033.
Notes
• T52, T55, and T58 capacitors are process sensitive.
PSL classification to JEDEC J-STD-075: R4G
• T54 and T59 capacitors with 100 % tin termination are process sensitive.
PSL classification to JEDEC J-STD-075: R6G
RECOMMENDED REFLOW PROFILES
Vishay recommends no more than 3 cycles of reflow in accordance with J-STD-020.
PROFILE FEATURE SnPb EUTECTIC ASSEMBLY LEAD (Pb)-FREE ASSEMBLY
PREHEAT AND SOAK
Temperature min. (TSmin.) 100 °C 150 °C
Temperature max. (TSmax.) 150 °C 200 °C
Time (tS) from (TSmin. to TSmax.) 60 s to 120 s 60 s to 120 s
RAMP UP
Ramp-up rate (TL to Tp) 3 °C/s maximum
Liquidus temperature (TL) 183 °C 217 °C
Time (tL) maintained above TL60 s to 150 s
Peak package body temperature (Tp) max. Depends on type and case - see table below
Time (tp) within 5 °C of the peak max. temperature 20 s 5 s
RAMP DOWN
Ramp-down rate (Tp to TL) 6 °C/s maximum
Time from 25 °C to peak temperature 6 min maximum 8 min maximum
PEAK PACKAGE BODY TEMPERATURE (Tp) MAXIMUM
TYPE CASE CODE PEAK PACKAGE BODY TEMPERATURE (TP) MAX.
SnPb EUTECTIC ASSEMBLY LEAD (Pb)-FREE ASSEMBLY
T55 J, P, A, T, B, Z, V, D
n/a
260 °C
T52 E5, M1 260 °C
T58 MM, M0, W9, W0, A0, AA, B0, BB 260 °C
T59 EE 220 °C 250 °C
T54 EE 220 °C 250 °C
Time
Temperature
tS
Time 25 °C to peak
tp
TP
TL
TSmin.
25
tL
TSmax. Preheat area
Max. ramp up rate = 3 °C/s
Max. ramp down rate = 6 °C/s
VISHAY.
gomecmvusnamom
www.v\shay,com/doc?91000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 9Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
MOLDED CAPACITORS, T55 TYPE
LEADFRAMELESS MOLDED CAPACITORS, ALL TYPES
PAD DIMENSIONS in millimeters
CASE /
DIMENSIONS
CAPACITOR SIZE PAD DIMENSIONS
L W G (max.) Z (min.) X (min.) Y (Ref.)
J 1.6 0.8 0.7 2.5 1.0 0.9
P 2.0 1.25 0.5 2.6 1.2 1.05
A 3.2 1.6 1.1 3.8 1.5 1.35
T / B 3.5 2.8 1.4 4.1 2.7 1.35
Z / V / D 7.3 4.3 4.1 8.2 2.9 2.05
PAD DIMENSIONS in inches [millimeters]
FAMILY CASE CODE A (NOM.) B (MIN.) C (NOM.) D (MIN.)
T52
E5 0.094 [2.40] 0.073 [1.85] 0.187 [4.75] 0.333 [8.45]
M1 0.161 [4.10] 0.073 [1.85] 0.187 [4.75] 0.333 [8.45]
T58
MM, M0 0.024 [0.61] 0.027 [0.70] 0.025 [0.64] 0.080 [2.03]
W0, W9 0.035 [0.89] 0.029 [0.74] 0.041 [1.05] 0.099 [2.52]
AA, A0, A2 0.047 [1.19] 0.042 [1.06] 0.065 [1.65] 0.148 [3.76]
BB, B0 0.094 [2.39] 0.044 [1.11] 0.072 [1.82] 0.159 [4.03]
T59 / T54 EE 0.209 [5.30] 0.098 [2.50] 0.169 [4.30] 0.366 [9.30]
Capacitor
Pattern
L
Y
Z
G
XW
A
BC
D
—
VISHAY.
V
gomechfilvlshayLom
Com/605791000
Polymer Guide
www.vishay.com Vishay
Revision: 09-Apr-2019 10 Document Number: 40076
For technical questions, contact: polytech@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
GUIDE TO APPLICATION
1. AC Ripple Current: the maximum allowable ripple
current shall be determined from the formula:
where,
P = power dissipation in W at +45 °C as given in
the tables in the product datasheets.
RESR = the capacitor equivalent series resistance at
the specified frequency.
2. AC Ripple Voltage: the maximum allowable ripple
voltage shall be determined from the formula:
or, from the formula:
where,
P = power dissipation in W at +45 °C as given in
the tables in the product datasheets.
RESR = The capacitor equivalent series resistance at
the specified frequency.
Z = The capacitor impedance at the specified
frequency.
2.1 The tantalum capacitors must be used in such a
condition that the sum of the working voltage and
ripple voltage peak values does not exceed the rated
voltage as shown in figure below.
3. Temperature Derating: power dissipation is
affected by the heat sinking capability of the
mounting surface. If these capacitors are to
be operated at temperatures above +45 °C, the
permissible ripple current (or voltage) shall be
calculated using the derating coefficient as shown in
the table below:
4. Reverse Voltage: the capacitors are not intended for
use with reverse voltage applied. However, they are
capable of withstanding momentary reverse voltage
peaks, which must not exceed the following values:
At 25 °C: 10 % of the rated voltage or 1 V, whichever
is smaller.
At 85 °C: 5 % of the rated voltage or 0.5 V, whichever
is smaller.
At 105 °C: 3 % of the rated voltage or 0.3 V,
whichever is smaller.
5. Mounting Precautions:
5.1 Limit Pressure on Capacitor Installation with
Mounter: pressure must not exceed 4.9 N with a tool
end diameter of 1.5 mm when applied to the
capacitors using an absorber, centering tweezers, or
similar (maximum permitted pressurization time: 5 s).
An excessively low absorber setting position would
result in not only the application of undue force to the
capacitors but capacitor and other component
scattering, circuit board wiring breakage, and / or
cracking as well, particularly when the capacitors are
mounted together with other chips having a height of
1 mm or less.
5.2 Flux Selection
5.2.1 Select a flux that contains a minimum of chlorine and
amine.
5.2.2 After flux use, the chlorine and amine in the flux
remain must be removed.
5.3 Cleaning After Mounting: the following solvents are
usable when cleaning the capacitors after mounting.
Never use a highly active solvent.
• Halogen organic solvent (HCFC225, etc.)
• Alcoholic solvent (IPA, ethanol, etc.)
• Petroleum solvent, alkali saponifying agent, water,
etc.
Circuit board cleaning must be conducted at a
temperature of not higher than 50 °C and for an
immersion time of not longer than 30 minutes. When
an ultrasonic cleaning method is used, cleaning must
be conducted at a frequency of 48 kHz or lower, at
an vibrator output of 0.02 W/cm3, at a temperature of
not higher than 40 °C, and for a time of 5 minutes or
shorter.
Notes
• Care must be exercised in cleaning process so that the
mounted capacitor will not come into contact with any
cleaned object or the like or will not get rubbed by a stiff
brush or similar. If such precautions are not taken
particularly when the ultrasonic cleaning method is
employed, terminal breakage may occur
• When performing ultrasonic cleaning under conditions
other than stated above, conduct adequate advance
checkout
MAXIMUM RIPPLE CURRENT TEMPERATURE
DERATING FACTOR
45 °C 1.0
55 °C 0.8
85 °C 0.6
105 °C 0.4
IRMS
P
RESR
------------=
VRMS ZP
RESR
------------=
VRMS IRMS x Z=
Voltage
Rated voltage
Ripple voltage
Operating
voltage
Working voltage
Time (s)
Products related to this Datasheet
CAP TANT POLY 22UF 10V 1206
CAP TANT POLY 22UF 4V 1206
CAP TANT POLY 68UF 4V 1206
CAP TANT POLY 4.7UF 6.3V 0805
CAP TANT POLY 220UF 6.3V 1411
CAP TANT POLY 100UF 4V 1206
CAP TANT POLY 15UF 12.5V 1411
CAP TANT POLY 330UF 16V 2924
CAP TANT POLY 10UF 6.3V 0805
CAP TANT POLY 10UF 10V 1206
CAP TANT POLY 4.7UF 10V 1206
CAP TANT POLY 22UF 6.3V 1411
CAP TANT POLY 4.7UF 6.3V 0603
CAP TANT POLY 3.3UF 6.3V 0603
CAP TANT POLY 150UF 30V 2917
CAP TANT POLY 3.3UF 10V 0805
CAP TANT POLY 3.3UF 6.3V 0805
CAP TANT POLY 4.7UF 10V 0805
CAP TANT POLY 100UF 4V 1411
CAP TANT POLY 100UF 6.3V 1411
CAP TANT POLY 33UF 10V 1411
CAP TANT POLY 3.3UF 10V 0603
CAP TANT POLY 150UF 6.3V 1411
CAP TANT POLY 47UF 6.3V 1411
CAP TANT POLY 33UF 6.3V 1411
CAP TANT POLY 15UF 4V 0805
CAP TANT POLY 15UF 12.5V 1411
CAP TANT POLY 22UF 6.3V 1411
CAP TANT POLY 47UF 35V 2917
CAP TANT POLY 47UF 35V 2917