CY4609 Quick Start Guide Datasheet by Cypress Semiconductor Corp
View All Related Products | Download PDF DatasheetHX3 USB 3.0 HUB REFERENCE DESIGN KIT (RDK)
CY4609 QUICK START GUIDE
Step 1: Configuring the HX3 Board
• Unpack the kit contents which includes RDK board, 5-V 4-A
AC-DC adapter and the USB 3.0 A to micro-B cable
• Ensure that the configuration mode select jumpers (J6
and J7)
are set for default operation, as shown above
Step 2: Powering the HX3
Board
• Plug the AC-DC adapter into an AC wall power receptacle.
Connect the power supply plug to the board’s DC supply
jack. The power LED (PWR) glows green to indicate that
the board is powered and the suspend status LED (SUSP)
glows amber to indicate that the hub is in suspend mode
2
1
3 4
56
Step 3: Connecting the HX3
Board
to a USB 3.0 PC / Laptop
• Connect the micro-B end of the USB cable to the
board’s
upstream port; connect the other end to the USB 3.0
receptacle on a PC / laptop. The SUSP LED* turns off
(on a PC / laptop running Windows 7 operating system)
Step 4: Demonstrating USB 3.0 Data Transfer
• Get a USB 3.0 certified flash drive and store a 2 GB file.
Connect the flash drive to one of the downstream ports
• Copy the 2 GB file from the flash drive to the PC / laptop
to transfer data in USB 3.0 mode
Step 5: Demonstrating Battery Charging
• Connect an Apple device or an USB battery charging
device to any of the downstream ports. The HX3 board
will charge the connected device
Note: When the Ghost Charging feature is enabled, charging
of the device stops momentarily and resumes in 1-2 seconds
Step 6: Demonstrating Ghost ChargingTM
• Disconnect the USB cable from the upstream port to detach
the board from the PC / laptop. The device connected to
the
downstream port continues to be charged using the
Ghost ChargingTM feature
Configuration
mode select
jumpers
Indicates the version of
HX3 Silicon. "C"
indicates HX3 *C Silicon
Note: Kits with HX3 *C
Silicon supports
internal ROM Boot.
Install jumpers on pins
1 and 2 of Jumpers
J6 and J7 to
boot from
Internal ROM
DC Supply
Jack (J1)
USB 3.0
port on the
PC/Laptop
USB cable
connected to
upstream port
Battery charging
through a
downstream port
USB 3.0 flash drive connected
to a downstream port
Power
LED (PWR)
J6
J7
* The behavior of the SUSP LED varies across operating systems.
For e.g, in Windows 8, the SUSP LED turns off momentarily and turns
on again when there is no further USB activity on the board
Suspend Status
LED (SUSP)
Suspend
Status
LED (SUSP)
Pin 3 Pin 2 Pin 1
It
‘I
JEYPRESS‘
mm” m mm.
© 2014 - 2017 Cypress Semiconductor Corporation. All rights reserved.
All trademarks or registered trademarks referenced herein are the properties of their respective owners.
Doc.#: 001-90183 Rev.*C
Downstream Port 3
(DS3/J3)
Downstream Port 2
(DS2/J5)
Downstream Port 1
(DS1/J9)
Power LED
(PWR)
Suspend
Status LED
(SUSP)
5-V DC
Supply
Jack (J1)
Configuration
Mode Select
Jumpers (J6 and J7)
USB 3.0 Upstream Port
(US/J8)
Downstream Port 4
(DS4 / J4)
HX3 (MPN:
CYUSB3304-
68LTXC)
Reset Switch
(SW1)
5-V to 3.3-V
Regulator (U2)
CY4609 QUICK START GUIDE
For the latest information about HX3 products, visit www.cypress.com/hx3
HX3 USB 3.0 HUB REFERENCE DESIGN KIT (RDK)
Kit Operation: CY4609 is the reference design kit for CYUSB3304-68LTXC, a 4-port USB 3.0 hub controller from
Cypress. The hub controller supports Low-Speed (LS), Full-Speed (FS), Hi-Speed (HS) and SuperSpeed (SS) peripherals
on all the four downstream ports. It goes into Suspend state to save power when the upstream port is not connected to
a PC / laptop. All the downstream ports are compliant to USB Battery Charging Specification v1.2; they also emulate
Apple charging. The hub controller also supports Ghost Charging, a unique feature where the downstream ports
emulate Dedicated Charging Port (DCP) to support battery charging even when the upstream port of the board is not
connected to a PC / laptop.
The hub controller can be configured for parameters such as vendor ID, product ID, etc. using a Windows based PC
tool named Blaster Plus. The configured values are stored in an on-board EEPROM. To access the Blaster Plus tool, the
kit user guide, and the hardware design files, download the RDK EXE file (CY4609HX3RDKSetup.exe) from
www.cypress.com/go/CY4609. Click the EXE file and follow the steps in the installer window.
Sensitive Area -
Do not touch
Products related to this Datasheet
EVAL BOARD HX3 USB HUB CYUSB3304