M‘
Am
—®
A Companion Chip For Atmel CryptoRF &
CryptoMemory Products
Features
• Companion Chip to CryptoRF® and CryptoMemory®
⎯ Securely implements host algorithms
⎯ Securely stores host secrets
⎯ Verifies Host Firmware Digests
• High Security Features in Hardware
⎯ CryptoMemory and CryptoRF F2 Algorithm
⎯ SHA-1 Standard Cryptographic Algorithm
⎯ 64-bit Mutual Authentication Protocol (Under License of ELVA)
⎯ Permanently Coded Serial Numbers
⎯ High Quality Random Number Generator (RNG)
⎯ Metal Shield Over Memory
⎯ Data Scrambling in Nonvolatile Memory
⎯ Delay Penalties to prevent Systematic Attacks
⎯ Reset Locking to prevent Illegal Power Cycling
⎯ Voltage and Frequency Monitors
• Host-side Crypto Functions
⎯ Authentication Challenge Generation
⎯ Device Challenge Response
⎯ Message Authentication Codes (MAC) Generation
⎯ Data Encryption and Decryption
⎯ Secure Authentication Key Management
• Secure Storage and Key Management
⎯ Up to 16 sets of 64-bits Diversified Host Keys
⎯ Eight Sets of Two 24-bit Passwords
⎯ Secure and Custom Personalization
⎯ Up to 232-Byte Read/Write Configurable User Data Area
• Nonvolatile Up Counters
⎯ Four sets Unidirectional Counters
⎯ 6.4 Million Maximum Counts Per Counter
• Application Features
⎯ Low Voltage Supply: 2.7V – 3.6V
⎯ 2-Wire Serial Interface (TWI, 5V Compatible)
⎯ Standard 8-lead SOIC Plastic Package, Green compliant (exceeds RoHS)
• High Reliability
⎯ Endurance : 100,000 Cycles
⎯ Data Retention : 10 years
⎯ ESD Protection : 3,000 V min. HBM
CryptoCompanion™
Chip for
CryptoMemory and
CryptoRF
AT88SC018
5277C–CryptoCompanion–9/09
hug://www.\ILmslgov/figsgubs/fig180-1.hlm
M‘
2 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1. Product Overview
The AT88SC018 is designed as the mate to Atmel’s CryptoRF® (CRF) and CryptoMemory® (CM) chips, collectively
referred to in the remainder of this document as CRF. Within the operation descriptions, the AT88SC018
CryptoCompanion chip is sometimes referred to as CMC or CryptoMemory Companion chip.
The AT88SC018 makes extensive use of the SHA-1 hash algorithm as specified in
http://www.itl.nist.gov/fipspubs/fip180-1.htm and elsewhere. In this document, the nomenclature SHA-1(a, b, c) means
to concatenate a, b & c in that order and then pad them to a block size of 64 bytes before computing the digest. The
AT88SC018 does not ever generate a SHA-1 digest of datasets larger than a single round
1.1. General Operation
The CRF chip contains secrets that must be known or derived by a host system in order to establish a trusted link
between the two and permit communications to happen. The AT88SC018 stores these secrets in an obscured way in
nonvolatile memory and contains all the circuitry necessary to perform the authentication, password and
encryption/decryption functions specified in the CRF datasheet. In this manner, the secrets do not ever need to be
revealed.
The general cryptographic strategy is as follows:
• Each CRF chip has a serial or identification number (ID) and authentication secret Gi stored in EEPROM. ID is freely
readable; Gi can never be read and is unique for all tags.
• The AT88SC018 contains an EEPROM that contains a set of common secrets (Fn). The AT88SC018 combines Fn
with ID and KID to compute a value of G that is expected to match that in the CRF chip. Specifically,
G = SHA-1(Fn, ID, KID)
• G is further diversified by the inclusion of a number (KID) generated by the host system in a manner of its choosing.
Typically, it will be the result of a cryptographic operation on the CRF ID value calculated using other data, secrets
and/or algorithms external to the AT88SC018. This permits scenarios that offer varying degrees of additional
security.
• The AT88SC018 includes a general purpose cryptographic quality random number generator which is used to seed a
mutual authentication process between the AT88SC018 and CRF. If the CRF confirms the CMC challenge, and the
CMC confirms the CRF response, then the host system proceeds with CRF operations. In this way the host system
may use the CRF without knowing the CRF's secrets directly.
1.2. CryptoCompanion Benefits
The following is a partial list of the benefits of using this chip versus storing the algorithms and secrets in standard
FLASH system memory.
• Keep confidential those core secrets that are used to authenticate with and communicate to/from CRF.
(Store them in EEPROM, use them on-chip)
• Flexible system implementation – multiple secrets and policies for different CRF locations within the system.
Multiple manufacturer setup options.
• Hardware encryption engines, avoids algorithm disclosure from reverse-compilation of system operating code.
• Full hardware security implementation makes it harder for an attacker (even with lab equipment) to get secrets stored
on the AT88SC018.
• Global secrets are protected using strong security, standard algorithm (SHA-1).
• Implements a crunching algorithm to prevent micro-controller based CRF replicas.
• Robust random number generation avoids accidental replay for all cryptographic operations using the system, not
just with respect to CRF.
A IIIEI.‘
CryptoCompanion Chip
3
5277C–CryptoCompanion–9/09
• Secure EEPROM storage for configuration information, etc. May permit reduction in the total BOM for the system.
• Easy to use – little programming required; no knowledge of security algorithms or protocols, fast time to market.
1.3. CryptoCompanion Security
The following is a partial list of the security features on this chip.
• Strong internal EEPROM encryption scheme
• Dynamically encrypted internal SRAM data.
• Programmable powerup penalty.
• Escalating Attack penalty.
• Authentication timeouts.
• Anti-tearing counters.
• Anti-tearing RNGSeed.
• Secure Personalization.
• Command usage limitations to prevent exhaustive attacks
• Uniquely encrypted F Secrets inside chip.
• High security Internal Clocking Scheme.
• Over and Under Voltage detection tampers.
• Internal Data integrity validation.
• Active shield over security sensitive blocks
1.4. Package, Pinout & IO
1.4.1. Pinout
All pins not otherwise specified are considered Test pins and should be grounded on the board.
1.4.1.1. VCC , Gnd
Power supply is 2.7 – 3.6V. Supply current less than 5 mA.
CryptoCompanion will be available to accept commands 60 ms after the later of VCC rising above 2.7V or Reset being
driven high if CryptoCompanion is in a security delay then this interval is significantly longer.
During Power Up, VCC must exhibit a monotonic ramp at a minimum rate of 50 mV/mS until VCC has crossed the 2.7V
level. During Power Down, VCC must exhibit a monotonic ramp at a minimum rate of 50 mV/mS once it has dropped
below the 2.5V boundary. CryptoCompanion does not support hot swapping or hot plugging.
VCC must be bypassed with high quality surface mount capacitors that are properly located on the board. Atmel
recommends two capacitors connected in parallel having a value of 1μF and 0.01μF. The capacitors should be
manufactured using X5R or X7R dielectric material. These capacitors should be connected to the AT88SC018 using a
total of no more than 1cm PC board traces. Atmel recommends the use of a ground plane and a trace length of less
than 0.5cm between the capacitors and the VCC pin. Failure to follow these recommendations may result in improper
operation.
1.4.1.2. SDA
Two wire interface data pin, 5 V compatible. Data setup time = 0.1 μs minimum data hold time = 0 μs min. The system
board must include an external pull-up resistor.
A IIIEI.‘
4 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.4.1.3. SCL
Two wire interface clock pin, 5 V compatible. Maximum SCL rate is 400KHz, min. TLOW = 1.2 μs, min. THIGH = 0.6 μs.
The system board must include an external pull-up resistor.
1.4.1.4. Reset (RST)
This active low input will reset all states within the AT88SC018. It is honored regardless of the state of PowerDown.
1.4.1.5. PowerDown(PDN)
When held low, the part operates normally. When held high the part will go to sleep and ignore all transitions on SDA
and SCL, power consumption will drop to less than 10 μA. There is a 50 ms delay between this pin falling and the first
transition on SDA or SCL that will be accepted by the chip.
1.4.2. Package
The AT88SC018 is packaged in an 8 lead SOIC package, pinout is as follows:
Table 1. 8 lead SOIC package pinout
Pin Number Pin Name
1 VCC
5 GND
7 SDA
8 SCL
4 RST
3 PDN
2,6 NC
Pins 2 & 6 are not internally connected and should be connected to ground on the PC board.
1.4.3. Connection Diagram
Figure 1. Connection Diagram
2.7v - 5.5v
2.7v - 3.6v
SDA
SCL
Microprocessor CryptoCompanion
Command Descnghons.
Command Descrig‘ions
A IIIEI.‘
CryptoCompanion Chip
5
5277C–CryptoCompanion–9/09
1.4.4. Environmental
The AT88SC018 is guaranteed to operate over the industrial temperature range of -40°to 85°C. ESD is rated at 2KV,
Human Body Model.
1.4.5. TWI Input/Output Operation
The AT88SC018 communicates to the system using a two wire interface (TWI), which is similar to SMBus™. The chip
operates as a slave and does not support clock stretching. This two wire protocol is identical to that supported by the
Atmel AT24C16B serial EEPROM chips. Refer to the datasheet on the Atmel web site for detailed timing and protocol
information.
The system processor is expected to properly format commands for the AT88SC018 (which may include information
from the CRF chip), and then process the outputs of the AT88SC018 (which may include sending some of the outputs
to the CRF chip).
The AT88SC018 cannot directly communicate with CRF or CM chips. Both CRF/CM and the AT88SC018 are slave
devices. The bus master may use one or two busses to communicate with them. Separate TWI addresses must be
used if both chips are on the same bus.
Table 2. AT88SC018 communications packets naming conventions.
AT88SC018
Name TWI Name Description
Device Address Device Name This byte selects a particular chip on the two wire bus. Bit 1 of this byte on the
AT88SC018 selects between accesses to command/data (if 0) or the status
register (if 1). Bit 0 of this byte is the standard two wire R/W pin, if 1 then the bytes
following the device address travel from the slave to the master (Read) if 0 these
bytes flow to the slave (Write).
Cmd Word Address If the device address specified a command input (TWI write), then this byte
specifies the command to be executed by the AT88SC018. This byte doesn’t exist
on read operations.
Size DataN The total number of bytes to follow this byte may be 0 in the case that there are no
operand bytes. This byte doesn’t exist on status read operations.
Data DataN+1 , … Operand input or output bytes as specified in the command descriptions in
Command Descriptions.
If the upper 6 bits of the device address byte sent over the TWI match the upper 6 bits of the Dev field in the EEPROM,
then the AT88SC018 may respond to this transmission, otherwise it will NACK this byte. Dev is set to a value of 0xC0
on shipment from Atmel.
In general, the AT88SC018 will fail to ACK (NACK) the device address byte if bit 1 of the device address is 0
(command/data transfer) and the AT88SC018 is busy.
The AT88SC018 is designed in such a way that the TWI Size field should be consistent with the count values specified
in the command parameter descriptions from Command Descriptions. If the TWI size field is inconsistent with the
command parameter count value, the AT88SC018 will respond in different ways depending on the specific command.
Some of these responses may include security penalties, other error indications or some input bytes may be silently
ignored.
M.
Command Descnghons.
Sechon 1.6.4.
6 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.4.5.1. Command Input
Table 3. Command Input Byte Sequence
Byte # Direction Name Description
0 To Slave Device
Address
This byte selects a particular chip on the two wire bus. Bit 1 of this byte should be 0 to
indicate a command transfer to the AT88SC018. Bit 0 of this byte should be 0 to
indicate that the data bytes travel from the master to the slave (TWI write).
1 To Slave Cmd The ordinal of the command to be executed by the AT88SC018, from the table below.
2 To Slave Size The total number of bytes to follow this byte may be 0 in the case that there are no
operand bytes.
3, … To Slave Data Operand bytes as specified in Command Descriptions.
If the command ordinal is legal, the AT88SC018 will ACK the command input and start processing. It takes a variable
amount of time to process the command, up to 20ms depending on the number of EEPROM pages to be written. If an
illegal command ordinal (≥0x15) is sent to the chip it will lock up for a “security delay”, then resume normal operation.
Refer to Section 1.6.4.
Values in the Cmd byte are chosen from the table below:
Table 4. Cmd Byte Values
Command Value
VerifyFlash 0x01
Startup 0x02
ChallengeResponse 0x03
Auth_1 0x04
Auth_2 0x05
EncryptPassword 0x06
Encryption_1 0x07
Encryption_2 0x08
GrindBytes 0x09
GetRandom 0x0A
IncrementCounter 0x0B
ReadCounter 0x0C
WriteMemory 0x0D
WriteMemoryEncrypted 0x0E
WriteMemoryAuthorized 0x0F
ReadMemory 0x10
ReadMemoryDigest 0x11
ReadManufacturingID 0x12
Lock 0x13
Clear 0x14
Crunch 0x15
in Command Descriglions.
A IIIEI.‘
CryptoCompanion Chip
7
5277C–CryptoCompanion–9/09
1.4.5.2. Command Output
The command output can be extracted from the AT88SC018 using the following byte sequence.
Table 5. Command Output Byte Sequence
Byte # Direction Name Description
0 To Slave Device Address This byte selects a particular chip on the two wire bus. Bit 1 of this byte
should be 0 to indicate that this is a command output. Bit 0 of this byte
should be 1 to indicate that the data will travel from the slave to the
master.
1 To Master Size The total number of bytes to follow this byte may be 0 in the case that
there are no output bytes.
2, … To Master Data Output bytes as specified in Command Descriptions.
Command output bytes can be repeatedly read from the AT88SC018 as they remain valid until a new command is sent
to the AT88SC018. Until <size> bytes of the new command have been sent, DataAvailable will remain set and that
number of bytes can be read from the SRAM output buffer, though the new input bytes will overwrite the old output
bytes.
Some commands do not have any data output, for instance ‘Clear’. On completion of these commands, the
DataAvailable bit will be cleared and the system can read just the size byte, which will have a value of 0.
1.4.5.3. Status
This register can be read to determine the current status or the error information using the following byte stream. This
sequence can be run at any time, regardless of whether or not the AT88SC018 is busy or locked.
Table 6. Byte Stream Sequence
Byte # Direction Name Description
0 To Slave Device Address This byte selects a particular chip on the two wire bus. Bit 1 of this byte
should be 1 to select the status register. Bit 0 of this byte is the
standard two wire R/W pin and should be 1 (data bytes travel from the
slave to the master).
1 To Master Status Returns the current value of the status register.
The status register value is described in the following table:
Table 7. Status Register Value
Byte # Name Description
0 Data Available The AT88SC018 has completed processing of the command and data is available in the
output buffer. A successfully completed command that does not have any output will
NOT set this bit.
1 Busy The AT88SC018 is processing a command and is unable to accept more input or provide
output, or it is in some sort of security penalty period.
2 StartupDone The ChallengeResponse command has successfully run this power cycle. Once set, this
bit will remain set until the next reset or power cycle.
3 – 4 Reserved Will always be 0.
5 – 7 Error An error occurred during prior input or command processing. The value of these three
bits denotes the particular condition that occurred.
The 8 error codes are used as follows:
M.
Section 1.6.2
(Sechon 1.6.3
Sechon 1.5.13
8 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
Table 8. Error Codes
Name Value Description
OK 0 Enabled, no error.
RstLocked 1 The AT88SC018 is disabled until the next power cycle or reset assertion. Whenever the
error bits are in this state, the Busy bit in the status register will also be asserted.
BadCmd 2 The formatting of the command was invalid, or one of the operands had an unacceptable
value.
TimeDelay 3 The AT88SC018 is disabled up for a certain period of time and will respond to
commands after this delay has elapsed. This delay may be a Power Delay
(Section 1.6.2) or Security Delay (Section 1.6.3). Whenever the error bits are in this
state, the Busy bit in the status register will also be asserted.
AuthFail 4 Either authentication must be completed prior to the execution of this command or there
was a problem during the execution of the auth commands themselves.
― 5
⎯ 6
⎯ 7
The system must poll this register (using TWI reads) after sending a command to the chip before attempting to read the
result.
This register cannot be written, attempts to do so will result in a NACK.
1.4.6. Byte Order
The AT88SC018 uses a big-endian byte order for all large integers (addresses, counters) which means that the most
significant byte appears first on the bus. Within this document, that byte is shown on the left side of the page. Arrays
(F values, cryptograms, passwords, digests) appear in index order, byte 0 first (or on the left of the page).
The two wire protocol specifies that the most significant bit within a byte appears first on the bus, and it appears on the
left side of the page.
1.5. Memory Architecture
The 4K bit (512 byte) EEPROM within the AT88SC018 is organized into a number of sections, each of which have
different access restrictions.
1.5.1. Memory Locking
On shipment from Atmel, certain locations are preloaded by Atmel, per Section 1.5.13. All other data locations are
unknown. The system manufacturer should load all areas important for proper system operation with the desired initial
values.
When this initialization is complete the Lock command should be executed which limits access to the memory per the
restrictions listed later in this section. The system can determine the current lock value by using the
ReadManufacturingID command to read out the ManufacturingID value (MfrID) and the lock byte.
The table below describes the encoding of the least significant two bits of the Lock byte. On shipment from Atmel,
Lock[1:0] will have a value of either 10 or 00, depending on the part number ordered. An AT88SC018 in either of these
two states is considered ‘unlocked’. It is not possible to change from one of these unlocked states to the other.
After the Lock command has been executed, the Lock byte will have the value 0xFF. Subsequent changes to the Lock
byte are impossible.
A IIIEI.‘
CryptoCompanion Chip
9
5277C–CryptoCompanion–9/09
Table 9. Memory Locking
LockBit 1 Lock Bit 0 (LSB) Meaning
1 1 Locked. ReadMemory and WriteMemory enabled, subject to the restrictions in this
section. WriteMemoryEncrypted and ReadMemoryDigest disabled.
1 0 Unlocked/Confidential. ReadMemoryDigest, WriteMemory and
WriteMemoryEncrypted enabled. ReadMemory disabled.
0 0 Unlocked. ReadMemory and WriteMemory enabled. WriteMemoryEncrypted and
ReadMemoryDigest disabled.
1.5.2. Secure Personalization
Customers desiring to write secrets into the AT88SC018 during personalization without exposing these secrets to
attackers should purchase the version of the chip in which Lock[1:0] is 10.
In these parts, Atmel will write a transport key into the EncKey location within EEPROM during wafer probe. Once the
AT88SC018 leaves the Atmel factory, the EncKey location cannot be written under any circumstances.
When the part is unlocked and therefore in the personalization phase, the WriteMemoryEncrypted command permits
the incoming data to be encrypted using EncKey as the encryption key. Data can also be written unencrypted if
desired. Verification of the EEPROM contents must use the ReadMemoryDigest command as ReadMemory is
prohibited in these parts as shipped. Once locked, the WriteMemoryEncrypted and ReadMemoryDigest commands are
prohibited – WriteMemory and ReadMemory are then enabled over a restricted address space.
The value written into EncKey will be the first 16 bytes of the SHA-1 digest of the concatenation of the 15 byte
ManufacturingID with a 16 byte secret provided to Atmel by the system manufacturer. The upper 6 bits of the Lock byte
will contain a secret tag assigned by Atmel to differentiate between various secrets that may have been used to
generate EncKey. This tag will be erased when the AT88SC018 is locked, leaving the Lock byte with the value 0xFF.
1.5.3. ManufacturingID (MfrID)
These 15 bytes contain unique wafer manufacturing information. This data can be used as the AT88SC018 serial
number if desired and can also be used by Atmel to track production of the part. It is written by Atmel at wafer test and
cannot be modified by the customer, regardless of whether or not the part has been locked.
The ManufacturingID value can only be obtained by executing the ReadManufacturingID command. Note, however,
that if Lock[1:0] is ‘10’, then the contents of the second 32 byte block which includes this value can be accessed with
ReadMemoryDigest. ReadMemory can never be used to access the first 48 bytes of memory (SHA Constant, EncKey,
MfrID & Lock).
A IIIEI.‘
10 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.5.4. Passwords
P0-P15. These are the passwords used to enable reading and/or writing of various zones in CRF. For example, CP0 is
the configuration byte for P0, and determines the particular attributes which govern the use of P0. The password
configuration bytes are organized as below:
Table 10. Password Configuration Bits.
Once the AT88SC018 is locked, these elements (P0-P15 & CP0-CP15) can never be read directly, nor can they be
written.
1.5.5. Nonvolatile Counters
The AT88SC018 implements 4 counters that can each increment to a maximum value of 6.4 million. They cannot be
reset, nor can they be decremented. Their current state can be read using the ReadCounter command and they are
incremented with the IncrementCounter command. It is recommended that the IncrementCounter command not be
issued after the counter has reached a value of 6.4 million. Access to these two commands does not require
authorization to have completed.
The above constraints only apply to a locked CMC. In an unlocked AT88SC018, the contents of the EEPROM locations
that hold the current state of the various counters can be freely read and/or written using ReadMemory
(ReadMemoryDigest) or WriteMemory (WriteMemoryEncrypted).
They should be initialized to a count of 0 before the AT88SC018 is locked, by writing the following values into all four of
the 16 byte counter areas: “0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0x00 0x00 0x00 0x00 0xFF 0x00 0x00 0x00”
at addresses “x0, x1, …”. Atmel recommends that all counters be properly initialized even if the application does not
utilize all of them.
1.5.6. RNGSeed
This location within the EEPROM is initialized during Atmel manufacturing with a 16 byte random number obtained
from an external high quality hardware random number generator. It is used as part of the input to the random number
generation capability within the AT88SC018. It may be read and/or written when the part is unlocked. Atmel does not
recommend that it be written to a fixed value.
1.5.7. Read Only Memory
When the part is locked, the memory in this area can be read but never written except as described in the next
paragraph. After the system has properly responded to the startup challenge, there are no restrictions on the reading of
this memory. This memory section starts at address 0x110 and extends to 0x100 | RW-Bound – 1.
RW-Bound must be at least 0x10 and less than 0xF8 or F-Bound, whichever is smaller.
Bit # Name Description
0 Encrypt If 1, EncryptPassword will return this password value in the clear. In this situation, the
password offers little security value but may be useful for mapping.
1 Connect If 1, then obey the “F number” restrictions below. If 0, ignore “F Number”.
2 – 3 Reserved Must be 0.
4 – 7 F Number The secret to which this password is connected. Unless the current authentication session
has been computed using this secret this password cannot be read in either clear or
encrypted mode.
A IIIEI.‘
CryptoCompanion Chip
11
5277C–CryptoCompanion–9/09
1.5.8. Read / Write Memory
The memory in this area has general read/write permissions, similar to a standard serial EEPROM. After the system
has properly responded to the startup challenge, there are no restrictions on the access to this memory.
The first byte in this section is at address 0x100 | RW-Bound. If RW-Bound is less than 0x10 the results will be
unpredictable.
1.5.9. Secrets
F0-F15. These secrets are used to generate the GC value for the particular CM/CRF chip based on the F1 algorithm,
SHA-1. Up to 16 F values that can be supported by the AT88SC018.
The low byte of the memory address of the first should be written into F-Bound. The 3 least significant bits of F-bound
are ignored. The first F value is always F0, independent of F-Bound. If F-bound is < RW-Bound or if F-Bound is < 0x80,
the results will be unpredictable.
Example
If F-Bound is 0xD0, the first F value is F0 at memory address 0x1D0. The last F value is F5 at address 0x1F8.
Example
If 0xFF is written into F-Bound, CMC will use only a single secret, named F0, which will be located at address 0x1F8
(since the low three bits of F-bound are ignored).
These elements can never be read directly, nor can they be written after the part has been locked.
1.5.10. CF0 – CF15
This location within the EEPROM is initialized during Atmel manufacturing with a 16 byte random number obtained
from an external high quality hardware random number generator. It is used internally within the AT88SC018. It may be
read and/or written when the part is unlocked. Atmel does not recommend that it be written to a fixed value.
1.5.11. Restricted Bytes
These locations within the EEPROM are initialized during Atmel manufacturing with a 4 byte random number obtained
from an external high quality hardware random number generator. It is used internally within the AT88SC018. It cannot
be read and/or written when the part is unlocked or locked. When reading from these locations, the result will be 0xFF
for these 4 bytes.
A IIIEI.‘
12 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.5.12. Memory Map
Figure 2. Memory Map
Least Significant Address Bits
0 1 2 3 4 5 6 7
0x000
0x008 SHA Constant
0x010
0x018 EncKey
0x020
0x028 ManufacturingID Lock
0x030 P0 CP0 P1 CP1
0x038 P2 CP2 P3 CP3
0x040 P4 CP4 P5 CP5
0x048 P6 CP6 P7 CP7
0x050 P8 CP8 P9 CP9
0x058 P10 CP10 P11 CP11
0x060 P12 CP12 P13 CP13
0x068 P14 CP14 P15 CP15
0x070
0x078 Counter0
0x080
0x088 Counter1
0x090
0x098 Counter2
0x0A0
0x0A8 Counter3
0x0B0
0x0B8 SystemSecret
0x0C0
0x0C8 CmcSecret
0x0D0
0x0D8 RNGSeed
0x0E0
0x0E8
0x0F0
FlashDigest
RstProt RW-Bound F-Bound Dev
0x0F8 CF0 CF1 CF2 CF3 CF4 CF5 CF6 CF7
0x100 CF8 CF9 CF10 CF11 CF12 CF13 CF14 CF15
0x108 Mode PwrDelay spare spare Restricted Restricted Restricted Restricted
0x110 Read Only Memory
…
0x178 Read / Write Memory
0x180 F0
0x188 F1
0x190 F2
0x198 F3
0x1A0 F4
0x1A8 F5
0x1B0 F6
0x1B8 F7
0x1C0 F8
0x1C8 F9
0x1D0 F10
0x1D8 F11
0x1E0 F12
0x1E8 F13
0x1F0 F14
Most Significant Address Bits
0x1F8 F15
See Sechon 1.5.2
Sechon
Sechons 1.5.1 L
Sechon 1.5.6
See Section 1.5.4
Sechon 1.5.10
Slanug Sechon 3.2 ChaHengeResgonse Sechon 3.3
Sechons 1.5.7 8.1.5.8
see Sechon 1.5.9
Sechon 3.1
Sechon
A IIIEI.‘
CryptoCompanion Chip
13
5277C–CryptoCompanion–9/09
1.5.13. Memory Initialization Values
Upon shipment from the Atmel factory, the following locations will have predefined values. The contents of all other
locations are not guaranteed by Atmel.
Table 11. Predefined Initial Memory Values
Name Initial Value
SHA Constant Defined by FIPS PUB 180-1.This is written at the Atmel factory and cannot subsequently be
changed.
EncKey Customer Specific, Contact Atmel. See Section 1.5.2 for more details.
ManufacturingID A unique value for all AT88SC018 chips, see Section 1.5.3
Lock xxxx_xx10 or xxxx_xx00, per Sections 1.5.1 & 1.5.2. Consult Atmel for ordering information.
RNGSeed Random values for each AT88SC018. See Section 1.5.6
Dev TWI bus address, shipped as 0xC0. See Section 1.5.4
CF0 – CF15 Random values for each AT88SC018. See Section 1.5.10
Certain values within the AT88SC018 memory array MUST be properly programmed prior to locking of the memory.
Failure to properly initialize these locations will result in unpredictable and/or unsecure operation of the part.
Table 12. Customer Defined Memory Values
Name Initial Value
SystemSecret,
CmcSecret
These values are used to perform a mutual authentication between the AT88SC018 and the
system processor. See the Startup (Section 3.2) and ChallengeResponse (Section 3.3) for more
details.
RW_Bound The boundary between ReadOnly and ReadWrite memory. See Sections 1.5.7 & 1.5.8 for more
information.
F_Bound Controls the number of F secrets in the array, see Section 1.5.9 for value limitations.
Mode The lower 2 bits control the way in which VerifyFlash is run, see Section 3.1 for more details.
The upper 5 bits MUST be ‘0’ for proper operation; other values may result in security or
functional issues.
FlashDigest If Mode.Bit[1:0] is set to 0, then this must be set to the proper value per the descriptions in the
VerifyFlash command, see Section 3.1.
M1
Section 1.4.1 1
14 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.6. Security Features
1.6.1. Environmental Detectors
The AT88SC018 contains an over and under voltage detector for VCC and includes a POR detector to prevent any
unknown startup states. If this detector is triggered, the AT88SC018 will be held in reset until the condition is cleared.
The operating clock is internally generated independent of SDA & SCL, and glitches on those pins are filtered out. The
AT88SC018 includes a metal obfuscation pattern over the memory block.
1.6.2. Reset Protection & Power Delay
There is a reset protection register in EEPROM (RstProt) that normally has a value of 1 before power is applied. On
reset, the AT88SC018 writes this register in the EEPROM to a value of 0, and starts a counter. That counter counts
1 MHz clocks up to a total delay interval of approximately 67 seconds, and at that time the AT88SC018 writes the
protection register to a value of 1. If a command is in progress when this time interval is reached, the register will be
updated at the completion of the command. After this write, the reset protection circuit goes idle until the next reset.
If at the time of reset or power-up the protection register already has a value of 0, then the AT88SC018 goes into a
“Power Delay” state for the same amount of time during which it will neither accept nor acknowledge any command. At
the end of the time interval, it will reset the register to a value of 1 and resume normal operation. A power-up or pin
reset during the “Power Delay” interval will restart the delay counter and start a new interval during which commands
will be ignored.
The AT88SC018 is designed to permit the system to execute the reset operation (and operate for at least 67 seconds)
a minimum of 1 million times. If the part is continuously reset every 67 seconds, this limit will be reached in about
2 years.
The Power Delay of 67 seconds is the maximum delay that the AT88SC018 can support. The actual delay is derived
from the contents PwrDelay byte within the EEPROM, according to the following table. The measured delay will vary by
up to +/- 25% over manufacturing and operating conditions.
Table 13. Reset Protection & Power Delay
PwrDelay Nominal Delay Interval PwrDelay Nominal Delay Interval
0x00 262ms 0x10 4.5s
0x01 524ms 0x20 8.7s
0x02 785ms 0x40 17s
0x04 1.3s 0x80 34s
0x08 2.4s 0xFF 67s
Other Unpredictable
Note: Short power delay times may decrease the overall security of the system.
The reset protection circuit and associated power delay operates regardless of whether the AT88SC018 is locked or
unlocked.
Failure to meet Power up and Power down conditions listed in Section 1.4.1.1 may result in invoking a reset protection
state, causing a “Power Delay” interval.
A IIIEI.‘
CryptoCompanion Chip
15
5277C–CryptoCompanion–9/09
1.6.3. Reset Locking
Certain conditions cause the AT88SC018 to lock up until the reset pin is asserted or the power is cycled. Depending on
the time interval from the last power-up, this action may or may not cause a delay to be enforced. During this time, the
status register will show the RstLocked error state and the busy pin will be asserted.
a) Some command other than VerifyFlash is attempted before Startup/ChallengeResponse has been run or some
command other than ChallengeResponse follows Startup.
b) ChallengeResponse is run but the preceding command is not Startup.
c) VerifyFlash fails for any reason other than that it has been disabled.
d) ChallengeResponse fails for any reason.
e) Second attempt to run VerifyFlash in a single power cycle.
1.6.4. Security Delay
When certain operations do not complete successfully, the AT88SC018 will enter a temporary security delay for a
period of time during which no commands will be honored by the AT88SC018. During this time, the system may read
the status register which will contain the TimeDelay error code & busy bit set.
The following conditions cause the AT88SC018 to enter a security delay when it is locked. Unlocked AT88SC018 chips
never enter the security delay sequence.
a) A second attempt to run Startup after the first has completed within the same power or reset cycle.
b) Some command other than Auth_2 follows Auth_1.
c) The values sent to the AT88SC018 for Auth_2 do not match those computed internally (authentication failed).
d) The values sent to the AT88SC018 for Encryption_2 do not match those computed internally (encryption key
verification failed).
e) An illegal command ordinal is sent to the AT88SC018.
The first time one of these conditions is detected after a power cycle or reset event, the AT88SC018 will delay ~260ms.
After each subsequent failure condition is detected, the AT88SC018 will delay for an interval twice the length of the
previous delay.
Once this doubling reaches a delay equal to or greater than PwrDelay, all subsequent failure conditions will trigger a
lockout interval equal to PwrDelay. The maximum Security Delay is 32s, regardless of the value of PwrDelay.
1.6.5. Command Sequencing
Depending on whether the AT88SC018 is locked or not, some commands must be executed in a certain order, this
section outlines those restrictions.
1.6.5.1. When the AT88SC018 is Unlocked
When the AT88SC018 is unlocked, there is no security delay and there is no requirement that Startup/Challenge be
executed prior to any other command. This strategy may facilitate quicker initialization.
Note: The Power Delay continues to be active when unlocked and authentication must still be run for those
commands that require it (EncryptPassword, Encryption_1&2, GrindBytes).
When the AT88SC018 is unlocked, the following commands are enabled:
• Read Memory can be run only if the least significant two bits of the lock byte in EEPROM are both 0. All locations
from 0x30 onwards can be read.
• ReadMemoryDigest can be run on all locations within the EEPROM if Lock[1:0] has a value of 0x10.
• WriteMemory can be run over all locations from 0x30 onwards.
• WriteMemoryEncrypted can only be run if Lock[1:0] has a value of 0x10.
• The Lock command can be run to exit the unlocked state.
M‘
from Section 1.6.3
16 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
1.6.5.2. When the AT88SC018 is Locked
When the AT88SC018 is locked, the security delays from Section 1.6.3 apply.
The first command run after powerup or a reset must be either VerifyFlash or Startup. If the first command is Startup,
then VerifyFlash cannot be run until the next power cycle. If the first command is VerifyFlash, then the next command
must be Startup. After Startup, the next command must always be Challenge Response.
No other command can be run until ChallengeResponse has successfully completed. Any attempt to run another
command prior to ChallengeResponse or a failure of the ChallengeResponse command will cause the AT88SC018 to
lock up until the next power cycle or reset assertion.
A complete and successful authentication sequence (Auth_1 & Auth_2) must be run prior to those commands that
require it: EncryptPassword, Encryption_1, Encryption_2 and GrindBytes. Failure to run the authentication sequence
will result in an error code in the status register but no delay.
When the AT88SC018 is locked, the following commands are disabled: WriteMemoryEncrypted, ReadMemoryDigest
and Lock. WriteMemory is available only for Read/Write memory (the region between RWBound and F-Bound).
ReadMemory is only available for ReadOnly + ReadWrite memory (the region between address 0x110 and F-Bound).
Any attempt to violate these restrictions will result in a BadCmd error message but no penalty.
2. CMC ÙCRF Authentication
The AT88SC018 supports the mutual authentication sequence of the CRF chip in a manner such that the shared
secrets are not ever exposed on the AT88SC018 or CRF busses. This section describes that mutual authentication
sequence. To be consistent with the parameter names in the command descriptions, the AT88SC018 is referred to by
its alternate name of CMC.
2.1. Nomenclature
Xi The subscript ‘i’ indicates a key index in the CRF memory array. CRF contains 4 sets of key values, only those
from a single set can be used in a successful authentication sequence.
YA, YE The superscripts ‘A’ and ‘E’ indicate the two possible phases of the crypto setup for CRF. ‘A’ indicates the
authentication phase which prefaces all cryptographic communication with CRF. The ‘E’ indicates the optional
encryption phase.
C The initial cryptogram state from CRF to CMC. It is the state generated as a result of a previous authentication
or encryption sequence and is unique.
CH, Ci These values are the challenge and response during the mutual authentication & encryption sequences. CHA
is the authentication challenge to CRF from CMC. CiA is the authentication response from CRF to CMC, CA is
the copy of this computed within CMC. CHE is the encryption challenge to CRF from CMC. CiE is the
encryption response from CRF to CMC, CE is the copy of this computed within CMC.
F2 This is the Atmel proprietary algorithm implemented within CMC and CRF. [A, B, C] = F2(X, Y, Z) indicates
that X, Y & Z are inputs to the F2 algorithm and that execution of the algorithm on these inputs yields the set
of outputs A, B & C.
G, Gi The secret stored in CRF or computed on CMC from ID and Fn.
ID This is the unique serial or identification number for CRF which is obtained from the Nc register within the CRF
EEPROM.
KID This is a constant generated by the external system in a manner of its choosing. It should typically be a
function of the ID number and an external secret, but may also include other information about the item to
which CRF is attached, the system configuration or other values held external to CMC. CMC treats KID as a
constant and does not interpret its value.
Q These are random values created in the RNG of CMC which are used as part of the authentication and
encryption sequences.
cf 33‘
CF SF
33‘ 03‘
E
A IIIEI.‘
CryptoCompanion Chip
17
5277C–CryptoCompanion–9/09
SA, SiA These are the encryption keys generated as part of the authentication sequence – SA is generated by CMC
and SiA is independently generated by CRF. Their value should be identical. The S keys generated by the
encryption sequence are ignored.
2.2. Authentication & Encryption Sequence
Table 14. Authentication & Encryption Sequence
CMC Command CMC Computation Dir. CRF Computation CRF Command
A. ⇐ ID, C Read Config
B. Auth_1 G = F1(Fn, KID, ID)
QA = RNG
[CHA, CA, SA] = F2 (G, C, QA)
CHA, QA
⇒
C.
⇐
[CH, CiA, SiA] = F2(Gi, Ci, QA)
CHA =? CH
CiA
Verify Crypto
D. Auth_2 CiA =? CA
E. Encrypt_1 QE = RNG
[CHE, CE, SE] = F2 (SA, CA,
QE)
CHE, QE
⇒
F.
⇐
[CH, CiE, SiE] = F2(SiA, CiA, QE)
CHE =? CH
CiE
Verify Crypto
G. Encrypt_2 CiE =? CE
3. Command Descriptions
3.1. VerifyFlash
System sends information to the AT88SC018 which would typically be based on the state of an external nonvolatile
(e.g. FLASH) program store. If the input digest indicates a problem, the AT88SC018 will set up the status register to
indicate a RstLocked error code but will accept no commands until the next reset or power cycle. This command can
be run once only per reset.
If Mode.Bit [1:0] == 00, this command simply verifies that the incoming digest matches that stored in memory. This is
useful if the external ASIC has hardware that can verify the boot code, in which case that hardware would respond to
the return code of this command.
If Mode.Bit [1:0] == 01, this command implements a simple signature mechanism for an externally loaded module. In
this case the FlashDigest stored in EEPROM is a secret also known by the entity that generates legal download
images. The system sends both the download digest and the signature to the AT88SC018; the AT88SC018 generates
a comparison signature using its stored value and verifies that they are the same. This mode is useful if the external
system has some confidence in the boot code, but does not have sufficient space to implement a full public key
signature verification module.
If Mode.Bit [1:0] == 11, this command is disabled. If Mode.Bit [1:0] == 00 or 01, then VerifyFlash MUST run before
startup. Mode.Bit [1:0] == 10 should not be used, if it is the VerifyFlash command will return OK without any
computation or comparison being performed.
M‘
e Sechon 2.2
18 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
Table 15. Inputs
Table 16. Outputs
3.2. Startup
The AT88SC018 resets all internal state, generates a 20 byte random number, and sends to system as challenge start.
To permit the system processor to mutually authenticate the AT88SC018, it will also compute a response to a
challenge from the system. CmcResponse = SHA-1(CmcChallenge, CmcSecret).
This command can be run only once per reset or power cycle.
Table 17. Inputs
Table 18. Outputs
3.3. ChallengeResponse
System sends 20 byte challenge response to the AT88SC018. The AT88SC018 computes SHA1 (SysChallenge,
SystemSecret) and compares with response. If incorrect, the AT88SC018 locks up until next time the reset pin is
asserted or power is removed.
The prior command must have been Startup, or the AT88SC018 will enter the RstLocked state.
Table 19. Inputs
Table 20. Outputs
3.4. Auth_1
Loads into the AT88SC018 the accessible information about the CRF for which authentication is to be computed and
builds the values needed for the CRF chip to perform its authentication sequence. This step computes the values of CA
and SA. These values are retained in volatile registers within the AT88SC018 (named C & S) for use during Auth_2 and
Encrypt_1. See Section 2.2 for more details on the authentication algorithm.
Execution of this command automatically resets any previous state including C & S registers, and causes a reset of the
crypto engine state.
Name Size Description
Digest 20 Digest of external memory.
Signature 20 SHA-1(Digest, FlashDigest), ignored if Mode.Bit [1:0] = 00.
Name Size Description
Name Size Description
CmcChallenge 20 Authentication challenge to the AT88SC018 from system processor.
Name Size Description
SysChallenge 20 Authentication challenge to system processor from RNG
CmcResponse 20 Challenge response to CmcChallenge
Name Size Description
SysResponse 20 Calculated response from system
Name Size Description
Sechon 1.6.3.
Sechon 2.2
see Section 1 6.3.
Ci
A IIIEI.‘
CryptoCompanion Chip
19
5277C–CryptoCompanion–9/09
After execution of Auth_1, the next command must be Auth_2. If it is not, the AT88SC018 locks up for some time. See
Section 1.6.3.
Table 21. Inputs
Table 22. Outputs
3.5. Auth_2
Receives the output of the CRF authentication command and verifies that the CRF chip has knowledge of G. See
Section 2.2 for more details on the authentication algorithm.
If the incoming CiA value is incorrect, the AT88SC018 locks up for some time, see Section 1.6.3.
The authentication times out when a delay of 1 second expire, at this point one must re-authenticate.
Table 23. Inputs
Table 24. Outputs
3.6. EncryptPassword
Compute an encrypted password to be sent to the CRF, using the current state of the crypto engine. This can be run at
any time after the authentication sequence has completed. This command is optional.
Table 25. Inputs
Table 26. Outputs
Name Size Description
C 8 Initial cryptogram seed from CRF
KID 16 Constant value to be included in G calculation.
ID 8 Serial number from which G is calculated. Referred to as Nc in CRF documentation.
Selector 1 Selects one of the F values from the EEPROM to be used for authentication.
Name Size Description
QA 8 Random number input to authentication sequence
CHA 8 Authentication challenge from Cmc to CRF.
Name Size Description
CiA 8 Authentication response from CRF to the AT88SC018, second half of mutual authentication
Name Size Description
Name Size Description
Selector 1 Which password to use
Name Size Description
EncPwd 3 Encrypted password to be sent to CRF.
ee Section 2.2
M‘
Sechon 1.6.3
Ci
20 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
3.7. Encryption_1
Similar to Auth_1, this sequence generates an intermediate value used for subsequent encryption of data to/from CRF.
This pass through the crypto engine is similar to the computation done during authentication with the exceptions that G
is replaced by S, the input C is replaced with the AT88SC018 register C, and QE is newly generated by the RNG on the
AT88SC018. See Section 2.2 for more details on the encryption algorithm.
A valid authentication sequence must be run before these commands, which will have set up the C & S registers. This
command (and its mate, Encryption_2) can be run multiple times per authentication sequence, but running it more than
once will cause the AT88SC018 to be out of synchronization with CRF until the next Auth_1/Auth_2 sequence is run.
After execution of Encryption_1, the next command must be Encryption_2. If not, the AT88SC018 will lock up for a
security delay.
Table 27. Inputs
Table 28. Outputs
3.8. Encryption_2
Similar to Auth_2, this sequence takes the encryption response from CRF and compares it the value computed at the
end of Encryption_1.
This command can only be run after the execution of Encryption_1. If the incoming CiE value is incorrect, the
AT88SC018 locks up for a security delay (refer to Section 1.6.3) and sets the error code in the status register to
AuthFail.
Table 29. Inputs
Table 30. Outputs
3.9. GrindBytes
Passes a variable number of bytes through the crypto engine on the AT88SC018 and sends the output of the crypto
engine back to the system. This command is used to keep the AT88SC018 in sync with the crypto engine on the CRF
chip, to decrypt encrypted data read from CRF, to encrypt data to be written to CRF and to generate or verify a
checksum.
The AT88SC018 does not interpret these bytes, merely passes them through the crypto engine.
GrindBytes cannot be run prior to the successful execution of the Auth_2 nor after the execution of the Clear command.
There is a limit of 4096 for maximum number of GrindBytes that can be run per Authentication.
Name Size Description
Name Size Description
QE 8 Random number for encryption sequence
CHE 8 Encryption challenge from AT88SC018 to CRF
Name Size Description
CiE 8 Authentication response from CRF to the AT88SC018
Name Size Description
A IIIEI.‘
CryptoCompanion Chip
21
5277C–CryptoCompanion–9/09
Table 31. Inputs
Table 32. Outputs
3.10. GetRandom
The AT88SC018 generates a 20 byte random number using its internal high quality random number generator and
outputs this value. There is no restriction on the system as to where these random numbers may be used – their
cryptographic quality makes them suitable for any operation on the system in addition to the CRF operations.
When the AT88SC018 is unlocked, the random numbers generated will follow a predictable pattern based on the state
of the RNGSeed EEPROM value and the number of power cycles since this seed has been written. This mechanism
facilitates testing.
Table 33. Inputs
Table 34. Outputs
3.11. IncrementCounter
Increment the value of the specified counter by 1.
Table 35. Inputs
Table 36. Outputs
Name Size Description
Size 1 One less than the number of bytes to be sent through crypto engine. If this byte is 0 grind
1 byte, if 0x13 grind 20 bytes. If ≥ 0x14, return BadCmd.
Data ⎯ Crypto engine input bytes, maximum 20.
Name Size Description
Data ⎯ Crypto engine output bytes, maximum 20.
Name Size Description
Name Size Description
Data 20 Random bytes from the RNG
Name Size Description
Counter 1 Counter index to be incremented, must be from 0-3. The upper 4 bits of this parameter are
ignored.
Name Size Description
A “El.
22 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
3.12. ReadCounter
Returns the 32 bit current state of the specified counter. There are no read restrictions on the counters.
Table 37. Inputs
Table 38. Outputs
3.13. WriteMemory
Writes the contents of the specified address and those following it up to the end of the read/write memory space. Prior
to locking, any byte after the lock byte can be written with this command. After the AT88SC018 has been locked, only
the read/write space can be written with this command.
The input data must always be 16 bytes long, though fewer bytes may be written into the EEPROM. While the
AT88SC018 ignores these pad bytes, Atmel recommends that they always be 0xFF.
Table 39. Inputs
Table 40. Outputs
3.14. WriteMemoryEncrypted
Writes a 16 byte page of the EEPROM, using the encryption algorithm described below. Smaller blocks of memory
cannot be written using this command.
This command cannot be run after the AT88SC018 has been locked.
Table 41. Inputs
Name Size Description
Counter 1 Counter index to be read, must be from 0-3. The upper 4 bits of this parameter are
ignored.
Name Size Description
Value 4 Current value of counter.
Name Size Description
Address 2 Address in EEPROM of the first byte of data to be written. The most significant 7 bits are
ignored.
Count 1 If 0, write 1 byte… if 0x0F, write 16 bytes. The upper 4 bits are ignored.
Data 16 Clear text bytes, padded to 16 bytes total.
Name Size Description
Name Size Description
Address 2 Address of the 16 byte page within EEPROM to which data is to be written. The least
significant 4 and most significant 7 bits are ignored.
Data 16 Encrypted data
Nonce 16 Random value used to seed encryption
A IIIEI.‘
CryptoCompanion Chip
23
5277C–CryptoCompanion–9/09
Table 42. Outputs
The AT88SC018 will compute the SHA-1 hash of (Address, EncKey, Nonce). The first 16 bytes of the resulting digest
will be used as an XOR key to decrypt the incoming data, which will then be written to the specified page in EEPROM.
3.15. ReadMemory
Reads the contents of the EEPROM from the specified address and those following it up to the end of R/W EEPROM.
Once locked, only the read-only and read/write spaces can be read. Addresses 0 through 0x2F may never be read.
Up to 16 bytes may be accessed within a single read operation.
This command can be run prior to locking of the memory only if the least two significant bits of the lock byte have a
value of 0.
Table 43. Inputs
Table 44. Outputs
3.16. ReadMemoryDigest
Reads the specified 32 byte block from the EEPROM, computes the SHA-1 digest of that block and returns that digest
to the user. This command provides a mechanism of verifying that the personalization of the chip completed correctly
before the one-time lock has been run.
Note: Specifying an address of 0 requires that the verifier know the value of EncKey.
This command cannot be run after the AT88SC018 has been locked or if the unlocked state is Lock[1:0] == 00. When it
can be run it can access all locations within the EEPROM.
Table 45. Inputs
Table 46. Outputs
Name Size Description
Name Size Description
Address
2 Address in EEPROM of the first byte of data to be read. The most significant 7 bits are
ignored.
Count 1 If 0, read 1 byte… if 0x0F, read 16 bytes. The upper 4 bits are ignored.
Name Size Description
Data ⎯ Clear text bytes, maximum of 16
Name Size Description
Address 2 Address of the 32 byte block within EEPROM which should be read. The least significant
5 and most significant 7 bits are ignored.
Name Size Description
Data 20 Digest of the selected 32 byte block of the EEPROM
M‘
Sec‘ion 1 5.1.
24 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
3.17. ReadManufacturingID
Reads the contents of the ManufacturingID and Lock Byte from the EEPROM. This command can always be executed,
regardless of whether or not the AT88SC018 has been locked.
Table 47. Inputs
Table 48. Outputs
3.18. Lock
Locks the current memory values into the AT88SC018, per the description in Section 1.5.1. Once Locked, the
AT88SC018 cannot be unlocked. After the execution of this command, the Lock Byte will have a value of 0xFF. This
command has no effect on locked parts.
There are no inputs or outputs to this command.
3.19. Clear
Clears the current authentication state, empties the C & S registers and prepares the chip for a new authentication. A
new startup challenge/response is NOT required. There are no input or output arguments to this command.
After execution of this command, the Auth_1 / Auth_2 sequence must be successfully completed before subsequent
execution of EncryptPassword, Encryption_1&2 and/or GrindBytes.
3.20. Crunch
Passes a random number of 8 bytes through the crunch engine on the AT88SC018 and sends the output of the crunch
engine back to the system. This command is used to ensure the AT88SC018 is talking with an actual CRF chip, which
should respond with the same answer in the given timeframe.
The AT88SC018 does not interpret these bytes, merely passes them through the crunch engine.
Table 49. Inputs
Table 50. Outputs
Name Size Description
Name Size Description
MfrID 16 ManufacturingID & Lock Byte
Name Size Description
Iterations 1 A maximum of 255 iterations can be run through the crunch engine. A 1 in this filed will
compute one Iteration through the crunch engine.
Data 8 Crunch engine input bytes.
Name Size Description
Data 8 Crunch engine output bytes.
A IIIEI.‘
CryptoCompanion Chip
25
5277C–CryptoCompanion–9/09
4. Command Execution Times
The following table lists the nominal execution times for the various commands above, subject to the assumptions
following the table.
Some of the commands take a variable amount of time based on the input parameters and/or the current state of the
AT88SC018. In general, the table below shows the worst case operational flow, subject to the list of assumptions
following the table. Actual execution time will vary from the nominal by ±25% due to variations of the internal oscillator.
This preliminary data is advisory in nature. Designs should not depend on the specific execution times below, but rather
use the standard handshake mechanisms described above. The values below are characterized on the part but are not
tested in production.
Table 51. Nominal Execution Times
Command Nominal Time Notes
VerifyFlash 4000 μs
Startup 8000 μs
ChallengeResponse 4000 μs
Auth_1 8000 μs
Auth_2 60 μs
EncryptPassword 100 μs
Encryption_1 4100 μs
Encryption_2 60 μs
GrindBytes 50 μs
GetRandom 4000 μs
IncrementCounter 50 μs + 10 ms (5 EE writes worst case)
ReadCounter 50 μs
WriteMemory 200 μs + 4 ms (2 EE writes, if not within a page)
WriteMemoryEncrypted 4100 μs + 2 ms (1 EE write)
ReadMemory 200 μs
ReadMemoryDigest 4000 μs
ReadManufacturingID 200 μs
Lock 8000 μs + 36 ms (18 EE write worst case)
Clear 5 μs
Assumptions:
1. TWI clock assumed to be at 400 KHz.
2. TWI command times – 0 bytes of data ~ 75 μs. Additional byte ~ 25 μs.
3. VerifyFlash command is run with "Mode.Bit [1:0] = 01" case.
4. GrindBytes command assumes 20 bytes of data.
5. WriteMemory and ReadMemory commands assume 16 bytes of data.
6. These processing times do not include data transfer on the TWI.
A IIIEI.‘
26 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
5. AC & DC Characteristics
Table 52. DC Characteristics (1)
Applicable over recommended operating range from VCC = +2.7 to 3.6 V,
TAC = -40o C to 85o C (unless otherwise noted)
Symbol Parameter Test Condition Min Typ Max Units
VCC Supply Voltage 2.7 3.6 V
ICC Supply Current 400kHz 5 mA
ISB Standby Current VIN = VCC or GND 15 μA
VIL SDA Input Low Voltage -0.3 VCC x 0.3 V
VIL CLK Input Low Voltage -0.3 VCC x 0.3 V
VIL RST Input Low Voltage -0.3 VCC x 0.3 V
VIL PDN Input Low Voltage -0.3 VCC x 0.3 V
VIH SDA Input High Voltage VCC x 0.7 5.25 V
VIH SCL Input High Voltage VCC x 0.7 5.25 V
VIH RST Input High Voltage VCC x 0.7 5.25 V
VIH PDN Input High Voltage VCC x 0.7 5.25 V
IIL SDA Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL SCL Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL RST Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIL PDN Input Low Current 0 < VIL < VCC x 0.15 -10 10 μA
IIH SDA Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH SCL Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH RST Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
IIH PDN Input High Current VCC x 0.7 < VIH < VCC -10 10 μA
VOH SDA Output High Voltage 20k Ohm External Pull-
up V
CC x 0.8 V
VOL SDA Output Low Voltage IOL = 1mA, Vcc=2.7V 0.4 V
Note: 1. Typical values at 25° C. Maximum values are characterized values and not test limits in production.
SCL
SDA IN
SDA OUT
‘su STA H
‘
4. ‘7 ‘F H‘GH ‘H
\
ILow ‘Low \
‘HD STA MD DAT 4‘ ‘quJAT 4’ ‘SU 8T0
‘AA tDH ‘—’ ‘BUF
A IIIEI.‘
CryptoCompanion Chip
27
5277C–CryptoCompanion–9/09
Table 53. AC Characteristics (1)
Applicable over recommended operating range from VCC = +2.7 to 3.6 V,
TAC = -40o C to 85o C, CL = 30pF (unless otherwise noted)
Symbol Parameter Min Max Units
fCLK Clock Frequency 0 400 kHz
Clock Duty cycle (2) 40 60 %
tR Rise Time - SDA, RST, PDN (2) 300 nS
tF Fall Time - SDA, RST, PDN (2) 300 nS
tR Rise Time - SCL (2) 300 nS
tF Fall Time - SCL (2) 300 nS
tAA Clock Low to Data Out Valid 900 nS
tHD.STA Start Hold Time 600 nS
tSU.STA Start Set-up Time 600 nS
tHD.DAT Data In Hold Time 100 nS
tSU.DAT Data In Set-up Time 100 nS
tSU.STO Stop Set-up Time 600 nS
tDH Data Out Hold Time 50 900 nS
Note: 1. Typical values at 25° C. Maximum values are characterized values and not test limits in production.
2. This parameter is not tested. Values are based on characterization and/or simulation data.
Figure 3. SCL: Serial Clock, SDA: Serial Data I/O®
A IIIEI.‘
28 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
6. Transport Key
Certain operational modes of CryptoCompanion chip require knowledge of a key for proper custom configuration.
When applicable, Atmel shall program customer provided key values at the factory for production orders. For generic
and sample orders, this key, available as a transport key, shall be:
0x17 0x44 0x1A 0x48 0xDA 0xDB 0x23 0xFB 0x70 0xCC 0xB8 0x43 0x09 0x20 0x59 0xEB
A IIIEI.‘
CryptoCompanion Chip
29
5277C–CryptoCompanion–9/09
7. Ordering Codes
Table 54. Ordering Codes
Ordering Code Package Voltage
Range
Memory Locking
(see
Section 1.5.1 for Lock Definitions) Temperature Range
AT88SC018-SU-CM 8S1 2.7V – 3.6V 00 (Unlocked) Green compliant (exceeds
RoHS), Industrial (-40o C to 85o
C), Bulk
AT88SC018-SU-CM-T 8S1 2.7V – 3.6V 00 (Unlocked) Green compliant (exeeds
RoHS), Industrial (-40o C to 85o
C), Tape and Reel
AT88SC018-SU-CN 8S1 2.7V – 3.6V 10 (Unlocked/Confidential) Green compliant (exceeds
RoHS), Industrial (-40o C to 85o
C), Bulk
AT88SC018-SU-CN-T 8S1 2.7V – 3.6V 10 (Unlocked/Confidential) Green compliant (exceeds
RoHS), Industrial (-40o C to 85o
C), Tape and Reel
Table 55. Package Type
Package Type Description
8S1 8-lead, 0.150” Wide, Plastic Gull Wing Small Outline Package (JEDEC SOIC)
/ \ A
EL 7 7,7,7
fiA
30 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
8. Package Drawing
Figure 4. 8S1 – JEDEC SOIC
Note:
COMMON DIMENSIONS
(Unit of Measure = mm)
SYMBOL MIN NOM MAX NOTE
A1 0.10 – 0.25
These drawings are for general information only. Refer to JEDEC Drawing MS-012, Variation AA for proper dimensions,
tolerances, datums, etc.
A 1.35 – 1.75
b 0.31 – 0.51
C 0.17 – 0.25
D 4.80 – 5.05
E1 3.81 – 3.99
E 5.79 – 6.20
e 1.27 BSC
L 0.40 – 1.27
0˚–8˚
Top View
End View
Side View
e
D
A
A1
N
E
1
C
E1
L
DRAWING NO.
1150 E. Cheyenne Mtn. Blvd.
Colorado Springs, CO 80906
REV.
8S1 B
10/07/03
TITLE
8S1, 8-lead (0.150" Wide Body), Plastic Gull Wing
Small Outline (JEDEC SOIC)
b
A IIIEI.‘
CryptoCompanion Chip
31
5277C–CryptoCompanion–9/09
9. Command Flow Diagrams
Figure 5. Command Input
Host Ö Device Device Ö Host
Device Address
0 0
Command
Number of bytes N
Data
…
N data
bytes
Data
Figure 6. Command Output
Host Ö Device Device Ö Host
Device Address
0 1
NACK if Busy …
Number of bytes N
Data
…
Data
Figure 7. Command Status
Host Ö Device Device Ö Host
Device Address
1 1
STATUS
A IIIEI.‘
32 CryptoCompanion Chip
5277C–CryptoCompanion–9/09
Appendix A. Revision History
Doc. Rev. Date Comments
5277C 9/2009 Finalized AC & DC Characteristics. Updated Counter information.
5277B 2/2009 Document updated. Changed to AT88SC018 part number.
5277A 2/2008 Initial document release.
A IIIEL
5277C–CrptoCompanion–9/09
Headquarters International
Atmel Corporation
2325 Orchard Parkway
San Jose, CA 95131
USA
Tel: 1(408) 441-0311
Fax: 1(408) 487-2600
Atmel Asia
Room 1219
Chinachem Golden Plaza
77 Mody Road Tsimshatsui
East Kowloon
Hong Kong
Tel: (852) 2721-9778
Fax: (852) 2722-1369
Atmel Europe
Le Krebs
8, Rue Jean-Pierre Timbaud
BP 309
78054 Saint-Quentin-en-
Yvelines Cedex
France
Tel: (33) 1-30-60-70-00
Fax: (33) 1-30-60-71-11
Atmel Japan
9F, Tonetsu Shinkawa Bldg.
1-24-8 Shinkawa
Chuo-ku, Tokyo 104-0033
Japan
Tel: (81) 3-3523-3551
Fax: (81) 3-3523-7581
Product Contact
Web Site
www.atmel.com
Technical Support
cryptomemory@atmel.com
Sales Contact
www.atmel.com/contacts
Literature Requests
www.atmel.com/literature
Disclaimer: The information in this document is provided in connection with Atmel products. No license, express or implied, by estoppel or otherwise, to any
intellectual property right is granted by this document or in connection with the sale of Atmel products. EXCEPT AS SET FORTH IN ATMEL’S TERMS AND
CONDITIONS OF SALE LOCATED ON ATMEL’S WEB SITE, ATMEL ASSUMES NO LIABILITY WHATSOEVER AND DISCLAIMS ANY EXPRESS, IMPLIED
OR STATUTORY WARRANTY RELATING TO ITS PRODUCTS INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY,
FITNESS FOR A PARTICULAR PURPOSE, OR NON-INFRINGEMENT. IN NO EVENT SHALL ATMEL BE LIABLE FOR ANY DIRECT, INDIRECT,
CONSEQUENTIAL, PUNITIVE, SPECIAL OR INCIDEN-TAL DAMAGES (INCLUDING, WITHOUT LIMITATION, DAMAGES FOR LOSS OF PROFITS, BUSINESS
INTERRUPTION, OR LOSS OF INFORMATION) ARISING OUT OF THE USE OR INABILITY TO USE THIS DOCUMENT, EVEN IF ATMEL HAS BEEN ADVISED
OF THE POSSIBILITY OF SUCH DAMAGES. Atmel makes no representations or warranties with respect to the accuracy or completeness of the contents of this
document and reserves the right to make changes to specifications and product descriptions at any time without notice. Atmel does not make any commitment to
update the information contained herein. Unless specifically provided otherwise, Atmel products are not suitable for, and shall not be used in, automotive
applications. Atmel’s products are not intended, authorized, or warranted for use as components in applications intended to support or sustain life.
© 2009 Atmel Corporation. All rights reserved. Atmel®, Atmel logo and combinations thereof, CryptoMemory®, CryptoRF®, and others are registered trademarks,
CryptoCompanion™, and others are trademarks of Atmel Corporation or its subsidiaries. Other terms and product names may be trademarks of others.
Products related to this Datasheet
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC
IC SECURITY COMPANION CHIP 8SOIC